<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: FlexRay vs. NestedVectorISR handling (S12XF512)</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexRay-vs-NestedVectorISR-handling-S12XF512/m-p/297471#M10258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I handled the problem with changing to FIFO - and it works :smileywink:-, but I still don't know the reason of this fault :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 May 2014 13:08:44 GMT</pubDate>
    <dc:creator>istvanreti</dc:creator>
    <dc:date>2014-05-15T13:08:44Z</dc:date>
    <item>
      <title>FlexRay vs. NestedVectorISR handling (S12XF512)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexRay-vs-NestedVectorISR-handling-S12XF512/m-p/297470#M10257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, the FR system is the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FR Drivers - Freescale "S12XFSTARTERKITE: S12XF 2-Node Starter Kit" from home page.&amp;nbsp; &lt;/LI&gt;&lt;LI&gt;Individual MessageBuffers (MB) &lt;/LI&gt;&lt;LI&gt;Node1: TX1, RX2, RX5&lt;/LI&gt;&lt;LI&gt;Node2: RX1, TX2, RX5&lt;/LI&gt;&lt;LI&gt;Node3 (faulty): RX1(MB0), RX2(MB1), TX5 &lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Node3 I had a problem with using FlexRay in a Nested Interrupt hierarchy system. On the one hand there is a BLDC motor control with some interrupts(Timers, PWM, SPI), and on the other hand I use FR for communication. BLDC interrupts are on a higher level than FR ISRs, so they can - actually they do - interrupt these FR communication interrupts - I checked it with an oscilloscope -. If Node2 is out of the system, there is no problem with node3, both the BLDC control and FR works good.&lt;/P&gt;&lt;P&gt;But if Node2 is connected in - and Node3 receive information in Slot2 -, at the event, when the receive function can not read Slot1's MB0 until the end of the Slot2 communication cycle - when Slot2's MB1 should start to read - MB0 (Slot1's MB) is overwritten... Is there anybody who know the reason, and maybe the solution? It would be great &lt;SPAN aria-label="Happy" class="emoticon_happy emoticon-inline" style="height:16px;width:16px;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For further info there is the scope's view:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;blue - communication signal&lt;/LI&gt;&lt;LI&gt;yellow - interrupt (read() function etc.)&lt;/LI&gt;&lt;LI&gt;green - fault indicator (inverted)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 10:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexRay-vs-NestedVectorISR-handling-S12XF512/m-p/297470#M10257</guid>
      <dc:creator>istvanreti</dc:creator>
      <dc:date>2014-05-14T10:12:09Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRay vs. NestedVectorISR handling (S12XF512)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexRay-vs-NestedVectorISR-handling-S12XF512/m-p/297471#M10258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I handled the problem with changing to FIFO - and it works :smileywink:-, but I still don't know the reason of this fault :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 13:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexRay-vs-NestedVectorISR-handling-S12XF512/m-p/297471#M10258</guid>
      <dc:creator>istvanreti</dc:creator>
      <dc:date>2014-05-15T13:08:44Z</dc:date>
    </item>
  </channel>
</rss>