<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 ISO-9141 Implementation for the MC33812</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297452#M10252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the development kit KIT33812ECUEVME from Freescale and want to read out some Data with the Diagnostic Interface ISO-9141.&lt;/P&gt;&lt;P&gt;did anyone know how to implement the ISO-9141 Trasceiver on the MC33812 in the c-code or have some desciription how to do that? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 May 2014 08:02:22 GMT</pubDate>
    <dc:creator>josh007</dc:creator>
    <dc:date>2014-05-14T08:02:22Z</dc:date>
    <item>
      <title>ISO-9141 Implementation for the MC33812</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297452#M10252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the development kit KIT33812ECUEVME from Freescale and want to read out some Data with the Diagnostic Interface ISO-9141.&lt;/P&gt;&lt;P&gt;did anyone know how to implement the ISO-9141 Trasceiver on the MC33812 in the c-code or have some desciription how to do that? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 08:02:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297452#M10252</guid>
      <dc:creator>josh007</dc:creator>
      <dc:date>2014-05-14T08:02:22Z</dc:date>
    </item>
    <item>
      <title>Re: ISO-9141 Implementation for the MC33812</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297453#M10253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A href="https://community.nxp.com/space/2017"&gt;16-bit Microcontrollers&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; ( &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt;&amp;nbsp;&amp;nbsp; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 09:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297453#M10253</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-05-14T09:48:25Z</dc:date>
    </item>
    <item>
      <title>Re: ISO-9141 Implementation for the MC33812</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297454#M10254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;okay thanks i did it ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 09:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297454#M10254</guid>
      <dc:creator>josh007</dc:creator>
      <dc:date>2014-05-14T09:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: ISO-9141 Implementation for the MC33812</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297455#M10255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;The ISO-9141 line on MC33812 can be connected to a target Device’s ISO-9141 line&amp;nbsp; that can communicate in ISO-9141 format.&amp;nbsp; The MC33812 then translates the ISO-9141 to&amp;nbsp; MTX for “Transmit” (Micro Transmits out) and MRX for “Receive” (Micro Receives).&amp;nbsp; Hence, as far as the micro code goes, all it needs to do is to do the “normal” communication through its Serial Communication pins (Tx, Rx) and talk to the MC33812.&amp;nbsp; The rest would be automatic through MC33812,&amp;nbsp; as far as converting the Serial lines into ISO-9141 format.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Also FYI, please note that we also have MC33813 and MC33814.&amp;nbsp; MC33813 is for Single Cyl engines and does everything MC33812 does plus the VRS circuit, is built-in.&amp;nbsp; Hence, avoids an additional external VRS chip.&amp;nbsp; The MC33814 is exactly same as MC33813 and is pin-to-pin compatible, but supports two Cyl engines. You can find all 3 datasheets for MC33812, MC33813 and MC33814 at&amp;nbsp; Freescale web.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Ivan&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 12:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297455#M10255</guid>
      <dc:creator>iggi</dc:creator>
      <dc:date>2014-05-15T12:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: ISO-9141 Implementation for the MC33812</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297456#M10256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;okay i understand this communcation between two mcus in ISO-9141 format. But does Freescale have some writte codes or explantations to integrate OBDII System to this Board that i can read out Data like the "error memory" or the values of the sensors with an OBD2-Tester ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 13:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ISO-9141-Implementation-for-the-MC33812/m-p/297456#M10256</guid>
      <dc:creator>josh007</dc:creator>
      <dc:date>2014-05-15T13:26:52Z</dc:date>
    </item>
  </channel>
</rss>