<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 9S12XEG384 bank F9 is not programmed in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/9S12XEG384-bank-F9-is-not-programmed/m-p/288478#M10136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I forgot to also perform in HCS12MultilinkCyclone Pro:&lt;/P&gt;&lt;P&gt;- Select derivative&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XEQ384&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Problem solved.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2013 11:44:41 GMT</pubDate>
    <dc:creator>leroy_o</dc:creator>
    <dc:date>2013-06-12T11:44:41Z</dc:date>
    <item>
      <title>9S12XEG384 bank F9 is not programmed</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/9S12XEG384-bank-F9-is-not-programmed/m-p/288477#M10135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem with the flashing of the F9 flash memory bank after having switched a project from 9S12XEG128 to 9S12EG384 recently.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The F9 flash memory bank is declared in the prm project file, also, F9 memory locations appear in the project.abs.s19 file, but this code is not programmed in actual flash memory.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use a Freescale PE USB multilink interface to perform the actual flashing, it worked with the 9S12XEG128, but after flashing, object code in the F9 bank appear as "FFFFFFFFFFFFFFFF...".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has someone encoutered the same kind of problem and solved it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 09:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/9S12XEG384-bank-F9-is-not-programmed/m-p/288477#M10135</guid>
      <dc:creator>leroy_o</dc:creator>
      <dc:date>2013-06-12T09:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: 9S12XEG384 bank F9 is not programmed</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/9S12XEG384-bank-F9-is-not-programmed/m-p/288478#M10136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I forgot to also perform in HCS12MultilinkCyclone Pro:&lt;/P&gt;&lt;P&gt;- Select derivative&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - MC9S12XEQ384&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Problem solved.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 11:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/9S12XEG384-bank-F9-is-not-programmed/m-p/288478#M10136</guid>
      <dc:creator>leroy_o</dc:creator>
      <dc:date>2013-06-12T11:44:41Z</dc:date>
    </item>
  </channel>
</rss>