/* * Copyright (c) 2014-2015, Freescale Semiconductor, Inc. * Copyright 2016-2017 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ /* Entry Point */ ENTRY(Reset_Handler) /* By default, the Bootloader is not used. */ /* gUseBootloaderLink_d = DEFINED(gUseBootloaderLink_d) ? gUseBootloaderLink_d : 0; */ /* By default, the NVM is not used. */ gUseNVMLink_d = DEFINED(gUseNVMLink_d) ? gUseNVMLink_d : 1; gNVMSectorCountLink_d = DEFINED(gNVMSectorCountLink_d) ? gNVMSectorCountLink_d : 32; /* /* By default, the internal storage is not used. */ /* gUseInternalStorageLink_d = DEFINED(gUseInternalStorageLink_d) ? gUseInternalStorageLink_d : 0; */ __ram_vector_table__ = DEFINED(__ram_vector_table__) ? __ram_vector_table__ : 1; /*-Memory Limits-*/ __region_ROM_start__ = (0x00000000); __region_ROM_end__ = (0x0007FFFF); /* Workaround for SRAM boundary GCC placement issue, not to place variables that are accessed by the code overlapping this boundary (forbidden by the Kinetis architecture) */ __region_RAM1_start__ = (0x1FFF8000); __region_RAM1_end__ = (0x1FFFFFFF); __region_RAM2_start__ = (0x20000000); __region_RAM2_end__ = (0x20017FFF); __vector_table_size__ = (48*4); __ram_vector_table_size__ = DEFINED(__ram_vector_table__) ? __vector_table_size__ : 0; _RAM_START_ = __region_RAM1_start__; _RAM_END_ = __region_RAM2_end__; m_interrupts_start = (__region_ROM_start__); m_interrupts_end = (m_interrupts_start + __vector_table_size__ - 1); m_flash_config_start = (0x400); m_flash_config_end = (0x410); /*-Sizes-*/ /* 2k flash sector size */ m_sector_size = ( 2 * 1024 ); __size_cstack__ = DEFINED(__stack_size__) ? __stack_size__ : 512; __size_heap__ = DEFINED(__heap_size__) ? __heap_size__ : 0; /*** FSL Product Info region ***/ m_fsl_prodInfo_start = (__region_ROM_end__ - m_sector_size + 1); m_fsl_prodInfo_end = (__region_ROM_end__); FREESCALE_PROD_DATA_BASE_ADDR = m_fsl_prodInfo_start; /*** NVM Configuration ***/ NV_STORAGE_SECTOR_SIZE = m_sector_size; NV_STORAGE_MAX_SECTORS = gNVMSectorCountLink_d; /* NV_STORAGE_MAX_SECTORS * NV_STORAGE_SECTOR_SIZE = total NV Storage space */ NV_STORAGE_START_ADDRESS = m_fsl_prodInfo_start - 1; NV_STORAGE_END_ADDRESS = NV_STORAGE_START_ADDRESS - (NV_STORAGE_MAX_SECTORS * NV_STORAGE_SECTOR_SIZE) + 1; NV_STORAGE_SECTOR_SIZE_C = (m_sector_size); NV_STORAGE_MAX_SECTORS_C = (gNVMSectorCountLink_d); NV_STORAGE_START_ADDRESS_C = (m_fsl_prodInfo_start - 1); NV_STORAGE_END_ADDRESS_C = (NV_STORAGE_START_ADDRESS_C - (NV_STORAGE_MAX_SECTORS_C * NV_STORAGE_SECTOR_SIZE_C) + 1); /* Define the limits of the memory regions*/ m_text_start = (m_interrupts_start); m_text_end = (NV_STORAGE_END_ADDRESS_C - 1); m_interrupts_ram_start = (__region_RAM2_start__); m_interrupts_ram_end = (m_interrupts_ram_start + __ram_vector_table_size__ - 1); __CSTACK_end__ = (__region_RAM2_end__); __CSTACK_start__ = (__CSTACK_end__ - __size_cstack__); __HEAP_end__ = (__CSTACK_start__ - 1); __HEAP_start__ = (__HEAP_end__ - __size_heap__ - 0x4); m_data1_start = (__region_RAM1_start__); m_data1_end = (__region_RAM1_end__); m_data2_start = (m_interrupts_ram_start); m_data2_end = (__HEAP_start__ - 1); __RAM_VECTOR_TABLE_SIZE = __ram_vector_table_size__; __BOOT_STACK_ADDRESS = m_data2_end - 0x0F; /* Specify the memory areas */ MEMORY { TEXT_region1 (RX) : ORIGIN = m_text_start, LENGTH = (m_flash_config_start - m_text_start) m_flash_config_region (RX) : ORIGIN = m_flash_config_start, LENGTH = (m_flash_config_end - m_flash_config_start) TEXT_region2 (RX) : ORIGIN = m_flash_config_end + 1, LENGTH = (m_text_end - m_flash_config_end - 1) NVM_region (RW) : ORIGIN = NV_STORAGE_END_ADDRESS_C, LENGTH = (NV_STORAGE_START_ADDRESS_C - NV_STORAGE_END_ADDRESS_C) DATA1_region (RW) : ORIGIN = m_data1_start, LENGTH = (m_data1_end - m_data1_start + 1) DATA2_region (RW) : ORIGIN = m_data2_start, LENGTH = (__region_RAM2_end__ - __region_RAM2_start__ + 1) PRODUCT_INFO_region (RX) : ORIGIN = m_fsl_prodInfo_start, LENGTH = (m_fsl_prodInfo_end - m_fsl_prodInfo_start) } /* Define output sections */ SECTIONS { /* Place in the first memory bank the memHeap */ /* .data1 : { ./framework/MemManager/Source/MemManager.o(.bss*) } > DATA1_region */ /* The startup code goes first into internal flash */ .interrupts : { __VECTOR_TABLE = .; . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ . = ALIGN(4); } > TEXT_region1 .freescale_prod_data : { . = ALIGN(4); KEEP(*(.FREESCALE_PROD_DATA)) . = ALIGN(4); } > PRODUCT_INFO_region .flash_config : { . = ALIGN(4); KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */ . = ALIGN(4); } > m_flash_config_region /* The program code and other data goes into internal flash */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); } > TEXT_region2 .NVM_TABLE : { . = ALIGN(4); PROVIDE(__start_NVM_TABLE = .); KEEP(*(.NVM_TABLE)); PROVIDE(__stop_NVM_TABLE = .); . = ALIGN(4); } > TEXT_region2 .VERSION_TAGS : { . = ALIGN(4); PROVIDE(__start_VERSION_TAGS = .); KEEP(*(.VERSION_TAGS)); PROVIDE(__stop_VERSION_TAGS = .); . = ALIGN(4); } > TEXT_region2 .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } > TEXT_region2 .ARM : { __exidx_start = .; *(.ARM.exidx*) __exidx_end = .; } > TEXT_region2 .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > TEXT_region2 .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > TEXT_region2 .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > TEXT_region2 .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > TEXT_region2 .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > TEXT_region2 __etext = .; /* define a global symbol at end of code */ __DATA_ROM = .; /* Symbol is used by startup for data initialization */ /* reserve MTB memory at the beginning of m_data */ .mtb : /* MTB buffer address as defined by the hardware */ { . = ALIGN(8); _mtb_start = .; KEEP(*(.mtb_buf)) /* need to KEEP Micro Trace Buffer as not referenced by application */ . = ALIGN(8); _mtb_end = .; } > DATA2_region .interrupts_ram : { . = ALIGN(4); __VECTOR_RAM__ = .; __interrupts_ram_start__ = .; /* Create a global symbol at data start */ *(.m_interrupts_ram) /* This is a user defined section */ . += __ram_vector_table_size__; . = ALIGN(4); __interrupts_ram_end__ = .; /* Define a global symbol at data end */ } > DATA2_region __VECTOR_RAM = __VECTOR_RAM__; __RAM_VECTOR_TABLE_SIZE_BYTES = (__interrupts_ram_end__ - __interrupts_ram_start__); .data : AT(__DATA_ROM) { . = ALIGN(4); __DATA_RAM = .; __data_start__ = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ KEEP(*(.jcr*)) . = ALIGN(4); __data_end__ = .; /* define a global symbol at data end */ } > DATA2_region __DATA_END = __DATA_ROM + (__data_end__ - __data_start__); text_end = ORIGIN(TEXT_region2) + LENGTH(TEXT_region2); ASSERT(__DATA_END <= text_end, "region m_text overflowed with text and data") /* Uninitialized data section */ .bss : { /* This is used by the startup in order to initialize the .bss section */ . = ALIGN(4); __START_BSS = .; __bss_start__ = .; *(.bss) *(.bss*) *(COMMON) /* *(EXCLUDE_FILE (./framework/MemManager/Source/MemManager.o) .bss*) */ . = ALIGN(4); __bss_end__ = .; __END_BSS = .; } > DATA2_region .heap : { . = ALIGN(8); __end__ = .; PROVIDE(end = .); __HeapBase = .; . += __size_heap__; __HeapLimit = .; } > DATA2_region .stack : { . = ALIGN(8); . += __size_cstack__; } > DATA2_region /* Initializes stack on the end of block */ __StackTop = ORIGIN(DATA2_region) + LENGTH(DATA2_region); __StackLimit = __StackTop - __size_cstack__; PROVIDE(__stack = __StackTop); .ARM.attributes 0 : { *(.ARM.attributes) } /* Remove this section to keep the nvm section on writting the device */ .NVM : { FILL(0xFFFFFFFF); . = ORIGIN(NVM_region) + LENGTH(NVM_region) - 1; BYTE(0xFF) } > NVM_region ASSERT(__StackLimit >= __HeapLimit, "region m_data overflowed with stack and heap") }