Connection from "127.0.0.1" via 127.0.0.1. Connection from port "60402" to 7224 Telnet server running on 127.0.0.1:51794 Unable to load libusb0.dll Copyright 2022 P&E Microcomputer Systems,Inc. Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.5.202210261806\win32\pegdbserver_power_console -device=MPC5746C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -Ü PEmicro Interface detected - Flash Version 10.81 Flash Data in range 0x00FC0000-0x00FC0003. Flash Data in range 0x00FC0010-0x00FC0013. Flash Data in range 0x00FC0400-0x00FC05E9. Flash Data in range 0x00FC1000-0x00FC10F3. Flash Data in range 0x00FC2000-0x00FC2BF7. Flash Data in range 0x00FC2C00-0x00FCB90F. CMD>RE Initializing. Device IDCODE is $00000084 Device ID revision is $00000001 MPC574xB/C/D Device detected. Target has been RESET and is active. CMD>CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.5.202210261806\win32\gdi\P&E\nxp_mpc5746c_1x32x736k_cflash.pcp Initializing. Device IDCODE is $00000084 Device ID revision is $00000001 MPC574xB/C/D Device detected. DOUBLE BUFFERING enabled. Initialized. ;version 1.06, 06/27/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [5746C_2944k] ;device NXP, MPC5746C, 1x32x736k, desc=CFlash ;begin_cs device=$00F90000, length=$002F0000, ram=$40000000 Loading programming algorithm ... Initializing Ram Block 0x40000000-0x4000FFFF. WARNING - Selected .PCP file has been modified. CRC16 = $2E34 Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Verifying object file CRC-16 to device ranges ... block 00FC0000-00FC0003 ... Calculated CRC-16 does not match block. (File = $FBBD, Device = $0000) Current content of flash does not match application to be programmed CMD>EM Erasing. Module has been erased. CMD>PM Programming. Processing Object File Data ... Error during programming. Error Programming flash of device Error occured during Flash programming. Device IDCODE is $00000084 Device ID revision is $00000001 Device IDCODE is $00000084 Device ID revision is $00000001 Starting reset script (C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.5.202210261806\win32\gdi\P&E\s32e200_mpc574xc.mac) ... REM This script is compatible with MPC574xC devices. REM Clean GPRs to remove residual data after using algorithm REM Initialize all of the Main SRAM - 512KB Initializing RAM from $40000000 to $4007FFFF. Initializing Ram Block 0x40000000-0x4007FFFF.