Connection from "127.0.0.1" via 127.0.0.1. Connection from port "54503" to 7224 Copyright 2018 P&E Microcomputer Systems,Inc. Command Line :C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -reseƐ P&E Interface detected - Flash Version 10.46 Flash Data in range 0x00800000-0x0080000F. Flash Data in range 0x00800400-0x00800617. Flash Data in range 0x00810000-0x00810133. Flash Data in range 0x00811000-0x00811803. Flash Data in range 0x00811810-0x0081331F. CMD>RE Initializing. Device IDCODE is $00000377 Device ID revision is $00000001 Initializing Ram Block 0x00300000-0x00307FFF. MPC5777C Device detected. Target has been RESET and is active. CMD>CM C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp Initializing. Device IDCODE is $00000377 Device ID revision is $00000001 Initializing Ram Block 0x00300000-0x00307FFF. MPC5777C Device detected. DOUBLE BUFFERING enabled. Initialized. ;version 1.04, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [5777C_8meg_highspeed] ;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed ;begin_cs device=$30800000, length=$00800000, ram=$00300000 Loading programming algorithm ... Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Verifying object file CRC-16 to device ranges ... block 00800000-0080000F ... Ok. block 00800400-00800617 ... Ok. block 00810000-00810133 ... Calculated CRC-16 does not match block. (File = $D446, Device = $3BDA) Current content of flash does not match application to be programmed CMD>EM Erasing. Module has been erased. CMD>PM Programming. Processing Object File Data ...