NOTICE: UDIMM 18ASF2G72HZ-3G2R1
Cold reset: set D_INIT
Cold reset: clear SDRAM_CFG_BI
NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1
NOTICE: BL2: v1.5-r9(release):LSDK-19.09-dirty
NOTICE: BL2: Built : 00:00:00, Jan 1 1970
NOTICE: BL31: v1.5-r9(release):LSDK-19.09-dirty
NOTICE: BL31: Built : 00:00:00, Jan 1 1970
NOTICE: Welcome to Castle BL31 Phase
U-Boot 2019.04+fsl+gce862bb (Nov 24 2023 - 15:21:24 +0000)
odin 2019.04-r0.18
SoC: LS1046AE Rev1.0 (0x87070010)
Clock Configuration:
CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz
CPU3(A72):1600 MHz
Bus: 600 MHz DDR: 2100 MT/s FMAN: 600 MHz
Reset Configuration Word (RCW):
00000000: 0c150010 08000000 00000000 00000000
00000010: 11335577 40000006 40044000 a1000000
00000020: 00000000 00000000 00000000 00038cf8
00000030: 20124004 00003101 00000096 00000002
Model: odin Calix XG1601 Board
Board: Odin-ArmTestCard, boot from QSPIDRAM: Reserving 16709632k for Calix u-boot image at: fbe00000
15.9 GiB (DDR4, 64-bit, CL=15, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
setup_reloc: After relocation bi_pramsize=1048576 bi_pramstart=d0000000
SEC0: RNG instantiated
Board type: 01
WARNING: Calling __hwconfig without a buffer and before environment is ready
Using SERDES1 Protocol: 4403 (0x1133)
Using SERDES2 Protocol: 21879 (0x5577)
MMC: FSL_SDHC: 0
Loading Environment from SPI Flash... SF: Detected mx25u25635f with page size 256 Bytes, erase size 64 KiB, total 32 MiB
OK
EEPROM: serial: 602301000018
In: serial
Out: serial
Err: serial
Net: SF: Detected mx25u25635f with page size 256 Bytes, erase size 64 KiB, total 32 MiB
Fman1: Uploading microcode version 108.4.9
Could not get PHY for FSL_MDIO1: addr 1
Failed to connect
PCIe0: pcie@3400000 Root Complex: x1 gen3
PCIe1: pcie@3500000 Root Complex: x1 gen2
PCIe2: pcie@3600000 Root Complex: no link
FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2
FE switch ID: 0xae02 0x5350 --> BCM53101 Rev 0
enable fwd for imp - BCM53134
Debug Ethernet PHY adr=0 id=0x0000 0x0000 --> unknown
Debug Ethernet PHY adr=1 id=0x0000 0x0000 --> unknown
Debug Ethernet PHY adr=3 id=0x0000 0x0000 --> unknown
Enter '0 s t o p 0' or '1 d e l a y 1' without spaces to stop/delay autoboot in 4 second(s)
=> setenv othbootargs runlevel=1 loglevel=8
=> run calix_boot_script_internal_imgx
resetting USB...
USB0: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
4800 bytes read in 27 ms (172.9 KiB/s)
## Executing script at 80a00000
Contents of mmc 0:1
1024 .
1024 ..
12288 lost+found
4096 imgx
3072 imgy
30 boot.img
run mst_script
3893 bytes read in 8 ms (474.6 KiB/s)
Executing machine subtype specific boot script
## Executing script at 83000000
running mst script - submachine: atna
7966067 bytes read in 472 ms (16.1 MiB/s)
Uncompressed size: 22317064 = 0x1548808
36302 bytes read in 43 ms (824.2 KiB/s)
7423461 bytes read in 438 ms (16.2 MiB/s)
run boot_it
index start size
------------------------------------------------
0 00000000d0000000 0000000000800000
1 00000000d0800000 0000000000020000
Attempting to boot with imgx on device mmc 0:1
bootargs: imgmnt=/media/sda2 imgdir=imgx img=image.rootfs rootdelay=2 slub_debug=F console=ttyS1,115200 uio_pdrv_genirq.of_id=generic-uio memmap=0x10000000!0xC0000000 pram_addr=D0800000 pram_size=0x20000 bootcountaddr=0xd0000000 bootcount_size=0x800000 bootcount=1 crashkernel=512M runlevel=1 loglevel=8
## Loading init Ramdisk from Legacy Image at a0000000 ...
Image Name: exa-image-initramfs-odin-2024011
Image Type: AArch64 Linux RAMDisk Image (uncompressed)
Data Size: 7423397 Bytes = 7.1 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
Using Device Tree in place at 0000000082000000, end 0000000082022fff
WARNING failed to get smmu node: FDT_ERR_NOTFOUND
WARNING failed to get smmu node: FDT_ERR_NOTFOUND
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 5.10.52+ga11753a89ec6 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP Fri Jan 12 02:49:41 UTC 2024
[ 0.000000] Machine model: LS1046A ODIN board
[ 0.000000] pmem reserved: 0x00000000c0000000 - 0x00000000d0000000 (256 MB)
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,qman-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] pmem reserved: 0x00000000c0000000 - 0x00000000d0000000 (256 MB)
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x0000000bff7fffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] node 0: [mem 0x00000000d0000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x0000000bfbffffff]
[ 0.000000] node 0: [mem 0x0000000bff000000-0x0000000bff7fffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000bff7fffff]
[ 0.000000] On node 0 totalpages: 4097536
[ 0.000000] DMA zone: 6904 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 441856 pages, LIFO batch:63
[ 0.000000] Normal zone: 57120 pages used for memmap
[ 0.000000] Normal zone: 3655680 pages, LIFO batch:63
[ 0.000000] cma: Reserved 16 MiB at 0x00000000fac00000
[ 0.000000] crashkernel reserved: 0x00000000dac00000 - 0x00000000fac00000 (512 MB)
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 31 pages/cpu s89752 r8192 d29032 u126976
[ 0.000000] pcpu-alloc: s89752 r8192 d29032 u126976 alloc=31*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: Spectre-v2
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 4033512
[ 0.000000] Kernel command line: imgmnt=/media/sda2 imgdir=imgx img=image.rootfs rootdelay=2 slub_debug=F console=ttyS1,115200 uio_pdrv_genirq.of_id=generic-uio memmap=0x10000000!0xC0000000 pram_addr=D0800000 pram_size=0x20000 bootcountaddr=0xd0000000 bootcount_size=0x800000 bootcount=1 crashkernel=512M runlevel=1 loglevel=8
[ 0.000000] pram buf is invalid, reset it
[ 0.000000] pram kerne log buf initialized: 7fd000, d0000000, ffff000050000000
[ 0.000000] printk: log_buf_len individual max cpu contribution: 131072 bytes
[ 0.000000] printk: log_buf_len total cpu_extra contributions: 393216 bytes
[ 0.000000] printk: log_buf_len min size: 262144 bytes
[ 0.000000] printk: log_buf_len: 1048576 bytes
[ 0.000000] printk: early log buf free: 259128(98%)
[ 0.000000] Dentry cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000d6c00000-0x00000000dac00000] (64MB)
[ 0.000000] Memory: 15420816K/16390144K available (11838K kernel code, 2338K rwdata, 3736K rodata, 3840K init, 1120K bss, 952944K reserved, 16384K cma-reserved)
[ 0.000000] ftrace: allocating 37607 entries in 147 pages
[ 0.000000] ftrace: allocated 147 pages with 4 groups
[ 0.000000] rcu: Hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: CONFIG_RCU_FANOUT set to non-default value of 32.
[ 0.000000] Rude variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 jiffies.
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] random: get_random_bytes called from start_kernel+0x314/0x508 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.000270] Console: colour dummy device 80x25
[ 0.000283] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=25000)
[ 0.000290] pid_max: default: 32768 minimum: 301
[ 0.000436] Mount-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.000487] Mountpoint-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.001188] rcu: Hierarchical SRCU implementation.
[ 0.001793] smp: Bringing up secondary CPUs ...
[ 0.002080] Detected PIPT I-cache on CPU1
[ 0.002107] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.002399] Detected PIPT I-cache on CPU2
[ 0.002417] CPU2: Booted secondary processor 0x0000000002 [0x410fd082]
[ 0.002709] Detected PIPT I-cache on CPU3
[ 0.002726] CPU3: Booted secondary processor 0x0000000003 [0x410fd082]
[ 0.002762] smp: Brought up 1 node, 4 CPUs
[ 0.002773] SMP: Total of 4 processors activated.
[ 0.002777] CPU features: detected: 32-bit EL0 Support
[ 0.002780] CPU features: detected: CRC32 instructions
[ 0.002805] CPU: All CPU(s) started at EL2
[ 0.002818] alternatives: patching kernel code
[ 0.003484] devtmpfs: initialized
[ 0.006611] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275000 ns
[ 0.006619] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.007397] NET: Registered protocol family 16
[ 0.008021] DMA: preallocated 2048 KiB GFP_KERNEL pool for atomic allocations
[ 0.008307] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.008737] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.008907] thermal_sys: Registered thermal governor 'step_wise'
[ 0.009206] cpuidle: using governor ladder
[ 0.009217] cpuidle: using governor menu
[ 0.009262] Bman ver:0a02,02,01
[ 0.011449] qman-fqd addr 0x0000000bff800000 size 0x800000
[ 0.011453] qman-pfdr addr 0x0000000bfc000000 size 0x2000000
[ 0.011459] Qman ver:0a01,03,02,01
[ 0.011545] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.011585] ASID allocator initialised with 65536 entries
[ 0.023445] Machine: LS1046A ODIN board
[ 0.023450] SoC family: QorIQ LS1046A
[ 0.023453] SoC ID: svr:0x87070010, Revision: 1.0
[ 0.027017] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.027023] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.027027] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.027031] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.027853] cryptd: max_cpu_qlen set to 1000
[ 0.029899] iommu: Default domain type: Passthrough
[ 0.030019] usbcore: registered new interface driver usbfs
[ 0.030036] usbcore: registered new interface driver hub
[ 0.030051] usbcore: registered new device driver usb
[ 0.030178] imx-i2c 2180000.i2c: can't get pinctrl, bus recovery not supported
[ 0.030314] i2c i2c-0: IMX I2C adapter registered
[ 0.030337] i2c i2c-0: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers
[ 0.030500] imx-i2c 21a0000.i2c: scl-gpios not found
[ 0.030709] i2c i2c-1: IMX I2C adapter registered
[ 0.030803] imx-i2c 21b0000.i2c: scl-gpios not found
[ 0.030904] i2c i2c-2: IMX I2C adapter registered
[ 0.031043] EDAC MC: Ver: 3.0.0
[ 0.031235] bman-fbpr addr 0x0000000bfe000000 size 0x1000000
[ 0.031257] Bman err interrupt handler present
[ 0.031714] Bman portal initialised, cpu 0
[ 0.031762] Bman portal initialised, cpu 1
[ 0.031807] Bman portal initialised, cpu 2
[ 0.031853] Bman portal initialised, cpu 3
[ 0.031856] Bman portals initialised
[ 0.032939] Qman err interrupt handler present
[ 0.033186] QMan: Allocated lookup table at (____ptrval____), entry count 131073
[ 0.033618] Qman portal initialised, cpu 0
[ 0.033657] Qman portal initialised, cpu 1
[ 0.033695] Qman portal initialised, cpu 2
[ 0.033732] Qman portal initialised, cpu 3
[ 0.033735] Qman portals initialised
[ 0.033804] Bman: BPID allocator includes range 32:32
[ 0.033847] Qman: FQID allocator includes range 256:256
[ 0.033851] Qman: FQID allocator includes range 32768:32768
[ 0.033897] Qman: CGRID allocator includes range 0:256
[ 0.034052] Qman: pool channel allocator includes range 1025:15
[ 0.034478] clocksource: Switched to clocksource arch_sys_counter
[ 0.252540] NET: Registered protocol family 2
[ 0.252957] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.256871] tcp_listen_portaddr_hash hash table entries: 8192 (order: 5, 131072 bytes, linear)
[ 0.256984] TCP established hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.257502] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
[ 0.258018] TCP: Hash tables configured (established 131072 bind 65536)
[ 0.258079] UDP hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.258272] UDP-Lite hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.258536] NET: Registered protocol family 1
[ 0.258733] RPC: Registered named UNIX socket transport module.
[ 0.258737] RPC: Registered udp transport module.
[ 0.258740] RPC: Registered tcp transport module.
[ 0.258743] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.258748] PCI: CLS 0 bytes, default 64
[ 0.258818] Trying to unpack rootfs image as initramfs...
[ 0.479591] Freeing initrd memory: 7244K
[ 0.480066] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.480999] workingset: timestamp_bits=46 max_order=22 bucket_order=0
[ 0.481287] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.481411] NFS: Registering the id_resolver key type
[ 0.481423] Key type id_resolver registered
[ 0.481426] Key type id_legacy registered
[ 0.481442] fuse: init (API version 7.32)
[ 0.481579] aufs 5.10-20230227
[ 0.506025] io scheduler mq-deadline registered
[ 0.506029] io scheduler kyber registered
[ 0.507046] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:
[ 0.507054] layerscape-pcie 3400000.pcie: Parsing ranges property...
[ 0.507068] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -> 0x0000000000
[ 0.507078] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -> 0x0040000000
[ 0.507154] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00
[ 0.507160] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.507164] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.507170] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])
[ 0.507175] pci_bus 0000:00: scanning bus
[ 0.507193] pci 0000:00:00.0: [1957:81c0] type 01 class 0x060400
[ 0.507207] pci 0000:00:00.0: reg 0x38: [mem 0x4040000000-0x40400007ff pref]
[ 0.507237] pci 0000:00:00.0: supports D1 D2
[ 0.507241] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 0.507246] pci 0000:00:00.0: PME# disabled
[ 0.508462] pci_bus 0000:00: fixups for bus
[ 0.508467] pci 0000:00:00.0: scanning [bus 01-ff] behind bridge, pass 0
[ 0.508508] pci_bus 0000:01: scanning bus
[ 0.509598] pci_bus 0000:01: fixups for bus
[ 0.509603] pci_bus 0000:01: bus scan returning with max=01
[ 0.509609] pci 0000:00:00.0: scanning [bus 01-ff] behind bridge, pass 1
[ 0.509614] pci_bus 0000:00: bus scan returning with max=ff
[ 0.509624] pci 0000:00:00.0: BAR 6: assigned [mem 0x4040000000-0x40400007ff pref]
[ 0.509630] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 0.509684] pcieport 0000:00:00.0: assign IRQ: got 86
[ 0.509748] pcieport 0000:00:00.0: PME: Signaling with IRQ 75
[ 0.509852] pcieport 0000:00:00.0: AER: enabled with IRQ 74
[ 0.509891] pcieport 0000:00:00.0: saving config space at offset 0x0 (reading 0x81c01957)
[ 0.509896] pcieport 0000:00:00.0: saving config space at offset 0x4 (reading 0x100107)
[ 0.509900] pcieport 0000:00:00.0: saving config space at offset 0x8 (reading 0x6040010)
[ 0.509904] pcieport 0000:00:00.0: saving config space at offset 0xc (reading 0x10008)
[ 0.509908] pcieport 0000:00:00.0: saving config space at offset 0x10 (reading 0x0)
[ 0.509912] pcieport 0000:00:00.0: saving config space at offset 0x14 (reading 0x0)
[ 0.509916] pcieport 0000:00:00.0: saving config space at offset 0x18 (reading 0xff0100)
[ 0.509920] pcieport 0000:00:00.0: saving config space at offset 0x1c (reading 0x1f1)
[ 0.509924] pcieport 0000:00:00.0: saving config space at offset 0x20 (reading 0xfff0)
[ 0.509928] pcieport 0000:00:00.0: saving config space at offset 0x24 (reading 0x1fff1)
[ 0.509931] pcieport 0000:00:00.0: saving config space at offset 0x28 (reading 0x0)
[ 0.509935] pcieport 0000:00:00.0: saving config space at offset 0x2c (reading 0x0)
[ 0.509939] pcieport 0000:00:00.0: saving config space at offset 0x30 (reading 0x0)
[ 0.509943] pcieport 0000:00:00.0: saving config space at offset 0x34 (reading 0x40)
[ 0.509947] pcieport 0000:00:00.0: saving config space at offset 0x38 (reading 0x40000000)
[ 0.509951] pcieport 0000:00:00.0: saving config space at offset 0x3c (reading 0x20156)
[ 0.510033] layerscape-pcie 3500000.pcie: host bridge /soc/pcie@3500000 ranges:
[ 0.510040] layerscape-pcie 3500000.pcie: Parsing ranges property...
[ 0.510052] layerscape-pcie 3500000.pcie: IO 0x4800010000..0x480001ffff -> 0x0000000000
[ 0.510061] layerscape-pcie 3500000.pcie: MEM 0x4840000000..0x487fffffff -> 0x0040000000
[ 0.510127] layerscape-pcie 3500000.pcie: PCI host bridge to bus 0001:00
[ 0.510131] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 0.510136] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 0.510141] pci_bus 0001:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])
[ 0.510145] pci_bus 0001:00: scanning bus
[ 0.510158] pci 0001:00:00.0: [1957:81c0] type 01 class 0x060400
[ 0.510171] pci 0001:00:00.0: reg 0x38: [mem 0x4840000000-0x48400007ff pref]
[ 0.510197] pci 0001:00:00.0: supports D1 D2
[ 0.510200] pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 0.510204] pci 0001:00:00.0: PME# disabled
[ 0.511377] pci_bus 0001:00: fixups for bus
[ 0.511382] pci 0001:00:00.0: scanning [bus 01-ff] behind bridge, pass 0
[ 0.511416] pci_bus 0001:01: scanning bus
[ 0.511500] pci 0001:01:00.0: [14e4:8470] type 00 class 0x020000
[ 0.511553] pci 0001:01:00.0: reg 0x10: [mem 0x4840100000-0x4840107fff 64bit pref]
[ 0.511588] pci 0001:01:00.0: reg 0x18: [mem 0x4840800000-0x4840ffffff 64bit pref]
[ 0.511901] pci 0001:01:00.0: PME# supported from D0 D3hot D3cold
[ 0.511911] pci 0001:01:00.0: PME# disabled
[ 0.512145] pci 0001:01:00.1: [14e4:8470] type 00 class 0x020000
[ 0.512197] pci 0001:01:00.1: reg 0x10: [mem 0x4841000000-0x4841007fff 64bit pref]
[ 0.512232] pci 0001:01:00.1: reg 0x18: [mem 0x4841800000-0x4841ffffff 64bit pref]
[ 0.512507] pci 0001:01:00.1: PME# supported from D0 D3hot D3cold
[ 0.512516] pci 0001:01:00.1: PME# disabled
[ 0.516610] pci_bus 0001:01: fixups for bus
[ 0.516615] pci_bus 0001:01: bus scan returning with max=01
[ 0.516621] pci 0001:00:00.0: scanning [bus 01-ff] behind bridge, pass 1
[ 0.516626] pci_bus 0001:00: bus scan returning with max=ff
[ 0.516635] pci 0001:00:00.0: BAR 9: assigned [mem 0x4840000000-0x48413fffff 64bit pref]
[ 0.516640] pci 0001:00:00.0: BAR 6: assigned [mem 0x4841400000-0x48414007ff pref]
[ 0.516646] pci 0001:01:00.0: BAR 2: assigned [mem 0x4840000000-0x48407fffff 64bit pref]
[ 0.516671] pci 0001:01:00.1: BAR 2: assigned [mem 0x4840800000-0x4840ffffff 64bit pref]
[ 0.516695] pci 0001:01:00.0: BAR 0: assigned [mem 0x4841000000-0x4841007fff 64bit pref]
[ 0.516719] pci 0001:01:00.1: BAR 0: assigned [mem 0x4841008000-0x484100ffff 64bit pref]
[ 0.516743] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
[ 0.516749] pci 0001:00:00.0: bridge window [mem 0x4840000000-0x48413fffff 64bit pref]
[ 0.516793] pcieport 0001:00:00.0: assign IRQ: got 87
[ 0.516852] pcieport 0001:00:00.0: PME: Signaling with IRQ 77
[ 0.516946] pcieport 0001:00:00.0: AER: enabled with IRQ 76
[ 0.516985] pcieport 0001:00:00.0: saving config space at offset 0x0 (reading 0x81c01957)
[ 0.516990] pcieport 0001:00:00.0: saving config space at offset 0x4 (reading 0x100107)
[ 0.516994] pcieport 0001:00:00.0: saving config space at offset 0x8 (reading 0x6040010)
[ 0.516997] pcieport 0001:00:00.0: saving config space at offset 0xc (reading 0x10008)
[ 0.517001] pcieport 0001:00:00.0: saving config space at offset 0x10 (reading 0x0)
[ 0.517005] pcieport 0001:00:00.0: saving config space at offset 0x14 (reading 0x0)
[ 0.517009] pcieport 0001:00:00.0: saving config space at offset 0x18 (reading 0xff0100)
[ 0.517013] pcieport 0001:00:00.0: saving config space at offset 0x1c (reading 0x200001f1)
[ 0.517016] pcieport 0001:00:00.0: saving config space at offset 0x20 (reading 0xfff0)
[ 0.517020] pcieport 0001:00:00.0: saving config space at offset 0x24 (reading 0x41314001)
[ 0.517024] pcieport 0001:00:00.0: saving config space at offset 0x28 (reading 0x0)
[ 0.517028] pcieport 0001:00:00.0: saving config space at offset 0x2c (reading 0x0)
[ 0.517032] pcieport 0001:00:00.0: saving config space at offset 0x30 (reading 0x0)
[ 0.517035] pcieport 0001:00:00.0: saving config space at offset 0x34 (reading 0x40)
[ 0.517039] pcieport 0001:00:00.0: saving config space at offset 0x38 (reading 0x40000000)
[ 0.517043] pcieport 0001:00:00.0: saving config space at offset 0x3c (reading 0x20157)
[ 0.517136] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 ranges:
[ 0.517142] layerscape-pcie 3600000.pcie: Parsing ranges property...
[ 0.517154] layerscape-pcie 3600000.pcie: IO 0x5000010000..0x500001ffff -> 0x0000000000
[ 0.517163] layerscape-pcie 3600000.pcie: MEM 0x5040000000..0x507fffffff -> 0x0040000000
[ 0.517233] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0002:00
[ 0.517237] pci_bus 0002:00: root bus resource [bus 00-ff]
[ 0.517242] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x0000-0xffff])
[ 0.517247] pci_bus 0002:00: root bus resource [mem 0x5040000000-0x507fffffff] (bus address [0x40000000-0x7fffffff])
[ 0.517251] pci_bus 0002:00: scanning bus
[ 0.517265] pci 0002:00:00.0: [1957:81c0] type 01 class 0x060400
[ 0.517279] pci 0002:00:00.0: reg 0x38: [mem 0x5040000000-0x50400007ff pref]
[ 0.517306] pci 0002:00:00.0: supports D1 D2
[ 0.517310] pci 0002:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 0.517314] pci 0002:00:00.0: PME# disabled
[ 0.518493] pci_bus 0002:00: fixups for bus
[ 0.518499] pci 0002:00:00.0: scanning [bus 01-ff] behind bridge, pass 0
[ 0.518534] pci_bus 0002:01: scanning bus
[ 0.519626] pci_bus 0002:01: fixups for bus
[ 0.519630] pci_bus 0002:01: bus scan returning with max=01
[ 0.519636] pci 0002:00:00.0: scanning [bus 01-ff] behind bridge, pass 1
[ 0.519641] pci_bus 0002:00: bus scan returning with max=ff
[ 0.519648] pci 0002:00:00.0: BAR 6: assigned [mem 0x5040000000-0x50400007ff pref]
[ 0.519652] pci 0002:00:00.0: PCI bridge to [bus 01-ff]
[ 0.519698] pcieport 0002:00:00.0: assign IRQ: got 88
[ 0.519756] pcieport 0002:00:00.0: PME: Signaling with IRQ 79
[ 0.519848] pcieport 0002:00:00.0: AER: enabled with IRQ 78
[ 0.519888] pcieport 0002:00:00.0: saving config space at offset 0x0 (reading 0x81c01957)
[ 0.519893] pcieport 0002:00:00.0: saving config space at offset 0x4 (reading 0x100107)
[ 0.519897] pcieport 0002:00:00.0: saving config space at offset 0x8 (reading 0x6040010)
[ 0.519901] pcieport 0002:00:00.0: saving config space at offset 0xc (reading 0x10008)
[ 0.519905] pcieport 0002:00:00.0: saving config space at offset 0x10 (reading 0x0)
[ 0.519909] pcieport 0002:00:00.0: saving config space at offset 0x14 (reading 0x0)
[ 0.519912] pcieport 0002:00:00.0: saving config space at offset 0x18 (reading 0xff0100)
[ 0.519916] pcieport 0002:00:00.0: saving config space at offset 0x1c (reading 0x1f1)
[ 0.519920] pcieport 0002:00:00.0: saving config space at offset 0x20 (reading 0xfff0)
[ 0.519924] pcieport 0002:00:00.0: saving config space at offset 0x24 (reading 0x1fff1)
[ 0.519928] pcieport 0002:00:00.0: saving config space at offset 0x28 (reading 0x0)
[ 0.519931] pcieport 0002:00:00.0: saving config space at offset 0x2c (reading 0x0)
[ 0.519935] pcieport 0002:00:00.0: saving config space at offset 0x30 (reading 0x0)
[ 0.519939] pcieport 0002:00:00.0: saving config space at offset 0x34 (reading 0x40)
[ 0.519943] pcieport 0002:00:00.0: saving config space at offset 0x38 (reading 0x40000000)
[ 0.519947] pcieport 0002:00:00.0: saving config space at offset 0x3c (reading 0x20158)
[ 0.537852] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.538625] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 52, base_baud = 18750000) is a 16550A
[ 0.538930] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 52, base_baud = 18750000) is a 16550A
[ 2.502447] printk: console [ttyS1] enabled
[ 2.506949] 21d0500.serial: ttyS2 at MMIO 0x21d0500 (irq = 53, base_baud = 18750000) is a 16550A
[ 2.516038] 21d0600.serial: ttyS3 at MMIO 0x21d0600 (irq = 53, base_baud = 18750000) is a 16550A
[ 2.527256] brd: module loaded
[ 2.533309] loop: module loaded
[ 2.536830] spi-nor spi0.0: mx25u25635f (32768 Kbytes)
[ 2.541993] 7 fixed-partitions partitions found on MTD device 1550000.spi-0
[ 2.548958] Creating 7 MTD partitions on "1550000.spi-0":
[ 2.554358] 0x000000100000-0x000000500000 : "U-Boot Image"
[ 2.560328] 0x000000a00000-0x000000a20000 : "U-Boot Env Pri"
[ 2.566450] 0x000000900000-0x000000940000 : "FMAN Ucode"
[ 2.572215] 0x000000b00000-0x000000f00000 : "BOOTLOG"
[ 2.577721] 0x000001200000-0x000001400000 : "CRASH-RECORD"
[ 2.583674] 0x000001600000-0x000001610000 : "Test"
[ 2.588922] 0x000000000000-0x000000100000 : "RCW"
[ 2.594212] spi-nor spi0.2: found cy14v101qs, expected m25p80
[ 2.600000] spi-nor spi0.2: cy14v101qs (128 Kbytes)
[ 2.604886] 1 fixed-partitions partitions found on MTD device 1550000.spi-2
[ 2.611854] Creating 1 MTD partitions on "1550000.spi-2":
[ 2.617255] 0x000000000000-0x000000020000 : "nvSRAM"
[ 2.623439] libphy: Fixed MDIO Bus: probed
[ 2.627894] tun: Universal TUN/TAP device driver, 1.6
[ 2.633217] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.638421] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.645558] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.651594] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.657593] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.663579] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.669553] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.675526] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.681496] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.687470] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.703195] Freescale FM module, FMD API version 21.1.0
[ 2.710879] Freescale FM Ports module
[ 2.714545] fsl_mac: mac.c:479:mac_load() fsl_mac: FSL FMan MAC API based driver
[ 2.722115] fsl_mac 1ae4000.ethernet: SGMII Interface 626F
[ 2.728628] fman_memac_init: enet_interface=0x50000 if_mode=0x00008006
[ 2.735165] fsl_mac 1ae4000.ethernet: FMan MEMAC
[ 2.739787] fsl_mac 1ae4000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b1
[ 2.746683] fsl_mac 1ae6000.ethernet: SGMII Interface 626F
[ 2.752176] fman_memac_init: enet_interface=0x50000 if_mode=0x00008006
[ 2.758709] fsl_mac 1ae6000.ethernet: FMan MEMAC
[ 2.763327] fsl_mac 1ae6000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b2
[ 2.770214] fsl_mac 1ae8000.ethernet: FOUND TBI Interface 626A 400
[ 2.777245] fsl_mac 1ae8000.ethernet: ADD BASEX 800803E8
[ 2.782563] fman_memac_init: enet_interface=0x80000 if_mode=0x00000002
[ 2.789151] fsl_mac 1ae8000.ethernet: FMan MEMAC
[ 2.793769] fsl_mac 1ae8000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b3
[ 2.800661] fsl_mac 1aea000.ethernet: FOUND TBI Interface 626A 400
[ 2.807667] fsl_mac 1aea000.ethernet: ADD BASEX 800803E8
[ 2.812984] fman_memac_init: enet_interface=0x80000 if_mode=0x00000002
[ 2.819570] fsl_mac 1aea000.ethernet: FMan MEMAC
[ 2.824188] fsl_mac 1aea000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b4
[ 2.831083] fsl_mac 1af0000.ethernet: SGMII Interface 1000
[ 2.837391] fman_memac_init: enet_interface=0x90000 if_mode=0x00000000
[ 2.843927] fsl_mac 1af0000.ethernet: FMan MEMAC
[ 2.848546] fsl_mac 1af0000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b5
[ 2.855440] fsl_mac 1af2000.ethernet: SGMII Interface 1000
[ 2.861766] fman_memac_init: enet_interface=0x90000 if_mode=0x00000000
[ 2.868304] fsl_mac 1af2000.ethernet: FMan MEMAC
[ 2.872923] fsl_mac 1af2000.ethernet: FMan MAC address: 1c:8b:76:35:6a:b6
[ 2.879740] fsl_dpa: dpaa_eth.c:1173:dpa_load() FSL DPAA Ethernet driver
[ 2.886442] fsl_dpa: FSL DPAA Ethernet debugfs entries
[ 2.892887] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth0
[ 2.902357] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth1
[ 2.911937] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth2
[ 2.921637] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth3
[ 2.931454] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth4
[ 2.941387] fsl_dpa: dpaa_eth.c:1116:dpaa_eth_priv_probe() fsl_dpa: Probed interface eth5
[ 2.949635] fsl_advanced: dpaa_eth_base.c:193:dpa_advanced_load() FSL DPAA Advanced drivers:
[ 2.958078] fsl_proxy: dpaa_eth_proxy.c:354:dpa_proxy_load() FSL DPAA Proxy initialization driver
[ 2.967056] fsl_oh: offline_port.c:824:oh_port_load() FSL FMan Offline Parsing port driver
[ 2.976531] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.983065] ehci-pci: EHCI PCI platform driver
[ 2.987520] ehci-platform: EHCI generic platform driver
[ 2.992856] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.999043] ohci-pci: OHCI PCI platform driver
[ 3.003496] ohci-platform: OHCI generic platform driver
[ 3.009104] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.014600] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 3.022318] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010810
[ 3.031730] xhci-hcd xhci-hcd.0.auto: irq 61, io mem 0x02f00000
[ 3.037947] hub 1-0:1.0: USB hub found
[ 3.041708] hub 1-0:1.0: 1 port detected
[ 3.045762] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.051253] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 3.058916] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 3.065666] hub 2-0:1.0: USB hub found
[ 3.069456] hub 2-0:1.0: 1 port detected
[ 3.073613] mousedev: PS/2 mouse device common for all mice
[ 3.079188] i2c /dev entries driver
[ 3.082833] loading AIX_IIC driver
[ 3.086255] AIX_IIC Driver running in interrupt mode
[ 3.091220] check fpga version
[ 3.094362] fpga version: 0x21
[ 3.118957] EDAC MC0: Giving out device to module fsl_ddr_edac controller fsl_mc_err: DEV fsl_mc_err (INTERRUPT)
[ 3.129162] fsl_ddr_edac acquired irq 18 for MC
[ 3.133693] fsl_ddr_edac MC err registered
[ 3.138251] qoriq-cpufreq qoriq-cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 3.146262] sdhci: Secure Digital Host Controller Interface driver
[ 3.152444] sdhci: Copyright(c) Pierre Ossman
[ 3.156799] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.163325] GACT probability NOT on
[ 3.166816] Mirror/redirect action on
[ 3.170532] Simple TC action Loaded
[ 3.174201] netem: version 1.3
[ 3.177265] u32 classifier
[ 3.179968] input device check on
[ 3.183627] Actions configured
[ 3.187302] IPVS: Registered protocols ()
[ 3.187994] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 3.191319] IPVS: Connection hash table configured (size=4096, memory=64Kbytes)
[ 3.206519] IPVS: ipvs loaded.
[ 3.209630] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 3.215330] Initializing XFRM netlink socket
[ 3.219660] NET: Registered protocol family 10
[ 3.224652] Segment Routing with IPv6
[ 3.228360] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.234478] NET: Registered protocol family 17
[ 3.238929] NET: Registered protocol family 15
[ 3.243392] Bridge firewalling registered
[ 3.247419] 8021q: 802.1Q VLAN Support v1.8
[ 3.251615] Key type dns_resolver registered
[ 3.259755] Freeing unused kernel memory: 3840K
[ 3.264526] Run /init as init process
[ 3.268189] with arguments:
[ 3.271154] /init
[ 3.273424] with environment:
[ 3.276562] HOME=/
[ 3.278917] TERM=linux
[ 3.281619] imgmnt=/media/sda2
[ 3.285018] imgdir=imgx
[ 3.287807] img=image.rootfs
[ 3.291032] slub_debug=F
[ 3.293909] pram_addr=D0800000
[ 3.297308] pram_size=0x20000
[ 3.300619] bootcount=1
[ 3.303408] runlevel=1
[ 3.312201] mmc0: new DDR MMC card at address 0001
[ 3.317184] Begin Initial RAM boot
[ 3.317323] mmcblk0: mmc0:0001 ATP 7.28 GiB
[ 3.325399] mmcblk0boot0: mmc0:0001 ATP partition 1 4.00 MiB
[ 3.331523] mmcblk0boot1: mmc0:0001 ATP partition 2 4.00 MiB
[ 3.337583] mmcblk0rpmb: mmc0:0001 ATP partition 3 4.00 MiB, chardev (246:0)
[ 3.345725] mmcblk0: p1 p2
e2fsck 1.46.5 (30-Dec-2021)
boot: recovering journal
Pass 1: Checking inodes, blocks, and sizes
[ 3.520882] random: fast init done / 5.6%
Pass 2: Checking directory structure
Pass 3: Checking directory connectivity
Pass 4: Checking reference counts
Pass 5: Checking group summary information
boot: 97/51200 files (30.9% non-contiguous), 50119/204800 blocks
e2fsck 1.46.5 (30-Dec-2021)
flash: recovering journal
Pass 1: Checking inodes, blocks, and sizes
Pass 2: Checking directory structure
Pass 3: Checking directory connectivity
Pass 4: Checking reference counts
Pass 5: Checking group summary information
Free blocks count wrong (249254, counted=268434).
Fix? yes
Free inodes count wrong (451112, coun[ 4.338656] udevd[180]: starting version 3.2.10
ted=451099).
Fi[ 4.343892] random: udevd: uninitialized urandom read (16 bytes read)
x? yes
flas[ 4.351597] random: udevd: uninitialized urandom read (16 bytes read)
h: ***** FILE SY[ 4.359399] random: udevd: uninitialized urandom read (16 bytes read)
STEM WAS MODIFIED *****
flash: 9461/460560 file[ 4.370204] udevd[181]: starting eudev-3.2.10
s (0.6% non-contiguous), 1571694/1840128 blocks
[ 4.906056] EXT4-fs (mmcblk0p1): mounting ext3 file system using the ext4 subsystem
[ 4.920403] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: data=ordered
[ 4.961461] EXT4-fs (mmcblk0p1): mounted filesystem with writeback data mode. Opts: errors=continue,user_xattr,barrier=1,data=writeback
[ 5.039933] aufs test_add:291:mount[1517]: uid/gid/perm /ro 0/0/0755, 0/0/01777
INIT: version 3.01 booting
1970-01-01T00:00:07.307376960+0000 UTC running [/etc/init.d/rc S]
1970-01-01T00:00:07.330175800+0000 UTC running [stty onlcr 0>&1]
1970-01-01T00:00:07.343373240+0000 UTC [stty onlcr 0>&1] done
[ 7.354676] Begin System boot
Starting udev
[ 7.523310] udevd[1597]: starting version 3.2.10
[ 7.540610] urandom_read: 4 callbacks suppressed
[ 7.540613] random: udevd: uninitialized urandom read (16 bytes read)
[ 7.551775] random: udevd: uninitialized urandom read (16 bytes read)
[ 7.558242] random: udevd: uninitialized urandom read (16 bytes read)
[ 7.584691] udevd[1598]: starting eudev-3.2.10
[ 7.650240] i2c i2c-1: Added multiplexed i2c bus 4
[ 7.655937] i2c i2c-1: Added multiplexed i2c bus 5
[ 7.662319] i2c i2c-1: Added multiplexed i2c bus 6
[ 7.676797] i2c i2c-1: Added multiplexed i2c bus 7
[ 7.688993] i2c i2c-1: Added multiplexed i2c bus 8
[ 7.700231] i2c i2c-1: Added multiplexed i2c bus 9
[ 7.707211] i2c i2c-1: Added multiplexed i2c bus 10
[ 7.707289] at24 0-0051: 256 byte spd EEPROM, read-only
[ 7.712503] i2c i2c-1: Added multiplexed i2c bus 11
[ 7.719530] at24 0-0052: 512 byte 24c04 EEPROM, writable, 1 bytes/write
[ 7.723611] pca954x 1-0070: registered 8 multiplexed busses for I2C switch pca9548
[ 7.729350] at24 5-0052: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[ 7.737308] i2c i2c-1: Added multiplexed i2c bus 12
[ 7.748349] i2c i2c-1: Added multiplexed i2c bus 13
[ 7.753797] i2c i2c-1: Added multiplexed i2c bus 14
[ 7.758829] i2c i2c-1: Added multiplexed i2c bus 15
[ 7.763822] i2c i2c-1: Added multiplexed i2c bus 16
[ 7.770114] i2c i2c-1: Added multiplexed i2c bus 17
[ 7.777206] bcm53xx 0x0000000001afc000:1e: probe b53_mdio_probe
[ 7.777453] ftm-alarm 29d0000.timer: registered as rtc1
[ 7.778519] i2c i2c-1: Added multiplexed i2c bus 18
[ 7.778732] i2c i2c-1: Added multiplexed i2c bus 19
[ 7.778737] pca954x 1-0071: registered 8 multiplexed busses for I2C switch pca9548
[ 7.779274] i2c i2c-2: Added multiplexed i2c bus 20
[ 7.779365] i2c i2c-2: Added multiplexed i2c bus 21
[ 7.779451] i2c i2c-2: Added multiplexed i2c bus 22
[ 7.779536] i2c i2c-2: Added multiplexed i2c bus 23
[ 7.779627] i2c i2c-2: Added multiplexed i2c bus 24
[ 7.779714] i2c i2c-2: Added multiplexed i2c bus 25
[ 7.779795] i2c i2c-2: Added multiplexed i2c bus 26
[ 7.779882] i2c i2c-2: Added multiplexed i2c bus 27
[ 7.779886] pca954x 2-0070: registered 8 multiplexed busses for I2C switch pca9548
[ 7.780404] i2c i2c-2: Added multiplexed i2c bus 28
[ 7.780498] i2c i2c-2: Added multiplexed i2c bus 29
[ 7.780582] i2c i2c-2: Added multiplexed i2c bus 30
[ 7.780659] i2c i2c-2: Added multiplexed i2c bus 31
[ 7.780738] i2c i2c-2: Added multiplexed i2c bus 32
[ 7.780818] i2c i2c-2: Added multiplexed i2c bus 33
[ 7.780899] i2c i2c-2: Added multiplexed i2c bus 34
[ 7.780987] i2c i2c-2: Added multiplexed i2c bus 35
[ 7.780991] pca954x 2-0071: registered 8 multiplexed busses for I2C switch pca9548
[ 7.781457] i2c i2c-3: Added multiplexed i2c bus 36
[ 7.781607] i2c i2c-3: Added multiplexed i2c bus 37
[ 7.781746] i2c i2c-3: Added multiplexed i2c bus 38
[ 7.781884] i2c i2c-3: Added multiplexed i2c bus 39
[ 7.782115] i2c i2c-3: Added multiplexed i2c bus 40
[ 7.782254] i2c i2c-3: Added multiplexed i2c bus 41
[ 7.782342] i2c i2c-3: Added multiplexed i2c bus 42
[ 7.782425] i2c i2c-3: Added multiplexed i2c bus 43
[ 7.782430] pca954x 3-0070: registered 8 multiplexed busses for I2C switch pca9548
[ 7.787468] bcm53xx 0x0000000001afc000:1e: found switch: BCM53134, rev 2
[ 7.854389] linux_kernel_bde: loading out-of-tree module taints kernel.
[ 7.928886] linux_kernel_bde: loading out-of-tree module taints kernel.
[ 7.946062] libphy: dsa slave smi: probed
[ 7.982346] linux-kernel-bde 0001:01:00.0: assign IRQ: got 87
[ 7.993888] _pci_probe: dev->device=0x8470, dev->vendor=0x14e4
[ 8.000180] bcm53xx 0x0000000001afc000:1e lan1 (uninitialized): PHY [dsa-0.0:00] driver [Generic PHY] (irq=POLL)
[ 8.008724] BDE determining MSI enable use_msi: 1
[ 8.014074] bcm53xx 0x0000000001afc000:1e lan2 (uninitialized): PHY [dsa-0.0:01] driver [Generic PHY] (irq=POLL)
[ 8.015192] BDE setting MSI, dev_type: 8101
[ 8.030502] linux-kernel-bde 0001:01:00.1: assign IRQ: got 87
[ 8.032986] bcm53xx 0x0000000001afc000:1e lan3 (uninitialized): PHY [dsa-0.0:02] driver [Generic PHY] (irq=POLL)
[ 8.075629] bcm53xx 0x0000000001afc000:1e lan4 (uninitialized): PHY [dsa-0.0:03] driver [Generic PHY] (irq=POLL)
[ 8.096628] bcm53xx 0x0000000001afc000:1e wan (uninitialized): validation of gmii with support 0000000,00000200,000062c0 and advertisement 0000000,00000000,000062c0 failed: -22
[ 8.113042] bcm53xx 0x0000000001afc000:1e wan (uninitialized): failed to connect to port 4: -22
[ 8.122214] bcm53xx 0x0000000001afc000:1e wan (uninitialized): error -22 setting up PHY for tree 0, switch 0, port 4
[ 8.140653] bcm53xx 0x0000000001afc000:1e: Using legacy PHYLIB callbacks. Please migrate to PHYLINK!
[ 8.154598] bcm53xx 0x0000000001afc000:1e: Configured port 8 for rgmii
[ 8.164499] DSA: tree 0 setup
[ 8.167825] Initializing module si5345, Version 1.0.
[ 8.179177] Device Part Number = 0x5345.
[ 8.185876] adt7470 19-002c: adt7470 chip found
[ 8.191052] nd_pmem namespace0.0: unable to guarantee persistence of writes
[ 8.200231] ltc4283 36-0015: Log Hot Swap Controller Fault Reg : 0x2
[ 8.209683] lm75 5-0048: hwmon6: sensor 'tmp100'
[ 8.211064] ucd9000 37-0073: probe: check
[ 8.214817] bmr4xx 38-000a: probe: check
[ 8.217872] pxe1610 40-0044: pmbus status word is 0x0
[ 8.218330] ucd9000 37-0073: Device ID UCD90320|3.0.0.3029|160915
[ 8.218334] ucd9000 37-0073: UCD Device FOUND: Configured(id->name), detected(mid->name) ucd90320
[ 8.220137] ucd9000 37-0073: ucd9000_probe1 num pages 28
[ 8.221183] pmbus 40-0045: pmbus status word is 0x841
[ 8.222266] bmr4xx 38-000a: Device ID BMR4582011002
[ 8.224889] Die Revision = 5, Device Grade = 1, Device Revision = 3.
[ 8.226359] lm75 12-0048: hwmon10: sensor 'lm75'
[ 8.227317] ucd9000 37-0073: Set cmds to UCD90320: mid->name ucd90320
[ 8.230185] lm75 12-0049: hwmon11: sensor 'lm75'
[ 8.233904] lm75 12-004b: hwmon12: sensor 'lm75'
[ 8.247965] bmr4xx 38-000a: BMR Power Cycle Counter: 0x0187
[ 8.250351] si5345 initialization complete.
[ 8.256675] ucd9000 37-0073: pmbus status word is 0x1801
[ 8.256768] lm75 13-004a: hwmon13: sensor 'lm75'
[ 8.259412] lm75 13-004c: hwmon14: sensor 'lm75'
[ 8.262988] rtc-pcf2127-i2c 14-0053: clear PWRMNG to enable RTC battery switch.
[ 8.264050] bmr4xx 38-000a: BMR Snapshot Capture
[ 8.266561] rtc-pcf2127-i2c 14-0053: RTC ctrl3:0
[ 8.270412] lm75 13-004d: hwmon15: sensor 'lm75'
[ 8.273838] rtc-pcf2127-i2c 14-0053: oscillator stop detected, date/time is not reliable
[ 8.273976] rtc-pcf2127-i2c 14-0053: registered as rtc0
[ 8.275088] bmr4xx 38-000a: READ_VIN_OLD : FFFF
[ 8.275093] bmr4xx 38-000a: READ_VOUT_OLD : FFFF
[ 8.279354] rtc-pcf2127-i2c 14-0053: oscillator stop detected, date/time is not reliable
[ 8.279358] rtc-pcf2127-i2c 14-0053: hctosys: unable to read the hardware clock
[ 8.288070] lm75 19-0048: hwmon16: sensor 'lm75'
[ 8.289896] bmr4xx 38-000a: READ_IOUT_OLD : FFFF
[ 8.289899] bmr4xx 38-000a: READ_DUTY_CYCLE_OLD : FFFF
[ 8.289903] bmr4xx 38-000a: READ_VIN : FFFF
[ 8.388856] bmr4xx 38-000a: READ_VOUT : FFFF
[ 8.393994] bmr4xx 38-000a: READ_IOUT : FFFF
[ 8.399131] bmr4xx 38-000a: READ_TEMPERATURE_1 : FFFF
[ 8.401007] pmbus 40-0045: exponent on page 0 is -8
[ 8.404268] bmr4xx 38-000a: READ_TEMPERATURE_2 : FFFF
[ 8.404272] bmr4xx 38-000a: Time in operation : FFFF
[ 8.419416] bmr4xx 38-000a: STATUS_WORD : FFFF
[ 8.424554] bmr4xx 38-000a: STATUS_BYTE : FF
[ 8.429517] bmr4xx 38-000a: STATUS_VOUT : FF
[ 8.434480] bmr4xx 38-000a: STATUS_IOUT : FF
[ 8.439444] bmr4xx 38-000a: STATUS_INPUT : FF
[ 8.444408] bmr4xx 38-000a: STATUS_TEMPERATURE : FF
[ 8.449372] bmr4xx 38-000a: STATUS_CML : FF
[ 8.454335] bmr4xx 38-000a: STATUS_OTHER : FF
[ 8.459298] bmr4xx 38-000a: STATUS_MFR_SPECIFIC : FF
[ 8.464261] bmr4xx 38-000a: SNAPSHOT cycles : FFFF
[ 8.469397] bmr4xx 38-000a: BMR Device FOUND: detected(mid->name) bmr458
[ 8.479825] bmr4xx 38-000a: bmr458 BMR status word : 0x0
[ 8.485165] bmr4xx 38-000a: Set cmds to BMR458: mid->name bmr458
[ 8.495157] bmr4xx 38-000a: pmbus status word is 0x0
[ 8.524989] bmr4xx 38-000a: exponent on page 0 is -11
[ 8.573769] ucd9000 37-0073: exponent on page 0 is -12
[ 8.671351] ucd9000 37-0073: exponent on page 1 is -14
[ 8.700730] ucd9000 37-0073: exponent on page 2 is -13
[ 8.831196] ucd9000 37-0073: exponent on page 3 is -12
[ 8.895454] ucd9000 37-0073: exponent on page 4 is -12
[ 8.925637] ucd9000 37-0073: exponent on page 5 is -13
[ 8.990712] ucd9000 37-0073: exponent on page 6 is -12
[ 9.020555] ucd9000 37-0073: exponent on page 7 is -14
[ 9.057376] pmbus 40-0046: pmbus status word is 0x0
[ 9.086612] ucd9000 37-0073: exponent on page 8 is -12
[ 9.111274] ucd9000 37-0073: exponent on page 9 is -14
[ 9.134788] ucd9000 37-0073: exponent on page 10 is -13
[ 9.158587] ucd9000 37-0073: exponent on page 11 is -14
[ 9.183064] ucd9000 37-0073: exponent on page 12 is -14
[ 9.207089] ucd9000 37-0073: exponent on page 13 is -14
[ 9.209765] pmbus 40-0046: exponent on page 0 is -8
[ 9.234275] ucd9000 37-0073: exponent on page 14 is -13
[ 9.256938] ucd9000 37-0073: exponent on page 15 is -14
[ 9.282235] ucd9000 37-0073: exponent on page 16 is -14
[ 9.305735] ucd9000 37-0073: exponent on page 17 is -13
[ 9.330116] ucd9000 37-0073: exponent on page 18 is -14
[ 9.354541] ucd9000 37-0073: exponent on page 19 is -14
[ 9.378654] ucd9000 37-0073: exponent on page 20 is -13
[ 9.400560] ucd9000 37-0073: exponent on page 21 is -14
[ 9.418338] ucd9000 37-0073: exponent on page 22 is -15
[ 9.436042] ucd9000 37-0073: exponent on page 23 is -14
[ 9.448446] ucd9000 37-0073: exponent on page 24 is -12
[ 9.460525] ucd9000 37-0073: exponent on page 25 is -12
[ 9.472609] ucd9000 37-0073: exponent on page 26 is -12
[ 9.484692] ucd9000 37-0073: exponent on page 27 is -12
[ 10.368368] ucd9000 37-0073: ucd9000_probe2 page 28
[ 10.449099] clx_shr_irq: no symbol version for pf_free
[ 10.454441] csi_init : Inserted
[ 10.474796] spi-nor spi1.2: First JEDEC id read failed; Attempting second read
[ 10.482111] spi-nor spi1.2: mx25l12805d (16384 Kbytes)
[ 10.487287] 2 fixed-partitions partitions found on MTD device spi1.2
[ 10.493648] Creating 2 MTD partitions on "spi1.2":
[ 10.498446] 0x000000000000-0x000000400000 : "SysFPGA-factory"
[ 10.507844] 0x000000400000-0x000000800000 : "SysFPGA-upgradable"
[ 10.519923] spi-blackburn 60000100.quadspi: bus 1 base (____ptrval____)
sysctl: cannot stat /proc/sys/kernel/panic_on_unrecovered_nmi: No such file or directory
[ 10.604345] rtc-pcf2127-i2c 14-0053: oscillator stop detected, date/time is not reliable
hwclock: RTC_RD_TIME: Invalid argument
Fri Mar 9 12:34:56 UTC 2018
mkdir: created directory '/var/core'
INIT: Entering runlevel: 1
2018-03-09T12:34:56.436335760+0000 UTC running [/etc/init.d/rc 1]
2018-03-09T12:34:56.439835080+0000 UTC running [stty onlcr 0>&1]
2018-03-09T12:34:56.453819960+0000 UTC [stty onlcr 0>&1] done
Skipping inithacks due to /FLASH/persist/inithacks/SKIP
Running pre-init scripts... DONE
starting rsyslogd ... done
Fri Mar 9 12:34:56 UTC 2018 === nvpd-build-init ====================
Fri Mar 9 12:34:56 UTC 2018 check_for_new_hw
MB_BID_ACCESS: i2c; MB_BID_LOC: 0-0052
Check for HW Changes
No HW Change
Fri Mar 9 12:35:00 UTC 2018 rm_schema_cache
Fri Mar 9 12:35:00 UTC 2018 new_nvpd_product
mkdir: created directory '/etc/schema'
/tmp/bpid_mark_root/backplane_id.xml doesn't exist
/tmp/bpid_mark_root/backplane_id.xml doesn't exist
2
Found feature-components.conf
03-09-2018 12:35:08.022279 engnum_builder: ../../git/src/engnum_builder.c.594: NODE Not found with xpath //bids/bid[equipment_type='00001014'][hw_compatibility_number='00000000']/serial_number
03-09-2018 12:35:08.022393 engnum_builder: ../../git/src/engnum_builder.c.539: Failed to find element in 'backplane'
03-09-2018 12:35:08.023835 engnum_builder: ../../git/src/engnum_builder.c.594: NODE Not found with xpath //bids/bid[equipment_type='3256'][hw_compatibility_number='0']/ethernet_start_mac
03-09-2018 12:35:08.023921 engnum_builder: ../../git/src/engnum_builder.c.539: Failed to find element in 'base'
03-09-2018 12:35:08.025342 engnum_builder: ../../git/src/engnum_builder.c.594: NODE Not found with xpath //bids/bid[equipment_type='00001014'][hw_compatibility_number='00000000']/ethernet_start_mac
03-09-2018 12:35:08.025425 engnum_builder: ../../git/src/engnum_builder.c.539: Failed to find element in 'backplane'
03-09-2018 12:35:08.028302 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028401 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028515 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028602 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028687 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028771 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028855 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.028939 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029023 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029107 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029191 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029273 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029366 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node [ 22.854535] random: crng init done
start_mac
03-09-2018 12:35:08.029455 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029539 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029624 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029706 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029789 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029871 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.029955 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030037 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030119 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030204 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030287 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030369 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030458 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030542 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030624 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030706 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030788 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030869 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.030950 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031032 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031114 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031195 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031276 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031358 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031444 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031526 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031607 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031689 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031770 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031851 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.031933 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032014 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032096 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032178 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032260 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032341 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032421 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032524 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032606 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032687 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032768 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032848 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.032926 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033005 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033086 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033164 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033243 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033321 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033401 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
03-09-2018 12:35:08.033501 engnum_builder: ../../git/src/engnum_builder.c.731: Start MAC not found at node start_mac
Fri Mar 9 12:35:08 UTC 2018 system_type: E7-2 codename: E7-2-XG1601
Fri Mar 9 12:35:08 UTC 2018 got card_type: controller from NVPD
Fri Mar 9 12:35:08 UTC 2018 run yang_platform_determination.py
sys_sn E7-2
platformDir /etc/platform/ and /etc/platform/E7-2
sys_sn /etc/confd/
copying files from /etc/E7-2/confd/ to /etc/confd/
copying files from /etc/E7-2/yang/ to /etc/yang/
copying files from /etc/E7-2/confd/yang/ to /etc/confd/yang/
copying files from /etc/E7-2/pyang-proc-schema/ to /etc/pyang-proc-schema/
copying files from /etc/E7-2/cnvt_config/ to /etc/cnvt_config/
Fri Mar 9 12:35:09 UTC 2018 run yang_platform_determination.py done
Fri Mar 9 12:35:09 UTC 2018 copy_config_files
Fri Mar 9 12:35:09 UTC 2018 Using: factory-config.e7-2.xml for factory-config
Fri Mar 9 12:35:09 UTC 2018 remove_unused_apps
Fri Mar 9 12:35:09 UTC 2018 Removing init scripts of unused apps ...
Fri Mar 9 12:35:10 UTC 2018 done
Fri Mar 9 12:35:10 UTC 2018
Starting bootInit: [ 24.879316] squashfs: Unknown parameter 'dax'
[ 24.883932] fuseblk: Unknown parameter 'dax'
[ 24.929516] EXT4-fs (pmem0): DAX enabled. Warning: EXPERIMENTAL, use at your own risk
[ 24.937371] EXT4-fs (pmem0): DAX unsupported by block device.
mount: /mnt/pram1: wrong fs type, bad option, bad superblock on /dev/pmem0, missing codepage or helper program, or other error.
[ 25.013105] ramoops: using module parameters
[ 25.017969] pstore: Using crash dump compression: deflate
[ 25.023389] printk: console [ramoops-1] enabled
[ 25.028296] pstore: Registered ramoops as persistent store backend
[ 25.034496] ramoops: using 0x20000@0xd0800000, ecc: 0
tar: varlog/bootInit.log: time stamp 2018-03-09 12:46:41 is 689.95254268 s in the future
tar: varlog/rotate_boot_dir.log: time stamp 2018-03-09 12:37:12 is 120.95237776 s in the future
tar: varlog/hotswap_path_fixup.log: time stamp 2018-03-09 12:37:13 is 121.95227064 s in the future
tar: varlog/confd_config_fixup.log: time stamp 2018-03-09 12:37:04 is 112.94943532 s in the future
tar: varlog/bid_pre_builder.log: time stamp 2018-03-09 12:37:11 is 119.94916732 s in the future
tar: varlog/sa_startup/vmstat.log: time stamp 2018-03-09 12:37:07 is 115.94904916 s in the future
tar: varlog/sa_startup/grabStartupData.log: time stamp 2018-03-09 12:37:04 is 112.94897664 s in the future
tar: varlog/sa_startup/par20180309: time stamp 2018-03-09 12:37:04 is 112.94890544 s in the future
tar: varlog/sa_startup: time stamp 2018-03-09 12:37:04 is 112.948848 s in the future
tar: varlog/login.log: time stamp 2018-03-09 12:37:35 is 143.94874488 s in the future
tar: varlog/opentftpd.log: time stamp 2018-03-09 12:36:22 is 70.94865872 s in the future
tar: varlog/rsyslogd.log: time stamp 2018-03-09 12:37:12 is 120.94858736 s in the future
tar: varlog/bid_builder.log: time stamp 2018-03-09 12:37:04 is 112.94849632 s in the future
tar: varlog/messages: time stamp 2018-03-09 12:46:38 is 686.9484216 s in the future
tar: varlog/upgrader.log: time stamp 2018-03-09 12:37:14 is 122.948351 s in the future
tar: varlog/img.log: time stamp 2018-03-09 12:37:44 is 152.94826856 s in the future
tar: varlog/wtmp: time stamp 2018-03-09 12:46:41 is 689.94763316 s in the future
tar: varlog/lastlog: time stamp 2018-03-09 12:37:35 is 143.947418 s in the future
tar: varlog/chassismgrd.log: time stamp 2018-03-09 12:37:10 is 118.9472492 s in the future
tar: varlog/restart_rsyslog.log: time stamp 2018-03-09 12:37:11 is 119.94717304 s in the future
tar: varlog/kernel: time stamp 2018-03-09 12:46:40 is 688.94335784 s in the future
tar: varlog/externalevents: time stamp 2018-03-09 12:37:11 is 119.94307048 s in the future
tar: varlog/imessages: time stamp 2018-03-09 12:37:11 is 119.94283856 s in the future
tar: varlog/nvpd-builder-init.log: time stamp 2018-03-09 12:37:04 is 112.94265612 s in the future
tar: varlog/externalalarms: time stamp 2018-03-09 12:37:11 is 119.94245428 s in the future
tar: varlog: time stamp 2018-03-09 12:37:44 is 152.94228836 s in the future
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/removed_apps.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/bootInit.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/rotate_boot_dir.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/rsyncd.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/confd_config_fixup.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/stderr/chassismgrd_err.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/bid_pre_builder.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/nvpd_parser.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/sa_startup/vmstat.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/sa_startup/grabStartupData.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/sa_startup/par20240129': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/rsyslogd.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/boot~': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/bid_builder.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/dmesg': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/wtmp': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/dsa_setup.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/chassis_channel_script.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/boot': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/lastlog': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/chassismgrd.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/restart_rsyslog.log': No such file or directory
fsync: can't open '/FLASH/persist/logs/boot-000123/varlog/kernel': No such file or directory
cp: cannot stat '/var/lilog/.': No such file or directory
tar: boot-000000/pram1/system/alarms/externalalarms.tar.xz: time stamp 2018-03-09 16:00:32 is 12319.1006766 s in the future
tar: boot-000000/pram1/system/alarms: time stamp 2018-03-09 16:00:32 is 12319.10053832 s in the future
tar: boot-000000/pram1/system/events/externalevents.tar.xz: time stamp 2018-03-09 16:00:32 is 12319.10034 s in the future
tar: boot-000000/pram1/system/events: time stamp 2018-03-09 16:00:32 is 12319.10017512 s in the future
tar: boot-000000/pram1/system: time stamp 2018-03-09 15:59:51 is 12278.10001204 s in the future
tar: boot-000000/pram1: time stamp 2024-01-29 16:36:30 is 185947277.09983464 s in the future
tar: boot-000000: time stamp 2024-01-29 16:36:30 is 185947277.099663 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.6: time stamp 2018-03-12 05:15:50 is 232837.09680292 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.33: time stamp 2018-03-11 13:46:47 is 177094.09328972 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.19: time stamp 2018-03-11 21:38:40 is 205407.09044044 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.28: time stamp 2018-03-11 16:29:58 is 186885.08769492 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.35: time stamp 2018-03-11 12:42:56 is 173263.08499556 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.41: time stamp 2018-03-11 09:36:34 is 162081.08219412 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.12: time stamp 2018-03-12 01:44:49 is 220176.0795204 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.34: time stamp 2018-03-11 13:14:43 is 175170.07667752 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.49: time stamp 2018-03-11 05:41:31 is 147978.07398428 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.15: time stamp 2018-03-11 23:59:36 is 213863.07082412 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.39: time stamp 2018-03-11 10:37:42 is 165749.0679796 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.50: time stamp 2018-03-11 05:13:14 is 146281.06527972 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.37: time stamp 2018-03-11 11:39:55 is 169482.06260888 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.27: time stamp 2018-03-11 17:03:26 is 188893.0598702 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.8: time stamp 2018-03-12 04:05:34 is 228621.0572436 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.10: time stamp 2018-03-12 02:55:27 is 224414.05445476 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.20: time stamp 2018-03-11 21:03:37 is 203304.051399 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.47: time stamp 2018-03-11 06:38:54 is 151421.04868632 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.22: time stamp 2018-03-11 19:54:03 is 199130.04602288 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.11: time stamp 2018-03-12 02:20:01 is 222288.04339776 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.17: time stamp 2018-03-11 22:49:10 is 209637.04075588 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.45: time stamp 2018-03-11 07:37:09 is 154916.03807608 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.14: time stamp 2018-03-12 00:34:46 is 215973.03541504 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.25: time stamp 2018-03-11 18:10:49 is 192936.0327198 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.30: time stamp 2018-03-11 15:23:51 is 182918.02985368 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.16: time stamp 2018-03-11 23:24:34 is 211761.02691656 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.5: time stamp 2018-03-12 05:50:54 is 234941.02404244 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.tar.xz: time stamp 2018-03-10 20:34:54 is 115181.02377536 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.3: time stamp 2018-03-12 07:01:03 is 239150.02115764 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.43: time stamp 2018-03-11 08:36:30 is 158477.01831776 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.13: time stamp 2018-03-12 01:09:44 is 218071.01551588 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.23: time stamp 2018-03-11 19:19:20 is 197047.01285864 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.42: time stamp 2018-03-11 09:06:24 is 160271.0102022 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.29: time stamp 2018-03-11 15:56:47 is 184894.00749824 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.31: time stamp 2018-03-11 14:51:07 is 180954.00467596 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.38: time stamp 2018-03-11 11:08:40 is 167607.00196688 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.32: time stamp 2018-03-11 14:18:52 is 179018.99929224 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.48: time stamp 2018-03-11 06:10:07 is 149693.99668332 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.7: time stamp 2018-03-12 04:40:46 is 230732.99397636 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.40: time stamp 2018-03-11 10:07:01 is 163907.9913146 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.1: time stamp 2018-03-12 08:11:32 is 243378.9886936 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.18: time stamp 2018-03-11 22:13:52 is 207518.98606044 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.46: time stamp 2018-03-11 07:07:55 is 153161.98333108 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.4: time stamp 2018-03-12 06:25:56 is 237042.98062732 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.26: time stamp 2018-03-11 17:37:04 is 190910.9779746 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.2: time stamp 2018-03-12 07:36:19 is 241265.97527464 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.44: time stamp 2018-03-11 08:06:36 is 156682.9724678 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.36: time stamp 2018-03-11 12:11:22 is 171368.96981656 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.24: time stamp 2018-03-11 18:45:09 is 194995.96713856 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.9: time stamp 2018-03-12 03:30:31 is 226517.96445992 s in the future
tar: boot-000001/pram1/system/alarms/externalalarms.21: time stamp 2018-03-11 20:28:41 is 201207.96169512 s in the future
tar: boot-000001/pram1/system/alarms: time stamp 2018-03-12 08:11:32 is 243378.96159276 s in the future
tar: boot-000001/pram1/system/events/externalevents.8: time stamp 2018-03-12 04:05:41 is 228627.95975596 s in the future
tar: boot-000001/pram1/system/events/externalevents.36: time stamp 2018-03-11 12:11:28 is 171374.95775988 s in the future
tar: boot-000001/pram1/system/events/externalevents.29: time stamp 2018-03-11 15:56:54 is 184900.95588456 s in the future
tar: boot-000001/pram1/system/events/externalevents.22: time stamp 2018-03-11 19:54:10 is 199136.9539184 s in the future
tar: boot-000001/pram1/system/events/externalevents.25: time stamp 2018-03-11 18:10:55 is 192941.95204788 s in the future
tar: boot-000001/pram1/system/events/externalevents.31: time stamp 2018-03-11 14:51:13 is 180959.95006444 s in the future
tar: boot-000001/pram1/system/events/externalevents.40: time stamp 2018-03-11 10:07:07 is 163913.94816936 s in the future
tar: boot-000001/pram1/system/events/externalevents.43: time stamp 2018-03-11 08:36:36 is 158482.94631976 s in the future
tar: boot-000001/pram1/system/events/externalevents.6: time stamp 2018-03-12 05:15:57 is 232843.94433548 s in the future
tar: boot-000001/pram1/system/events/externalevents.30: time stamp 2018-03-11 15:23:57 is 182923.94245092 s in the future
tar: boot-000001/pram1/system/events/externalevents.50: time stamp 2018-03-11 05:13:20 is 146286.9405142 s in the future
tar: boot-000001/pram1/system/events/externalevents.35: time stamp 2018-03-11 12:43:03 is 173269.93860844 s in the future
tar: boot-000001/pram1/system/events/externalevents.39: time stamp 2018-03-11 10:37:48 is 165754.93658796 s in the future
tar: boot-000001/pram1/system/events/externalevents.46: time stamp 2018-03-11 07:08:01 is 153167.9347208 s in the future
tar: boot-000001/pram1/system/events/externalevents.33: time stamp 2018-03-11 13:46:53 is 177099.93273872 s in the future
tar: boot-000001/pram1/system/events/externalevents.37: time stamp 2018-03-11 11:40:01 is 169487.93088096 s in the future
tar: boot-000001/pram1/system/events/externalevents.34: time stamp 2018-03-11 13:14:51 is 175177.92895376 s in the future
tar: boot-000001/pram1/system/events/externalevents.14: time stamp 2018-03-12 00:34:53 is 215979.9270896 s in the future
tar: boot-000001/pram1/system/events/externalevents.47: time stamp 2018-03-11 06:39:00 is 151426.92513548 s in the future
tar: boot-000001/pram1/system/events/externalevents.9: time stamp 2018-03-12 03:30:38 is 226524.92317828 s in the future
tar: boot-000001/pram1/system/events/externalevents.32: time stamp 2018-03-11 14:18:59 is 179025.92126972 s in the future
tar: boot-000001/pram1/system/events/externalevents.4: time stamp 2018-03-12 06:26:04 is 237050.91934104 s in the future
tar: boot-000001/pram1/system/events/externalevents.17: time stamp 2018-03-11 22:49:18 is 209644.91747376 s in the future
tar: boot-000001/pram1/system/events/externalevents.5: time stamp 2018-03-12 05:51:01 is 234947.91552612 s in the future
tar: boot-000001/pram1/system/events/externalevents.48: time stamp 2018-03-11 06:10:13 is 149699.9136488 s in the future
tar: boot-000001/pram1/system/events/externalevents.19: time stamp 2018-03-11 21:38:47 is 205413.9116422 s in the future
tar: boot-000001/pram1/system/events/externalevents.24: time stamp 2018-03-11 18:45:15 is 195001.9097792 s in the future
tar: boot-000001/pram1/system/events/externalevents.20: time stamp 2018-03-11 21:03:44 is 203310.90783796 s in the future
tar: boot-000001/pram1/system/events/externalevents.45: time stamp 2018-03-11 07:37:15 is 154921.90597808 s in the future
tar: boot-000001/pram1/system/events/externalevents.2: time stamp 2018-03-12 07:36:26 is 241272.90405144 s in the future
tar: boot-000001/pram1/system/events/externalevents.16: time stamp 2018-03-11 23:24:41 is 211767.90214896 s in the future
tar: boot-000001/pram1/system/events/externalevents.42: time stamp 2018-03-11 09:06:31 is 160277.90021948 s in the future
tar: boot-000001/pram1/system/events/externalevents.44: time stamp 2018-03-11 08:06:43 is 156689.89822836 s in the future
tar: boot-000001/pram1/system/events/externalevents.13: time stamp 2018-03-12 01:09:51 is 218077.89633748 s in the future
tar: boot-000001/pram1/system/events/externalevents.23: time stamp 2018-03-11 19:19:27 is 197053.894411 s in the future
tar: boot-000001/pram1/system/events/externalevents.10: time stamp 2018-03-12 02:55:34 is 224420.8925168 s in the future
tar: boot-000001/pram1/system/events/externalevents.49: time stamp 2018-03-11 05:41:37 is 147983.8905966 s in the future
tar: boot-000001/pram1/system/events/externalevents.12: time stamp 2018-03-12 01:44:56 is 220182.88868408 s in the future
tar: boot-000001/pram1/system/events/externalevents.15: time stamp 2018-03-11 23:59:43 is 213869.88668276 s in the future
tar: boot-000001/pram1/system/events/externalevents.41: time stamp 2018-03-11 09:36:41 is 162087.88480388 s in the future
tar: boot-000001/pram1/system/events/externalevents.21: time stamp 2018-03-11 20:28:48 is 201214.88288468 s in the future
tar: boot-000001/pram1/system/events/externalevents.1: time stamp 2018-03-12 08:11:40 is 243386.88100556 s in the future
tar: boot-000001/pram1/system/events/externalevents.27: time stamp 2018-03-11 17:03:33 is 188899.8790454 s in the future
tar: boot-000001/pram1/system/events/externalevents.3: time stamp 2018-03-12 07:01:11 is 239157.87713688 s in the future
tar: boot-000001/pram1/system/events/externalevents.38: time stamp 2018-03-11 11:08:46 is 167612.87519244 s in the future
tar: boot-000001/pram1/system/events/externalevents.26: time stamp 2018-03-11 17:37:11 is 190917.87308292 s in the future
tar: boot-000001/pram1/system/events/externalevents.11: time stamp 2018-03-12 02:20:09 is 222295.87119416 s in the future
tar: boot-000001/pram1/system/events/externalevents.28: time stamp 2018-03-11 16:30:05 is 186891.8691712 s in the future
tar: boot-000001/pram1/system/events/externalevents.tar.xz: time stamp 2018-03-10 20:34:54 is 115180.86906204 s in the future
tar: boot-000001/pram1/system/events/externalevents.7: time stamp 2018-03-12 04:40:53 is 230739.86726448 s in the future
tar: boot-000001/pram1/system/events/externalevents.18: time stamp 2018-03-11 22:13:59 is 207525.8653366 s in the future
tar: boot-000001/pram1/system/events: time stamp 2018-03-12 08:11:40 is 243386.86526284 s in the future
tar: boot-000001/pram1/system/boottime: time stamp 2018-03-09 16:00:32 is 12318.8651566 s in the future
tar: boot-000001/pram1/system: time stamp 2018-03-09 16:00:32 is 12318.86509432 s in the future
tar: boot-000001/pram1: time stamp 2018-03-09 16:00:31 is 12317.86503452 s in the future
tar: boot-000001: time stamp 2018-03-09 16:00:31 is 12317.86497492 s in the future
tar: bootCnt: time stamp 2018-03-10 20:34:54 is 115180.86487564 s in the future
tar: boot_current: time stamp 2018-03-10 20:34:54 is 115180.86478716 s in the future
tar: boot_previous: time stamp 2018-03-09 16:00:31 is 12317.86468936 s in the future
0x00
2018-03-09T12:35:13.291736160+0000 UTC /usr/bin/scripts/bearer_watchdog.sh: Set bearer wdt timeout to be 2.5 minutes
done
No kdump kernel image found.
Starting /etc/rc1.d/S10init_hw_odin:
Link /usr/sbin/plmgrd --> /usr/sbin/plmgrd_e7
## lan1 Phy 0 ##
write: PhyAddr 0x0 RegAddr 0x0 RegVal 0x2100
Initializing dpaa ethernet
done
Starting logproxyd: done
Starting watchdog daemon...done
SKIP PMON UPGRADE CHECK
Running post-init scripts... done
Scheduling bootcount_whacker.sh ...Running post-init script rl_led.sh done
odin login: root
Password:
root@odin:~# uname -a
Linux odin 5.10.52+ga11753a89ec6 #1 SMP Fri Jan 12 02:49:41 UTC 2024 aarch64 aarch64 aarch64 GNU/Linux