U-Boot 2016.012.0+ga9b437f (Dec 18 2020 - 11:44:30 +0530) CPU0: P5040, Version: 2.1, (0x82040021) Core: e5500, Version: 1.2, (0x80240012) Clock Configuration: CPU0:2000 MHz, CPU1:2000 MHz, CPU2:2000 MHz, CPU3:2000 MHz, CCB:800 MHz, DDR:800 MHz (1600 MT/s data rate) (Asynchronous), LBC:100 MHz FMAN1: 600 MHz FMAN2: 600 MHz QMAN: 400 MHz PME: 400 MHz L1: D-cache 32 KiB enabled I-cache 32 KiB enabled Reset Configuration Word (RCW): 00000000: 90e00000 00000000 a8a89800 00440000 00000010: 189f8fff 00303000 fe800000 61000000 00000020: 00000000 00000000 00000000 c8da8000 00000030: a0000000 00000000 00000000 00000000 I2C: ready Board: P5040DS, SERDES Reference Clocks: Should be Bank1=100Mhz Bank2=100Mhz Bank3=125Mhz SPI: ready DRAM: Initializing....using SPD Detected UDIMM 18KSF1G72HZ-1G6P1 There is no rank on CS0 for controller 1. Not enough bank(chip-select) for CS0+CS1 on controller 1, interleaving disabled! 6 GiB left unmapped Testing 0x00000000 - 0x7fffffff Testing 0x80000000 - 0xffffffff Testing 0x100000000 - 0x17fffffff Testing 0x180000000 - 0x1ffffffff Remap DDR 6 GiB left unmapped 8 GiB (DDR3, 64-bit, CL=11, ECC on) DDR Chip-Select Interleaving Mode: CS0+CS1 POST memory PASSED Flash: 256 MiB L2: 512 KiB enabled Corenet Platform Cache: 2 MiB enabled NAND: fsl_elbc_nand: address did not match any chip selects 0 MiB MMC: FSL_SDHC: 0 *** Warning - bad CRC, using default environment EEPROM: Read failed. PCIe1: disabled PCIe2: disabled PCIe3: disabled In: serial Out: serial Err: serial Warning: SERDES bank 2 expects reference clock 161.1328123MHz, but actual is 100MHz Net: Initializing Fman Fman1: DTSEC5 set to unknown interface 13 Fman1: Uploading microcode version 106.1.18 Could not get PHY for SUPER_HYDRA_FM1_SGMII_MDIO: addr 5 Failed to connect Fman2: Uploading microcode version 106.1.18 Could not get PHY for SUPER_HYDRA_FM2_SGMII_MDIO: addr 0 Failed to connect Could not get PHY for SUPER_HYDRA_FM2_TGEC_MDIO: addr 0 Failed to connect FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1 Hit any key to stop autoboot: 0 => =>