l'u-boot : U-Boot 2020.04-g2f62d479 (Nov 23 2021 - 16:48:44 +0100) CPU: i.MX6ULL rev1.1 792 MHz (running at 396 MHz) CPU: Industrial temperature grade (-40C to 105C) at 48C Reset cause: POR Model: Conduent Ticket Validator VAL900 Board: VAL900_IMX6 I2C: ready DRAM: 512 MiB MMC: FSL_SDHC: 0, FSL_SDHC: 1 Fail to setup video link In: serial Out: serial Err: serial PSN: 000001 LOGO: 82145400, version 01.01 patch 003 Net: No ethernet found. Normal Boot Hit any key to stop autoboot: 0 setenv fdtfile imx6ull-uce050-val.dtb trying to boot from emmc... switch to partitions #0, OK mmc1(part 0) is current device SD/MMC/EMMC found on device 1 Checking in boot partition for: /uEnv.txt ... 29 bytes read in 10 ms (2 KiB/s) Loaded environment from /uEnv.txt Checking if uenvcmd is set ... Running uenvcmd ... try hardware partition for booting ... Checking for: /boot/uEnv.txt ... 52 bytes read in 15 ms (2.9 KiB/s) Loaded environment from /boot/uEnv.txt Using: dtb=imx6ull-uce050-val.dtb ... Checking if uname_r is set in /boot/uEnv.txt... Running uname_boot ... Using: mmcroot=PARTUUID=230246c8-06b7-49a4-ae10-dd5805a413d6 ro ... loading /boot/vmlinuz-5.4.70-armv7-x38 ... 7200624 bytes read in 179 ms (38.4 MiB/s) loading /boot/dtbs/imx6ull-uce050-val.dtb ... 38290 bytes read in 24 ms (1.5 MiB/s) debug: [console=ttymxc0,115200 root=PARTUUID=230246c8-06b7-49a4-ae10-dd5805a413d6 ro rootfstype=ext4 rootwait] ... debug: [bootz 0x80800000 - 0x83000000] ... Kernel image @ 0x80800000 [ 0x000000 - 0x6ddf70 ] ## Flattened Device Tree blob at 83000000 Booting using the fdt blob at 0x83000000 Using Device Tree in place at 83000000, end 8300c591 ft_system_setup for mx6 Starting kernel ...