[ 0.000000] Booting Linux on physical CPU 0xf00 [ 0.000000] Linux version 5.4.3 (jenkins@saturn) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #1 SMP Thu Apr 9 00:20:42 CST 2020 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=30c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: LS1021A TWR Board [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 64 MiB at 0x00000000ac000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.0 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.0 [ 0.000000] percpu: Embedded 21 pages/cpu s53324 r8192 d24500 u86016 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259840 [ 0.000000] Kernel command line: root=/dev/ram0 rw console=ttyS0,115200 cma=64M@0x0-0xb0000000 [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0xa72e0000-0xab2e0000] (64MB) [ 0.000000] Memory: 863700K/1048576K available (14336K kernel code, 1956K rwdata, 5692K rodata, 2048K init, 686K bss, 119340K reserved, 65536K cma-reserved, 262144K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=2. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] random: get_random_bytes called from start_kernel+0x330/0x4ec with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 12.50MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049cda, max_idle_ns: 440795202628 ns [ 0.000005] sched_clock: 56 bits at 12MHz, resolution 80ns, wraps every 4398046511080ns [ 0.000015] Switching to timer-based delay loop, resolution 80ns [ 0.001818] Console: colour dummy device 80x30 [ 0.001864] Calibrating delay loop (skipped), value calculated using timer frequency.. 25.00 BogoMIPS (lpj=125000) [ 0.001877] pid_max: default: 32768 minimum: 301 [ 0.002038] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.002054] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.002833] CPU: Testing write buffer coherency: ok [ 0.003203] CPU0: update cpu_capacity 1024 [ 0.003215] CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00 [ 0.003809] Setting up static identity map for 0x80400000 - 0x80400184 [ 0.004435] rcu: Hierarchical SRCU implementation. [ 0.005744] EFI services will not be available. [ 0.005940] smp: Bringing up secondary CPUs ... [ 0.006694] CPU1: update cpu_capacity 1024 [ 0.006701] CPU1: thread -1, cpu 1, socket 15, mpidr 80000f01 [ 0.006869] smp: Brought up 1 node, 2 CPUs [ 0.006887] SMP: Total of 2 processors activated (50.00 BogoMIPS). [ 0.006895] CPU: All CPU(s) started in HYP mode. [ 0.006901] CPU: Virtualization extensions available. [ 0.007462] devtmpfs: initialized [ 0.012608] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5 [ 0.012869] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.012889] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.015077] pinctrl core: initialized pinctrl subsystem [ 0.016614] DMI not present or invalid. [ 0.017106] NET: Registered protocol family 16 [ 0.020172] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.022256] cpuidle: using governor menu [ 0.022567] No ATAGs? [ 0.022664] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.022678] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.024641] Serial: AMBA PL011 UART driver [ 0.029680] Machine: LS1021A TWR Board [ 0.029691] SoC family: QorIQ LS1021A [ 0.029698] SoC ID: svr:0x87081110, Revision: 1.0 [ 0.080694] AT91: Could not find identification node [ 0.083159] iommu: Default domain type: Translated [ 0.083478] vgaarb: loaded [ 0.084340] SCSI subsystem initialized [ 0.084855] usbcore: registered new interface driver usbfs [ 0.084917] usbcore: registered new interface driver hub [ 0.084977] usbcore: registered new device driver usb [ 0.085709] imx-i2c 2180000.i2c: can't get pinctrl, bus recovery not supported [ 0.086230] i2c i2c-0: IMX I2C adapter registered [ 0.086282] i2c i2c-0: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers [ 0.086512] imx-i2c 2190000.i2c: can't get pinctrl, bus recovery not supported [ 0.086848] i2c i2c-1: IMX I2C adapter registered [ 0.086890] i2c i2c-1: using dma0chan18 (tx) and dma0chan19 (rx) for DMA transfers [ 0.087692] pps_core: LinuxPPS API ver. 1 registered [ 0.087701] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.087722] PTP clock support registered [ 0.087902] EDAC MC: Ver: 3.0.0 [ 0.089189] No BMan portals available! [ 0.089380] No QMan portals available! [ 0.089601] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree [ 0.089880] fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller [ 0.089933] fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks [ 0.091766] clocksource: Switched to clocksource arch_sys_counter [ 0.529188] thermal_sys: Registered thermal governor 'step_wise' [ 0.529654] NET: Registered protocol family 2 [ 0.530293] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) [ 0.530322] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) [ 0.530391] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.530490] TCP: Hash tables configured (established 8192 bind 8192) [ 0.530587] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.530635] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.530814] NET: Registered protocol family 1 [ 0.531378] RPC: Registered named UNIX socket transport module. [ 0.531390] RPC: Registered udp transport module. [ 0.531398] RPC: Registered tcp transport module. [ 0.531405] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.531420] PCI: CLS 0 bytes, default 64 [ 0.531941] Trying to unpack rootfs image as initramfs... [ 1.301542] Freeing initrd memory: 14768K [ 1.303095] kvm [1]: vgic interrupt IRQ16 [ 1.303199] kvm [1]: Hyp mode initialized successfully [ 1.304026] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available [ 1.304593] Bus freq driver module loaded [ 1.306058] Initialise system trusted keyrings [ 1.306309] workingset: timestamp_bits=14 max_order=18 bucket_order=4 [ 1.317163] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 1.317981] NFS: Registering the id_resolver key type [ 1.318014] Key type id_resolver registered [ 1.318023] Key type id_legacy registered [ 1.318064] ntfs: driver 2.1.32 [Flags: R/O]. [ 1.318629] fuse: init (API version 7.31) [ 1.354600] Key type asymmetric registered [ 1.354616] Asymmetric key parser 'x509' registered [ 1.354678] bounce: pool size: 64 pages [ 1.354736] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248) [ 1.354747] io scheduler mq-deadline registered [ 1.354756] io scheduler kyber registered [ 1.372472] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges: [ 1.372525] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -> 0x00000000 [ 1.372565] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -> 0x40000000 [ 1.372833] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00 [ 1.372850] pci_bus 0000:00: root bus resource [bus 00-ff] [ 1.372862] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 1.372875] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff]) [ 1.372913] pci 0000:00:00.0: [1957:0e0a] type 01 class 0x060400 [ 1.372965] pci 0000:00:00.0: reg 0x38: [mem 0x28000000-0x280007ff pref] [ 1.373050] pci 0000:00:00.0: supports D1 D2 [ 1.373062] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot [ 1.374316] PCI: bus0: Fast back to back transfers disabled [ 1.375365] PCI: bus1: Fast back to back transfers enabled [ 1.375410] pci 0000:00:00.0: BAR 6: assigned [mem 0x4040000000-0x40400007ff pref] [ 1.375427] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 1.375805] pcieport 0000:00:00.0: PME: Signaling with IRQ 47 [ 1.376206] pcieport 0000:00:00.0: AER: enabled with IRQ 48 [ 1.448978] Serial: 8250/16550 driver, 5 ports, IRQ sharing enabled [ 1.453651] printk: console [ttyS0] disabled [ 1.453737] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 34, base_baud = 9375000) is a 16550A [ 2.304207] printk: console [ttyS0] enabled [ 2.309716] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 34, base_baud = 9375000) is a 16550A [ 2.319286] SuperH (H)SCI(F) driver initialized [ 2.324769] msm_serial: driver initialized [ 2.329008] STMicroelectronics ASC driver initialized [ 2.335164] 2950000.serial: ttyLP0 at MMIO 0x2950000 (irq = 39, base_baud = 6250000) is a FSL_LPUART [ 2.344715] fsl-lpuart 2950000.serial: DMA tx channel request failed, operating without tx DMA [ 2.353323] fsl-lpuart 2950000.serial: DMA rx channel request failed, operating without rx DMA [ 2.362243] STM32 USART driver initialized [ 2.368732] imx sema4 driver is registered. [ 2.374751] panel-simple panel: panel supply power not found, using dummy regulator [ 2.391949] brd: module loaded [ 2.404988] loop: module loaded [ 2.411083] imx ahci driver is registered. [ 2.415858] ahci-qoriq 3200000.sata: 3200000.sata supply ahci not found, using dummy regulator [ 2.424585] ahci-qoriq 3200000.sata: 3200000.sata supply phy not found, using dummy regulator [ 2.433191] ahci-qoriq 3200000.sata: 3200000.sata supply target not found, using dummy regulator [ 2.442142] ahci-qoriq 3200000.sata: AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl platform mode [ 2.450975] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc [ 2.459830] ahci-qoriq 3200000.sata: port 0 is not capable of FBS [ 2.466947] scsi host0: ahci-qoriq [ 2.470759] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 28 [ 2.480879] physmap-flash 60000000.nor: physmap platform flash device: [mem 0x60000000-0x67ffffff] [ 2.489919] 60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e [ 2.499894] Amd/Fujitsu Extended Query Table at 0x0040 [ 2.505042] Amd/Fujitsu Extended Query version 1.3. [ 2.510070] number of CFI chips: 1 [ 2.527249] libphy: Fixed MDIO Bus: probed [ 2.532921] tun: Universal TUN/TAP device driver, 1.6 [ 2.538194] CAN device driver interface [ 2.542955] bgmac_bcma: Broadcom 47xx GBit MAC driver loaded [ 2.549615] libphy: Freescale PowerQUICC MII Bus: probed [ 2.573773] libphy: Freescale PowerQUICC MII Bus: probed [ 2.584790] fsl-gianfar soc:ethernet@2d10000: enabled errata workarounds, flags: 0x4 [ 2.603802] fsl-gianfar soc:ethernet@2d10000 eth0: mac: 00:00:00:00:00:00 [ 2.610559] fsl-gianfar soc:ethernet@2d10000 eth0: Running with NAPI enabled [ 2.617592] fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[0]: 256 [ 2.624964] fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[1]: 256 [ 2.632335] fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[0]: 256 [ 2.639694] fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[1]: 256 [ 2.647648] fsl-gianfar soc:ethernet@2d50000: enabled errata workarounds, flags: 0x4 [ 2.666550] fsl-gianfar soc:ethernet@2d50000 eth1: mac: 00:00:00:00:00:00 [ 2.673323] fsl-gianfar soc:ethernet@2d50000 eth1: Running with NAPI enabled [ 2.680337] fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[0]: 256 [ 2.687716] fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[1]: 256 [ 2.695087] fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[0]: 256 [ 2.702458] fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[1]: 256 [ 2.710376] fsl-gianfar soc:ethernet@2d90000: enabled errata workarounds, flags: 0x4 [ 2.729269] fsl-gianfar soc:ethernet@2d90000 eth2: mac: 00:00:00:00:00:00 [ 2.736042] fsl-gianfar soc:ethernet@2d90000 eth2: Running with NAPI enabled [ 2.743067] fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[0]: 256 [ 2.750425] fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[1]: 256 [ 2.757794] fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[0]: 256 [ 2.765164] fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[1]: 256 [ 2.772880] Freescale FM module, FMD API version 21.1.0 [ 2.778327] Freescale FM Ports module [ 2.781993] fsl_mac: fsl_mac: FSL FMan MAC API based driver [ 2.787718] fsl_dpa: FSL DPAA Ethernet driver [ 2.792206] fsl_advanced: FSL DPAA Advanced drivers: [ 2.797143] fsl_proxy: FSL DPAA Proxy initialization driver [ 2.802834] fsl_oh: FSL FMan Offline Parsing port driver [ 2.803243] ata1: SATA link down (SStatus 0 SControl 300) [ 2.808457] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k [ 2.819294] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 2.825259] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k [ 2.832198] igb: Copyright (c) 2007-2014 Intel Corporation. [ 2.841504] pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver [ 2.848932] usbcore: registered new interface driver pegasus [ 2.854621] usbcore: registered new interface driver asix [ 2.860023] usbcore: registered new interface driver ax88179_178a [ 2.866131] usbcore: registered new interface driver cdc_ether [ 2.871998] usbcore: registered new interface driver smsc75xx [ 2.877759] usbcore: registered new interface driver smsc95xx [ 2.883529] usbcore: registered new interface driver net1080 [ 2.889190] usbcore: registered new interface driver cdc_subset [ 2.895124] usbcore: registered new interface driver zaurus [ 2.900726] usbcore: registered new interface driver cdc_ncm [ 2.907065] dwc3 3100000.usb3: Failed to get clk 'ref': -2 [ 2.915604] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 2.922141] ehci-pci: EHCI PCI platform driver [ 2.926605] ehci-platform: EHCI generic platform driver [ 2.932052] ehci-orion: EHCI orion driver [ 2.936202] SPEAr-ehci: EHCI SPEAr driver [ 2.940326] ehci-st: EHCI STMicroelectronics driver [ 2.945342] ehci-exynos: EHCI EXYNOS driver [ 2.949638] ehci-atmel: EHCI Atmel driver [ 2.953776] tegra-ehci: Tegra EHCI driver [ 2.957909] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 2.964091] ohci-pci: OHCI PCI platform driver [ 2.968567] ohci-platform: OHCI generic platform driver [ 2.973953] SPEAr-ohci: OHCI SPEAr driver [ 2.978077] ohci-st: OHCI STMicroelectronics driver [ 2.983091] ohci-atmel: OHCI Atmel driver [ 2.987628] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.993140] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 3.001120] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66c hci version 0x100 quirks 0x0000000002010810 [ 3.010554] xhci-hcd xhci-hcd.0.auto: irq 46, io mem 0x03100000 [ 3.017665] hub 1-0:1.0: USB hub found [ 3.021442] hub 1-0:1.0: 1 port detected [ 3.025827] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 3.031295] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 3.038942] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed [ 3.046331] hub 2-0:1.0: USB hub found [ 3.050100] hub 2-0:1.0: 1 port detected [ 3.055723] usbcore: registered new interface driver usb-storage [ 3.066552] ftm-alarm 29d0000.timer0: registered as rtc1 [ 3.073912] i2c /dev entries driver [ 3.081929] pps pps0: new PPS source ptp0 [ 3.093014] imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0) [ 3.102387] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver [ 3.109724] sdhci: Secure Digital Host Controller Interface driver [ 3.115924] sdhci: Copyright(c) Pierre Ossman [ 3.122046] Synopsys Designware Multimedia Card Interface Driver [ 3.129299] sdhci-pltfm: SDHCI platform and OF driver helper [ 3.161911] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit [ 3.172970] ledtrig-cpu: registered to indicate activity on CPUs [ 3.180022] usbcore: registered new interface driver usbhid [ 3.185642] usbhid: USB HID core driver [ 3.191320] No fsl,qman node [ 3.194221] Freescale USDPAA process driver [ 3.198379] fsl-usdpaa: no region found [ 3.202210] Freescale USDPAA process IRQ driver [ 3.210177] drop_monitor: Initializing network drop monitor service [ 3.217059] IPVS: Registered protocols () [ 3.221126] IPVS: Connection hash table configured (size=4096, memory=32Kbytes) [ 3.228668] IPVS: ipvs loaded. [ 3.232026] Initializing XFRM netlink socket [ 3.237036] NET: Registered protocol family 10 [ 3.242761] Segment Routing with IPv6 [ 3.246653] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 3.253257] NET: Registered protocol family 17 [ 3.257700] NET: Registered protocol family 15 [ 3.262214] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 3.275135] can: controller area network core (rev 20170425 abi 9) [ 3.281352] NET: Registered protocol family 29 [ 3.285799] can: raw protocol (rev 20170425) [ 3.290046] can: broadcast manager protocol (rev 20170425 t) [ 3.295701] can: netlink gateway (rev 20190810) max_hops=1 [ 3.301356] 8021q: 802.1Q VLAN Support v1.8 [ 3.305879] Key type dns_resolver registered [ 3.310267] ThumbEE CPU extension supported. [ 3.314548] Registering SWP/SWPB emulation handler [ 3.319661] Loading compiled-in X.509 certificates [ 3.330004] hctosys: unable to open rtc device (rtc0)