#ifndef __LED_PERIPHERIES_H__ #define __LED_PERIPHERIES_H__ #include "clock_S32K1xx.h" #include "devassert.h" #include "device_registers.h" #include "lpspi_hw_access.h" #include "lpspi_master_driver.h" #include "lpspi_shared_function.h" #include "lpspi_slave_driver.h" #include "pins_gpio_hw_access.h" #include "pins_port_hw_access.h" #include "rtwtypes.h" #include "pins_driver.h" #include "osif.h" /******************************************************************************* * Definitions ******************************************************************************/ #define LED_INSTANCE_RED PTD #define LED_PIN_RED 15 #define LED_INSTANCE_GREEN PTD #define LED_PIN_GREEN 16 #define LED_INSTANCE_BLUE PTD #define LED_PIN_BLUE 0 #define PIN_INPUT 0 #define PIN_OUTPUT 1 #define PIN_LOW 0 #define PIN_HIGH 1 /******************************************************************************* * LED Initialization ******************************************************************************/ void led_init(); /******************************************************************************* * LED Turn Off ******************************************************************************/ void led_off(); /******************************************************************************* * LED Turn On ******************************************************************************/ void led_on(); /******************************************************************************* * Delay in amount of Milliseconds ******************************************************************************/ void delay_m(); #endif /*__LED_PERIPHERIES_H__*/ /******************************************************************************* * EOF; ******************************************************************************/