Connection from "127.0.0.1" via 127.0.0.1. Connection from port "58205" to 7224 Telnet server running on 127.0.0.1:51794 Copyright 2018 P&E Microcomputer Systems,Inc. Command Line :C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port¤ CMD>RE Initializing. Device IDCODE is $00000377 Device ID revision is $00000001 MPC5777C Device detected. Target has been RESET and is active. CMD>CM C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp Initializing. Device IDCODE is $00000377 Device ID revision is $00000001 MPC5777C Device detected. Initialized. ;version 1.04, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [5777C_8meg_highspeed] ;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed ;begin_cs device=$30800000, length=$00800000, ram=$00300000 Loading programming algorithm ... Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Verifying object file CRC-16 to device ranges ... block 00840400-00840617 ... Calculated CRC-16 does not match block. (File = $4082, Device = $B370) Current content of flash does not match application to be programmed CMD>EM Erasing. Module has been erased. CMD>PM Programming. Processing Object File Data ... . Programmed. CMD>VC Verifying object file CRC-16 to device ranges ... block 00840400-00840617 ... Ok. block 00850000-00850133 ... Ok. block 00851000-00851803 ... Ok. block 00851810-0085735B ... Ok. Checksum Verification Successful. (Cumulative CRC-16=$5EF2) CMD>RE Initializing. Device IDCODE is $00000377 Device ID revision is $00000001 MPC5777C Device detected. Target has been RESET and is active. Device IDCODE is $00000377 Device ID revision is $00000001 Starting reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\s32e200_mpc5777c.mac) ... REM This script is compatible with MPC5777C devices. REM Clean GPRs to remove residual data after using algorithm REM Setup MMU for for Periph B Modules REM Base address = $FFE0_0000 REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access Once Status Register Result = $0209 REM Set up MMU to put internal Flash at 0... REM Virtual address 0x0 -> Physical address = $0000_0000 REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access Once Status Register Result = $0209 REM Set up MMU for External Memory REM Base address = $2000_0000 REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access Once Status Register Result = $0209 REM Set up MMU for Internal SRAM REM Base address = $4000_0000 REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access Once Status Register Result = $0209 REM Set up MMU for Periph A Modules REM Base address = $C3E0_0000 REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access Once Status Register Result = $0209 REM Initialize all of the Main SRAM - 512KB Initializing RAM from $40000000 to $4007FFFF. Reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\s32e200_mpc5777c.mac) completed. MPC5777C Device detected. No breakpoints currently set. Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "58205" from 7224 Target Disconnected.