/* * Copyright (c) 2016, Freescale Semiconductor, Inc. * Copyright 2016-2017 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #ifndef _FSL_PHY_H_ #define _FSL_PHY_H_ #include "fsl_enet.h" /*! * @addtogroup phy_driver * @{ */ /******************************************************************************* * Definitions ******************************************************************************/ /*! @brief PHY driver version */ #define FSL_PHY_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) /*!< Version 2.0.0. */ /*! @brief Defines the PHY registers. */ #define PHY_BASICCONTROL_REG 0x00U /*!< The PHY basic control register. */ #define PHY_BASICSTATUS_REG 0x01U /*!< The PHY basic status register. */ #define PHY_ID1_REG 0x02U /*!< The PHY ID one register. */ #define PHY_ID2_REG 0x03U /*!< The PHY ID two register. */ #define PHY_AUTONEG_ADVERTISE_REG 0x04U /*!< The PHY auto-negotiate advertise register. */ #define PHY_SEPCIAL_CONTROL_REG 0x10U /*!< The PHY control two register. */ #define PHY_SEPCIAL_CONTROL_REG1 0x1FU //#define PHY_CONTROL_ID1 0x07U /*!< The PHY ID1*/ #define PHY_CONTROL_ID1 0x20005C90 /*!< The PHY ID1*///for dp8348 /*! @brief Defines the mask flag in basic control register. */ #define PHY_BCTL_DUPLEX_MASK 0x0100U /*!< The PHY duplex bit mask. */ #define PHY_BCTL_RESTART_AUTONEG_MASK 0x0200U /*!< The PHY restart auto negotiation mask. */ #define PHY_BCTL_AUTONEG_MASK 0x1000U /*!< The PHY auto negotiation bit mask. */ #define PHY_BCTL_SPEED_MASK 0x2000U /*!< The PHY speed bit mask. */ #define PHY_BCTL_LOOP_MASK 0x4000U /*!< The PHY loop bit mask. */ #define PHY_BCTL_RESET_MASK 0x8000U /*!< The PHY reset bit mask. */ /*!@brief Defines the mask flag of operation mode in special control register*/ #define PHY_SPECIALCTL_AUTONEGDONE_MASK 0x1000U /*!< The PHY auto-negotiation complete mask. */ #define PHY_SPECIALCTL_DUPLEX_MASK 0x0010U /*!< The PHY duplex mask. */ #define PHY_SPECIALCTL_100SPEED_MASK 0x0008U /*!< The PHY speed mask. */ #define PHY_SPECIALCTL_10SPEED_MASK 0x0004U /*!< The PHY speed mask. */ #define PHY_SPECIALCTL_SPEEDUPLX_MASK 0x001cU /*!< The PHY speed and duplex mask. */ /*! @brief Defines the mask flag in basic status register. */ #define PHY_BSTATUS_LINKSTATUS_MASK 0x0001U /*!< The PHY link status mask. */ /*! @brief Defines the mask flag in PHY auto-negotiation advertise register. */ #define PHY_ALL_CAPABLE_MASK 0x1e0U /*! @brief Defines the PHY status. */ enum _phy_status { kStatus_PHY_SMIVisitTimeout = MAKE_STATUS(kStatusGroup_PHY, 0), /*!< ENET PHY SMI visit timeout. */ }; /*! @brief Defines the PHY link speed. This is align with the speed for ENET MAC. */ typedef enum _phy_speed { kPHY_Speed10M = 0U, /*!< ENET PHY 10M speed. */ kPHY_Speed100M /*!< ENET PHY 100M speed. */ } phy_speed_t; /*! @brief Defines the PHY link duplex. */ typedef enum _phy_duplex { kPHY_HalfDuplex = 0U, /*!< ENET PHY half duplex. */ kPHY_FullDuplex /*!< ENET PHY full duplex. */ } phy_duplex_t; /******************************************************************************* * API ******************************************************************************/ #if defined(__cplusplus) extern "C" { #endif /*! * @name PHY Driver * @{ */ /*! * @brief Initializes PHY. * * This function initialize the SMI interface and initialize PHY. * The SMI is the MII management interface between PHY and MAC, which should be * firstly initialized before any other operation for PHY. The PHY initialize with auto-negotiation. * * @param base ENET peripheral base address. * @param phyAddr The PHY address. * @param srcClock_Hz The module clock frequency - system clock for MII management interface - SMI. * @retval kStatus_Success PHY initialize success * @retval kStatus_Fail PHY initialize fail */ status_t PHY_Init(ENET_Type *base, uint32_t phyAddr, uint32_t srcClock_Hz); /*! * @brief PHY Write function. This function write data over the SMI to * the specified PHY register. This function is called by all PHY interfaces. * * @param base ENET peripheral base address. * @param phyAddr The PHY address. * @param phyReg The PHY register. * @param data The data written to the PHY register. * @retval kStatus_Success PHY write success * @retval kStatus_PHY_SMIVisitTimeout PHY SMI visit time out */ status_t PHY_Write(ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t data); /*! * @brief PHY Read function. This interface read data over the SMI from the * specified PHY register. This function is called by all PHY interfaces. * * @param base ENET peripheral base address. * @param phyAddr The PHY address. * @param phyReg The PHY register. * @param dataPtr The address to store the data read from the PHY register. * @retval kStatus_Success PHY read success * @retval kStatus_PHY_SMIVisitTimeout PHY SMI visit time out */ status_t PHY_Read(ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t *dataPtr); /*! * @brief Gets the PHY link status. * * @param base ENET peripheral base address. * @param phyAddr The PHY address. * @param status The link up or down status of the PHY. * - true the link is up. * - false the link is down. * @retval kStatus_Success PHY get link status success * @retval kStatus_PHY_SMIVisitTimeout PHY SMI visit time out */ status_t PHY_GetLinkStatus(ENET_Type *base, uint32_t phyAddr, bool *status); /*! * @brief Gets the PHY link speed and duplex. * * @param base ENET peripheral base address. * @param phyAddr The PHY address. * @param speed The address of PHY link speed. * @param duplex The link duplex of PHY. * @retval kStatus_Success PHY get link speed and duplex success * @retval kStatus_PHY_SMIVisitTimeout PHY SMI visit time out */ status_t PHY_GetLinkSpeedDuplex(ENET_Type *base, uint32_t phyAddr, phy_speed_t *speed, phy_duplex_t *duplex); /* @} */ #if defined(__cplusplus) } #endif /*! @}*/ #endif /* _FSL_PHY_H_ */