/* * Copyright 2017-2018 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #ifndef _BOARD_H_ #define _BOARD_H_ #include "clock_config.h" #include "fsl_common.h" #include "fsl_reset.h" #include "fsl_gpio.h" #include "fsl_iocon.h" /******************************************************************************* * Definitions ******************************************************************************/ /*! @brief The board name */ #define BOARD_NAME "LPCXpresso55S69" /*! @brief The UART to use for debug messages. */ /* TODO: rename UART to USART */ #define BOARD_DEBUG_UART_TYPE kSerialPort_Uart #define BOARD_DEBUG_UART_BASEADDR (uint32_t) USART0 #define BOARD_DEBUG_UART_INSTANCE 0U #define BOARD_DEBUG_UART_CLK_FREQ 12000000U #define BOARD_DEBUG_UART_CLK_ATTACH kFRO12M_to_FLEXCOMM0 #define BOARD_DEBUG_UART_RST kFC0_RST_SHIFT_RSTn #define BOARD_DEBUG_UART_CLKSRC kCLOCK_Flexcomm0 #define BOARD_UART_IRQ_HANDLER FLEXCOMM0_IRQHandler #define BOARD_UART_IRQ FLEXCOMM0_IRQn #define BOARD_ACCEL_I2C_BASEADDR I2C4 #define BOARD_ACCEL_I2C_CLOCK_FREQ 12000000 #define BOARD_DEBUG_UART_TYPE_CORE1 kSerialPort_Uart #define BOARD_DEBUG_UART_BASEADDR_CORE1 (uint32_t) USART1 #define BOARD_DEBUG_UART_INSTANCE_CORE1 1U #define BOARD_DEBUG_UART_CLK_FREQ_CORE1 12000000U #define BOARD_DEBUG_UART_CLK_ATTACH_CORE1 kFRO12M_to_FLEXCOMM1 #define BOARD_DEBUG_UART_RST_CORE1 kFC1_RST_SHIFT_RSTn #define BOARD_DEBUG_UART_CLKSRC_CORE1 kCLOCK_Flexcomm1 #define BOARD_UART_IRQ_HANDLER_CORE1 FLEXCOMM1_IRQHandler #define BOARD_UART_IRQ_CORE1 FLEXCOMM1_IRQn #ifndef BOARD_DEBUG_UART_BAUDRATE #define BOARD_DEBUG_UART_BAUDRATE 115200U #endif /* BOARD_DEBUG_UART_BAUDRATE */ #ifndef BOARD_DEBUG_UART_BAUDRATE_CORE1 #define BOARD_DEBUG_UART_BAUDRATE_CORE1 115200U #endif /* BOARD_DEBUG_UART_BAUDRATE_CORE1 */ #define BOARD_CODEC_I2C_BASEADDR I2C4 #define BOARD_CODEC_I2C_CLOCK_FREQ 12000000 #define BOARD_CODEC_I2C_INSTANCE 4 #ifndef BOARD_LED_RED_GPIO #define BOARD_LED_RED_GPIO GPIO #endif #define BOARD_LED_RED_GPIO_PORT 1U #ifndef BOARD_LED_RED_GPIO_PIN #define BOARD_LED_RED_GPIO_PIN 6U #endif #ifndef BOARD_LED_BLUE_GPIO #define BOARD_LED_BLUE_GPIO GPIO #endif #define BOARD_LED_BLUE_GPIO_PORT 1U #ifndef BOARD_LED_BLUE_GPIO_PIN #define BOARD_LED_BLUE_GPIO_PIN 6U #endif #ifndef BOARD_LED_GREEN_GPIO #define BOARD_LED_GREEN_GPIO GPIO #endif #define BOARD_LED_GREEN_GPIO_PORT 1U #ifndef BOARD_LED_GREEN_GPIO_PIN #define BOARD_LED_GREEN_GPIO_PIN 7U #endif #ifndef BOARD_SW1_GPIO #define BOARD_SW1_GPIO GPIO #endif #define BOARD_SW1_GPIO_PORT 0U #ifndef BOARD_SW1_GPIO_PIN #define BOARD_SW1_GPIO_PIN 5U #endif #define BOARD_SW1_NAME "SW1" #define BOARD_SW1_IRQ PIN_INT0_IRQn #define BOARD_SW1_IRQ_HANDLER PIN_INT0_IRQHandler #ifndef BOARD_SW2_GPIO #define BOARD_SW2_GPIO GPIO #endif #define BOARD_SW2_GPIO_PORT 1U #ifndef BOARD_SW2_GPIO_PIN #define BOARD_SW2_GPIO_PIN 18U #endif #define BOARD_SW2_NAME "SW2" #define BOARD_SW2_IRQ PIN_INT1_IRQn #define BOARD_SW2_IRQ_HANDLER PIN_INT1_IRQHandler #define BOARD_SW2_GPIO_PININT_INDEX 1 #ifndef BOARD_SW3_GPIO #define BOARD_SW3_GPIO GPIO #endif #define BOARD_SW3_GPIO_PORT 1U #ifndef BOARD_SW3_GPIO_PIN #define BOARD_SW3_GPIO_PIN 9U #endif #define BOARD_SW3_NAME "SW3" #define BOARD_SW3_IRQ PIN_INT1_IRQn #define BOARD_SW3_IRQ_HANDLER PIN_INT1_IRQHandler #define BOARD_SW3_GPIO_PININT_INDEX 1 /* Board led color mapping */ #define LOGIC_LED_ON 0U #define LOGIC_LED_OFF 1U #define LED_RED_INIT(output) \ { \ IOCON_PinMuxSet(IOCON, BOARD_LED_RED_GPIO_PORT, BOARD_LED_RED_GPIO_PIN, IOCON_DIGITAL_EN); \ GPIO_PinInit(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, BOARD_LED_RED_GPIO_PIN, \ &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)}); /*!< Enable target LED1 */ \ } #define LED_RED_ON() \ GPIO_PortClear(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, \ 1U << BOARD_LED_RED_GPIO_PIN) /*!< Turn on target LED1 */ #define LED_RED_OFF() \ GPIO_PortSet(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, \ 1U << BOARD_LED_RED_GPIO_PIN) /*!< Turn off target LED1 \ \ \ \ \ \ \ \ \ \ \ */ #define LED_RED_TOGGLE() \ GPIO_PortToggle(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, \ 1U << BOARD_LED_RED_GPIO_PIN) /*!< Toggle on target LED1 */ #define LED_BLUE_INIT(output) \ { \ IOCON_PinMuxSet(IOCON, BOARD_LED_BLUE_GPIO_PORT, BOARD_LED_BLUE_GPIO_PIN, IOCON_DIGITAL_EN); \ GPIO_PinInit(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, BOARD_LED_BLUE_GPIO_PIN, \ &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)}); /*!< Enable target LED1 */ \ } #define LED_BLUE_ON() \ GPIO_PortClear(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \ 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Turn on target LED1 */ #define LED_BLUE_OFF() \ GPIO_PortSet(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \ 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Turn off target LED1 */ #define LED_BLUE_TOGGLE() \ GPIO_PortToggle(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \ 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Toggle on target LED1 */ #define LED_GREEN_INIT(output) \ GPIO_PinInit(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, BOARD_LED_GREEN_GPIO_PIN, \ &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)}) /*!< Enable target LED1 */ #define LED_GREEN_ON() \ GPIO_PortClear(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \ 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Turn on target LED1 */ #define LED_GREEN_OFF() \ GPIO_PortSet(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \ 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Turn off target LED1 */ #define LED_GREEN_TOGGLE() \ GPIO_PortToggle(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \ 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Toggle on target LED1 */ /* Display. */ #define BOARD_LCD_DC_GPIO GPIO #define BOARD_LCD_DC_GPIO_PORT 1U #define BOARD_LCD_DC_GPIO_PIN 5U /* Serial MWM WIFI */ #define BOARD_SERIAL_MWM_PORT_CLK_FREQ CLOCK_GetFlexCommClkFreq(2) #define BOARD_SERIAL_MWM_PORT USART2 #define BOARD_SERIAL_MWM_PORT_IRQn FLEXCOMM2_IRQn #define BOARD_SERIAL_MWM_RST_WRITE(output) #if defined(__cplusplus) extern "C" { #endif /* __cplusplus */ /******************************************************************************* * API ******************************************************************************/ void BOARD_InitDebugConsole(void); void BOARD_InitDebugConsole_Core1(void); #if defined(SDK_I2C_BASED_COMPONENT_USED) && SDK_I2C_BASED_COMPONENT_USED void BOARD_I2C_Init(I2C_Type *base, uint32_t clkSrc_Hz); status_t BOARD_I2C_Send(I2C_Type *base, uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *txBuff, uint8_t txBuffSize); status_t BOARD_I2C_Receive(I2C_Type *base, uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *rxBuff, uint8_t rxBuffSize); void BOARD_Accel_I2C_Init(void); status_t BOARD_Accel_I2C_Send(uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint32_t txBuff); status_t BOARD_Accel_I2C_Receive( uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *rxBuff, uint8_t rxBuffSize); void BOARD_Codec_I2C_Init(void); status_t BOARD_Codec_I2C_Send( uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, const uint8_t *txBuff, uint8_t txBuffSize); status_t BOARD_Codec_I2C_Receive( uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize); #endif /* SDK_I2C_BASED_COMPONENT_USED */ #if defined(__cplusplus) } #endif /* __cplusplus */ #endif /* _BOARD_H_ */