/* * Copyright 2019 ,2021 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ /*********************************************************************************************************************** * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file * will be overwritten if the respective MCUXpresso Config Tools is used to update this file. **********************************************************************************************************************/ /* clang-format off */ /* * TEXT BELOW IS USED AS SETTING FOR TOOLS ************************************* !!GlobalInfo product: Pins v9.0 processor: LPC55S69 package_id: LPC55S69JBD100 mcu_data: ksdk2_0 processor_version: 9.0.0 board: LPCXpresso55S69 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS *********** */ /* clang-format on */ #include "fsl_common.h" #include "fsl_gpio.h" #include "fsl_iocon.h" #include "pin_mux.h" /* FUNCTION ************************************************************************************************************ * * Function Name : BOARD_InitBootPins * Description : Calls initialization functions. * * END ****************************************************************************************************************/ void BOARD_InitBootPins(void) { BOARD_InitPins(); } /* clang-format off */ /* * TEXT BELOW IS USED AS SETTING FOR TOOLS ************************************* BOARD_InitPins: - options: {callFromInitBoot: 'true', prefix: BOARD_, coreID: cm33_core0, enableClock: 'true'} - pin_list: - {pin_num: '1', peripheral: GPIO, signal: 'PIO1, 4', pin_signal: PIO1_4/FC0_SCK/SD0_D0/CTIMER2_MAT1/SCT0_OUT0/FREQME_GPIO_CLK_A, direction: OUTPUT, mode: pullUp, slew_rate: standard, invert: disabled, open_drain: disabled} - {pin_num: '21', peripheral: SWD, signal: SWO, pin_signal: PIO0_10/FC6_SCK/CT_INP10/CTIMER2_MAT0/FC1_TXD_SCL_MISO_WS/SCT0_OUT2/SWO/SECURE_GPIO0_10/ADC0_1, mode: inactive, slew_rate: standard, invert: disabled, open_drain: disabled, asw: disabled} * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS *********** */ /* clang-format on */ /* FUNCTION ************************************************************************************************************ * * Function Name : BOARD_InitPins * Description : Configures pin routing and optionally pin electrical features. * * END ****************************************************************************************************************/ /* Function assigned for the Cortex-M33 (Core #0) */ void BOARD_InitPins(void) { /* Enables the clock for the I/O controller.: Enable Clock. */ CLOCK_EnableClock(kCLOCK_Iocon); /* Enables the clock for the GPIO1 module */ CLOCK_EnableClock(kCLOCK_Gpio1); gpio_pin_config_t LED_BULE_config = { .pinDirection = kGPIO_DigitalOutput, .outputLogic = 0U }; /* Initialize GPIO functionality on pin PIO1_4 (pin 1) */ GPIO_PinInit(BOARD_LED_BULE_GPIO, BOARD_LED_BULE_PORT, BOARD_LED_BULE_PIN, &LED_BULE_config); const uint32_t port0_pin10_config = (/* Pin is configured as SWO */ IOCON_PIO_FUNC6 | /* No addition pin function */ IOCON_PIO_MODE_INACT | /* Standard mode, output slew rate control is enabled */ IOCON_PIO_SLEW_STANDARD | /* Input function is not inverted */ IOCON_PIO_INV_DI | /* Enables digital function */ IOCON_PIO_DIGITAL_EN | /* Open drain is disabled */ IOCON_PIO_OPENDRAIN_DI | /* Analog switch is open (disabled) */ IOCON_PIO_ASW_DI); /* PORT0 PIN10 (coords: 21) is configured as SWO */ IOCON_PinMuxSet(IOCON, 0U, 10U, port0_pin10_config); const uint32_t LED_BULE = (/* Pin is configured as PIO1_4 */ IOCON_PIO_FUNC0 | /* Selects pull-up function */ IOCON_PIO_MODE_PULLUP | /* Standard mode, output slew rate control is enabled */ IOCON_PIO_SLEW_STANDARD | /* Input function is not inverted */ IOCON_PIO_INV_DI | /* Enables digital function */ IOCON_PIO_DIGITAL_EN | /* Open drain is disabled */ IOCON_PIO_OPENDRAIN_DI); /* PORT1 PIN4 (coords: 1) is configured as PIO1_4 */ IOCON_PinMuxSet(IOCON, BOARD_LED_BULE_PORT, BOARD_LED_BULE_PIN, LED_BULE); } /*********************************************************************************************************************** * EOF **********************************************************************************************************************/