/* * Copyright (c) 2016, Freescale Semiconductor, Inc. * Copyright 2016 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #ifndef __USB_DEVICE_LPC3511IP_H__ #define __USB_DEVICE_LPC3511IP_H__ #include "fsl_device_registers.h" /*! * @addtogroup usb_device_controller_lpcip3511_driver * @{ */ /******************************************************************************* * Definitions ******************************************************************************/ /*! @brief The reserved buffer size, the buffer is for the memory copy if the application transfer buffer is ((not 64 bytes alignment) || (not in the same 64K ram) || (HS && OUT && not multiple of 4)) */ #define USB_DEVICE_IP3511_ENDPOINT_RESERVED_BUFFER_SIZE (5U * 1024U) /*! @brief Use one bit to represent one reserved 64 bytes to allocate the buffer by uint of 64 bytes. */ #define USB_DEVICE_IP3511_BITS_FOR_RESERVED_BUFFER ((USB_DEVICE_IP3511_ENDPOINT_RESERVED_BUFFER_SIZE + 63U) / 64U) /*! @brief How many IPs support the reserved buffer */ #define USB_DEVICE_IP3511_RESERVED_BUFFER_FOR_COPY (USB_DEVICE_CONFIG_LPCIP3511FS + USB_DEVICE_CONFIG_LPCIP3511HS) /*! @brief Prime all the double endpoint buffer at the same time, if the transfer length is larger than max packet size. */ #define USB_DEVICE_IP3511_DOUBLE_BUFFER_ENABLE (1u) #if ((defined(USB_DEVICE_CONFIG_LPCIP3511HS)) && (USB_DEVICE_CONFIG_LPCIP3511HS > 0U)) #define USB_LPC3511IP_Type USBHSD_Type #define USB_DEVICE_IP3511_ENDPOINTS_NUM FSL_FEATURE_USBHSD_EP_NUM #else #define USB_LPC3511IP_Type USB_Type #define USB_DEVICE_IP3511_ENDPOINTS_NUM FSL_FEATURE_USB_EP_NUM #endif /*! @brief USB high-speed device in endpoint TX data corruption */ #define USB_DEVICE_LPC5460X_IP3511_ERRATA_3_22_FIX (0u) /* for out endpoint,only use buffer toggle, disable prime double buffer at the same time*/ /*host send data less than maxpacket size and in endpoint prime length more more than maxpacketsize, there will be state * mismtach*/ #if USB_DEVICE_IP3511_DOUBLE_BUFFER_ENABLE #define USB_DEVICE_IP3511_DISABLE_OUT_DOUBLE_BUFFER (1u) #else #define USB_DEVICE_IP3511_DISABLE_OUT_DOUBLE_BUFFER (0u) #endif #define USB_DEVICE_IP3511HS_LPM_ADPPROBE_ATTACH_DEBOUNCE_COUNT (3) /* if FSL_FEATURE_USBHSD_HAS_EXIT_HS_ISSUE is true: * Enable this macro to exit HS mode automatically if the user case is: * host and device keep cable connected, and host turn off vbus to simulate detachment. * If user disconnects the cable, there is no issue and don't need enable this macro. * There is one delay in the isr if enable this macro. */ #define USB_DEVICE_IP3511HS_FORCE_EXIT_HS_MODE_ENABLE (0u) /*! @brief Endpoint state structure */ typedef struct _usb_device_lpc3511ip_endpoint_state_struct { uint8_t *transferBuffer; /*!< Address of buffer containing the data to be transmitted */ uint32_t transferLength; /*!< Length of data to transmit. */ uint32_t transferDone; /*!< The data length has been transferred*/ uint32_t transferPrimedLength; /*!< it may larger than transferLength, because the primed length may larger than the transaction length. */ uint8_t *epPacketBuffer; /*!< The max packet buffer for copying*/ union { uint32_t state; /*!< The state of the endpoint */ struct { uint32_t maxPacketSize : 11U; /*!< The maximum packet size of the endpoint */ uint32_t stalled : 1U; /*!< The endpoint is stalled or not */ uint32_t transferring : 1U; /*!< The endpoint is transferring */ uint32_t zlt : 1U; /*!< zlt flag */ uint32_t stallPrimed : 1U; uint32_t epPacketCopyed : 1U; /*!< whether use the copy buffer */ uint32_t epControlDefault : 5u; /*!< The EP command/status 26~30 bits */ uint32_t doubleBufferBusy : 2U; /*!< How many buffers are primed, for control endpoint it is not used */ uint32_t producerOdd : 1U; /*!< When priming one transaction, prime to this endpoint buffer */ uint32_t consumerOdd : 1U; /*!< When transaction is done, read result from this endpoint buffer */ uint32_t endpointType : 2U; uint32_t reserved1 : 5U; } stateBitField; } stateUnion; union { uint16_t epBufferStatus; /* If double buff is disable, only epBufferStatusUnion[0] is used; For control endpoint, only epBufferStatusUnion[0] is used. */ struct { uint16_t transactionLength : 11U; uint16_t epPacketCopyed : 1U; } epBufferStatusField; } epBufferStatusUnion[2]; } usb_device_lpc3511ip_endpoint_state_struct_t; /*! @brief LPC USB controller (IP3511) state structure */ typedef struct _usb_device_lpc3511ip_state_struct { /*!< control data buffer, must align with 64 */ uint8_t *controlData; /*!< 8 bytes' setup data, must align with 64 */ uint8_t *setupData; /*!< 4 bytes for zero length transaction, must align with 64 */ uint8_t *zeroTransactionData; /* Endpoint state structures */ usb_device_lpc3511ip_endpoint_state_struct_t endpointState[(USB_DEVICE_IP3511_ENDPOINTS_NUM * 2)]; usb_device_handle deviceHandle; /*!< (4 bytes) Device handle used to identify the device object belongs to */ USB_LPC3511IP_Type *registerBase; /*!< (4 bytes) ip base address */ volatile uint32_t *epCommandStatusList; /* endpoint list */ #if (defined(USB_DEVICE_CONFIG_CHARGER_DETECT) && (USB_DEVICE_CONFIG_CHARGER_DETECT > 0U)) && \ (defined(FSL_FEATURE_SOC_USBHSDCD_COUNT) && (FSL_FEATURE_SOC_USBHSDCD_COUNT > 0U)) void *dcdHandle; /*!< Dcd handle used to identify the device object belongs to */ #endif uint8_t controllerId; /*!< Controller ID */ uint8_t isResetting; /*!< Is doing device reset or not */ uint8_t deviceSpeed; /*!< some controller support the HS */ #if ((defined(USB_DEVICE_IP3511_RESERVED_BUFFER_FOR_COPY)) && (USB_DEVICE_IP3511_RESERVED_BUFFER_FOR_COPY > 0U)) uint8_t *epReservedBuffer; uint8_t epReservedBufferBits[(USB_DEVICE_IP3511_BITS_FOR_RESERVED_BUFFER + 7) / 8]; #endif #if ((defined(USB_DEVICE_CONFIG_LPCIP3511HS)) && (USB_DEVICE_CONFIG_LPCIP3511HS > 0U)) uint8_t controllerSpeed; #endif #if (defined(USB_DEVICE_CONFIG_DETACH_ENABLE) && (USB_DEVICE_CONFIG_DETACH_ENABLE)) uint8_t deviceState; /*!< Is device attached,1 attached,0 detached */ #endif #if (defined(USB_DEVICE_CONFIG_LOW_POWER_MODE) && (USB_DEVICE_CONFIG_LOW_POWER_MODE > 0U)) #if (defined(USB_DEVICE_CONFIG_LPM_L1) && (USB_DEVICE_CONFIG_LPM_L1 > 0U)) uint8_t lpmRemoteWakeUp; #endif #endif #if ((defined(USB_DEVICE_CONFIG_LPCIP3511HS)) && (USB_DEVICE_CONFIG_LPCIP3511HS > 0U)) #if (defined(FSL_FEATURE_USBHSD_INTERRUPT_DATAX_ISSUE_VERSION_CHECK) && \ (FSL_FEATURE_USBHSD_INTERRUPT_DATAX_ISSUE_VERSION_CHECK)) uint8_t hsInterruptIssue; #endif #endif } usb_device_lpc3511ip_state_struct_t; /*! * @name USB device controller (IP3511) functions * @{ */ /******************************************************************************* * API ******************************************************************************/ #if defined(__cplusplus) extern "C" { #endif /*! * @brief Initializes the USB device controller instance. * * This function initializes the USB device controller module specified by the controllerId. * * @param[in] controllerId The controller ID of the USB IP. See the enumeration type usb_controller_index_t. * @param[in] handle Pointer of the device handle used to identify the device object belongs to. * @param[out] controllerHandle An out parameter used to return the pointer of the device controller handle to the * caller. * * @return A USB error code or kStatus_USB_Success. */ usb_status_t USB_DeviceLpc3511IpInit(uint8_t controllerId, usb_device_handle handle, usb_device_controller_handle *controllerHandle); /*! * @brief Deinitializes the USB device controller instance. * * This function deinitializes the USB device controller module. * * @param[in] controllerHandle Pointer of the device controller handle. * * @return A USB error code or kStatus_USB_Success. */ usb_status_t USB_DeviceLpc3511IpDeinit(usb_device_controller_handle controllerHandle); /*! * @brief Sends data through a specified endpoint. * * This function sends data through a specified endpoint. * * @param[in] controllerHandle Pointer of the device controller handle. * @param[in] endpointAddress Endpoint index. * @param[in] buffer The memory address to hold the data need to be sent. * @param[in] length The data length need to be sent. * * @return A USB error code or kStatus_USB_Success. * * @note The return value indicates whether the sending request is successful or not. The transfer completion is * notified by the * corresponding callback function. * Currently, only one transfer request can be supported for a specific endpoint. * If there is a specific requirement to support multiple transfer requests for a specific endpoint, the application * should implement a queue in the application level. * The subsequent transfer can begin only when the previous transfer is done (a notification is obtained through the * endpoint * callback). */ usb_status_t USB_DeviceLpc3511IpSend(usb_device_controller_handle controllerHandle, uint8_t endpointAddress, uint8_t *buffer, uint32_t length); /*! * @brief Receives data through a specified endpoint. * * This function receives data through a specified endpoint. * * @param[in] controllerHandle Pointer of the device controller handle. * @param[in] endpointAddress Endpoint index. * @param[in] buffer The memory address to save the received data. * @param[in] length The data length to be received. * * @return A USB error code or kStatus_USB_Success. * * @note The return value indicates whether the receiving request is successful or not. The transfer completion is * notified by the * corresponding callback function. * Currently, only one transfer request can be supported for a specific endpoint. * If there is a specific requirement to support multiple transfer requests for a specific endpoint, the application * should implement a queue in the application level. * The subsequent transfer can begin only when the previous transfer is done (a notification is obtained through the * endpoint * callback). */ usb_status_t USB_DeviceLpc3511IpRecv(usb_device_controller_handle controllerHandle, uint8_t endpointAddress, uint8_t *buffer, uint32_t length); /*! * @brief Cancels the pending transfer in a specified endpoint. * * The function is used to cancel the pending transfer in a specified endpoint. * * @param[in] controllerHandle ointer of the device controller handle. * @param[in] ep Endpoint address, bit7 is the direction of endpoint, 1U - IN, abd 0U - OUT. * * @return A USB error code or kStatus_USB_Success. */ usb_status_t USB_DeviceLpc3511IpCancel(usb_device_controller_handle controllerHandle, uint8_t ep); /*! * @brief Controls the status of the selected item. * * The function is used to control the status of the selected item. * * @param[in] controllerHandle Pointer of the device controller handle. * @param[in] type The selected item. Please refer to enumeration type usb_device_control_type_t. * @param[in,out] param The parameter type is determined by the selected item. * * @return A USB error code or kStatus_USB_Success. */ usb_status_t USB_DeviceLpc3511IpControl(usb_device_controller_handle controllerHandle, usb_device_control_type_t type, void *param); /*! @} */ #if defined(__cplusplus) } #endif /*! @} */ #endif /* __USB_DEVICE_LPC3511IP_H__ */