/* * Copyright 2018-2020 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #include "fsl_iap.h" /* Component ID definition, used by tools. */ #ifndef FSL_COMPONENT_ID #define FSL_COMPONENT_ID "platform.drivers.iap" #endif #define HZ_TO_KHZ_DIV 1000U /******************************************************************************* * Definitions ******************************************************************************/ /*! @brief IAP_ENTRY API function type */ typedef void (*IAP_ENTRY_T)(uint32_t cmd[], uint32_t stat[]); /******************************************************************************* * Prototypes ******************************************************************************/ /*! * @brief Translate the IAP return status. * * @param status IAP status return from the IAP function. * * @return sdk status code. */ static inline status_t translate_iap_status(uint32_t status); /*! * @brief IAP_ENTRY API function type. * * Wrapper for rom iap call. * * @param cmd_param IAP command and relevant parameter array. * @param status_result IAP status result array. */ static inline void iap_entry(uint32_t *cmd_param, uint32_t *status_result); /******************************************************************************* * Variables ******************************************************************************/ /******************************************************************************* * Code ******************************************************************************/ static inline status_t translate_iap_status(uint32_t status) { status_t ret = (status_t)status; /* Translate IAP return code to sdk status code */ if (status != (uint32_t)kStatus_Success) { ret = MAKE_STATUS((int32_t)kStatusGroup_IAP, (int32_t)status); } return ret; } static inline void iap_entry(uint32_t *cmd_param, uint32_t *status_result) { __disable_irq(); ((IAP_ENTRY_T)FSL_FEATURE_SYSCON_IAP_ENTRY_LOCATION)(cmd_param, status_result); __enable_irq(); } /*! * @brief Read part identification number. * * This function is used to read the part identification number. * * @param partID Address to store the part identification number. * * @retval kStatus_IAP_Success Api has been executed successfully. */ status_t IAP_ReadPartID(uint32_t *partID) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadPartId; iap_entry(command, result); *partID = result[1]; return translate_iap_status(result[0]); } /*! * @brief Read boot code version number. * * This function is used to read the boot code version number. * * @param bootCodeVersion Address to store the boot code version. * * @retval kStatus_IAP_Success Api has been executed successfully. * * note Boot code version is two 32-bit words. Word 0 is the major version, word 1 is the minor version. */ status_t IAP_ReadBootCodeVersion(uint32_t *bootCodeVersion) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_Read_BootromVersion; iap_entry(command, result); bootCodeVersion[0] = result[1]; bootCodeVersion[1] = result[2]; return translate_iap_status(result[0]); } /*! * @brief Reinvoke ISP. * * This function is used to invoke the boot loader in ISP mode. It maps boot vectors and configures the peripherals for * ISP. * * @param ispTyoe ISP type selection. * @param status store the possible status. * * @retval kStatus_IAP_ReinvokeISPConfig reinvoke configuration error. * * note The error response will be returned when IAP is disabled or an invalid ISP type selection appears. The call * won't return unless an error occurs, so there can be no status code. */ void IAP_ReinvokeISP(uint8_t ispType, uint32_t *status) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; //uint8_t ispParameterArray[8]; command[0] = (uint32_t)kIapCmd_IAP_ReinvokeISP; // Note: Error in V2.8.2 SDK has wrong parameters here // ISP Type is passed in 2nd byte of command, not in parameter Array //(void)memset(ispParameterArray, 0, sizeof(uint8_t) * 8U); //ispParameterArray[1] = ispType; //ispParameterArray[7] = ispParameterArray[0] ^ ispParameterArray[1] ^ ispParameterArray[2] ^ ispParameterArray[3] ^ // ispParameterArray[4] ^ ispParameterArray[5] ^ ispParameterArray[6]; //command[1] = (uint32_t)ispParameterArray; command[1] =ispType; iap_entry(command, result); *status = (uint32_t)translate_iap_status(result[0]); } /*! * @brief Read unique identification. * * This function is used to read the unique id. * * @param uniqueID store the uniqueID. * * @retval kStatus_IAP_Success Api has been executed successfully. */ status_t IAP_ReadUniqueID(uint32_t *uniqueID) { #if defined(FSL_FEATURE_IAP_READ_UNIQUE_ID_NOWORK) && FSL_FEATURE_IAP_READ_UNIQUE_ID_NOWORK uint32_t *result = (uint32_t *)0x01000100; uint8_t i = 0; for (i = 0; i < 4; i++) uniqueID[i] = result[i]; return kStatus_IAP_Success; #else uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadUid; iap_entry(command, result); uniqueID[0] = result[1]; uniqueID[1] = result[2]; uniqueID[2] = result[3]; uniqueID[3] = result[4]; return translate_iap_status(result[0]); #endif } #if defined(FSL_FEATURE_IAP_HAS_READ_FACTORY_SETTINGS_FUNCTION) && FSL_FEATURE_IAP_HAS_READ_FACTORY_SETTINGS_FUNCTION /*! * @brief Read factory settings. * * This function reads the factory settings for calibration registers. * * @param dstRegAddr Address of the targeted calibration register. * @param factoryValue Store the factory value * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_ParamError Param0 is not one of the supported calibration registers. */ status_t IAP_ReadFactorySettings(uint32_t dstRegAddr, uint32_t *factoryValue) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadFactorySettings; command[1] = dstRegAddr; iap_entry(command, result); *factoryValue = result[1]; return translate_iap_status(result[0]); } #endif /* FSL_FEATURE_IAP_HAS_READ_FACTORY_SETTINGS_FUNCTION */ #if defined(FSL_FEATURE_IAP_HAS_FLASH_FUNCTION) && FSL_FEATURE_IAP_HAS_FLASH_FUNCTION /*! * @brief Prepare sector for write operation. * * This function prepares sector(s) for write/erase operation. This function must be called before calling the * IAP_CopyRamToFlash() or IAP_EraseSector() or IAP_ErasePage() function. The end sector number must be greater than or * equal to the start sector number. * * @param startSector Start sector number. * @param endSector End sector number. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_InvalidSector Sector number is invalid or end sector number is greater than start sector number. * @retval kStatus_IAP_Busy Flash programming hardware interface is busy. */ status_t IAP_PrepareSectorForWrite(uint32_t startSector, uint32_t endSector) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_PrepareSectorforWrite; command[1] = startSector; command[2] = endSector; iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Copy RAM to flash. * * This function programs the flash memory. Corresponding sectors must be prepared via IAP_PrepareSectorForWrite before * calling this function. The addresses should be a 256 byte boundary and the number of bytes should be 256 | 512 | * 1024 | 4096. * * @param dstAddr Destination flash address where data bytes are to be written. * @param srcAddr Source ram address from where data bytes are to be read. * @param numOfBytes Number of bytes to be written. * @param systemCoreClock SystemCoreClock in Hz. It is converted to KHz before calling the rom IAP function. When the * flash controller has a fixed reference clock, this parameter is bypassed. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_SrcAddrError Source address is not on word boundary. * @retval kStatus_IAP_DstAddrError Destination address is not on a correct boundary. * @retval kStatus_IAP_SrcAddrNotMapped Source address is not mapped in the memory map. * @retval kStatus_IAP_DstAddrNotMapped Destination address is not mapped in the memory map. * @retval kStatus_IAP_CountError Byte count is not multiple of 4 or is not a permitted value. * @retval kStatus_IAP_NotPrepared Command to prepare sector for write operation has not been executed. * @retval kStatus_IAP_Busy Flash programming hardware interface is busy. */ status_t IAP_CopyRamToFlash(uint32_t dstAddr, uint32_t *srcAddr, uint32_t numOfBytes, uint32_t systemCoreClock) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_CopyRamToFlash; command[1] = dstAddr; command[2] = (uint32_t)srcAddr; command[3] = numOfBytes; #if !(defined(FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) && FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) command[4] = systemCoreClock / HZ_TO_KHZ_DIV; #endif /* FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK */ iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Erase sector. * * This function erases sector(s). The end sector number must be greater than or equal to the start sector number. * * @param startSector Start sector number. * @param endSector End sector number. * @param systemCoreClock SystemCoreClock in Hz. It is converted to KHz before calling the rom IAP function. When the * flash controller has a fixed reference clock, this parameter is bypassed. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_InvalidSector Sector number is invalid or end sector number is greater than start sector number. * @retval kStatus_IAP_NotPrepared Command to prepare sector for write operation has not been executed. * @retval kStatus_IAP_Busy Flash programming hardware interface is busy. */ status_t IAP_EraseSector(uint32_t startSector, uint32_t endSector, uint32_t systemCoreClock) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_EraseSector; command[1] = startSector; command[2] = endSector; #if !(defined(FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) && FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) command[3] = systemCoreClock / HZ_TO_KHZ_DIV; #endif /* FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK */ iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Erase page. * * This function erases page(s). The end page number must be greater than or equal to the start page number. * * @param startPage Start page number. * @param endPage End page number. * @param systemCoreClock SystemCoreClock in Hz. It is converted to KHz before calling the rom IAP function. When the * flash controller has a fixed reference clock, this parameter is bypassed. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_InvalidSector Page number is invalid or end page number is greater than start page number. * @retval kStatus_IAP_NotPrepared Command to prepare sector for write operation has not been executed. * @retval kStatus_IAP_Busy Flash programming hardware interface is busy. */ status_t IAP_ErasePage(uint32_t startPage, uint32_t endPage, uint32_t systemCoreClock) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ErasePage; command[1] = startPage; command[2] = endPage; #if !(defined(FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) && FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK) command[3] = systemCoreClock / HZ_TO_KHZ_DIV; #endif /* FSL_FEATURE_SYSCON_HAS_FLASH_REFERENCE_CLOCK */ iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Blank check sector(s) * * Blank check single or multiples sectors of flash memory. The end sector number must be greater than or equal to the * start sector number. It can be used to verify the sector erasure after IAP_EraseSector call. * * @param startSector Start sector number. * @param endSector End sector number. * @retval kStatus_IAP_Success One or more sectors are in erased state. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_SectorNotblank One or more sectors are not blank. */ status_t IAP_BlankCheckSector(uint32_t startSector, uint32_t endSector) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_BlankCheckSector; command[1] = startSector; command[2] = endSector; iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Compare memory contents of flash with ram. * * This function compares the contents of flash and ram. It can be used to verify the flash memory contents after * IAP_CopyRamToFlash call. * * @param dstAddr Destination flash address. * @param srcAddr Source ram address. * @param numOfBytes Number of bytes to be compared. * * @retval kStatus_IAP_Success Contents of flash and ram match. * @retval kStatus_IAP_NoPower Flash memory block is powered down. * @retval kStatus_IAP_NoClock Flash memory block or controller is not clocked. * @retval kStatus_IAP_AddrError Address is not on word boundary. * @retval kStatus_IAP_AddrNotMapped Address is not mapped in the memory map. * @retval kStatus_IAP_CountError Byte count is not multiple of 4 or is not a permitted value. * @retval kStatus_IAP_CompareError Destination and source memory contents do not match. */ status_t IAP_Compare(uint32_t dstAddr, uint32_t *srcAddr, uint32_t numOfBytes) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_Compare; command[1] = dstAddr; command[2] = (uint32_t)srcAddr; command[3] = numOfBytes; iap_entry(command, result); return translate_iap_status(result[0]); } #if defined(FSL_FEATURE_IAP_HAS_FLASH_EXTENDED_SIGNATURE_READ) && FSL_FEATURE_IAP_HAS_FLASH_EXTENDED_SIGNATURE_READ /*! * @brief Extended Read signature. * * This function calculates the signature value for one or more pages of on-chip flash memory. * * @param startPage Start page number. * @param endPage End page number. * @param numOfStates Number of wait states. * @param signature Address to store the signature value. * * @retval kStatus_IAP_Success Api has been executed successfully. */ status_t IAP_ExtendedFlashSignatureRead(uint32_t startPage, uint32_t endPage, uint32_t numOfStates, uint32_t *signature) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ExtendedReadSignature; command[1] = startPage; command[2] = endPage; command[3] = numOfStates; command[4] = 0; iap_entry(command, result); signature[0] = result[4]; signature[1] = result[3]; signature[2] = result[2]; signature[3] = result[1]; return translate_iap_status(result[0]); } #endif /* FSL_FEATURE_IAP_HAS_FLASH_EXTENDED_SIGNATURE_READ */ #if defined(FSL_FEATURE_IAP_HAS_FLASH_SIGNATURE_READ) && FSL_FEATURE_IAP_HAS_FLASH_SIGNATURE_READ /*! * @brief Read flash signature. * * This funtion is used to obtain a 32-bit signature value of the entire flash memory. * * @param signature Address to store the 32-bit generated signature value. * * @retval kStatus_IAP_Success Api has been executed successfully. */ status_t IAP_ReadFlashSignature(uint32_t *signature) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadSignature; iap_entry(command, result); *signature = result[1]; return translate_iap_status(result[0]); } #endif /* FSL_FEATURE_IAP_HAS_FLASH_SIGNATURE_READ */ #endif /* FSL_FEATURE_IAP_HAS_FLASH_FUNCTION */ #if (defined(FSL_FEATURE_IAP_HAS_EEPROM_FUNCTION) && (FSL_FEATURE_IAP_HAS_EEPROM_FUNCTION == 1)) /*! * @brief Read EEPROM page. * * This function is used to read given page of EEPROM into the memory provided. * * @param pageNumber EEPROM page number. * @param dstAddr Memory address to store the value read from EEPROM. * @param systemCoreClock Current core clock frequency in kHz. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_InvalidSector Sector number is invalid. * @retval kStatus_IAP_DstAddrNotMapped Destination address is not mapped in the memory map. * * note Value 0xFFFFFFFF of systemCoreClock will retain the timing and clock settings for EEPROM. */ status_t IAP_ReadEEPROMPage(uint32_t pageNumber, uint32_t *dstAddr, uint32_t systemCoreClock) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadEEPROMPage; command[1] = pageNumber; command[2] = (uint32_t)dstAddr; command[3] = systemCoreClock / HZ_TO_KHZ_DIV; iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Write EEPROM page. * * This function is used to write given data in the provided memory to a page of EEPROM. * * @param pageNumber EEPROM page number. * @param srcAddr Memory address holding data to be stored on to EEPROM page. * @param systemCoreClock Current core clock frequency in kHz. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_InvalidSector Sector number is invalid. * @retval kStatus_IAP_SrcAddrNotMapped Source address is not mapped in the memory map. * * note Value 0xFFFFFFFF of systemCoreClock will retain the timing and clock settings for EEPROM */ status_t IAP_WriteEEPROMPage(uint32_t pageNumber, uint32_t *srcAddr, uint32_t systemCoreClock) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_WriteEEPROMPage; command[1] = pageNumber; command[2] = (uint32_t)srcAddr; command[3] = systemCoreClock / HZ_TO_KHZ_DIV; iap_entry(command, result); return translate_iap_status(result[0]); } #endif /* FSL_FEATURE_IAP_HAS_EEPROM_FUNCTION */ #if defined(FSL_FEATURE_IAP_HAS_FAIM_FUNCTION) && FSL_FEATURE_IAP_HAS_FAIM_FUNCTION /*! * @brief Read FAIM page. * * This function is used to read given page of FAIM into the memory provided. * * @param pageNumber FAIM page number. * @param dstAddr Memory address to store the value read from FAIM. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_DstAddrNotMapped Destination address is not mapped in the memory map. */ status_t IAP_ReadFAIMPage(uint32_t pageNumber, uint32_t *dstAddr) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_ReadFAIMPage; command[1] = pageNumber; command[2] = (uint32_t)dstAddr; iap_entry(command, result); return translate_iap_status(result[0]); } /*! * @brief Write FAIM page. * * This function is used to write given data in the provided memory to a page of G. * * @param pageNumber FAIM page number. * @param srcAddr Memory address holding data to be stored on to FAIM page. * * @retval kStatus_IAP_Success Api has been executed successfully. * @retval kStatus_IAP_SrcAddrNotMapped Source address is not mapped in the memory map. */ status_t IAP_WriteFAIMPage(uint32_t pageNumber, uint32_t *srcAddr) { uint32_t command[5] = {0x00U}; uint32_t result[5] = {0x00U}; command[0] = (uint32_t)kIapCmd_IAP_WriteFAIMPage; command[1] = pageNumber; command[2] = (uint32_t)srcAddr; iap_entry(command, result); return translate_iap_status(result[0]); } #endif /* FSL_FEATURE_IAP_HAS_FAIM_FUNCTION */