/** ****************************************************************************** * @file lwipopts.h * This file is based on \src\include\lwip\opt.h ****************************************************************************** * Copyright (c) 2013-2016, Freescale Semiconductor, Inc. * Copyright 2016-2018 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #ifndef __LWIPOPTS_H__ #define __LWIPOPTS_H__ #if USE_RTOS /** * SYS_LIGHTWEIGHT_PROT==1: if you want inter-task protection for certain * critical regions during buffer allocation, deallocation and memory * allocation and deallocation. */ #define SYS_LIGHTWEIGHT_PROT 1 /** * NO_SYS==0: Use RTOS */ #define NO_SYS 0 /** * LWIP_NETCONN==1: Enable Netconn API (require to use api_lib.c) */ #define LWIP_NETCONN 1 /** * LWIP_SOCKET==1: Enable Socket API (require to use sockets.c) */ #define LWIP_SOCKET 1 /** * LWIP_SO_RCVTIMEO==1: Enable receive timeout for sockets/netconns and * SO_RCVTIMEO processing. */ #define LWIP_SO_RCVTIMEO 1 #else /** * NO_SYS==1: Bare metal lwIP */ #define NO_SYS 1 /** * LWIP_NETCONN==0: Disable Netconn API (require to use api_lib.c) */ #define LWIP_NETCONN 0 /** * LWIP_SOCKET==0: Disable Socket API (require to use sockets.c) */ #define LWIP_SOCKET 0 #endif /* ---------- Core locking ---------- */ #define LWIP_TCPIP_CORE_LOCKING 1 void sys_lock_tcpip_core(void); #define LOCK_TCPIP_CORE() sys_lock_tcpip_core() void sys_unlock_tcpip_core(void); #define UNLOCK_TCPIP_CORE() sys_unlock_tcpip_core() void sys_check_core_locking(void); #define LWIP_ASSERT_CORE_LOCKED() sys_check_core_locking() void sys_mark_tcpip_thread(void); #define LWIP_MARK_TCPIP_THREAD() sys_mark_tcpip_thread() /* ---------- Memory options ---------- */ /** * MEM_ALIGNMENT: should be set to the alignment of the CPU * 4 byte alignment -> #define MEM_ALIGNMENT 4 * 2 byte alignment -> #define MEM_ALIGNMENT 2 */ #ifndef MEM_ALIGNMENT #define MEM_ALIGNMENT 4 #endif /** * MEM_SIZE: the size of the heap memory. If the application will send * a lot of data that needs to be copied, this should be set high. * */ #ifndef MEM_SIZE #define MEM_SIZE (40 * 1024) #endif /* MEMP_NUM_PBUF: the number of memp struct pbufs. If the application sends a lot of data out of ROM (or other static memory), this should be set high. */ #ifndef MEMP_NUM_PBUF #define MEMP_NUM_PBUF 20 #endif /* MEMP_NUM_UDP_PCB: the number of UDP protocol control blocks. One per active UDP "connection". */ #ifndef MEMP_NUM_UDP_PCB //#define MEMP_NUM_UDP_PCB 6 #define MEMP_NUM_UDP_PCB 16 #endif /* MEMP_NUM_TCP_PCB: the number of simulatenously active TCP connections. */ #ifndef MEMP_NUM_TCP_PCB #define MEMP_NUM_TCP_PCB 10 #endif /* MEMP_NUM_TCP_PCB_LISTEN: the number of listening TCP connections. */ #ifndef MEMP_NUM_TCP_PCB_LISTEN #define MEMP_NUM_TCP_PCB_LISTEN 6 #endif /* MEMP_NUM_TCP_SEG: the number of simultaneously queued TCP segments. */ #ifndef MEMP_NUM_TCP_SEG #define MEMP_NUM_TCP_SEG 22 #endif /* MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts. */ #ifndef MEMP_NUM_SYS_TIMEOUT #define MEMP_NUM_SYS_TIMEOUT 10 #endif /* ---------- Pbuf options ---------- */ /* PBUF_POOL_SIZE: the number of buffers in the pbuf pool. */ #ifndef PBUF_POOL_SIZE #define PBUF_POOL_SIZE 16 //#define PBUF_POOL_SIZE 8 #endif /* PBUF_POOL_BUFSIZE: the size of each pbuf in the pbuf pool. */ /* Default value is defined in lwip\src\include\lwip\opt.h as * LWIP_MEM_ALIGN_SIZE(TCP_MSS+40+PBUF_LINK_ENCAPSULATION_HLEN+PBUF_LINK_HLEN)*/ /* ---------- TCP options ---------- */ #ifndef LWIP_TCP #define LWIP_TCP 1 #endif #ifndef TCP_TTL #define TCP_TTL 255 #endif /* Controls if TCP should queue segments that arrive out of order. Define to 0 if your device is low on memory. */ #ifndef TCP_QUEUE_OOSEQ #define TCP_QUEUE_OOSEQ 0 #endif /* TCP Maximum segment size. */ #ifndef TCP_MSS #define TCP_MSS (1500 - 40) /* TCP_MSS = (Ethernet MTU - IP header size - TCP header size) */ #endif /* TCP sender buffer space (bytes). */ #ifndef TCP_SND_BUF #define TCP_SND_BUF (6 * TCP_MSS) // 2 #endif /* TCP sender buffer space (pbufs). This must be at least = 2 * TCP_SND_BUF/TCP_MSS for things to work. */ #ifndef TCP_SND_QUEUELEN #define TCP_SND_QUEUELEN (3 * TCP_SND_BUF) / TCP_MSS // 6 #endif /* TCP receive window. */ #ifndef TCP_WND #define TCP_WND (2 * TCP_MSS) #endif /* Enable backlog*/ #ifndef TCP_LISTEN_BACKLOG #define TCP_LISTEN_BACKLOG 1 #endif /* ---------- Network Interfaces options ---------- */ /* Support netif api (in netifapi.c). */ #ifndef LWIP_NETIF_API #define LWIP_NETIF_API 1 #endif /* ---------- ICMP options ---------- */ #ifndef LWIP_ICMP #define LWIP_ICMP 1 #endif /* ---------- DHCP options ---------- */ /* Enable DHCP module. */ #ifndef LWIP_DHCP //#define LWIP_DHCP 1 #define LWIP_DHCP 0 #endif /* ---------- UDP options ---------- */ #ifndef LWIP_UDP #define LWIP_UDP 1 #endif #ifndef UDP_TTL #define UDP_TTL 255 #endif /* ---------- Statistics options ---------- */ #ifndef LWIP_STATS #define LWIP_STATS 1 #endif #ifndef LWIP_PROVIDE_ERRNO #define LWIP_PROVIDE_ERRNO 1 #endif /* -------------------------------------- ---------- Checksum options ---------- -------------------------------------- */ /* Some MCU allow computing and verifying the IP, UDP, TCP and ICMP checksums by hardware: - To use this feature let the following define uncommented. - To disable it and process by CPU comment the the checksum. */ //#define CHECKSUM_BY_HARDWARE #ifdef CHECKSUM_BY_HARDWARE /* CHECKSUM_GEN_IP==0: Generate checksums by hardware for outgoing IP packets.*/ #define CHECKSUM_GEN_IP 0 /* CHECKSUM_GEN_UDP==0: Generate checksums by hardware for outgoing UDP packets.*/ #define CHECKSUM_GEN_UDP 0 /* CHECKSUM_GEN_TCP==0: Generate checksums by hardware for outgoing TCP packets.*/ #define CHECKSUM_GEN_TCP 0 /* CHECKSUM_CHECK_IP==0: Check checksums by hardware for incoming IP packets.*/ #define CHECKSUM_CHECK_IP 0 /* CHECKSUM_CHECK_UDP==0: Check checksums by hardware for incoming UDP packets.*/ #define CHECKSUM_CHECK_UDP 0 /* CHECKSUM_CHECK_TCP==0: Check checksums by hardware for incoming TCP packets.*/ #define CHECKSUM_CHECK_TCP 0 #else /* CHECKSUM_GEN_IP==1: Generate checksums in software for outgoing IP packets.*/ #define CHECKSUM_GEN_IP 1 /* CHECKSUM_GEN_UDP==1: Generate checksums in software for outgoing UDP packets.*/ #define CHECKSUM_GEN_UDP 1 /* CHECKSUM_GEN_TCP==1: Generate checksums in software for outgoing TCP packets.*/ #define CHECKSUM_GEN_TCP 1 /* CHECKSUM_CHECK_IP==1: Check checksums in software for incoming IP packets.*/ #define CHECKSUM_CHECK_IP 1 /* CHECKSUM_CHECK_UDP==1: Check checksums in software for incoming UDP packets.*/ #define CHECKSUM_CHECK_UDP 1 /* CHECKSUM_CHECK_TCP==1: Check checksums in software for incoming TCP packets.*/ #define CHECKSUM_CHECK_TCP 1 #endif /** * DEFAULT_THREAD_STACKSIZE: The stack size used by any other lwIP thread. * The stack size value itself is platform-dependent, but is passed to * sys_thread_new() when the thread is created. */ #ifndef DEFAULT_THREAD_STACKSIZE #define DEFAULT_THREAD_STACKSIZE 3000 #endif /** * DEFAULT_THREAD_PRIO: The priority assigned to any other lwIP thread. * The priority value itself is platform-dependent, but is passed to * sys_thread_new() when the thread is created. */ #ifndef DEFAULT_THREAD_PRIO //#define DEFAULT_THREAD_PRIO 3 #define DEFAULT_THREAD_PRIO 5 #endif /* ------------------------------------ ---------- Debugging options ---------- ------------------------------------ */ #define LWIP_DEBUG #ifdef LWIP_DEBUG #define U8_F "c" #define S8_F "c" #define X8_F "02x" #define U16_F "u" #define S16_F "d" #define X16_F "x" #define U32_F "u" #define S32_F "d" #define X32_F "x" #define SZT_F "u" #endif //#define TCPIP_MBOX_SIZE 32 #define TCPIP_MBOX_SIZE 40 #define TCPIP_THREAD_STACKSIZE 1024 //#define TCPIP_THREAD_STACKSIZE (4096) #define TCPIP_THREAD_PRIO 3 /** * DEFAULT_RAW_RECVMBOX_SIZE: The mailbox size for the incoming packets on a * NETCONN_RAW. The queue size value itself is platform-dependent, but is passed * to sys_mbox_new() when the recvmbox is created. */ #define DEFAULT_RAW_RECVMBOX_SIZE 12 /** * DEFAULT_UDP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a * NETCONN_UDP. The queue size value itself is platform-dependent, but is passed * to sys_mbox_new() when the recvmbox is created. */ #define DEFAULT_UDP_RECVMBOX_SIZE 20 /** * DEFAULT_TCP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a * NETCONN_TCP. The queue size value itself is platform-dependent, but is passed * to sys_mbox_new() when the recvmbox is created. */ #define DEFAULT_TCP_RECVMBOX_SIZE 12 /** * DEFAULT_ACCEPTMBOX_SIZE: The mailbox size for the incoming connections. * The queue size value itself is platform-dependent, but is passed to * sys_mbox_new() when the acceptmbox is created. */ #define DEFAULT_ACCEPTMBOX_SIZE 12 #if (LWIP_DNS || LWIP_IGMP || LWIP_IPV6) && !defined(LWIP_RAND) /* When using IGMP or IPv6, LWIP_RAND() needs to be defined to a random-function returning an u32_t random value*/ #include "lwip/arch.h" u32_t lwip_rand(void); #define LWIP_RAND() lwip_rand() #endif #endif /* __LWIPOPTS_H__ */ /*****END OF FILE****/