/*********************************************************************************************************************** * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file * will be overwritten if the respective MCUXpresso Config Tools is used to update this file. **********************************************************************************************************************/ #include "dcd.h" /* Component ID definition, used by tools. */ #ifndef FSL_COMPONENT_ID #define FSL_COMPONENT_ID "platform.drivers.xip_board" #endif #if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1) #if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1) #if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__) __attribute__((section(".boot_hdr.dcd_data"), used)) #elif defined(__ICCARM__) #pragma location = ".boot_hdr.dcd_data" #endif /* TEXT BELOW IS USED AS SETTING FOR TOOLS ************************************* !!GlobalInfo product: DCDx v3.0 processor: MIMXRT1021xxxxx package_id: MIMXRT1021DAG5A mcu_data: ksdk2_0 processor_version: 11.0.1 board: MIMXRT1020-EVK output_format: c_array * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/ /* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */ const uint8_t dcd_data[] = { /* HEADER */ /* Tag */ 0xD2, /* Image Length */ 0x03, 0x40, /* Version */ 0x41, /* COMMANDS */ /* group: 'Imported Commands' */ /* #1.1-87, command header bytes for merged 'Write - value' command */ 0xCC, 0x02, 0xBC, 0x04, /* #1.1, command: write_value, address: CCM_CCGR0, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x68, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.2, command: write_value, address: CCM_CCGR1, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x6C, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.3, command: write_value, address: CCM_CCGR2, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x70, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.4, command: write_value, address: CCM_CCGR3, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x74, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.5, command: write_value, address: CCM_CCGR4, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x78, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.6, command: write_value, address: CCM_CCGR5, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x7C, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.7, command: write_value, address: CCM_CCGR6, value: 0xFFFFFFFF, size: 4 */ 0x40, 0x0F, 0xC0, 0x80, 0xFF, 0xFF, 0xFF, 0xFF, /* #1.8, command: write_value, address: CCM_ANALOG_PLL_SYS, value: 0x2001, size: 4 */ 0x40, 0x0D, 0x80, 0x30, 0x00, 0x00, 0x20, 0x01, /* #1.9, command: write_value, address: CCM_ANALOG_PFD_528, value: 0x180000, size: 4 */ 0x40, 0x0D, 0x81, 0x00, 0x00, 0x18, 0x00, 0x00, /* #1.10, command: write_value, address: CCM_CBCDR, value: 0xA8340, size: 4 */ 0x40, 0x0F, 0xC0, 0x14, 0x00, 0x0A, 0x83, 0x40, /* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_00, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00, /* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_01, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00, /* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_02, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00, /* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_03, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00, /* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_04, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00, /* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_05, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00, /* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_06, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00, /* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_07, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00, /* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_08, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00, /* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_09, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00, /* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_10, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00, /* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_11, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00, /* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_12, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00, /* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_13, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00, /* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_14, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00, /* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_15, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00, /* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_16, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00, /* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_17, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00, /* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_18, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00, /* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_19, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00, /* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_20, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00, /* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_21, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00, /* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_22, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00, /* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_23, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00, /* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_24, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00, /* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_25, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00, /* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_26, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00, /* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_28, value: 0x10, size: 4 */ 0x40, 0x1F, 0x80, 0x84, 0x00, 0x00, 0x00, 0x10, /* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_29, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00, /* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_30, value: 0x00, size: 4 */ 0x40, 0x1F, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00, /* #1.41, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_00, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x88, 0x00, 0x00, 0x00, 0xE1, /* #1.42, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_01, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x8C, 0x00, 0x00, 0x00, 0xE1, /* #1.43, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_02, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x90, 0x00, 0x00, 0x00, 0xE1, /* #1.44, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_03, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x94, 0x00, 0x00, 0x00, 0xE1, /* #1.45, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_04, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x98, 0x00, 0x00, 0x00, 0xE1, /* #1.46, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_05, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0x9C, 0x00, 0x00, 0x00, 0xE1, /* #1.47, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_06, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xA0, 0x00, 0x00, 0x00, 0xE1, /* #1.48, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_07, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xA4, 0x00, 0x00, 0x00, 0xE1, /* #1.49, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_08, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xA8, 0x00, 0x00, 0x00, 0xE1, /* #1.50, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_09, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xAC, 0x00, 0x00, 0x00, 0xE1, /* #1.51, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_10, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xB0, 0x00, 0x00, 0x00, 0xE1, /* #1.52, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_11, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xB4, 0x00, 0x00, 0x00, 0xE1, /* #1.53, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_12, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xB8, 0x00, 0x00, 0x00, 0xE1, /* #1.54, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_13, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xBC, 0x00, 0x00, 0x00, 0xE1, /* #1.55, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_14, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xC0, 0x00, 0x00, 0x00, 0xE1, /* #1.56, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_15, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xC4, 0x00, 0x00, 0x00, 0xE1, /* #1.57, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_16, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xC8, 0x00, 0x00, 0x00, 0xE1, /* #1.58, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_17, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xCC, 0x00, 0x00, 0x00, 0xE1, /* #1.59, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_18, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xD0, 0x00, 0x00, 0x00, 0xE1, /* #1.60, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_19, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xD4, 0x00, 0x00, 0x00, 0xE1, /* #1.61, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_20, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xD8, 0x00, 0x00, 0x00, 0xE1, /* #1.62, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_21, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xDC, 0x00, 0x00, 0x00, 0xE1, /* #1.63, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_22, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xE0, 0x00, 0x00, 0x00, 0xE1, /* #1.64, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_23, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xE4, 0x00, 0x00, 0x00, 0xE1, /* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_24, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xE8, 0x00, 0x00, 0x00, 0xE1, /* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_25, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xEC, 0x00, 0x00, 0x00, 0xE1, /* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_26, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xF0, 0x00, 0x00, 0x00, 0xE1, /* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_28, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xF8, 0x00, 0x00, 0x00, 0xE1, /* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_29, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x81, 0xFC, 0x00, 0x00, 0x00, 0xE1, /* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_30, value: 0xE1, size: 4 */ 0x40, 0x1F, 0x82, 0x00, 0x00, 0x00, 0x00, 0xE1, /* #1.71, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */ 0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04, /* #1.72, command: write_value, address: SEMC_BMCR0, value: 0x81, size: 4 */ 0x40, 0x2F, 0x00, 0x08, 0x00, 0x00, 0x00, 0x81, /* #1.73, command: write_value, address: SEMC_BMCR1, value: 0x81, size: 4 */ 0x40, 0x2F, 0x00, 0x0C, 0x00, 0x00, 0x00, 0x81, /* #1.74, command: write_value, address: SEMC_BR0, value: 0x80000019, size: 4 */ 0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x19, /* #1.75, command: write_value, address: SEMC_BR1, value: 0x8200001A, size: 4 */ 0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1A, /* #1.76, command: write_value, address: SEMC_BR2, value: 0x8400001A, size: 4 */ 0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1A, /* #1.77, command: write_value, address: SEMC_IOCR, value: 0x7988, size: 4 */ 0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x79, 0x88, /* #1.78, command: write_value, address: SEMC_SDRAMCR0, value: 0xA06, size: 4 */ 0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0A, 0x06, /* #1.79, command: write_value, address: SEMC_SDRAMCR1, value: 0x452811, size: 4 */ 0x40, 0x2F, 0x00, 0x44, 0x00, 0x45, 0x28, 0x11, /* #1.80, command: write_value, address: SEMC_SDRAMCR2, value: 0x70708, size: 4 */ 0x40, 0x2F, 0x00, 0x48, 0x00, 0x07, 0x07, 0x08, /* #1.81, command: write_value, address: SEMC_SDRAMCR3, value: 0x6050A00, size: 4 */ 0x40, 0x2F, 0x00, 0x4C, 0x06, 0x05, 0x0A, 0x00, /* #1.82, command: write_value, address: SEMC_DBICR0, value: 0x2000, size: 4 */ 0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x20, 0x00, /* #1.83, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */ 0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88, /* #1.84, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */ 0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02, /* #1.85, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */ 0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00, /* #1.86, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */ 0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00, /* #1.87, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */ 0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F, /* #2, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */ 0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01, /* #3.1-2, command header bytes for merged 'Write - value' command */ 0xCC, 0x00, 0x14, 0x04, /* #3.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */ 0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00, /* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */ 0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C, /* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */ 0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01, /* #5.1-2, command header bytes for merged 'Write - value' command */ 0xCC, 0x00, 0x14, 0x04, /* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */ 0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00, /* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */ 0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C, /* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */ 0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01, /* #7.1-3, command header bytes for merged 'Write - value' command */ 0xCC, 0x00, 0x1C, 0x04, /* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x30, size: 4 */ 0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x30, /* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */ 0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00, /* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */ 0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A, /* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */ 0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01, /* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x6050A01, size: 4 */ 0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x06, 0x05, 0x0A, 0x01 }; /* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */ #else const uint8_t dcd_data[] = {0x00}; #endif /* XIP_BOOT_HEADER_DCD_ENABLE */ #endif /* XIP_BOOT_HEADER_ENABLE */