/* * Copyright (c) 2015, Freescale Semiconductor, Inc. * Copyright 2016-2017 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #include #include "board.h" #include "fsl_debug_console.h" #include "fsl_enet.h" #include "fsl_phy.h" #if defined(FSL_FEATURE_MEMORY_HAS_ADDRESS_OFFSET) && FSL_FEATURE_MEMORY_HAS_ADDRESS_OFFSET #include "fsl_memory.h" #endif #include "pin_mux.h" #include "clock_config.h" #include "fsl_gpio.h" #include "fsl_iomuxc.h" /******************************************************************************* * Definitions ******************************************************************************/ #define EXAMPLE_ENET ENET #define EXAMPLE_PHY 0x02U #define CORE_CLK_FREQ CLOCK_GetFreq(kCLOCK_AhbClk) #define ENET_RXBD_NUM (4) #define ENET_TXBD_NUM (4) #define ENET_RXBUFF_SIZE (ENET_FRAME_MAX_FRAMELEN) #define ENET_TXBUFF_SIZE (ENET_FRAME_MAX_FRAMELEN) #define ENET_DATA_LENGTH (1000) #define ENET_TRANSMIT_DATA_NUM (20) #ifndef APP_ENET_BUFF_ALIGNMENT #define APP_ENET_BUFF_ALIGNMENT ENET_BUFF_ALIGNMENT #endif /******************************************************************************* * Prototypes ******************************************************************************/ /*! @brief Build ENET broadcast frame. */ static void ENET_BuildBroadCastFrame(void); /******************************************************************************* * Variables ******************************************************************************/ /*! @brief Buffer descriptors should be in non-cacheable region and should be align to "ENET_BUFF_ALIGNMENT". */ AT_NONCACHEABLE_SECTION_ALIGN(enet_rx_bd_struct_t g_rxBuffDescrip[ENET_RXBD_NUM], ENET_BUFF_ALIGNMENT); AT_NONCACHEABLE_SECTION_ALIGN(enet_tx_bd_struct_t g_txBuffDescrip[ENET_TXBD_NUM], ENET_BUFF_ALIGNMENT); /*! @brief The data buffers can be in cacheable region or in non-cacheable region. * If use cacheable region, the alignment size should be the maximum size of "CACHE LINE SIZE" and "ENET_BUFF_ALIGNMENT" * If use non-cache region, the alignment size is the "ENET_BUFF_ALIGNMENT". */ SDK_ALIGN(uint8_t g_rxDataBuff[ENET_RXBD_NUM][SDK_SIZEALIGN(ENET_RXBUFF_SIZE, APP_ENET_BUFF_ALIGNMENT)], APP_ENET_BUFF_ALIGNMENT); SDK_ALIGN(uint8_t g_txDataBuff[ENET_TXBD_NUM][SDK_SIZEALIGN(ENET_TXBUFF_SIZE, APP_ENET_BUFF_ALIGNMENT)], APP_ENET_BUFF_ALIGNMENT); enet_handle_t g_handle; uint8_t g_frame[ENET_DATA_LENGTH + 14]; uint32_t g_testTxNum = 0; /*! @brief The MAC address for ENET device. */ uint8_t g_macAddr[6] = {0xd4, 0xbe, 0xd9, 0x45, 0x22, 0x60}; /******************************************************************************* * Code ******************************************************************************/ void BOARD_InitModuleClock(void) { const clock_enet_pll_config_t config = { .enableClkOutput = true, .enableClkOutput25M = false, .loopDivider = 1, }; CLOCK_InitEnetPll(&config); } void delay(void) { volatile uint32_t i = 0; for (i = 0; i < 1000000; ++i) { __asm("NOP"); /* delay */ } } /*! @brief Build Frame for transmit. */ static void ENET_BuildBroadCastFrame(void) { uint32_t count = 0; uint32_t length = ENET_DATA_LENGTH - 14; for (count = 0; count < 6U; count++) { g_frame[count] = 0xFFU; } memcpy(&g_frame[6], &g_macAddr[0], 6U); g_frame[12] = (length >> 8) & 0xFFU; g_frame[13] = length & 0xFFU; for (count = 0; count < length; count++) { g_frame[count + 14] = count % 0xFFU; } } /*! * @brief Main function */ int main(void) { enet_config_t config; uint32_t length = 0; uint32_t sysClock; bool link = false; phy_speed_t speed; phy_duplex_t duplex; uint32_t txnumber = 0; status_t status; enet_data_error_stats_t eErrStatic; /* Hardware Initialization. */ gpio_pin_config_t gpio_config = {kGPIO_DigitalOutput, 0, kGPIO_NoIntmode}; BOARD_ConfigMPU(); BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); BOARD_InitModuleClock(); IOMUXC_EnableMode(IOMUXC_GPR, kIOMUXC_GPR_ENET1TxClkOutputDir, true); GPIO_PinInit(GPIO1, 9, &gpio_config); GPIO_PinInit(GPIO1, 10, &gpio_config); /* pull up the ENET_INT before RESET. */ GPIO_WritePinOutput(GPIO1, 10, 1); GPIO_WritePinOutput(GPIO1, 9, 0); delay(); GPIO_WritePinOutput(GPIO1, 9, 1); PRINTF("\r\n ENET example start.\r\n"); /* prepare the buffer configuration. */ enet_buffer_config_t buffConfig[] = { { ENET_RXBD_NUM, ENET_TXBD_NUM, SDK_SIZEALIGN(ENET_RXBUFF_SIZE, APP_ENET_BUFF_ALIGNMENT), SDK_SIZEALIGN(ENET_TXBUFF_SIZE, APP_ENET_BUFF_ALIGNMENT), &g_rxBuffDescrip[0], &g_txBuffDescrip[0], &g_rxDataBuff[0][0], &g_txDataBuff[0][0], } }; /* Get default configuration. */ /* * config.miiMode = kENET_RmiiMode; * config.miiSpeed = kENET_MiiSpeed100M; * config.miiDuplex = kENET_MiiFullDuplex; * config.rxMaxFrameLen = ENET_FRAME_MAX_FRAMELEN; */ ENET_GetDefaultConfig(&config); /* Set SMI to get PHY link status. */ sysClock = CORE_CLK_FREQ; status = PHY_Init(EXAMPLE_ENET, EXAMPLE_PHY, sysClock); while (status != kStatus_Success) { PRINTF("\r\nPHY Auto-negotiation failed. Please check the cable connection and link partner setting.\r\n"); status = PHY_Init(EXAMPLE_ENET, EXAMPLE_PHY, sysClock); } PHY_GetLinkStatus(EXAMPLE_ENET, EXAMPLE_PHY, &link); if (link) { /* Get the actual PHY link speed. */ PHY_GetLinkSpeedDuplex(EXAMPLE_ENET, EXAMPLE_PHY, &speed, &duplex); /* Change the MII speed and duplex for actual link status. */ config.miiSpeed = (enet_mii_speed_t)speed; config.miiDuplex = (enet_mii_duplex_t)duplex; } ENET_Init(EXAMPLE_ENET, &g_handle, &config, &buffConfig[0], &g_macAddr[0], sysClock); ENET_ActiveRead(EXAMPLE_ENET); /* Build broadcast for sending. */ ENET_BuildBroadCastFrame(); while (1) { /* Get the Frame size */ status = ENET_GetRxFrameSize(&g_handle, &length); /* Call ENET_ReadFrame when there is a received frame. */ if (length != 0) { /* Received valid frame. Deliver the rx buffer with the size equal to length. */ uint8_t *data = (uint8_t *)malloc(length); status = ENET_ReadFrame(EXAMPLE_ENET, &g_handle, data, length); if (status == kStatus_Success) { PRINTF(" A frame received. the length %d ", length); PRINTF(" Dest Address %02x:%02x:%02x:%02x:%02x:%02x Src Address %02x:%02x:%02x:%02x:%02x:%02x \r\n", data[0], data[1], data[2], data[3], data[4], data[5], data[6], data[7], data[8], data[9], data[10], data[11]); } free(data); } else if (status == kStatus_ENET_RxFrameError) { /* Update the received buffer when error happened. */ /* Get the error information of the received g_frame. */ ENET_GetRxErrBeforeReadFrame(&g_handle, &eErrStatic); /* update the receive buffer. */ ENET_ReadFrame(EXAMPLE_ENET, &g_handle, NULL, 0); } } }