SEGGER J-Link GDB Server V6.98a GUI Version JLinkARM.dll V6.98a (DLL compiled Mar 5 2021 17:01:09) -----GDB Server start settings----- GDBInit file: none GDB Server Listening port: 2331 SWO raw output listening port: 2332 Terminal I/O port: 2333 Accept remote connection: yes Generate logfile: off Verify download: on Init regs on start: off Silent mode: off Single run mode: off Target connection timeout: 5000 ms ------J-Link related settings------ J-Link Host interface: USB J-Link script: none J-Link settings file: none ------Target related settings------ Target device: MIMXRT1176xxxA_M7 Target interface: SWD Target interface speed: 4000kHz Target endian: little Connecting to J-Link... J-Link is connected. Firmware: J-Link V11 compiled Feb 4 2021 12:59:17 Hardware: V11.00 S/N: 261002723 OEM: SEGGER-EDU Feature(s): FlashBP, GDB Checking target voltage... Target voltage: 3.30 V Listening on TCP/IP port 2331 Connecting to target... Connected to target Waiting for GDB connection...Connected to 127.0.0.1 Reading all registers Read 4 bytes @ address 0x3000D214 (Data = 0x46BD3708) Read 2 bytes @ address 0x3000D214 (Data = 0x3708) Received monitor command: reset Resetting target Received monitor command: halt Halting target CPU... ...Target halted (PC = 0x00223104) Downloading 512 bytes @ address 0x30000400 - Verified OK Downloading 48 bytes @ address 0x30001000 - Verified OK Downloading 1024 bytes @ address 0x30002000 - Verified OK Downloading 12672 bytes @ address 0x30002400 - Verified OK Downloading 8 bytes @ address 0x30005580 - Verified OK Downloading 4 bytes @ address 0x30005588 - Verified OK Downloading 4 bytes @ address 0x3000558C - Verified OK Downloading 100 bytes @ address 0x30005590 - Verified OK ERROR: Failed to prepare RAMCode using RAM Error while determining flash info (Bank @ 0x30000000) Writing register (PC = 0x300024bc) Received monitor command: reset Resetting target Received monitor command: go Starting target CPU... ERROR: Could not start CPU core. (ErrorCode: -1)