/* * Copyright 2020 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ /*********************************************************************************************************************** * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file * will be overwritten if the respective MCUXpresso Config Tools is used to update this file. **********************************************************************************************************************/ #include "dcd.h" /* Component ID definition, used by tools. */ #ifndef FSL_COMPONENT_ID #define FSL_COMPONENT_ID "platform.drivers.xip_board" #endif #if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1) #if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1) #if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__) __attribute__((section(".boot_hdr.dcd_data"), used)) #elif defined(__ICCARM__) #pragma location = ".boot_hdr.dcd_data" #endif /* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */ const uint8_t dcd_data[] = { /*0000*/ 0xD2, 0x05, 0x08, 0x41, 0xCC, 0x04, 0x5C, 0x04, 0x40, 0xCC, 0x02, 0x00, 0x00, 0x00, 0x06, 0x02, /*0010*/ 0x40, 0x0E, 0x80, 0x10, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00, /*0020*/ 0x40, 0x0E, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00, /*0030*/ 0x40, 0x0E, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00, /*0040*/ 0x40, 0x0E, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00, /*0050*/ 0x40, 0x0E, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00, /*0060*/ 0x40, 0x0E, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00, /*0070*/ 0x40, 0x0E, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00, /*0080*/ 0x40, 0x0E, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00, /*0090*/ 0x40, 0x0E, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00, /*00a0*/ 0x40, 0x0E, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00, /*00b0*/ 0x40, 0x0E, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00, /*00c0*/ 0x40, 0x0E, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00, /*00d0*/ 0x40, 0x0E, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00, /*00e0*/ 0x40, 0x0E, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00, /*00f0*/ 0x40, 0x0E, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00, /*0100*/ 0x40, 0x0E, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00, /*0110*/ 0x40, 0x0E, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00, /*0120*/ 0x40, 0x0E, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00, /*0130*/ 0x40, 0x0E, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00, /*0140*/ 0x40, 0x0E, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x10, /*0150*/ 0x40, 0x0E, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xB4, 0x00, 0x00, 0x00, 0x00, /*0160*/ 0x40, 0x0E, 0x80, 0xB8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xBC, 0x00, 0x00, 0x00, 0x00, /*0170*/ 0x40, 0x0E, 0x80, 0xC0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xC4, 0x00, 0x00, 0x00, 0x00, /*0180*/ 0x40, 0x0E, 0x80, 0xC8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xCC, 0x00, 0x00, 0x00, 0x00, /*0190*/ 0x40, 0x0E, 0x80, 0xD0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xD4, 0x00, 0x00, 0x00, 0x00, /*01a0*/ 0x40, 0x0E, 0x80, 0xD8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xDC, 0x00, 0x00, 0x00, 0x00, /*01b0*/ 0x40, 0x0E, 0x80, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xE4, 0x00, 0x00, 0x00, 0x00, /*01c0*/ 0x40, 0x0E, 0x80, 0xE8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xEC, 0x00, 0x00, 0x00, 0x00, /*01d0*/ 0x40, 0x0E, 0x80, 0xF0, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xF4, 0x00, 0x00, 0x00, 0x00, /*01e0*/ 0x40, 0x0E, 0x80, 0xF8, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x80, 0xFC, 0x00, 0x00, 0x00, 0x00, /*01f0*/ 0x40, 0x0E, 0x81, 0x00, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x81, 0x04, 0x00, 0x00, 0x00, 0x00, /*0200*/ 0x40, 0x0E, 0x81, 0x08, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0E, 0x82, 0x54, 0x00, 0x00, 0x00, 0x08, /*0210*/ 0x40, 0x0E, 0x82, 0x58, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x5C, 0x00, 0x00, 0x00, 0x08, /*0220*/ 0x40, 0x0E, 0x82, 0x60, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x64, 0x00, 0x00, 0x00, 0x08, /*0230*/ 0x40, 0x0E, 0x82, 0x68, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x6C, 0x00, 0x00, 0x00, 0x08, /*0240*/ 0x40, 0x0E, 0x82, 0x70, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x74, 0x00, 0x00, 0x00, 0x08, /*0250*/ 0x40, 0x0E, 0x82, 0x78, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x7C, 0x00, 0x00, 0x00, 0x08, /*0260*/ 0x40, 0x0E, 0x82, 0x80, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x84, 0x00, 0x00, 0x00, 0x08, /*0270*/ 0x40, 0x0E, 0x82, 0x88, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x8C, 0x00, 0x00, 0x00, 0x08, /*0280*/ 0x40, 0x0E, 0x82, 0x90, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x94, 0x00, 0x00, 0x00, 0x08, /*0290*/ 0x40, 0x0E, 0x82, 0x98, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0x9C, 0x00, 0x00, 0x00, 0x08, /*02a0*/ 0x40, 0x0E, 0x82, 0xA0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xA4, 0x00, 0x00, 0x00, 0x08, /*02b0*/ 0x40, 0x0E, 0x82, 0xA8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xAC, 0x00, 0x00, 0x00, 0x08, /*02c0*/ 0x40, 0x0E, 0x82, 0xB0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xB4, 0x00, 0x00, 0x00, 0x08, /*02d0*/ 0x40, 0x0E, 0x82, 0xB8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xBC, 0x00, 0x00, 0x00, 0x08, /*02e0*/ 0x40, 0x0E, 0x82, 0xC0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xC4, 0x00, 0x00, 0x00, 0x08, /*02f0*/ 0x40, 0x0E, 0x82, 0xC8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xCC, 0x00, 0x00, 0x00, 0x08, /*0300*/ 0x40, 0x0E, 0x82, 0xD0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xD4, 0x00, 0x00, 0x00, 0x08, /*0310*/ 0x40, 0x0E, 0x82, 0xD8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xDC, 0x00, 0x00, 0x00, 0x08, /*0320*/ 0x40, 0x0E, 0x82, 0xE0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xE4, 0x00, 0x00, 0x00, 0x08, /*0330*/ 0x40, 0x0E, 0x82, 0xE8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xEC, 0x00, 0x00, 0x00, 0x08, /*0340*/ 0x40, 0x0E, 0x82, 0xF0, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xF4, 0x00, 0x00, 0x00, 0x08, /*0350*/ 0x40, 0x0E, 0x82, 0xF8, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x82, 0xFC, 0x00, 0x00, 0x00, 0x08, /*0360*/ 0x40, 0x0E, 0x83, 0x00, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x04, 0x00, 0x00, 0x00, 0x08, /*0370*/ 0x40, 0x0E, 0x83, 0x08, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x0C, 0x00, 0x00, 0x00, 0x08, /*0380*/ 0x40, 0x0E, 0x83, 0x10, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x14, 0x00, 0x00, 0x00, 0x08, /*0390*/ 0x40, 0x0E, 0x83, 0x18, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x1C, 0x00, 0x00, 0x00, 0x08, /*03a0*/ 0x40, 0x0E, 0x83, 0x20, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x24, 0x00, 0x00, 0x00, 0x08, /*03b0*/ 0x40, 0x0E, 0x83, 0x28, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x2C, 0x00, 0x00, 0x00, 0x08, /*03c0*/ 0x40, 0x0E, 0x83, 0x30, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x34, 0x00, 0x00, 0x00, 0x08, /*03d0*/ 0x40, 0x0E, 0x83, 0x38, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x83, 0x3C, 0x00, 0x00, 0x00, 0x08, /*03e0*/ 0x40, 0x0E, 0x84, 0x00, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x84, 0x04, 0x00, 0x00, 0x00, 0x08, /*03f0*/ 0x40, 0x0E, 0x84, 0x08, 0x00, 0x00, 0x00, 0x08, 0x40, 0x0E, 0x84, 0x0C, 0x00, 0x00, 0x00, 0x08, /*0400*/ 0x40, 0x0D, 0x40, 0x00, 0x10, 0x00, 0x00, 0x04, 0x40, 0x0D, 0x40, 0x08, 0x00, 0x00, 0x00, 0x81, /*0410*/ 0x40, 0x0D, 0x40, 0x0C, 0x00, 0x00, 0x00, 0x81, 0x40, 0x0D, 0x40, 0x10, 0x80, 0x00, 0x00, 0x1D, /*0420*/ 0x40, 0x0D, 0x40, 0x40, 0x00, 0x00, 0x0F, 0x32, 0x40, 0x0D, 0x40, 0x44, 0x00, 0x77, 0x2A, 0x22, /*0430*/ 0x40, 0x0D, 0x40, 0x48, 0x00, 0x01, 0x0A, 0x0D, 0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x04, 0x08, /*0440*/ 0x40, 0x0D, 0x40, 0x90, 0x80, 0x00, 0x00, 0x00, 0x40, 0x0D, 0x40, 0x94, 0x00, 0x00, 0x00, 0x02, /*0450*/ 0x40, 0x0D, 0x40, 0x98, 0x00, 0x00, 0x00, 0x00, 0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0F, /*0460*/ 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, /*0470*/ 0xC0, 0x00, 0x04, 0x00, 0xCC, 0x00, 0x14, 0x04, 0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03, /*0480*/ 0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, /*0490*/ 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xCC, 0x00, 0x14, 0x04, /*04a0*/ 0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03, 0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C, /*04b0*/ 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, /*04c0*/ 0xC0, 0x00, 0x04, 0x00, 0xCC, 0x00, 0x1C, 0x04, 0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03, /*04d0*/ 0x40, 0x0D, 0x40, 0xA0, 0x00, 0x00, 0x00, 0x33, 0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0A, /*04e0*/ 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, 0xC0, 0x00, 0x04, 0x00, /*04f0*/ 0xC0, 0x00, 0x04, 0x00, 0xCC, 0x00, 0x14, 0x04, 0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03, /*0500*/ 0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x04, 0x09, }; /* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */ #else const uint8_t dcd_data[] = {0x00}; #endif /* XIP_BOOT_HEADER_DCD_ENABLE */ #endif /* XIP_BOOT_HEADER_ENABLE */