Starting kernel ... Linux version 2.6.35.3-01073-g90430a4-dirty (xavier@xavier-ubuntu-4138) (gcc version 4.4.0 (GCC) ) #143 PREEMPT Fri Sep 23 15:50:34 CEST 2011 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: Freescale MX53 LOCO Board Memory policy: ECC disabled, Data cache writeback Built 1 zonelists in Zone order, mobility grouping on. Total pages: 234496 Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 di0_primary calibration ip=dhcp PID hash table entries: 4096 (order: 2, 16384 bytes) Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 416MB 512MB = 928MB total Memory: 931984k/931984k available, 18288k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xf9e00000 - 0xffe00000 ( 96 MB) vmalloc : 0xe0800000 - 0xf4000000 ( 312 MB) lowmem : 0x80000000 - 0xe0000000 (1536 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .init : 0x80008000 - 0x80039000 ( 196 kB) .text : 0x80039000 - 0x80876000 (8436 kB) .data : 0x808a0000 - 0x80905240 ( 405 kB) SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Hierarchical RCU implementation. RCU-based detection of stalled CPUs is disabled. Verbose stalled-CPUs detection is disabled. NR_IRQS:368 MXC GPIO hardware MXC IRQ initialized MXC_Early serial console at MMIO 0x53fbc000 (options '115200') bootconsole [ttymxc0] enabled Console: colour dummy device 80x30 Calibrating delay loop... 999.42 BogoMIPS (lpj=4997120) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok regulator: core version 0.5 NET: Registered protocol family 16 i.MX IRAM pool: 128 KB@0xe0840000 IRAM READY CPU is i.MX53 Revision 2.1 Using SDMA I.API MXC DMA API initialized IMX usb wakeup probe IMX usb wakeup probe bio: create slab at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb da9052_ssc_i2c 0-0048: 2 - da9052_i2c_read:master_xfer Failed!! da9052_i2c_is_connected - i2c read failed............. IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) Advanced Linux Sound Architecture Driver Version 1.0.23. Bluetooth: Core ver 2.15 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized Switching to clocksource mxc_timer1 NET: Registered protocol family 2 IP route cache hash table entries: 32768 (order: 5, 131072 bytes) TCP established hash table entries: 131072 (order: 8, 1048576 bytes) TCP bind hash table entries: 65536 (order: 6, 262144 bytes) TCP: Hash tables configured (established 131072 bind 65536) TCP reno registered UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. Unpacking initramfs... Freeing initrd memory: 176K LPMode driver module loaded Static Power Management for Freescale i.MX5 PM driver module loaded sdram autogating driver module loaded Bus freq driver module loaded DI0 is primary DVFS driver module loaded i.MXC CPU frequency driver mxc_cpufreq_driver_init: failed to get gp regulator ashmem: initialized msgmni has been set to 1820 alg: No test for stdrng (krng) cryptodev: driver loaded. io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) regulator: get() with no identifier By setting, SII driver will not be enabled By setting, LDB driver will not be enabled mxc_ipu mxc_ipu: Channel already disabled 9 mxc_ipu mxc_ipu: Channel already uninitialized 9 mxc_ipu mxc_ipu: Channel already disabled 7 mxc_ipu mxc_ipu: Channel already uninitialized 7 mxc_ipu mxc_ipu: Channel already disabled 10 mxc_ipu mxc_ipu: Channel already uninitialized 10 Serial: MXC Internal UART driver mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX console [ttymxc0] enabled, bootconsole disabled console [ttymxc0] enabled, bootconsole disabled mxcintuart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a Freescale i.MX mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 33) is a Freescale i.MX mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX mxcintuart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a Freescale i.MX loop: module loaded pmem_adsp: 0 init pmem_gpu: 1 init MXC MTD nand Driver 3.0 i.MX GPMI NFC vcan: Virtual CAN interface driver Freescale FlexCAN Driver FEC Ethernet Driver fec_enet_mii_bus: probed PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered PPP MPPE Compression module registered NET: Registered protocol family 24 tun: Universal TUN/TAP device driver, 1.6 tun: (C) 1999-2004 Max Krasnyansky ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 1 fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200 fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. usbcore: registered new interface driver usbserial usbserial: USB Serial Driver core USB Serial support registered for GSM modem (1-port) usbcore: registered new interface driver option option: v0.7.2:USB Driver for GSM modems ARC USBOTG Device Controller driver (1 August 2005) Android usb driver initialize android_usb gadget: android_usb ready fsl-usb2-udc: bind to driver android_usb android gadget: register function adb android gadget: register function usb_mass_storage android gadget: register function rndis rndis_function_bind_config MAC: 00:00:00:00:00:00 android_usb gadget: using random self ethernet address android_usb gadget: using random host ethernet address usb0: MAC 7e:48:c6:3a:1b:f2 usb0: HOST MAC 82:24:bb:e9:7b:e9 android_usb gadget: usb_mass_storage, version: 2009/09/11 android_usb gadget: Number of LUNs=3 lun0: LUN: removable file: (no medium) lun1: LUN: removable file: (no medium) lun2: LUN: removable file: (no medium) mice: could not register psaux device, error: -16 mice: PS/2 mouse device common for all mice input: gpio-keys as /devices/platform/gpio-keys/input/input0 MXC keypad loaded usbcore: registered new interface driver usbtouchscreen using rtc device, mxc_rtc, for alarms mxc_rtc mxc_rtc.0: rtc core: registered mxc_rtc as rtc0 usb 1-1: new full speed USB device using fsl-ehci and address 2 i2c /dev entries driver IR NEC protocol handler initialized IR RC5(x) protocol handler initialized IR RC6 protocol handler initialized IR JVC protocol handler initialized IR Sony protocol handler initialized Linux video capture interface: v2.00 mxc_v4l2_output mxc_v4l2_output.0: Registered device video1 usbcore: registered new interface driver uvcvideo USB Video Class driver (v0.1.0) APM Battery Driver MXC WatchDog Driver 2.0 MXC Watchdog # 0 Timer: initial timeout 60 sec device-mapper: ioctl: 4.17.0-ioctl (2010-03-05) initialised: dm-devel@redhat.com Bluetooth: Virtual HCI driver ver 1.3 Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCIATH3K protocol initialized Bluetooth: Generic Bluetooth USB driver ver 0.6 usbcore: registered new interface driver btusb VPU initialized mxc_asrc registered gpu mmu enabled mxsdhci: MXC Secure Digital Host Controller Interface driver mxsdhci: MXC SDHCI Controller Driver. mmc0: SDHCI detect irq 0 irq 1 INTERNAL DMA mxsdhci: MXC SDHCI Controller Driver. mmc1: SDHCI detect irq 203 irq 3 INTERNAL DMA usbcore: registered new interface driver usbhid usbhid: USB HID core driver logger: created 64K log 'log_main' logger: created 256K log 'log_events' logger: created 64K log 'log_radio' logger: created 64K log 'log_system' Cirrus Logic CS42888 ALSA SoC Codec Driver input: eGalax Inc. USB TouchController as /devices/platform/fsl-ehci.1/usb1/1-1/1-1:1.0/input/input1 sgtl5000-i2c 1-000a: SGTL5000 revision 17 generic-usb 0003:0EEF:7304.0001: input: USB HID v2.10 Pointer [eGalax Inc. USB TouchController] on usb-fsl-ehci.1-1/input0 mxc_spdif mxc_spdif.0: MXC SPDIF Audio Transmitter No device for codec mxc spdif No device for DAI mxc spdif No device for DAI imx-ssi-1-0 No device for DAI imx-ssi-1-1 No device for DAI imx-ssi-2-0 No device for DAI imx-ssi-2-1 No device for DAI imx-spdif-dai capture=0 ext_ram=0 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=f8016000 buf->area=e0856000 size=24576 capture=1 ext_ram=0 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=cf428000 buf->area=fb02b000 size=24576 asoc: SGTL5000 <-> imx-ssi-2-0 mapping ok mmc0: new high speed SD card at address 0002 mmcblk0: mmc0:0002 00000 1.90 GiB mmcblk0: p1 p2 p3 < p5 p6 > p4 capture=0 ext_ram=1 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=cf458000 buf->area=fb031000 size=24576 asoc: mxc spdif <-> imx-spdif-dai mapping ok ALSA device list: #0: imx-3stack (SGTL5000) #1: imx-3stack-spdif (mxc spdif) nf_conntrack version 0.5.0 (14565 buckets, 58260 max) IPv4 over IPv4 tunneling driver GRE over IPv4 tunneling driver ip_tables: (C) 2000-2006 Netfilter Core Team TCP cubic registered NET: Registered protocol family 10 IPv6 over IPv4 tunneling driver NET: Registered protocol family 17 NET: Registered protocol family 15 can: controller area network core (rev 20090105 abi 8) NET: Registered protocol family 29 can: raw protocol (rev 20090105) can: broadcast manager protocol (rev 20090105 t) Bluetooth: L2CAP ver 2.14 Bluetooth: L2CAP socket layer initialized Bluetooth: SCO (Voice Link) ver 0.6 Bluetooth: SCO socket layer initialized Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: HIDP (Human Interface Emulation) ver 1.2 L2TP core driver, V2.0 PPPoL2TP kernel driver, V2.0 VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2 mxc_rtc mxc_rtc.0: setting system clock to 1970-01-02 00:05:18 UTC (86718) eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1) ADDRCONF(NETDEV_UP): usb0: link is not ready Sending DHCP requests . PHY: 0:00 - Link is Up - 100/Full DHCP/BOOTP: Ignoring delayed packet ., OK IP-Config: Got DHCP answer from 0.0.0.0, my address is 172.17.10.54 IP-Config: Complete: device=eth0, addr=172.17.10.54, mask=255.255.0.0, gw=172.17.240.245, host=172.17.10.54, domain=TREM.BOD, nis-domain=(none), bootserver=0.0.0.0, rootserver=0.0.0.0, rootpath= Freeing init memory: 196K init: cannot open '/initlogo.rle' EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) EXT4-fs (mmcblk0p5): warning: maximal mount count reached, running e2fsck is recommended EXT4-fs (mmcblk0p5): recovery complete EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null) EXT4-fs (mmcblk0p6): warning: maximal mount count reached, running e2fsck is recommended EXT4-fs (mmcblk0p6): recovery complete EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null) init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery' enabling adb # warning: `rild' uses 32-bit capabilities (legacy support in use) pmem: request for physical address of pmem region from process 2067. request_suspend_state: on (3->0) at 18950314378 (1970-01-02 00:05:35.465766251 UTC) Not all allocated memory blocks were freed. Doing it now. Freeing list entry #0, gpuaddr=166000 Freeing list entry #1, gpuaddr=167000 Freeing list entry #2, gpuaddr=177000 Freeing list entry #3, gpuaddr=1a9000 Freeing list entry #6, gpuaddr=1fa000 Freeing list entry #7, gpuaddr=1fc000 Freeing list entry #8, gpuaddr=21c000 Freeing list entry #104, gpuaddr=e50000 #