ERROR: linux-imx-6.6.36+git-r0 do_patch: Could not apply patches for imx93frdm. ERROR: linux-imx-6.6.36+git-r0 do_patch: Patch failures can be resolved in the linux source directory /home/ad/POC/yocto_imx/frdm-imx93/tmp/work/imx93frdm-poky-linux/linux-imx/6.6.36+git/git) ERROR: linux-imx-6.6.36+git-r0 do_patch: ExecutionError('/home/ad/POC/yocto_imx/frdm-imx93/tmp/work/imx93frdm-poky-linux/linux-imx/6.6.36+git/temp/run.do_patch.1766297', 1, None, None) ERROR: Logfile of failure stored in: /home/ad/POC/yocto_imx/frdm-imx93/tmp/work/imx93frdm-poky-linux/linux-imx/6.6.36+git/temp/log.do_patch.1766297 Log data follows: | DEBUG: Executing python function extend_recipe_sysroot | NOTE: Direct dependencies are ['/home/ad/POC/yocto_imx/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_populate_sysroot', '/home/ad/POC/yocto_imx/sources/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot', 'virtual:native:/home/ad/POC/yocto_imx/sources/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot'] | NOTE: Installed into sysroot: [] | NOTE: Skipping as already exists in sysroot: ['gettext-minimal-native', 'cmake-native', 'libtool-native', 'quilt-native', 'texinfo-dummy-native', 'kern-tools-native', 'openssl-native', 'expat-native', 'ncurses-native', 'zlib-native', 'git-native', 'make-native', 'patch-native', 'perl-native', 'bzip2-native', 'xz-native', 'zstd-native', 'attr-native', 'ca-certificates-native', 'curl-native', 'gdbm-native'] | DEBUG: Python function extend_recipe_sysroot finished | DEBUG: Executing shell function do_patch | [INFO]: fence post found, starting after: patches//./0005-Add-CTP-support-for-waveshare-panel.patch | (6/20) 0006-arm64-dts-add-imx93-11x11-frdm-tianma-wvga-panel-dts.patch | [INFO]: check of .kernel-meta//patches//./0006-arm64-dts-add-imx93-11x11-frdm-tianma-wvga-panel-dts.patch with "git am" did not pass, trying reduced context. | [INFO]: Context reduced git-am of .kernel-meta//patches//./0006-arm64-dts-add-imx93-11x11-frdm-tianma-wvga-panel-dts.patch with "git am" did not work, trying "apply". | error: unable to normalize alternate object path: /home/ad/POC/yocto_imx/downloads//git2/github.com.nxp-imx.linux-imx.git//objects | error: unable to normalize alternate object path: /home/ad/POC/yocto_imx/downloads//git2/github.com.nxp-imx.linux-imx.git//objects | error: unable to normalize alternate object path: /home/ad/POC/yocto_imx/downloads//git2/github.com.nxp-imx.linux-imx.git//objects | fatal: update_ref failed for ref 'ORIG_HEAD': cannot update ref 'ORIG_HEAD': trying to write ref 'ORIG_HEAD' with nonexistent object d23d64eea5111e1607efcce1d601834fceec92cb | error: unable to normalize alternate object path: /home/ad/POC/yocto_imx/downloads//git2/github.com.nxp-imx.linux-imx.git//objects | error: unable to normalize alternate object path: /home/ad/POC/yocto_imx/downloads//git2/github.com.nxp-imx.linux-imx.git//objects | error: failed to read arch/arm64/boot/dts/freescale/Makefile | error: arch/arm64/boot/dts/freescale/Makefile: patch does not apply | [ERROR]: Application of .kernel-meta//patches//./0006-arm64-dts-add-imx93-11x11-frdm-tianma-wvga-panel-dts.patch failed. | Patch needs to be refreshed. Sample resolution script: | .git/rebase-apply/resolve_rejects | ERROR: Could not apply patches for imx93frdm. | ERROR: Patch failures can be resolved in the linux source directory /home/ad/POC/yocto_imx/frdm-imx93/tmp/work/imx93frdm-poky-linux/linux-imx/6.6.36+git/git) | WARNING: exit code 1 from a shell command. ERROR: Task (/home/ad/POC/yocto_imx/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_patch) failed with exit code '1' NOTE: Tasks Summary: Attempted 3043 tasks of which 3036 didn't need to be rerun and 1 failed. Summary: 1 task failed: /home/ad/POC/yocto_imx/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_patch Summary: There were 3 ERROR messages, returning a non-zero exit code.