[Header] Version = 4.3 Hash Algorithm = sha256 Engine = CAAM Engine Configuration = 0 Certificate Format = X509 Signature Format = CMS [Install SRK] # Index of the key location in the SRK table to be installed File = "../cst-3.4.1/crts/SRK_1_2_3_4_table.bin" Source index = 0 [Install CSFK] # Key used to authenticate the CSF data File = "../cst-3.4.1/crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem" [Authenticate CSF] [Install Key] # Key slot index used to authenticate the key to be installed Verification index = 0 # Target key slot in HAB key store where key will be installed Target index = 2 # Key to install File = "../cst-3.4.1/crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem" [Authenticate Data] # Key slot index used to authenticate the image data Verification index = 2 # Authenticate Start Address, Offset, Length and file Blocks = 0x401fcdc0 0x58000 0x1020 "flash.bin", \ 0x40200000 0x5B000 0x102040 "flash.bin", \ 0x40302040 0x15D040 0xCBB0 "flash.bin", \ 0x970000 0x169BF0 0xB150 "flash.bin", \ 0x56000000 0x174D40 0x7CFA0 "flash.bin"