U-Boot SPL 2022.04-lf_v2022.04+g1c881f4 (Jun 07 2022 - 05:16:02 +0000) Normal Boot Trying to boot from MMC2_2 Primary set selected Load image from MMC/SD 0x7b000 U-Boot 2022.04-lf_v2022.04+g1c881f4 (Jun 07 2022 - 05:16:02 +0000) CPU: NXP i.MX8QM RevB A53 at 1200 MHz at 27C Model: NXP i.MX8QM MEK Board: iMX8QM MEK Boot: SD1 DRAM: 5.8 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x51] Core: 183 devices, 29 uclasses, devicetree: separate MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from MMC... OK [*]-Video Link 0it6263_i2c_reg_read, read err 3 faill to read from it6263 revision, ret 3 (1280 x 720) [0] dpu@56180000, video [1] lvds-channel@0, display [2] lvds-to-hdmi-bridge@4c, video_bridge In: serial Out: serial Err: serial BuildInfo: - SCFW 8172eaea, SECO-FW c9de51c0, IMX-MKIMAGE a8bb8edb, ATF c6a19b1 - U-Boot 2022.04-lf_v2022.04+g1c881f4 switch to partitions #0, OK mmc1 is current device flash target is MMC:1 Net: eth0: ethernet@5b040000 [PRIME], eth1: ethernet@5b050000 Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device Failed to load 'boot.scr' 30931456 bytes read in 345 ms (85.5 MiB/s) Booting from mmc ... 106496 bytes read in 3 ms (33.9 MiB/s) Loading hdp firmware from 0x000000009c000000 offset 0x0000000000002000 Loading hdp firmware Complete 135035 bytes read in 4 ms (32.2 MiB/s) ## Flattened Device Tree blob at 83000000 Booting using the fdt blob at 0x83000000 ERROR: reserving fdt memory region failed (addr=901ff000 size=1000 flags=4) Using Device Tree in place at 0000000083000000, end 0000000083023f7a Disable pwm@5a190000 rsrc 188 not owned Disable clock-controller@5a590000 rsrc 188 not owned Disable jr@40000 rsrc 502 not owned Disable mu@31580000 rsrc 505 not owned Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.15.32-lts-next+gfa6c316 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.2.0, GNU SMP PREEMPT Tue Jun 7 02:34:46 UTC 2022 [ 0.000000] Machine model: Freescale i.MX8QM MEK [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 960 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool [ 0.000000] earlycon: lpuart32 at MMIO32 0x000000005a060000 (options '') [ 0.000000] printk: bootconsole [lpuart32] enabled [ 0.000000] NUMA: No NUMA configuration found [ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x000000097fffffff] [ 0.000000] NUMA: NODE_DATA [mem 0x97f457800-0x97f459fff] [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080200000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x000000097fffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff] [ 0.000000] node 0: [mem 0x0000000084000000-0x00000000863fffff] [ 0.000000] node 0: [mem 0x0000000086400000-0x0000000087ffffff] [ 0.000000] node 0: [mem 0x0000000092000000-0x0000000094bfffff] [ 0.000000] node 0: [mem 0x0000000094c00000-0x00000000fdffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x000000088fffffff] [ 0.000000] node 0: [mem 0x0000000890000000-0x000000097fffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 20 pages/cpu s41176 r8192 d32552 u81920 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1499400 [ 0.000000] Policy zone: Normal [ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw cpufreq.default_ [ 0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear) [ 0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0x00000000bc000000-0x00000000c0000000] (64MB) [ 0.000000] Memory: 4547508K/6092800K available (18560K kernel code, 1534K rwdata, 7072K rodata, 2944K init, 541a-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=6. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 512 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000 [ 0.000000] ITS: No ITS available, not enabling LPIs [ 0.000000] random: get_random_bytes called from start_kernel+0x474/0x660 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 44079520 [ 0.000001] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns [ 0.008791] Console: colour dummy device 80x25 [ 0.012968] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000 [ 0.023145] pid_max: default: 32768 minimum: 301 [ 0.027804] LSM: Security Framework initializing [ 0.032425] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.039937] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.049397] rcu: Hierarchical SRCU implementation. [ 0.055948] EFI services will not be available. [ 0.060381] smp: Bringing up secondary CPUs ... [ 0.065758] Detected VIPT I-cache on CPU1 [ 0.065792] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000 [ 0.065839] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.066953] Detected VIPT I-cache on CPU2 [ 0.066971] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000 [ 0.066995] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.068059] Detected VIPT I-cache on CPU3 [ 0.068076] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000 [ 0.068099] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.070302] CPU features: detected: Spectre-v2 [ 0.070310] CPU features: detected: Spectre-v3a [ 0.070313] CPU features: detected: Spectre-BHB [ 0.070319] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.070322] Detected PIPT I-cache on CPU4 [ 0.070338] GICv3: CPU4: found redistributor 100 region 0:0x0000000051b80000 [ 0.070363] CPU4: Booted secondary processor 0x0000000100 [0x410fd082] [ 0.071458] Detected PIPT I-cache on CPU5 [ 0.071471] GICv3: CPU5: found redistributor 101 region 0:0x0000000051ba0000 [ 0.071488] CPU5: Booted secondary processor 0x0000000101 [0x410fd082] [ 0.071549] smp: Brought up 1 node, 6 CPUs [ 0.182958] SMP: Total of 6 processors activated. [ 0.187645] CPU features: detected: 32-bit EL0 Support [ 0.192776] CPU features: detected: 32-bit EL1 Support [ 0.197895] CPU features: detected: CRC32 instructions [ 0.217211] CPU: All CPU(s) started at EL2 [ 0.220996] alternatives: patching kernel code [ 0.226564] devtmpfs: initialized [ 0.245976] KASLR disabled due to lack of seed [ 0.250239] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.259830] futex hash table entries: 2048 (order: 5, 131072 bytes, linear) [ 0.305505] pinctrl core: initialized pinctrl subsystem [ 0.311069] DMI not present or invalid. [ 0.314987] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.325254] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations [ 0.332582] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.340673] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.348433] audit: initializing netlink subsys (disabled) [ 0.353872] audit: type=2000 audit(0.256:1): state=initialized audit_enabled=0 res=1 [ 0.354474] thermal_sys: Registered thermal governor 'step_wise' [ 0.361464] thermal_sys: Registered thermal governor 'power_allocator' [ 0.368111] cpuidle: using governor menu [ 0.378466] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.385108] ASID allocator initialised with 65536 entries [ 0.392337] Serial: AMBA PL011 UART driver [ 0.396147] imx mu driver is registered. [ 0.400011] imx rpmsg driver is registered. [ 0.463694] platform bus@57240000:ldb@572410e0: Fixing up cyclic dependency with 57180000.dpu [ 0.477234] platform 57228000.dsi_host: Fixing up cyclic dependency with 57180000.dpu [ 0.487453] platform 56268000.hdmi: Fixing up cyclic dependency with 56180000.dpu [ 0.512506] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.518913] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.525568] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.532255] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.540057] cryptd: max_cpu_qlen set to 1000 [ 0.548455] ACPI: Interpreter disabled. [ 0.553941] iommu: Default domain type: Translated [ 0.558484] iommu: DMA domain TLB invalidation policy: strict mode [ 0.564933] vgaarb: loaded [ 0.567697] SCSI subsystem initialized [ 0.571488] usbcore: registered new interface driver usbfs [ 0.576665] usbcore: registered new interface driver hub [ 0.581955] usbcore: registered new device driver usb [ 0.589102] mc: Linux media interface: v0.10 [ 0.593054] videodev: Linux video capture interface: v2.00 [ 0.598596] pps_core: LinuxPPS API ver. 1 registered [ 0.603458] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.612589] PTP clock support registered [ 0.616844] EDAC MC: Ver: 3.0.0 [ 0.621572] FPGA manager framework [ 0.624702] Advanced Linux Sound Architecture Driver Initialized. [ 0.631257] Bluetooth: Core ver 2.22 [ 0.634506] NET: Registered PF_BLUETOOTH protocol family [ 0.639790] Bluetooth: HCI device and connection manager initialized [ 0.646135] Bluetooth: HCI socket layer initialized [ 0.650998] Bluetooth: L2CAP socket layer initialized [ 0.656043] Bluetooth: SCO socket layer initialized [ 0.661795] imx-scu scu: NXP i.MX SCU Initialized [ 0.681551] random: fast init done [ 0.696254] imx8qm-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp [ 0.705695] imx8qm-pinctrl scu:pinctrl: initialized IMX pinctrl driver [ 0.714918] clocksource: Switched to clocksource arch_sys_counter [ 0.720862] VFS: Disk quotas dquot_6.6.0 [ 0.724629] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.731620] pnp: PnP ACPI: disabled [ 0.769455] NET: Registered PF_INET protocol family [ 0.774323] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.784510] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear) [ 0.792818] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.801014] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear) [ 0.808938] TCP: Hash tables configured (established 65536 bind 65536) [ 0.815252] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear) [ 0.822046] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear) [ 0.829351] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.835165] RPC: Registered named UNIX socket transport module. [ 0.840762] RPC: Registered udp transport module. [ 0.845434] RPC: Registered tcp transport module. [ 0.850123] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.857285] PCI: CLS 0 bytes, default 64 [ 0.861590] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.871155] kvm [1]: IPA Size Limit: 40 bits [ 0.876238] kvm [1]: vgic-v2@52020000 [ 0.879572] kvm [1]: GIC system register CPU interface enabled [ 0.885490] kvm [1]: vgic interrupt IRQ9 [ 0.889464] kvm [1]: Hyp mode initialized successfully [ 0.898003] Initialise system trusted keyrings [ 0.902235] workingset: timestamp_bits=42 max_order=21 bucket_order=0 [ 0.913989] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.919982] NFS: Registering the id_resolver key type [ 0.924719] Key type id_resolver registered [ 0.928867] Key type id_legacy registered [ 0.932934] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.939573] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.946961] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 0.953346] 9p: Installing v9fs 9p2000 file system support [ 0.993551] Key type asymmetric registered [ 0.997310] Asymmetric key parser 'x509' registered [ 1.002216] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243) [ 1.009558] io scheduler mq-deadline registered [ 1.014075] io scheduler kyber registered [ 1.037860] EINJ: ACPI disabled. [ 1.218748] mxs-dma 5b810000.dma-apbh: initialized [ 1.227564] Bus freq driver module loaded [ 1.239408] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 1.250052] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 69, base_baud = 5000000) is a FSL_LPUAR[ 1.2592d [ 1.259224] printk: console [ttyLP0] enabled [ 1.267642] printk: bootconsole [lpuart32] disabled [ 1.267642] printk: bootconsole [lpuart32] disabled [ 1.278135] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 70, base_baud = 5000000) is a FSL_LPUART [ 1.289431] arm-smmu 51400000.iommu: probing hardware configuration... [ 1.295983] arm-smmu 51400000.iommu: SMMUv2 with: [ 1.300700] arm-smmu 51400000.iommu: stage 1 translation [ 1.306112] arm-smmu 51400000.iommu: stage 2 translation [ 1.311522] arm-smmu 51400000.iommu: nested translation [ 1.316852] arm-smmu 51400000.iommu: stream matching with 32 register groups [ 1.324007] arm-smmu 51400000.iommu: 32 context banks (0 stage-2 only) [ 1.330639] arm-smmu 51400000.iommu: Supported page sizes: 0x61311000 [ 1.337176] arm-smmu 51400000.iommu: Stage-1: 48-bit VA -> 48-bit IPA [ 1.343714] arm-smmu 51400000.iommu: Stage-2: 48-bit IPA -> 48-bit PA [ 1.423207] imx-drm display-subsystem: parent device of /bus@56240000/ldb@562410e0/lvds-channel@0 is not availab [ 1.457875] loop: module loaded [ 1.464356] megasas: 07.717.02.00-rc1 [ 1.471193] imx ahci driver is registered. [ 1.487023] tun: Universal TUN/TAP device driver, 1.6 [ 1.494087] thunder_xcv, ver 1.0 [ 1.497361] thunder_bgx, ver 1.0 [ 1.500634] nicpf, ver 1.0 [ 1.508949] hclge is initializing [ 1.512288] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version [ 1.519519] hns3: Copyright (c) 2017 Huawei Corporation. [ 1.524881] e1000: Intel(R) PRO/1000 Network Driver [ 1.529770] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 1.535557] e1000e: Intel(R) PRO/1000 Network Driver [ 1.540525] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 1.546481] igb: Intel(R) Gigabit Ethernet Network Driver [ 1.551890] igb: Copyright (c) 2007-2014 Intel Corporation. [ 1.557508] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 1.563781] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 1.570143] sky2: driver version 1.30 [ 1.575255] usbcore: registered new interface driver r8152 [ 1.580980] VFIO - User Level meta-driver version: 0.3 [ 1.591532] cdns3-imx 5b110000.usb: Adding to iommu group 0 [ 1.599537] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.606087] ehci-pci: EHCI PCI platform driver [ 1.610602] ehci-platform: EHCI generic platform driver [ 1.616577] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 1.622807] ohci-pci: OHCI PCI platform driver [ 1.627309] ohci-platform: OHCI generic platform driver [ 1.634419] usbcore: registered new interface driver uas [ 1.639778] usbcore: registered new interface driver usb-storage [ 1.645866] usbcore: registered new interface driver usbserial_generic [ 1.652418] usbserial: USB Serial support registered for generic [ 1.658457] usbcore: registered new interface driver ftdi_sio [ 1.664259] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.671622] usbcore: registered new interface driver usb_serial_simple [ 1.678175] usbserial: USB Serial support registered for carelink [ 1.684290] usbserial: USB Serial support registered for zio [ 1.689975] usbserial: USB Serial support registered for funsoft [ 1.696004] usbserial: USB Serial support registered for flashloader [ 1.702384] usbserial: USB Serial support registered for google [ 1.708321] usbserial: USB Serial support registered for libtransistor [ 1.714872] usbserial: USB Serial support registered for vivopay [ 1.720900] usbserial: USB Serial support registered for moto_modem [ 1.727303] usbserial: USB Serial support registered for motorola_tetra [ 1.734012] usbserial: USB Serial support registered for novatel_gps [ 1.740477] usbserial: USB Serial support registered for hp4x [ 1.746297] usbserial: USB Serial support registered for suunto [ 1.752255] usbserial: USB Serial support registered for siemens_mpi [ 1.758693] usbcore: registered new interface driver usb_ehset_test [ 1.773324] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0 [ 1.782786] imx-sc-rtc scu:rtc: registered as rtc0 [ 1.787924] imx-sc-rtc scu:rtc: setting system clock to 1970-01-01T00:06:42 UTC (402) [ 1.796656] i2c_dev: i2c /dev entries driver [ 1.810764] Bluetooth: HCI UART driver ver 2.3 [ 1.815226] Bluetooth: HCI UART protocol H4 registered [ 1.820377] Bluetooth: HCI UART protocol BCSP registered [ 1.825712] Bluetooth: HCI UART protocol LL registered [ 1.830860] Bluetooth: HCI UART protocol ATH3K registered [ 1.836279] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 1.842760] Bluetooth: HCI UART protocol Broadcom registered [ 1.848444] Bluetooth: HCI UART protocol QCA registered [ 1.858776] sdhci: Secure Digital Host Controller Interface driver [ 1.864982] sdhci: Copyright(c) Pierre Ossman [ 1.871266] Synopsys Designware Multimedia Card Interface Driver [ 1.879104] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.886946] sdhci-esdhc-imx 5b010000.mmc: Adding to iommu group 1 [ 1.893210] ledtrig-cpu: registered to indicate activity on CPUs [ 1.901943] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 1.908887] usbcore: registered new interface driver usbhid [ 1.914475] usbhid: USB HID core driver [ 1.921436] mxc-isi 58100000.isi: mxc_isi.0 registered successfully [ 1.928609] mxc-isi 58110000.isi: mxc_isi.1 registered successfully [ 1.931010] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA [ 1.935555] mxc-isi 58120000.isi: mxc_isi.2 registered successfully [ 1.948896] mxc-isi 58130000.isi: mxc_isi.3 registered successfully [ 1.955827] mxc-isi 58140000.isi: mxc_isi.4 registered successfully [ 1.962738] mxc-isi 58150000.isi: mxc_isi.5 registered successfully [ 1.969661] mxc-isi 58160000.isi: mxc_isi.6 registered successfully [ 1.976572] mxc-isi 58170000.isi: mxc_isi.7 registered successfully [ 1.995421] cs_system_cfg: CoreSight Configuration manager initialised [ 2.005679] optee: probing for conduit method. [ 2.010158] optee: revision 3.17 (98499642) [ 2.011141] optee: initialized driver [ 2.026251] Galcore version 6.4.3.p4.398061 [ 2.039050] mmc0: new HS400 MMC card at address 0001 [ 2.044634] mmcblk0: mmc0:0001 R1J57L 29.1 GiB [ 2.045029] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu1_ss on minor 0 [ 2.058653] Alternate GPT is invalid, using primary GPT. [ 2.059112] mxc_emvsim 5a0d0000.sim0: emvsim register success [ 2.064031] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17 p18 p19 p20 p21 [ 2.076084] NET: Registered PF_LLC protocol family [ 2.080909] mmcblk0boot0: mmc0:0001 R1J57L 8.00 MiB [ 2.083636] NET: Registered PF_INET6 protocol family [ 2.089600] mmcblk0boot1: mmc0:0001 R1J57L 8.00 MiB [ 2.094011] Segment Routing with IPv6 [ 2.099296] mmcblk0rpmb: mmc0:0001 R1J57L 4.00 MiB, chardev (234:0) [ 2.101940] In-situ OAM (IOAM) with IPv6 [ 2.112151] NET: Registered PF_PACKET protocol family [ 2.117319] Bluetooth: RFCOMM TTY layer initialized [ 2.122227] Bluetooth: RFCOMM socket layer initialized [ 2.127385] Bluetooth: RFCOMM ver 1.11 [ 2.131141] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 2.136457] Bluetooth: BNEP filters: protocol multicast [ 2.141692] Bluetooth: BNEP socket layer initialized [ 2.146656] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 2.152585] Bluetooth: HIDP socket layer initialized [ 2.157876] 8021q: 802.1Q VLAN Support v1.8 [ 2.162075] lib80211: common routines for IEEE802.11 drivers [ 2.167807] 9pnet: Installing 9P2000 support [ 2.172097] tsn generic netlink module v1 init... [ 2.176849] Key type dns_resolver registered [ 2.181368] Loading compiled-in X.509 certificates [ 2.205782] mxs_phy 5b100000.usbphy: supply phy-3p0 not found, using dummy regulator [ 2.238887] imx-lpi2c 58226000.i2c: use pio mode [ 2.244158] i2c 2-006a: Fixing up cyclic dependency with 58227000.csi [ 2.263120] max9286_mipi 2-006a: max9286_read_reg:read reg error: reg=1e [ 2.269854] max9286 is not found, chip id reg 0x1e = 0x(ffffffff) [ 2.276147] i2c i2c-2: LPI2C adapter registered [ 2.282088] imx-lpi2c 58246000.i2c: use pio mode [ 2.287263] i2c 3-006a: Fixing up cyclic dependency with 58247000.csi [ 2.303106] max9286_mipi 3-006a: max9286_read_reg:read reg error: reg=1e [ 2.309841] max9286 is not found, chip id reg 0x1e = 0x(ffffffff) [ 2.316043] i2c i2c-3: LPI2C adapter registered [ 2.321556] imx-lpi2c 5a800000.i2c: use pio mode [ 2.326893] isl29018 4-0044: supply vcc not found, using dummy regulator [ 2.333769] isl29018 4-0044: No cache defaults, reading back from HW [ 2.357842] i2c i2c-4: supply vdd not found, using dummy regulator [ 2.364310] i2c i2c-4: supply vddio not found, using dummy regulator [ 2.403386] max732x 4-0068: failed reading [ 2.407510] max732x: probe of 4-0068 failed with error -5 [ 2.471897] i2c 4-0051: Fixing up cyclic dependency with 5b130000.usb [ 2.480327] i2c i2c-4: LPI2C adapter registered [ 2.486015] gpio-430 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file [ 2.495008] imx-lpi2c 5a810000.i2c: using scl,sda for recovery [ 2.500876] imx-lpi2c 5a810000.i2c: use pio mode [ 2.506196] i2c i2c-5: LPI2C adapter registered [ 2.522230] pwm-backlight lvds_backlight@0: supply power not found, using dummy regulator [ 2.534379] pwm-backlight lvds_backlight@1: supply power not found, using dummy regulator [ 2.563812] dpu-core 56180000.dpu: driver probed [ 2.572005] dpu-core 57180000.dpu: driver probed [ 2.578945] ahci-imx 5f020000.sata: Adding to iommu group 2 [ 2.584801] ahci-imx 5f020000.sata: phy impedance ratio is not specified. [ 2.591661] ahci-imx 5f020000.sata: No cache used with register defaults set! [ 2.599395] ahci-imx 5f020000.sata: supply ahci not found, using dummy regulator [ 2.606919] ahci-imx 5f020000.sata: supply phy not found, using dummy regulator [ 2.614309] ahci-imx 5f020000.sata: supply target not found, using dummy regulator [ 2.622183] ahci-imx 5f020000.sata: external osc is used. [ 2.630459] ahci-imx 5f020000.sata: no ahb clock. [ 2.635248] ahci-imx 5f020000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode [ 2.644154] ahci-imx 5f020000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sadm sds apst [ 2.654900] scsi host0: ahci-imx [ 2.658386] ata1: SATA max UDMA/133 mmio [mem 0x5f020000-0x5f02ffff] port 0x100 irq 127 [ 2.669783] fec 5b040000.ethernet: Adding to iommu group 3 [ 2.676091] pps pps0: new PPS source ptp0 [ 2.683511] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing. [ 2.691439] fec 5b040000.ethernet eth0: registered PHC device 0 [ 2.698839] cdns-usb3 5b130000.usb: Adding to iommu group 0 [ 2.774947] sdhci-esdhc-imx 5b020000.mmc: Adding to iommu group 1 [ 2.781562] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO [ 2.786681] sdhci-esdhc-imx 5b020000.mmc: Got WP GPIO [ 2.794934] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0 [ 2.822931] mxc-mipi-csi2 58247000.csi: lanes: 4, name: mxc-mipi-csi2.1 [ 2.823646] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA [ 2.830534] imx-rproc imx8qm_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb" [ 2.846125] imx-rproc imx8qm_cm4@0: No txdb, ret -22 [ 2.851660] remoteproc remoteproc0: imx-rproc is available [ 2.857226] remoteproc remoteproc0: attaching to imx-rproc [ 2.863245] remoteproc0#vdev0buffer: assigned reserved memory node vdevbuffer [ 2.871044] virtio_rpmsg_bus virtio0: rpmsg host is online [ 2.876568] remoteproc0#vdev0buffer: registered virtio0 (type 7) [ 2.882694] remoteproc0#vdev1buffer: assigned reserved memory node vdevbuffer [ 2.890322] virtio_rpmsg_bus virtio1: rpmsg host is online [ 2.895843] remoteproc0#vdev1buffer: registered virtio1 (type 7) [ 2.901955] remoteproc remoteproc0: remote processor imx-rproc is now attached [ 2.910255] imx-rproc imx8x_cm4@1: mbox_request_channel_byname() could not locate channel named "txdb" [ 2.919577] imx-rproc imx8x_cm4@1: No txdb, ret -22 [ 2.924746] remoteproc remoteproc1: imx-rproc is available [ 2.930320] remoteproc remoteproc1: attaching to imx-rproc [ 2.935929] remoteproc1#vdev0buffer: assigned reserved memory node vdevbuffer [ 2.943561] virtio_rpmsg_bus virtio2: rpmsg host is online [ 2.949085] virtio_rpmsg_bus virtio2: creating channel rpmsg-i2c-channel addr 0x1 [ 2.950896] remoteproc1#vdev0buffer: registered virtio2 (type 7) [ 2.956760] i2c-rpmsg virtio2.rpmsg-i2c-channel.-1.1: new channel: 0x400 -> 0x1! [ 2.962706] remoteproc1#vdev1buffer: assigned reserved memory node vdevbuffer [ 2.970133] virtio_rpmsg_bus virtio3: rpmsg host is online [ 2.982179] ata1: SATA link down (SStatus 0 SControl 300) [ 2.982856] remoteproc1#vdev1buffer: registered virtio3 (type 7) [ 2.994585] remoteproc remoteproc1: remote processor imx-rproc is now attached [ 2.999036] virtio_rpmsg_bus virtio1: creating channel rpmsg-openamp-demo-channel addr 0x1e [ 3.033984] imx-lpi2c 56247000.i2c: use pio mode [ 3.040720] it6263 6-004c: Probe failed. Remote port 'lvds-channel@0' disabled [ 3.048002] i2c i2c-6: LPI2C adapter registered [ 3.053048] imx-lpi2c 57247000.i2c: use pio mode [ 3.057963] i2c 7-004c: Fixing up cyclic dependency with bus@57240000:ldb@572410e0 [ 3.065970] it6263 7-004c: Probe failed. Remote port 'lvds-channel@0' disabled [ 3.073298] i2c i2c-7: LPI2C adapter registered [ 3.078655] imx-lpi2c 56226000.i2c: use pio mode [ 3.083677] i2c i2c-8: LPI2C adapter registered [ 3.088827] imx-lpi2c 57226000.i2c: use pio mode [ 3.093731] i2c 9-003d: Fixing up cyclic dependency with 57228000.dsi_host [ 3.100790] adv7511 9-003d: supply avdd not found, using dummy regulator [ 3.107564] adv7511 9-003d: supply dvdd not found, using dummy regulator [ 3.109699] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 3.114301] adv7511 9-003d: supply pvdd not found, using dummy regulator [ 3.121765] mmcblk1: mmc1:aaaa SD32G 29.7 GiB [ 3.127651] adv7511 9-003d: supply a2vdd not found, using dummy regulator [ 3.134453] mmcblk1: p1 p2 [ 3.138898] adv7511 9-003d: supply v3p3 not found, using dummy regulator [ 3.148413] adv7511 9-003d: supply v1p2 not found, using dummy regulator [ 3.155510] adv7511 9-003d: Probe failed. Remote port 'dsi_host@57228000' disabled [ 3.163231] i2c i2c-9: LPI2C adapter registered [ 3.168275] pca953x 1-0020: using no AI [ 3.195282] cs42xx8 1-0048: found device, revision 4 [ 3.200382] imx_rpmsg_i2c bus@5a000000:i2c-rpbus-1: add I2C adapter i2c-rpmsg-adapter successfully [ 3.211938] imx6q-pcie 5f010000.pcie: No cache used with register defaults set! [ 3.212642] imx6q-pcie 5f000000.pcie: No cache used with register defaults set! [ 3.214027] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops) [ 3.214187] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops) [ 3.214676] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops) [ 3.215145] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops) [ 3.215582] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops) [ 3.216018] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops) [ 3.219253] cdns-mhdp-imx 56268000.hdmi: Direct firmware load for hdmitxfw.bin failed with error -2 [ 3.219262] cdns-mhdp-imx 56268000.hdmi: Falling back to sysfs fallback for: hdmitxfw.bin [ 3.219311] [drm] Started firmware! [ 3.246932] imx6q-pcie 5f010000.pcie: PCIe PLL is locked. [ 3.254244] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.254933] imx6q-pcie 5f000000.pcie: PCIe PLL is locked. [ 3.255005] imx6q-pcie 5f000000.pcie: iATU unroll: disabled [ 3.255010] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound [ 3.255018] imx6q-pcie 5f000000.pcie: host bridge /bus@5f000000/pcie@0x5f000000 ranges: [ 3.255046] imx6q-pcie 5f000000.pcie: IO 0x006ff80000..0x006ff8ffff -> 0x0000000000 [ 3.255061] imx6q-pcie 5f000000.pcie: MEM 0x0060000000..0x006fefffff -> 0x0060000000 [ 3.255156] imx6q-pcie 5f000000.pcie: iATU unroll: disabled [ 3.255160] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound [ 3.257319] imx6q-pcie 5f010000.pcie: iATU unroll: disabled [ 3.259968] [drm] HDP FW Version - ver 34559 verlib 20560 [ 3.264515] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1 [ 3.271181] cdns-mhdp-imx 56268000.hdmi: lane-mapping 0x93 [ 3.271190] [drm] Both HDCP 1.4 and 2.2 are enabled [ 3.271725] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound [ 3.272981] imx-drm display-subsystem: bound 56268000.hdmi (ops cdns_mhdp_imx_ops) [ 3.273022] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /bus@57220000/dsi_host@57228000 to encoder D [ 3.273051] imx-drm display-subsystem: bound 57228000.dsi_host (ops nwl_dsi_component_ops) [ 3.273294] imx-drm display-subsystem: bound bus@57240000:ldb@572410e0 (ops imx8qm_ldb_ops) [ 3.273744] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1 [ 3.274872] imx-drm display-subsystem: [drm] Cannot find any crtc or sizes [ 3.280139] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present! [ 3.280204] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present! [ 3.280208] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present! [ 3.280211] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present! [ 3.280215] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present! [ 3.281248] xhci-hcd xhci-hcd.1.auto: hcc params 0x200073c8 hci version 0x100 quirks 0x0000002200018010 [ 3.286068] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0 [ 3.286185] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 3.287165] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 3.287225] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 3.287230] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db [ 3.288971] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges: [ 3.292157] ALSA device list: [ 3.292164] No soundcards found. [ 3.292484] xhci-hcd xhci-hcd.1.auto: irq 252, io mem 0x5b130000 [ 3.297892] imx6q-pcie 5f010000.pcie: IO 0x007ff80000..0x007ff8ffff -> 0x0000000000 [ 3.304108] hub 1-0:1.0: USB hub found [ 3.308774] imx6q-pcie 5f010000.pcie: MEM 0x0070000000..0x007fefffff -> 0x0070000000 [ 3.314375] hub 1-0:1.0: 1 port detected [ 3.322098] imx6q-pcie 5f010000.pcie: iATU unroll: disabled [ 3.330284] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.338119] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound [ 3.346310] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2 [ 3.601305] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 3.608026] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 3.616716] hub 2-0:1.0: USB hub found [ 3.620519] hub 2-0:1.0: 1 port detected [ 4.255418] imx6q-pcie 5f000000.pcie: Phy link never came up [ 4.261779] imx6q-pcie: probe of 5f000000.pcie failed with error -110 [ 4.352732] imx6q-pcie 5f010000.pcie: Phy link never came up [ 4.359635] imx6q-pcie: probe of 5f010000.pcie failed with error -110 [ 4.379041] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: none. [ 4.388855] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 4.398012] devtmpfs: mounted [ 4.402172] Freeing unused kernel memory: 2944K [ 4.406923] Run /sbin/init as init process [ 4.579443] systemd[1]: System time before build time, advancing clock. [ 4.608460] systemd[1]: systemd 250.4-1-gc3aead5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -Q -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 4.641712] systemd[1]: Detected architecture arm64. Welcome to NXP i.MX Release Distro 5.15-kirkstone (kirkstone)! [ 4.695874] systemd[1]: Hostname set to . [ 4.781859] systemd-sysv-generator[319]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit fileile for compatibility. Please update package to include a native systemd unit file, in order to make it more safe a [ 4.808101] systemd-sysv-generator[319]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. A for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and [ 4.832923] systemd-sysv-generator[319]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. A for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and [ 4.857379] systemd-sysv-generator[319]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Autor compatibility. Please update package to include a native systemd unit file, in order to make it more safe and ro [ 4.881213] systemd-sysv-generator[319]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. A for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and [ 4.907043] systemd-sysv-generator[319]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit filfile for compatibility. Please update package to include a native systemd unit file, in order to make it more safe [ 4.933131] systemd-sysv-generator[319]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Autom compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robu [ 4.956823] systemd-sysv-generator[319]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Autor compatibility. Please update package to include a native systemd unit file, in order to make it more safe and ro [ 5.349697] systemd[1]: Queued start job for default target Graphical Interface. [ 5.473796] systemd[1]: Created slice Slice /system/getty. [ OK ] Created slice Slice /system/getty. [ 5.497314] systemd[1]: Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/modprobe. [ 5.521293] systemd[1]: Created slice Slice /system/serial-getty. [ OK ] Created slice Slice /system/serial-getty. [ 5.545142] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 5.567374] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 5.591204] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 5.615447] systemd[1]: Reached target Host and Network Name Lookups. [ OK ] Reached target Host and Network Name Lookups. [ 5.639164] systemd[1]: Reached target Path Units. [ OK ] Reached target Path Units. [ 5.659135] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 5.679130] systemd[1]: Reached target Slice Units. [ OK ] Reached target Slice Units. [ 5.699144] systemd[1]: Reached target Swaps. [ OK ] Reached target Swaps. [ 5.721584] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 5.743039] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 5.763708] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 5.783404] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 5.807989] systemd[1]: Listening on Journal Audit Socket. [ OK ] Listening on Journal Audit Socket. [ 5.831616] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 5.855735] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 5.876066] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 5.900435] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 5.923614] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 5.943618] systemd[1]: Listening on User Database Manager Socket. [ OK ] Listening on User Database Manager Socket. [ 5.973939] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 6.001194] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 6.030148] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 6.051879] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathE [ 6.075791] systemd[1]: Mounting Temporary Directory /tmp... Mounting Temporary Directory /tmp... [ 6.104731] systemd[1]: Starting Create List of Static Device Nodes... Starting Create List of Static Device Nodes... [ 6.130840] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs...[ 6.139018] usb 2-1: new SuperSpeed USB device number 2 using xh [ 6.162462] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm...[ 6.171374] usb-storage 2-1:1.0: USB Mass Storage device detected [ 6.179756] scsi host1: usb-storage 2-1:1.0 [ 6.198657] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 6.212883] fuse: init (API version 7.34) [ 6.228409] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 6.247403] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (Condit [ 6.260801] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not [ 6.273862] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 6.292190] systemd[1]: Starting Journal Service... Starting Journal Service... [ 6.319603] systemd[1]: Load Kernel Modules was skipped because all trigger condition checks failed. [ 6.333622] systemd[1]: Starting Generate network units from Kernel command line... Starting Generate network …ts from Kernel command line... [ 6.367437] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 6.390392] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null). Quota mode: none. [ 6.411628] systemd[1]: Starting Apply Kernel Variables... Starting Apply Kernel Variables... [ 6.439998] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 6.470651] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 6.491740] systemd[1]: Mounted Huge Pages File System. [ OK ] Mounted Huge Pages File System. [ 6.511561] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory /tmp. [ OK ] Finished Create List of Static Device Nodes. [ OK ] Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [ OK ] Finished Generate network units from Kernel command line. [ OK ] Finished Remount Root and Kernel File Systems. [ OK ] Finished Apply Kernel Variables. Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... [ 6.797610] systemd-journald[334]: Received client request to flush runtime journal. Starting Create Static Device Nodes in /dev... [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Finished Create Static Device Nodes [ 6.893357] random: crng init done in /dev. [ OK ] Reached target Preparation for Local File Systems. Mounting /var/volatile... Starting Rule-based Manage…for Device Events and Files... [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Finished Load/Save Random Seed. [ OK ] Finished Create Volatile Files and Directories. [ OK ] Started Rule-based Manager for Device Events and Files. Starting Network Time Synchronization... Starting Record System Boot/Shutdown in UTMP... [ OK ] Finished Record System Boot/Shutdown[ 7.210030] scsi 1:0:0:0: Direct-Access Kingston DataTraveler 3 in UTMP. [ 7.259057] sd 1:0:0:0: [sda] 60538881 512-byte logical blocks: (31.0 GB/28.9 GiB) [ 7.267092] sd 1:0:0:0: [sda] Write Protect is off [ 7.273008] sd 1:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA [ 7.296964] sda: sda1 [ 7.300579] sd 1:0:0:0: [sda] Attached SCSI removable disk [ 7.472466] systemd-journald[334]: Oldest entry in /run/log/journal/79c67bb4120146d0aa57e063bceef629/system.jourle retention duration (1month), suggesting rotation. [ 7.490345] systemd-journald[334]: /run/log/journal/79c67bb4120146d0aa57e063bceef629/system.journal: Journal hea-date, rotating. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Set. [ 7.592755] caam 31400000.crypto: device ID = 0x0a16040000000100 (Era 9) [ 7.599561] caam 31400000.crypto: job rings = 1, qi = 0 [ 7.607916] remoteproc remoteproc2: imx-dsp-rproc is available [ 7.619509] [VPU Encoder] enable mu for core[0] [ 7.630612] [VPU Decoder] firmware version is 1.8.3 [ 7.631783] [VPU Encoder] vpu encoder core[0] firmware version is 1.3.1 [ OK ] Finished Coldplug All udev Devices. [ 7.750715] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned. [ OK ] Reached target System Initialization. [ 7.775776] mx8-img-md: Registered mxc_isi.0.capture as /dev/video1 [ OK ] Started Daily rotation of log files mx8-img-md: Registered mxc_isi.1.capture as /dev/video2 [0m. [ 7.801290] mx8-img-md: Registered mxc_isi.2.capture as /dev/video3 [ 7.809357] debugfs: File 'Playback' in directory 'dapm' already present! [ 7.816229] debugfs: File 'Capture' in directory 'dapm' already present! [ OK ] Started Daily Cleanup of Temporary D[ 7.826956] mx8-img-md: Registered mxc_isi.3.capture as /dev/video4 irectories. [ OK ] Reached target Timer Units.[ 7.852366] mx8-img-md: Registered mxc_isi.4.capture as /dev/video5 [ 7.859690] mx8-img-md: Registered mxc_isi.5.capture as /dev/video6 [ OK ] Listening on Avahi mDNS/DNS-SD Stack[ 7.869653] mx8-img-md: Registered mxc_isi.6.capture as /dev/video7 Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. [ 7.895025] mx8-img-md: Registered mxc_isi.7.capture as /dev/video8 [ 7.906246] unregister ISI channel: mxc_isi.0 Starting Docker Socket for the API...[ 7.910985] unregister ISI channel: mxc_isi.1 [ 7.922636] unregister ISI channel: mxc_isi.2 [ 7.927400] unregister ISI channel: mxc_isi.3 [ 7.932244] unregister ISI channel: mxc_isi.4 [ 7.936888] unregister ISI channel: mxc_isi.5 [ 7.942116] unregister ISI channel: mxc_isi.6 [ 7.946733] unregister ISI channel: mxc_isi.7 [ OK ] Listening on dropbear.socket. Starting Weston socket... [ 7.995835] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video1 (81,3) [ 8.010007] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video2 (81,4) Starting Console System Startup Logging... [ OK ] Listening on Docker Socket for the API. [ OK ] Listening on Weston socket. [ OK ] Finished Console System Startup Logging. [ 8.119531] debugfs: File 'Capture' in directory 'dapm' already present! [ 8.146645] input: imx-audio-hdmi-tx HDMI Jack as /devices/platform/sound-hdmi-tx/sound/card3/input1 [ OK ] Created slice Slice /system/systemd-backlight. [ OK ] Created slice Slice /system/systemd-fsck. [ OK ] Reached target Socket Units. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. Starting D-Bus System Message Bus... [ OK ] Started Linux Firmware Loader Daemon. [ 8.433774] caam algorithms registered in /proc/crypto [ 8.452091] caam 31400000.crypto: caam pkc algorithms registered in /proc/crypto [ 8.459842] caam 31400000.crypto: rng crypto API alg registered prng-caam [ OK ] Started Configuration for i.MX GPU ([ 8.466927] caam 31400000.crypto: registering rng-caam Former rc_gpu.S). Starting IPv6 Packet Filtering Framework...[ 8.512803] Device caam-keygen registered Starting IPv4 Packet Filtering Framework... Starting Network Time Service (one-shot ntpdate mode)... Starting Telephony service... [ OK ] Started System Logging Service. Starting Load/Save Screen … backlight:lvds_backlight@0... Starting Load/Save Screen … backlight:lvds_backlight@1... Starting User Login Management... [ OK ] Started TEE Supplicant. [ OK ] Started D-Bus System Message Bus. [ OK ] Finished IPv6 Packet Filtering Framework. [ OK ] Finished IPv4 Packet Filtering Framework. [ OK ] Finished Network Time Service (one-shot ntpdate mode). [ OK ] Finished Load/Save Screen …of backlight:lvds_backlight@0. [ OK ] Finished Load/Save Screen …of backlight:lvds_backlight@1. [ OK ] Found device DataTraveler_3.0 1. [ OK ] Started Telephony service. [ OK ] Started User Login Management. [ OK ] Reached target Preparation for Network. [ OK ] Reached target Hardware activated USB gadget. Starting Save/Restore Sound Card State... Starting Connection service... Starting File System Check on /dev/sda1... Starting Network Configuration... [ OK ] Found device /dev/mmcblk1p1. [ OK ] Finished Save/Restore Sound Card State. [ OK ] Started Connection service. [ OK ] Reached target Sound Card. Starting Avahi mDNS/DNS-SD Stack... Starting File System Check on /dev/mmcblk0p10... Starting File System Check on /dev/mmcblk0p12... Starting File System Check on /dev/mmcblk0p14... Starting File System Check on /dev/mmcblk0p15... Starting File System Check on /dev/mmcblk0p16... Starting File System Check on /dev/mmcblk0p17... Starting File System Check on /dev/mmcblk0p7... Starting File System Check on /dev/mmcblk0p8... Starting File System Check on /dev/mmcblk0p9... Starting File System Check on /dev/mmcblk1p1... [ OK ] Started Network Configuration. [ OK ] Reached target Network. Starting containerd container runtime... [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Respond to IPv6 Node Information Queries. Starting /etc/rc.local Compatibility... [ OK ] Started Network Router Discovery Daemon. Starting Permit User Sessions... [ OK ] Finished File System Check on /dev/mmcblk0p10. Mounting /run/media/mmcblk0p10... [ OK ] Started /etc/rc.local Compatibility. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Finished File System Check on /dev/mmcblk0p12. [ OK ] Finished File System Check on /dev/mmcblk0p14. [ OK ] Finished File System Check on /dev/mmcblk0p16. [ OK ] Finished Permit User Sessions. [ OK ] Finished File System Check on /dev/mmcblk0p7. [ OK ] Finished File System Check on /dev/mmcblk0p15. [ OK ] Finished [ 9.905283] EXT4-fs (mmcblk0p10): mounted filesystem without journal. Opts: (null). Quota mode File System Check on /dev/mmcblk0p17. Mounting /run/media/mmcblk0p12... Mounting /run/media/mmcblk0p14... Mounting /run/media/mmcblk0p15... Mounting /run/media/mmcblk0p16... [ 9.957864] EXT4-fs (mmcblk0p15): mounted filesystem without journal. Opts: (null). Quota mode: none. Mounting /run/media/mmcblk0p17... Mounting /run/media/mmcblk0p7... [ OK ] Started Getty on tty1.[ 9.985846] EXT4-fs (mmcblk0p14): mounted filesystem without journal. Opts: (null [ 9.992362] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: (null). Quota mode: none. [ OK ] Started Serial Getty on ttyLP0.[ 10.011566] ext4 filesystem being mounted at /run/media/mmcblk0p12 suppoff) [ OK ] Reached target Login Prompts. Starting Weston, a Wayland…ositor, as a system service... [ 10.043340] EXT4-fs (mmcblk0p16): mounted filesystem without journal. Opts: (null). Quota mode: none. [ OK ] Finished File System Check on /dev/mmcblk0p8. [ OK ] Finished File System[ 10.063134] EXT4-fs (mmcblk0p17): mounted filesystem without journal. Opts: (null). Check on /dev/mmcblk0p9. [ 10.074413] EXT4-fs (mmcblk0p7): mounted filesystem without journal. Opts: (null). Quota mode: none. [ OK ] Finished File System Check on /dev/mmcblk1p1. [ OK ] Mounted /run/media/mmcblk0p10. [ OK ] Mounted /run/media/mmcblk0p12. [ OK ] Mounted /run/media/mmcblk0p14. [ OK ] Mounted /run/media/mmcblk0p15. [ OK ] Mounted /run/media/mmcblk0p16. [ OK ] Mounted /run/media/mmcblk0p17. [ OK ] Mounted /run/media/mmcblk0p7. Mounting /run/media/mmcblk0p8... Mounting /run/media/mmcblk0p9... Mounting /run/media/mmcblk1p1... Starting Hostname Service...[ 10.185723] EXT4-fs (mmcblk0p8): mounted filesystem without journal. Opts: Starting WPA supplicant... [ 10.206100] EXT4-fs (mmcblk0p9): mounted filesystem without journal. Opts: (null). Quota mode: none. [ OK ] Mounted /run/media/mmcblk0p8. [ OK ] Mounted /run/media/mmcblk0p9. [ OK ] Mounted /run/media/mmcblk1p1. Starting User Database Manager... [ 10.351203] fsl-audmix 59840000.amix: Started TDM1 needed for config propagation! [ OK ] Started User Database Manager. [ OK ] Started WPA supplicant. [ OK ] Started Hostname Service. [ OK ] Created slice User Slice of UID 0. Starting User Runtime Directory /run/user/0... [ OK ] Finished File System Check on /dev/sda1. Mounting /run/media/sda1... [ OK ] Finished User Runtime Directory /run/user/0. Starting User Manager for UID 0... [ 10.953743] audit: type=1006 audit(1694796927.192:2): pid=1283 uid=0 old-auid=4294967295 auid=0 tty=(none) old-s [ 10.966263] audit: type=1300 audit(1694796927.192:2): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffffa ppid=1 pid=1283 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" e) [ 10.992860] audit: type=1327 audit(1694796927.192:2): proctitle="(systemd)" [ OK ] Mounted /run/media/sda1. [ OK ] Started containerd container runtime. [ OK ] Reached target Multi-User System. [ OK ] Started User Manager for UID 0. [ OK ] Started Session c1 of User root. [ 11.624745] audit: type=1006 audit(1694796927.864:3): pid=1254 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses [ 11.637078] audit: type=1300 audit(1694796927.864:3): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffffa ppid=1 pid=1254 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe= [ 11.663225] audit: type=1327 audit(1694796927.864:3): proctitle="(weston)" [ OK ] Started Weston, a Wayland …mpositor, as a system service. [ OK ] Reached target Graphical Interface. Starting Record Runlevel Change in UTMP... [ OK ] Finished Record Runlevel Change in UTMP. NXP i.MX Release Distro 5.15-kirkstone imx8qmmek ttyLP0 imx8qmmek login: [ 33.862956] vref_1v8: disabling imx8qmmek login: imx8qmmek login: imx8qmmek login: root root@imx8qmmek:~# root@imx8qmmek:~# root@imx8qmmek:~# ls root@imx8qmmek:~# root@imx8qmmek:~# cd / root@imx8qmmek:/# root@imx8qmmek:/# df Filesystem 1K-blocks Used Available Use% Mounted on /dev/root 30448348 6394908 22483708 23% / devtmpfs 2273752 4 2273748 1% /dev tmpfs 2766744 0 2766744 0% /dev/shm tmpfs 1106700 12204 1094496 2% /run tmpfs 4096 0 4096 0% /sys/fs/cgroup tmpfs 2766748 4 2766744 1% /tmp tmpfs 2766744 212 2766532 1% /var/volatile /dev/mmcblk0p10 241764 127540 109068 54% /run/media/mmcblk0p10 /dev/mmcblk0p15 634796 548204 73696 89% /run/media/mmcblk0p15 /dev/mmcblk0p14 634796 548204 73696 89% /run/media/mmcblk0p14 /dev/mmcblk0p12 11760 160 11116 2% /run/media/mmcblk0p12 /dev/mmcblk0p16 1777588 219552 1541652 13% /run/media/mmcblk0p16 /dev/mmcblk0p17 1777588 219552 1541652 13% /run/media/mmcblk0p17 /dev/mmcblk0p7 1523628 1105136 402108 74% /run/media/mmcblk0p7 /dev/mmcblk0p8 1523628 1105136 402108 74% /run/media/mmcblk0p8 /dev/mmcblk0p9 241764 127540 109068 54% /run/media/mmcblk0p9 /dev/mmcblk1p1 84998 33706 51292 40% /run/media/mmcblk1p1 tmpfs 553348 8 553340 1% /run/user/0 /dev/sda1 30253024 11301504 18951520 38% /run/media/sda1 root@imx8qmmek:/# cd /run/media/sda1/ root@imx8qmmek:/run/media/sda1# ls 1920x1080.mp4 Alarms Download Pictures avc.bin glob 1K_double_16K_2m.wav Audiobooks FFmpeg_test Podcasts cama1_vtc_c.mp4 lspc 1K_double_32K_2m.wav CAMP_MOT_MBAFF_L30 LOST.DIR Recordings cama3_vtc_b.avc outp 1K_single_48K_2m.wav CVFC1_Sony_C.zip Movies Ringtones dmabuf_encode.h264 outp '??? - ????.ogg' DCIM Music 'System Volume Information' fm1_output.mp4 outp AUD_MW_E.264 Documents Notifications android-cts fm2_output.mp4 sdca root@imx8qmmek:/run/media/sda1# root@imx8qmmek:/run/media/sda1# root@imx8qmmek:/run/media/sda1# cd test/ root@imx8qmmek:/run/media/sda1/test# ls BA1_Sony_D CAMASL3_Sony_B CVFC1_Sony_C FM1_FT_E FM2_SVA_C.zip MR5_TANDBERG_C SP1_BT_A.zip cavlc BA2_Sony_F CANL2_Sony_E FM1_BT_B FM1_FT_E.zip MR4_TANDBERG_C MR5_TANDBERG_C.zip cama2_vtc_b sp2_b BA_MW_D CVBS3_Sony_C FM1_BT_B.zip FM2_SVA_C MR4_TANDBERG_C.zip SP1_BT_A cama3_vtc_b sp2_b root@imx8qmmek:/run/media/sda1/test# root@imx8qmmek:/run/media/sda1/test# cd CVFC1_Sony_C/ root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# ls CVFC1_Sony_C-readme.txt CVFC1_Sony_C-trace.txt CVFC1_Sony_C.jsv CVFC1_Sony_C.yuv CVFC1_Sony_C_nogray.yuv test. root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ le --key 3 --source 2 --name output.dec.yuv > parser --key 0 --name CVFC1_Sony_C.jsv --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x65515 total frame number : 50 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.CVFC1_Sony_C.jsv.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 26 60 300 168 capture min buffers : 8 capture request buffers : 11, memory : 1 decoder fmt : na12 decoder capture : 300 x 168, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.CVFC1_Sony_C.jsv.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.CVFC1_Sony_C.jsv.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 50 -> 50 decoder frame fps : 179.304; time:0.278s; count = 50 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 50 release memory : 0 root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# ls -l total 127712 -rwxrwx--- 1 root disk 799 Apr 13 2005 CVFC1_Sony_C-readme.txt -rwxrwx--- 1 root disk 111353245 Apr 13 2005 CVFC1_Sony_C-trace.txt -rwxrwx--- 1 root disk 414997 Apr 13 2005 CVFC1_Sony_C.jsv -rwxrwx--- 1 root disk 7603200 Feb 27 2004 CVFC1_Sony_C.yuv -rwxrwx--- 1 root disk 3780000 Feb 27 2004 CVFC1_Sony_C_nogray.yuv -rwxrwx--- 1 root disk 3780000 Sep 15 16:57 output.dec.yuv -rwxrwx--- 1 root disk 3780000 Sep 15 16:36 test.yuv root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# md5sum output.dec.yuv CVFC1_Sony_C_nogray.yuv d2aeaea0b9da3509442377a849cc2ff1 output.dec.yuv 9fdb17e17d332b5d9752362c9c7ff9b0 CVFC1_Sony_C_nogray.yuv root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# cd ../MR MR4_TANDBERG_C/ MR5_TANDBERG_C/ root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# cd ../MR MR4_TANDBERG_C/ MR5_TANDBERG_C/ root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# cd ../MR4_TANDBERG_C/ root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# ls MR4_TANDBERG_C.264 MR4_TANDBERG_C.yuv MR4_TANDBERG_C_readme.txt MR4_TANDBERG_C_trace.txt output.dec.yuv test.y root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ --source 1 --fmt I420 \ ofile --key 3 --source 2 --name output.dec.yuv > parser --key 0 --name MR4_TANDBERG_C.264 --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x5d49f total frame number : 300 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.MR4_TANDBERG_C.264.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 176 144 capture min buffers : 8 capture request buffers : 11, memory : 1 decoder fmt : na12 decoder capture : 176 x 144, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.MR4_TANDBERG_C.264.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.MR4_TANDBERG_C.264.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 300 -> 300 decoder frame fps : 381.297; time:0.786s; count = 300 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 300 release memory : 0 root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# ls -l total 54112 -rwxrwx--- 1 root disk 382111 Feb 23 2004 MR4_TANDBERG_C.264 -rwxrwx--- 1 root disk 11404800 Nov 3 2003 MR4_TANDBERG_C.yuv -rwxrwx--- 1 root disk 1012 Feb 23 2004 MR4_TANDBERG_C_readme.txt -rwxrwx--- 1 root disk 20731547 Nov 25 2003 MR4_TANDBERG_C_trace.txt -rwxrwx--- 1 root disk 11404800 Sep 15 16:59 output.dec.yuv -rwxrwx--- 1 root disk 11404800 Sep 15 16:38 test.yuv root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# md5sum MR4_TANDBERG_C.yuv output.dec.yuv 5f5f14beca549172487bb74c4d3ba8f9 MR4_TANDBERG_C.yuv a27dd395b0cb190ba2d40201197ba436 output.dec.yuv root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR4_TANDBERG_C# cd ../ root@imx8qmmek:/run/media/sda1/test# root@imx8qmmek:/run/media/sda1/test# cd MR5_TANDBERG_C/ root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# LS -sh: LS: command not found root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# ls MR5_TANDBERG_C.264 MR5_TANDBERG_C.yuv MR5_TANDBERG_C_readme.txt MR5_TANDBERG_C_trace.txt root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ 3 --source 2 --name output.dec.yuv > parser --key 0 --name MR5_TANDBERG_C.264 --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x5d620 total frame number : 300 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.MR5_TANDBERG_C.264.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 176 144 capture min buffers : 8 capture request buffers : 11, memory : 1 decoder fmt : na12 decoder capture : 176 x 144, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.MR5_TANDBERG_C.264.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.MR5_TANDBERG_C.264.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 300 -> 300 decoder frame fps : 377.375; time:0.794s; count = 300 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 300 release memory : 0 root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# md5sum MR5_TANDBERG_C.yuv output.dec.yuv 5f5f14beca549172487bb74c4d3ba8f9 MR5_TANDBERG_C.yuv a27dd395b0cb190ba2d40201197ba436 output.dec.yuv root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# root@imx8qmmek:/run/media/sda1/test/MR5_TANDBERG_C# cd ../SP1_BT_A/ root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# ls sp1_bt_a.h264 sp1_bt_a.yuv sp1_bt_a_trace.txt root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ ource 1 --fmt I420 \ ofile --key 3 --source 2 --name output.dec.yuv > parser --key 0 --name sp1_bt_a.h264 --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x45c48 total frame number : 400 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.sp1_bt_a.h264.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 176 144 capture min buffers : 4 capture request buffers : 7, memory : 1 decoder fmt : na12 decoder capture : 176 x 144, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.sp1_bt_a.h264.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.sp1_bt_a.h264.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 400 -> 400 decoder frame fps : 379.984; time:1.52s; count = 400 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 400 release memory : 0 root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# ls output.dec.yuv sp1_bt_a.h264 sp1_bt_a.yuv sp1_bt_a_trace.txt root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# ls -l total 100608 -rwxrwx--- 1 root disk 15206400 Sep 15 17:02 output.dec.yuv -rwxrwx--- 1 root disk 285768 Nov 24 2003 sp1_bt_a.h264 -rwxrwx--- 1 root disk 15206400 Nov 24 2003 sp1_bt_a.yuv -rwxrwx--- 1 root disk 72279791 Nov 24 2003 sp1_bt_a_trace.txt root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# md5sum output.dec.yuv sp1_bt_a.yuv b5427c3d710735d7f408e679cfa82bad output.dec.yuv ca0b3580f448cc1e07f81a4756273b59 sp1_bt_a.yuv root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# root@imx8qmmek:/run/media/sda1/test/SP1_BT_A# cd ../sp2_bt_b/ root@imx8qmmek:/run/media/sda1/test/sp2_bt_b# ls H26L root@imx8qmmek:/run/media/sda1/test/sp2_bt_b# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b# cd H26L/ root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L# ls BitstreamExchange root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L# cd BitstreamExchange/ root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# ls sp2_bt_b.h264 sp2_bt_b.yuv sp2_bt_b_trace.txt root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ key 3 --source 2 --name output.dec.yuv > parser --key 0 --name sp2_bt_b.h264 --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x30efb total frame number : 400 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.sp2_bt_b.h264.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 176 144 capture min buffers : 4 capture request buffers : 7, memory : 1 decoder fmt : na12 decoder capture : 176 x 144, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.sp2_bt_b.h264.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.sp2_bt_b.h264.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 400 -> 400 decoder frame fps : 410.205; time:0.975s; count = 400 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 400 release memory : 0 root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# ls -l total 82960 -rwxrwx--- 1 root disk 15206400 Sep 15 17:03 output.dec.yuv -rwxrwx--- 1 root disk 200443 Dec 19 2003 sp2_bt_b.h264 -rwxrwx--- 1 root disk 15206400 Dec 19 2003 sp2_bt_b.yuv -rwxrwx--- 1 root disk 54281530 Dec 19 2003 sp2_bt_b_trace.txt root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# md5sum sp2_bt_b.yuv sp2_bt_b.h264 77fef826070d3d17174529b16765bb24 sp2_bt_b.yuv 14e87c6747461ef7abd045d7ed09ead1 sp2_bt_b.h264 root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# root@imx8qmmek:/run/media/sda1/test/sp2_bt_b/H26L/BitstreamExchange# cd ../../../CVFC1_Sony_C/ root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# LS -sh: LS: command not found root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# ls CVFC1_Sony_C-readme.txt CVFC1_Sony_C-trace.txt CVFC1_Sony_C.jsv CVFC1_Sony_C.yuv CVFC1_Sony_C_nogray.yuv outpu root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# rm output.dec.yuv root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# ls CVFC1_Sony_C-readme.txt CVFC1_Sony_C-trace.txt CVFC1_Sony_C.jsv CVFC1_Sony_C.yuv CVFC1_Sony_C_nogray.yuv test. root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ ofile --key 3 --source 2 --name output.dec.yuv> parser --key 0 --name CVFC1_Sony_C.jsv --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x65515 total frame number : 50 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.CVFC1_Sony_C.jsv.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 26 60 300 168 capture min buffers : 8 capture request buffers : 11, memory : 1 decoder fmt : na12 decoder capture : 300 x 168, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.CVFC1_Sony_C.jsv.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.CVFC1_Sony_C.jsv.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 50 -> 50 decoder frame fps : 179.49; time:0.279s; count = 50 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 50 release memory : 0 root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# md5sum output.dec.yuv CVFC1_Sony_C.yuv d2aeaea0b9da3509442377a849cc2ff1 output.dec.yuv 90bca6748d05bc34fd567c659c49292a CVFC1_Sony_C.yuv root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# root@imx8qmmek:/run/media/sda1/test/CVFC1_Sony_C# cd ../FM1_FT_E/ root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# ls FM1_FT_E.264 FM1_FT_E.yuv FM1_FT_E_Trace.txt FM1_FT_E_readme.txt output.dec.yuv root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ --fmt I420 \ ofile --key 3 --source 2 --name output.dec.yuv > parser --key 0 --name FM1_FT_E.264 --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x38e3f total frame number : 305 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.FM1_FT_E.264.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 176 144 capture min buffers : 4 capture request buffers : 7, memory : 1 decoder fmt : na12 decoder capture : 176 x 144, count = 0 connect <1, 2> connect <2, 3> start : convert.2 start : output.output.dec.yuv.3 stopping : parser.FM1_FT_E.264.0 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.FM1_FT_E.264.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 305 -> 300 decoder frame fps : 377.239; time:0.795s; count = 300 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 300 release memory : 0 root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# md5sum FM1_FT_E.yuv output.dec.yuv bf2d60e2a0140368e087580a8565fc99 FM1_FT_E.yuv d935c85ffc6079c8dadcbfe05a4e0a6d output.dec.yuv root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# root@imx8qmmek:/run/media/sda1/test/FM1_FT_E# cd ../ root@imx8qmmek:/run/media/sda1/test# ls BA1_Sony_D CAMASL3_Sony_B CVFC1_Sony_C FM1_FT_E FM2_SVA_C.zip MR5_TANDBERG_C SP1_BT_A.zip cavlc BA2_Sony_F CANL2_Sony_E FM1_BT_B FM1_FT_E.zip MR4_TANDBERG_C MR5_TANDBERG_C.zip cama2_vtc_b sp2_b BA_MW_D CVBS3_Sony_C FM1_BT_B.zip FM2_SVA_C MR4_TANDBERG_C.zip SP1_BT_A cama3_vtc_b sp2_b root@imx8qmmek:/run/media/sda1/test# root@imx8qmmek:/run/media/sda1/test# cd CAMASL3_Sony_B/ root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# ls CAMASL3_Sony_B-readme.txt CAMASL3_Sony_B-trace.txt CAMASL3_Sony_B.jsv CAMASL3_Sony_B.yuv output.yuv root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# /unit_tests/V4L2_VPU/mxc_v4l2_vpu_enc.out \ 20 \ ofile --key 3 --source 2 --name output.dec.yuv > parser --key 0 --name CAMASL3_Sony_B.jsv --fmt h264 \ > decoder --key 1 --source 0 \ > convert --key 2 --source 1 --fmt I420 \ > ofile --key 3 --source 2 --name output.dec.yuv mxc_v4l2_vpu_test.out V2.1 init total file size: 0x11ed2 total frame number : 17 connect <0, 1> decode capture format: unknown foramt check v4l2 devcie /dev/video0 for h264 to unknown foramt check v4l2 devcie /dev/video1 for h264 to unknown foramt check v4l2 devcie /dev/video2 for h264 to unknown foramt check v4l2 devcie /dev/video12 for h264 to unknown foramt H264 H.264 is found open /dev/video12 init : decoder output.1 start : start : parser.CAMASL3_Sony_B.jsv.0 start : decoder output.1 H264 H.264 is found output min buffers : 8 output request buffers : 11, memory : 1 Loop run Receive Source Change, fd = 5 init : decoder capture.1 start : decoder capture.1 crop info, 0 0 192 128 capture min buffers : 8 capture request buffers : 11, memory : 1 decoder fmt : na12 decoder capture : 192 x 128, count = 0 connect <1, 2> connect <2, 3> start : convert.2 stopping : parser.CAMASL3_Sony_B.jsv.0 start : output.output.dec.yuv.3 flush decoder Receive EOS, fd = 5 dqbuf : EPIPE decoder output finish, capture: 1, 0 stopping : decoder output.1 stop : decoder output.1 stopping : decoder capture.1 stopping : convert.2 stopping : output.output.dec.yuv.3 stop : parser.CAMASL3_Sony_B.jsv.0 stop : output.output.dec.yuv.3 stop : convert.2 stop : decoder capture.1 stopping : stop : Loop done -------- disconnect <0, 1> disconnect <1, 2> disconnect <2, 3> decoder frame count : 17 -> 17 decoder frame fps : 233.431; time:0.72s; count = 17 cleanup : decoder output.1 cleanup : decoder capture.1 output.dec.yuv frame count : 17 release memory : 0 root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# ls CAMASL3_Sony_B-readme.txt CAMASL3_Sony_B-trace.txt CAMASL3_Sony_B.jsv CAMASL3_Sony_B.yuv output.dec.yuv output root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# md5sum CAMASL3_Sony_B.yuv output.dec.yuv d95dc479f23791df4f166145e5c011a4 CAMASL3_Sony_B.yuv d95dc479f23791df4f166145e5c011a4 output.dec.yuv root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B# root@imx8qmmek:/run/media/sda1/test/CAMASL3_Sony_B#