U-Boot SPL 2022.04-g534ef312df (Sep 11 2024 - 09:54:15 +0800) DDRINFO: start DRAM init DDRINFO: DRAM rate 4000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from MMC2 NOTICE: BL31: v2.6(release):43e7343944 NOTICE: BL31: Built : 03:00:34, May 24 2023 U-Boot 2022.04-g534ef312df (Sep 11 2024 - 09:54:15 +0800) CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz) CPU: Industrial temperature grade (-40C to 105C) at 42C Reset cause: POR Model: NXP i.MX8MPlus LPDDR4 EVK board DRAM: 2 GiB Core: 85 devices, 23 uclasses, devicetree: separate MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial BuildInfo: - ATF 43e7343 flash target is MMC:2 Net: Warning: ethernet@30bf0000 (eth1) using random MAC address - a6:f2:9d:37:1c:b9 Could not get PHY for FEC0: addr 1 Could not get PHY for FEC0: addr 1 eth1: ethernet@30bf0000 [PRIME] Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 verify OK, boot 'boot_a' boota: ramdisk overlap detected!!! redirecting ramdisk from 0x44680000 to 0x46e90000 Kernel load addr 0x40480000 size 21507 KiB kernel @ 40480000 (42467328) ramdisk @ 46e90000 (22956079) fdt @ 46e80000 (62597) switch to partitions #0, OK mmc2(part 0) is current device 277 bytes read in 1 ms (270.5 KiB/s) ## Executing script at 60000000 done Moving Image from 0x40480000 to 0x40600000, end=42e80000 ## Flattened Device Tree blob at 46e80000 Booting using the fdt blob at 0x46e80000 Using Device Tree in place at 0000000046e80000, end 0000000046e92484 Starting kernel ... [ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000][ T0] Linux version 5.15.74-ge32688ce04b2 (leo@b9d99992678e) (Android (8490178, based on r450784d) clang version 14.0.6 (https://android.googlesource.com/toolchain/llvm-project 4c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.6) #4 SMP PREEMPT Wed Sep 11 05:30:56 UTC 2024 [ 0.000000][ T0] Machine model: NXP i.MX8MPlus EVK board [ 0.000000][ T0] Stack Depot is disabled [ 0.000000][ T0] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200') [ 0.000000][ T0] printk: bootconsole [ec_imx6q0] enabled [ 0.000000][ T0] efi: UEFI not found. [ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB [ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool [ 0.000000][ T0] kvm [0]: Reserved 16 MiB at 0xbec00000 [ 0.000000][ T0] Zone ranges: [ 0.000000][ T0] DMA32 [mem 0x0000000040000000-0x00000000bfffffff] [ 0.000000][ T0] Normal empty [ 0.000000][ T0] Movable zone start for each node [ 0.000000][ T0] Early memory node ranges [ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000823fffff] [ 0.000000][ T0] node 0: [mem 0x0000000082400000-0x00000000943fffff] [ 0.000000][ T0] node 0: [mem 0x0000000094400000-0x00000000bfffffff] [ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff] [ 0.000000][ T0] cma: Reserved 620 MiB at 0x0000000096000000 [ 0.000000][ T0] psci: probing for conduit method from DT. [ 0.000000][ T0] psci: PSCIv1.1 detected in firmware. [ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs [ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000][ T0] psci: SMC Calling Convention v1.2 [ 0.000000][ T0] Load bootconfig: 997 bytes 63 nodes [ 0.000000][ T0] percpu: Embedded 29 pages/cpu s81752 r8192 d28840 u118784 [ 0.000000][ T0] Detected VIPT I-cache on CPU0 [ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0 [ 0.000000][ T0] CPU features: detected: GIC system register CPU interface [ 0.000000][ T0] CPU features: detected: ARM erratum 845719 [ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000][ T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init firmware_class.path=/vendor/firmware loop.max_part=7 bootconfig transparent_hugepage=never swiotlb=65536 moal.mod_para=wifi_mod_para.conf pci=nomsi cma=1184M@0x400M-0x1000M bootconfig buildvariant=userdebug cma=620M [ 0.000000][ T0] cgroup: Disabling pressure control group feature [ 0.000000][ T0] Unknown kernel command line parameters "buildvariant=userdebug", will be passed to user space. [ 0.000000][ T0] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000][ T0] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off [ 0.000000][ T0] Memory: 1045296K/2097152K available (18176K kernel code, 2246K rwdata, 18864K rodata, 1408K init, 604K bss, 416976K reserved, 634880K cma-reserved) [ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000][ T0] trace event string verifier disabled [ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation. [ 0.000000][ T0] rcu: RCU event tracing is enabled. [ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled. [ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4. [ 0.000000][ T0] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000][ T0] Trampoline variant of Tasks RCU enabled. [ 0.000000][ T0] Tracing variant of Tasks RCU enabled. [ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000][ T0] GICv3: 160 SPIs implemented [ 0.000000][ T0] GICv3: 0 Extended SPIs implemented [ 0.000000][ T0] GICv3: Distributor has no Range Selector support [ 0.000000][ T0] Root IRQ handler: gic_handle_irq.10d7cf410c142aff6d31b6303c3f9f87.cfi_jt [ 0.000000][ T0] GICv3: 16 PPIs implemented [ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000 [ 0.000000][ T0] ITS: No ITS available, not enabling LPIs [ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none). [ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____) [ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys). [ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns [ 0.000000][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns [ 0.009535][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000) [ 0.019781][ T0] pid_max: default: 32768 minimum: 301 [ 0.025402][ T0] LSM: Security Framework initializing [ 0.030533][ T0] SELinux: Initializing. [ 0.034961][ T0] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.042796][ T0] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.053697][ T1] rcu: Hierarchical SRCU implementation. [ 0.057870][ T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build [ 0.065709][ T1] EFI services will not be available. [ 0.070988][ T1] smp: Bringing up secondary CPUs ... [ 0.076509][ T0] Detected VIPT I-cache on CPU1 [ 0.076539][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000 [ 0.076577][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.077356][ T0] Detected VIPT I-cache on CPU2 [ 0.077378][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000 [ 0.077400][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.078127][ T0] Detected VIPT I-cache on CPU3 [ 0.078148][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000 [ 0.078168][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.078262][ T1] smp: Brought up 1 node, 4 CPUs [ 0.139411][ T1] SMP: Total of 4 processors activated. [ 0.144820][ T1] CPU features: detected: 32-bit EL0 Support [ 0.150704][ T1] CPU features: detected: 32-bit EL1 Support [ 0.156548][ T1] CPU features: detected: CRC32 instructions [ 0.162427][ T1] CPU features: detected: Protected KVM [ 0.167928][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching [ 0.187033][ T1] CPU: All CPU(s) started at EL2 [ 0.189031][ T19] alternatives: patching kernel code [ 0.210931][ T1] Registered cp15_barrier emulation handler [ 0.213874][ T1] Registered setend emulation handler [ 0.219114][ T1] KASLR disabled due to lack of seed [ 0.224442][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.234787][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.261925][ T1] pinctrl core: initialized pinctrl subsystem [ 0.266564][ T1] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.274020][ T1] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.279670][ T1] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.288224][ T1] audit: initializing netlink subsys (disabled) [ 0.294456][ T44] audit: type=2000 audit(0.192:1): state=initialized audit_enabled=0 res=1 [ 0.295105][ T1] thermal_sys: Registered thermal governor 'step_wise' [ 0.302755][ T1] thermal_sys: Registered thermal governor 'user_space' [ 0.309486][ T1] thermal_sys: Registered thermal governor 'power_allocator' [ 0.316730][ T1] cpuidle: using governor menu [ 0.328511][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.335841][ T1] ASID allocator initialised with 65536 entries [ 0.342026][ T1] Serial: AMBA PL011 UART driver [ 0.346751][ T1] imx rpmsg driver is registered. [ 0.352572][ T1] printk: console [ramoops-1] enabled [ 0.356894][ T1] pstore: Registered ramoops as persistent store backend [ 0.363738][ T1] ramoops: using 0x100000@0x94400000, ecc: 0 [ 0.401541][ T1] platform 32fd8000.hdmi: Fixing up cyclic dependency with 32fc6000.lcd-controller [ 0.429173][ T1] iommu: Default domain type: Translated [ 0.431923][ T1] iommu: DMA domain TLB invalidation policy: strict mode [ 0.439589][ T1] SCSI subsystem initialized [ 0.443645][ T1] usbcore: registered new interface driver usbfs [ 0.449683][ T1] usbcore: registered new interface driver hub [ 0.455689][ T1] usbcore: registered new device driver usb [ 0.461591][ T1] mc: Linux media interface: v0.10 [ 0.466429][ T1] videodev: Linux video capture interface: v2.00 [ 0.472713][ T1] pps_core: LinuxPPS API ver. 1 registered [ 0.478304][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.488202][ T1] PTP clock support registered [ 0.492868][ T1] EDAC MC: Ver: 3.0.0 [ 0.497775][ T1] FPGA manager framework [ 0.500852][ T1] Advanced Linux Sound Architecture Driver Initialized. [ 0.508155][ T1] Bluetooth: Core ver 2.22 [ 0.511929][ T1] NET: Registered PF_BLUETOOTH protocol family [ 0.517940][ T1] Bluetooth: HCI device and connection manager initialized [ 0.525032][ T1] Bluetooth: HCI socket layer initialized [ 0.530629][ T1] Bluetooth: L2CAP socket layer initialized [ 0.536435][ T1] Bluetooth: SCO socket layer initialized [ 0.542178][ T1] nfc: nfc_init: NFC Core ver 0.1 [ 0.546940][ T1] NET: Registered PF_NFC protocol family [ 0.552801][ T1] clocksource: Switched to clocksource arch_sys_counter [ 0.616038][ T1] VFS: Disk quotas dquot_6.6.0 [ 0.617898][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.626554][ T1] NET: Registered PF_INET protocol family [ 0.631182][ T1] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.640347][ T1] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.648570][ T1] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.656990][ T1] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.665781][ T1] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear) [ 0.673910][ T1] TCP: Hash tables configured (established 16384 bind 16384) [ 0.681069][ T1] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.688426][ T1] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.696437][ T1] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.702654][ T1] NET: Registered PF_XDP protocol family [ 0.708143][ T1] PCI: CLS 0 bytes, default 64 [ 0.713197][ T8] Trying to unpack rootfs image as initramfs... [ 0.718993][ T1] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.728872][ T1] kvm [1]: IPA Size Limit: 40 bits [ 0.748359][ T1] kvm [1]: GICv3: no GICV resource entry [ 0.751074][ T1] kvm [1]: disabling GICv2 emulation [ 0.756239][ T1] kvm [1]: GIC system register CPU interface enabled [ 0.762990][ T1] kvm [1]: vgic interrupt IRQ9 [ 0.767789][ T1] kvm [1]: Protected nVHE mode initialized successfully [ 0.776305][ T1] Initialise system trusted keyrings [ 0.780004][ T1] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.797131][ T1] fuse: init (API version 7.36) [ 0.841081][ T1] Key type asymmetric registered [ 0.843057][ T1] Asymmetric key parser 'x509' registered [ 0.849007][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 237) [ 0.856897][ T1] io scheduler mq-deadline registered [ 0.862085][ T1] io scheduler kyber registered [ 0.867076][ T1] io scheduler bfq registered [ 0.888210][ T1] brd: module loaded [ 0.902384][ T1] loop: module loaded [ 0.905700][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information. [ 0.912020][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld . All Rights Reserved. [ 0.923214][ T1] MACsec IEEE 802.1AE [ 0.926926][ T1] tun: Universal TUN/TAP device driver, 1.6 [ 0.932105][ T1] CAN device driver interface [ 0.937390][ T1] PPP generic driver version 2.4.2 [ 0.941620][ T1] PPP BSD Compression module registered [ 0.946929][ T1] PPP Deflate Compression module registered [ 0.952710][ T1] PPP MPPE Compression module registered [ 0.958199][ T1] NET: Registered PF_PPPOX protocol family [ 0.963877][ T1] PPTP driver version 0.8.5 [ 0.968568][ T1] usbcore: registered new interface driver rtl8150 [ 0.974739][ T1] usbcore: registered new interface driver r8152 [ 0.980972][ T1] usbcore: registered new interface driver asix [ 0.987082][ T1] usbcore: registered new interface driver ax88179_178a [ 0.993886][ T1] usbcore: registered new interface driver cdc_ether [ 0.997756][ T8] Freeing initrd memory: 22416K [ 1.000412][ T1] usbcore: registered new interface driver cdc_eem [ 1.011539][ T1] usbcore: registered new interface driver cdc_ncm [ 1.017903][ T1] usbcore: registered new interface driver aqc111 [ 1.024192][ T1] usbcore: registered new interface driver r8153_ecm [ 1.032075][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.037969][ T1] ehci-pci: EHCI PCI platform driver [ 1.043166][ T1] ehci-platform: EHCI generic platform driver [ 1.049917][ T1] usbcore: registered new interface driver cdc_acm [ 1.055466][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters [ 1.064505][ T1] usbcore: registered new interface driver uas [ 1.070304][ T1] usbcore: registered new interface driver usb-storage [ 1.077288][ T1] usbcore: registered new interface driver xpad [ 1.083531][ T1] usbcore: registered new interface driver uvcvideo [ 1.089592][ T1] gspca_main: v2.14.0 registered [ 1.094944][ T1] device-mapper: uevent: version 1.0.3 [ 1.100014][ T1] device-mapper: ioctl: 4.45.0-ioctl (2021-03-22) initialised: dm-devel@redhat.com [ 1.109326][ T1] Bluetooth: HCI UART driver ver 2.3 [ 1.114099][ T1] Bluetooth: HCI UART protocol H4 registered [ 1.119987][ T1] Bluetooth: HCI UART protocol LL registered [ 1.125922][ T1] Bluetooth: HCI UART protocol Broadcom registered [ 1.132224][ T1] Bluetooth: HCI UART protocol QCA registered [ 1.139378][ T1] sdhci: Secure Digital Host Controller Interface driver [ 1.145083][ T1] sdhci: Copyright(c) Pierre Ossman [ 1.150168][ T1] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.157321][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 1.163753][ T1] hid: raw HID events driver (C) Jiri Kosina [ 1.170945][ T1] usbcore: registered new interface driver usbhid [ 1.175867][ T1] usbhid: USB HID core driver [ 1.180729][ T1] ashmem: initialized [ 1.184683][ T1] gnss: GNSS driver registered with major 507 [ 1.190930][ T1] usbcore: registered new interface driver snd-usb-audio [ 1.197538][ T1] GACT probability NOT on [ 1.201341][ T1] Mirror/redirect action on [ 1.205737][ T1] netem: version 1.3 [ 1.209569][ T1] u32 classifier [ 1.212875][ T1] input device check on [ 1.217257][ T1] Actions configured [ 1.222697][ T1] xt_time: kernel timezone is -0000 [ 1.226577][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver [ 1.233135][ T1] gre: GRE over IPv4 demultiplexor driver [ 1.238256][ T1] ip_gre: GRE over IPv4 tunneling driver [ 1.244928][ T1] IPv4 over IPsec tunneling driver [ 1.249238][ T1] Initializing XFRM netlink socket [ 1.253769][ T1] IPsec XFRM device driver [ 1.258701][ T1] NET: Registered PF_INET6 protocol family [ 1.266304][ T1] Segment Routing with IPv6 [ 1.268113][ T1] In-situ OAM (IOAM) with IPv6 [ 1.272978][ T1] mip6: Mobile IPv6 [ 1.277122][ T1] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.284001][ T1] ip6_gre: GRE over IPv6 tunneling driver [ 1.289127][ T1] NET: Registered PF_PACKET protocol family [ 1.294455][ T1] NET: Registered PF_KEY protocol family [ 1.300109][ T1] can: controller area network core [ 1.305151][ T1] NET: Registered PF_CAN protocol family [ 1.310554][ T1] can: raw protocol [ 1.314213][ T1] can: broadcast manager protocol [ 1.319135][ T1] can: netlink gateway - max_hops=1 [ 1.325101][ T1] Bluetooth: RFCOMM TTY layer initialized [ 1.329789][ T1] Bluetooth: RFCOMM socket layer initialized [ 1.335666][ T1] Bluetooth: RFCOMM ver 1.11 [ 1.340113][ T1] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 1.346755][ T1] Bluetooth: HIDP socket layer initialized [ 1.352462][ T1] l2tp_core: L2TP core driver, V2.0 [ 1.357523][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0 [ 1.363029][ T1] 8021q: 802.1Q VLAN Support v1.8 [ 1.367951][ T1] tipc: Activated (version 2.0.0) [ 1.373064][ T1] NET: Registered PF_TIPC protocol family [ 1.378544][ T1] tipc: Started in single node mode [ 1.383810][ T1] NET: Registered PF_IEEE802154 protocol family [ 1.389927][ T1] NET: Registered PF_VSOCK protocol family [ 1.396233][ T1] registered taskstats version 1 [ 1.400173][ T1] Loading compiled-in X.509 certificates [ 1.406942][ T65] cryptomgr_probe (65) used greatest stack depth: 14032 bytes left [ 1.409276][ T1] Loaded X.509 cert 'Build time autogenerated kernel key: e1a8cd0511fc8fc39c1cf60902045dc4afd50c27' [ 1.426317][ T1] page_owner is disabled [ 1.428390][ T1] Key type ._fscrypt registered [ 1.432949][ T1] Key type .fscrypt registered [ 1.437581][ T1] Key type fscrypt-provisioning registered [ 1.443570][ T1] pstore: Using crash dump compression: deflate [ 1.454126][ T1] OF: fdt: not creating '/sys/firmware/fdt': CRC check failed [ 1.458749][ T1] ALSA device list: [ 1.462316][ T1] No soundcards found. [ 1.466528][ T1] Warning: unable to open an initial console. [ 1.473142][ T1] Freeing unused kernel memory: 1408K [ 1.501170][ T1] Run /init as init process [ 1.506247][ T1] init: init first stage started! [ 1.511901][ T1] init: alias lines in modules.alias must have 3 entries, not 4 [ 1.517176][ T1] init: alias lines in modules.alias must have 3 entries, not 4 [ 1.534072][ T1] init: alias lines in modules.alias must have 3 entries, not 4 [ 1.542957][ T1] init: Loading module /lib/modules/zsmalloc.ko with args '' [ 1.547812][ T1] zsmalloc: module verification failed: signature and/or required key missing - tainting kernel [ 1.559355][ T1] init: Loaded kernel module /lib/modules/zsmalloc.ko [ 1.565082][ T1] init: Loading module /lib/modules/zram.ko with args '' [ 1.573657][ T1] zram: Added device: zram0 [ 1.575792][ T1] init: Loaded kernel module /lib/modules/zram.ko [ 1.582734][ T1] init: Loading module /lib/modules/soc-imx8m.ko with args '' [ 1.590668][ T1] SoC: i.MX8MP revision 1.1 [ 1.593937][ T1] init: Loaded kernel module /lib/modules/soc-imx8m.ko [ 1.653897][ T1] Bus freq driver module loaded [ 1.659056][ T1] trusty trusty: failed to get version: -1 [ 1.661992][ T1] trusty trusty: selected api version: 0 (requested 5) [ 1.676186][ T1] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver [ 1.694509][ T1] printk: console [ttymxc1] enabled [ 1.694509][ T1] printk: console [ttymxc1] enabled [ 1.701824][ T1] printk: bootconsole [ec_imx6q0] disabled [ 1.701824][ T1] printk: bootconsole [ec_imx6q0] disabled [ 1.720081][ T1] i2c i2c-0: IMX I2C adapter registered [ 1.726593][ T1] i2c i2c-1: IMX I2C adapter registered [ 1.733063][ T1] i2c i2c-2: IMX I2C adapter registered [ 1.741125][ T1] i2c_dev: i2c /dev entries driver [ 1.761096][ T1] nxp-pca9450 0-0025: pca9450bc probed. [ 1.771899][ T1] pwm-backlight lvds_backlight: supply power not found, using dummy regulator [ 1.788398][ T8] sdhci-esdhc-imx 30b40000.mmc: allocated mmc-pwrseq [ 1.788985][ T10] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 1.821713][ T55] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA [ 1.829842][ T8] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA [ 1.839535][ T10] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 1.866830][ T1] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator [ 1.876194][ T1] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator [ 1.890686][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: trusty driver failed to probe! nr=0xb5000000 error=-1. Use normal mode. [ 1.904028][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0 [ 1.923255][ T41] mmc2: new HS400 Enhanced strobe MMC card at address 0001 [ 1.931536][ T41] mmcblk2: mmc2:0001 8GTF4R 7.28 GiB [ 1.941659][ T41] Alternate GPT is invalid, using primary GPT. [ 1.947796][ T41] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17 [ 1.958056][ T41] mmcblk2boot0: mmc2:0001 8GTF4R 4.00 MiB [ 1.965551][ T41] mmcblk2boot1: mmc2:0001 8GTF4R 4.00 MiB [ 1.972864][ T41] mmcblk2rpmb: mmc2:0001 8GTF4R 512 KiB, chardev (511:0) [ 1.981412][ T1] dwhdmi-imx 32fd8000.hdmi: Detected HDMI TX controller v2.13a with HDCP (samsung_dw_hdmi_phy2) [ 1.994017][ T1] dwhdmi-imx 32fd8000.hdmi: registered DesignWare HDMI I2C bus driver [ 2.011577][ T1] imx-lcdifv3 32e80000.lcd-controller: lcdif: failed to get response of echo. Use normal mode. [ 2.031521][ T1] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc]) [ 2.041963][ T1] imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc]) [ 2.052358][ T1] imx-drm display-subsystem: bound imx-lcdifv3-crtc.2 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc]) [ 2.062755][ T1] imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_ops [dw_hdmi_imx]) [ 2.072474][ T1] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0 [ 2.104529][ T1] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.110778][ T1] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 2.119660][ T1] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010 [ 2.129897][ T1] xhci-hcd xhci-hcd.0.auto: irq 241, io mem 0x38200000 [ 2.136919][ T1] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.143137][ T1] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 2.151515][ T1] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed [ 2.158940][ T1] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15 [ 2.167926][ T1] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.175867][ T1] usb usb1: Product: xHCI Host Controller [ 2.181458][ T1] usb usb1: Manufacturer: Linux 5.15.74-ge32688ce04b2 xhci-hcd [ 2.188869][ T1] usb usb1: SerialNumber: xhci-hcd.0.auto [ 2.194852][ T1] hub 1-0:1.0: USB hub found [ 2.199345][ T1] hub 1-0:1.0: 1 port detected [ 2.204393][ T1] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 2.213345][ T1] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.15 [ 2.222326][ T1] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.230349][ T1] usb usb2: Product: xHCI Host Controller [ 2.235941][ T1] usb usb2: Manufacturer: Linux 5.15.74-ge32688ce04b2 xhci-hcd [ 2.243359][ T1] usb usb2: SerialNumber: xhci-hcd.0.auto [ 2.249321][ T1] hub 2-0:1.0: USB hub found [ 2.257532][ T1] hub 2-0:1.0: 1 port detected [ 2.269190][ T1] __power_supply_register: Expected proper parent device for 'battery' [ 2.277762][ T1] __power_supply_register: Expected proper parent device for 'usb' [ 2.299781][ T1] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 supported-hw 0x80 0x4 [ 2.318852][ T1] imx8_isi_hw: module is from the staging directory, the quality is unknown, you have been warned. [ 2.331576][ T1] imx8_isi_mem2mem: module is from the staging directory, the quality is unknown, you have been warned. [ 2.344991][ T1] imx8_isi_capture: module is from the staging directory, the quality is unknown, you have been warned. [ 2.358452][ T1] imx8_capture: module is from the staging directory, the quality is unknown, you have been warned. [ 2.371293][ T1] isi-capture 32e00000.isi:cap_device: deferring 32e00000.isi:cap_device device registration [ 2.381715][ T1] isi-m2m 32e00000.isi:m2m_device: deferring 32e00000.isi:m2m_device device registration [ 2.391530][ T1] mxc-isi 32e00000.isi: mxc_isi.0 registered successfully [ 2.399568][ T1] imx8_mipi_csi2_sam: module is from the staging directory, the quality is unknown, you have been warned. [ 2.400022][ T10] isi-m2m 32e00000.isi:m2m_device: Register m2m success for ISI.0 [ 2.425844][ T38] imx-sdma 30bd0000.dma-controller: firmware found. [ 2.432478][ T38] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6 [ 2.433977][ T10] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 43, base_baud = 5000000) is a IMX [ 2.449875][ T10] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 34, base_baud = 5000000) is a IMX [ 2.451626][ T32] imx-sdma 30e10000.dma-controller: firmware found. [ 2.460360][ T10] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 35, base_baud = 5000000) is a IMX [ 2.465951][ T80] usb 1-1: new high-speed USB device number 2 using xhci-hcd [ 2.475422][ T20] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 2.475738][ T42] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 2.482718][ T32] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 2.482971][ T93] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 2.498924][ T1] trusty trusty: trusty-log not supported on secure side. [ 2.525776][ T1] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1) [ 2.535993][ T1] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr [ 2.544186][ T1] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices [ 2.552775][ T1] basler_camera_driver_vvcam: loading out-of-tree module taints kernel. [ 2.565106][ T1] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned. [ 2.577445][ T1] mx8-img-md: Registered mxc_isi.0.capture as /dev/video1 [ 2.587205][ T1] enter viv_dwe_init_module [ 2.594897][ T1] enter viv_isp_init_module [ 2.602256][ T1] enter viv_video_init_module [ 2.636240][ T1] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 2.646871][ T1] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 2.668397][ T80] usb 1-1: New USB device found, idVendor=05e3, idProduct=0610, bcdDevice=93.05 [ 2.677412][ T80] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0 [ 2.685298][ T80] usb 1-1: Product: USB2.1 Hub [ 2.689979][ T80] usb 1-1: Manufacturer: GenesysLogic [ 2.700832][ T1] pcf857x 2-0020: probed [ 2.714301][ T1] usbcore: registered new interface driver option [ 2.720705][ T1] usbserial: USB Serial support registered for GSM modem (1-port) [ 2.730442][ T1] usbcore: registered new interface driver simcom_wwan [ 2.737548][ T80] hub 1-1:1.0: USB hub found [ 2.742355][ T80] hub 1-1:1.0: 4 ports detected [ 2.749839][ T1] st_lsm6dsx_i2c 1-006a: supply vdd not found, using dummy regulator [ 2.757994][ T1] st_lsm6dsx_i2c 1-006a: supply vddio not found, using dummy regulator [ 2.801868][ T38] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd [ 2.825461][ T1] st_lsm6dsx_i2c 1-006a: failed to read whoami register [ 2.836864][ T38] usb 2-1: New USB device found, idVendor=05e3, idProduct=0620, bcdDevice=93.05 [ 2.845793][ T38] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0 [ 2.853660][ T38] usb 2-1: Product: USB3.1 Hub [ 2.858324][ T38] usb 2-1: Manufacturer: GenesysLogic [ 2.859131][ T1] usbcore: registered new interface driver pl2303 [ 2.869931][ T1] usbserial: USB Serial support registered for pl2303 [ 2.896856][ T38] hub 2-1:1.0: USB hub found [ 2.902274][ T38] hub 2-1:1.0: 4 ports detected [ 2.913836][ T98] random: fsck.f2fs: uninitialized urandom read (40 bytes read) [ 2.922974][ T1] fsck.f2fs: linker: Warning: failed to find generated linker configuration from "/linkerconfig/ld.config.txt" [ 2.928917][ T98] random: fsck.f2fs: uninitialized urandom read (40 bytes read) [ 2.934778][ T1] fsck.f2fs: WARNING: linker: Warning: failed to find generated linker configuration from "/linkerconfig/ld.config.txt" [ 2.942537][ T98] random: fsck.f2fs: uninitialized urandom read (4 bytes read) [ 2.963829][ T1] fsck.f2fs: Info: Fix the reported corruption. [ 2.970115][ T1] fsck.f2fs: Info: not exist /proc/version! [ 2.975937][ T1] fsck.f2fs: Info: Segments per section = 1 [ 2.981767][ T1] fsck.f2fs: Info: Sections per zone = 1 [ 2.987315][ T1] fsck.f2fs: Info: sector size = 512 [ 2.992516][ T1] fsck.f2fs: Info: total sectors = 131072 (64 MB) [ 2.998869][ T1] fsck.f2fs: Info: MKFS version [ 3.003652][ T1] fsck.f2fs: "5.15.74-ge32688ce04b2" [ 3.011421][ T98] fsck.f2fs (98) used greatest stack depth: 11952 bytes left [ 3.027231][ T1] F2FS-fs (mmcblk2p11): Mounted with checkpoint version = 67b9ad2 [ 3.107617][ T1] device-mapper: verity: sha256 using implementation "sha256-ce" [ 3.121121][ T1] erofs: (device dm-5): mounted with root inode @ nid 59. [ 3.135732][ T1] device-mapper: verity: sha256 using implementation "sha256-ce" [ 3.148711][ T1] erofs: (device dm-6): mounted with root inode @ nid 38. [ 3.158281][ T1] device-mapper: verity: sha256 using implementation "sha256-ce" [ 3.171838][ T1] erofs: (device dm-7): mounted with root inode @ nid 42. [ 3.181276][ T1] device-mapper: verity: sha256 using implementation "sha256-ce" [ 3.194458][ T1] erofs: (device dm-8): mounted with root inode @ nid 39. [ 3.203888][ T1] device-mapper: verity: sha256 using implementation "sha256-ce" [ 3.216907][ T1] erofs: (device dm-9): mounted with root inode @ nid 39. [ 3.271931][ T1] printk: init: 14 output lines suppressed due to ratelimiting [ 3.279399][ T1] printk: init: 225 output lines suppressed due to ratelimiting [ 3.425535][ T1] init: Opening SELinux policy [ 3.432895][ T1] init: Falling back to standard signature check. TODO implementent support for fsverity SEPolicy. [ 3.443598][ T1] init: Error: Apex SEPolicy failed signature check [ 3.450099][ T1] init: Loading APEX Sepolicy from /system/etc/selinux/apex/SEPolicy.zip [ 3.458435][ T1] init: Failed to open package /system/etc/selinux/apex/SEPolicy.zip: No such file or directory [ 3.482305][ T1] init: Loading SELinux policy [ 3.513879][ T1] SELinux: Permission bpf in class capability2 not defined in policy. [ 3.522025][ T1] SELinux: Permission checkpoint_restore in class capability2 not defined in policy. [ 3.531452][ T1] SELinux: Permission bpf in class cap2_userns not defined in policy. [ 3.539552][ T1] SELinux: Permission checkpoint_restore in class cap2_userns not defined in policy. [ 3.549096][ T1] SELinux: Class mctp_socket not defined in policy. [ 3.555650][ T1] SELinux: the above unknown classes and permissions will be denied [ 3.571190][ T1] SELinux: policy capability network_peer_controls=1 [ 3.577972][ T1] SELinux: policy capability open_perms=1 [ 3.583649][ T1] SELinux: policy capability extended_socket_class=1 [ 3.590296][ T1] SELinux: policy capability always_check_network=0 [ 3.596844][ T1] SELinux: policy capability cgroup_seclabel=0 [ 3.602953][ T1] SELinux: policy capability nnp_nosuid_transition=1 [ 3.609576][ T1] SELinux: policy capability genfs_seclabel_symlinks=0 [ 3.616375][ T1] SELinux: policy capability ioctl_skip_cloexec=0 [ 3.830460][ T44] audit: type=1403 audit(3.652:2): auid=4294967295 ses=4294967295 lsm=selinux res=1 [ 3.839146][ T1] selinux: SELinux: Loaded file_contexts [ 3.845281][ T1] selinux: [ 3.886319][ T1] init: init second stage started! [ 3.945669][ T1] init: Using Android DT directory /proc/device-tree/firmware/android/ [ 3.960658][ T1] init: Couldn't load property file '/system_dlkm/etc/build.prop': open() failed: No such file or directory: No such file or directory [ 3.974488][ T1] init: Couldn't load property file '/vendor/default.prop': open() failed: No such file or directory: No such file or directory [ 3.992006][ T1] init: Couldn't load property file '/odm_dlkm/etc/build.prop': open() failed: No such file or directory: No such file or directory [ 4.009647][ T1] init: Overriding previous property 'bluetooth.profile.asha.central.enabled':'false' with new value 'true' [ 4.021091][ T1] init: Overriding previous property 'bluetooth.profile.bas.client.enabled':'false' with new value 'true' [ 4.034568][ T1] init: Setting product property ro.product.brand to 'Android' (from ro.product.product.brand) [ 4.044821][ T1] init: Setting product property ro.product.device to 'evk_8mp' (from ro.product.product.device) [ 4.055237][ T1] init: Setting product property ro.product.manufacturer to 'nxp' (from ro.product.product.manufacturer) [ 4.122072][ T125] random: init: uninitialized urandom read (40 bytes read) [ 4.147377][ T125] random: init: uninitialized urandom read (40 bytes read) [ 4.154996][ T125] random: init: uninitialized urandom read (4 bytes read) [ 4.278085][ T126] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.v33: No such file or directory [ 4.289405][ T126] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.v33: No such file or directory [ 4.304434][ T126] linkerconfig (126) used greatest stack depth: 11328 bytes left [ 4.346526][ T127] ueventd: ueventd started! [ 4.355189][ T127] selinux: SELinux: Loaded file_contexts [ 4.361203][ T127] selinux: [ 4.365343][ T127] ueventd: Parsing file /system/etc/ueventd.rc... [ 4.371904][ T127] ueventd: Added '/vendor/etc/ueventd.rc' to import list [ 4.379002][ T127] ueventd: Added '/odm/etc/ueventd.rc' to import list [ 4.386856][ T127] ueventd: Parsing file /vendor/etc/ueventd.rc... [ 4.393794][ T127] ueventd: Parsing file /odm/etc/ueventd.rc... [ 4.400006][ T127] ueventd: Unable to read config file '/odm/etc/ueventd.rc': open() failed: No such file or directory [ 4.424232][ T128] apexd: Bootstrap subcommand detected [ 4.431264][ T128] cutils-trace: Error opening trace file: No such file or directory (2) [ 4.661022][ T128] apexd: wait for '/dev/loop-control' took 189ms [ 4.685466][ T128] apexd: Pre-allocated 15 loopback devices [ 4.691388][ T128] apexd: Scanning /system/apex for pre-installed ApexFiles [ 4.698906][ T128] apexd: Found pre-installed APEX /system/apex/com.android.adbd.capex [ 4.710475][ T128] apexd: Found pre-installed APEX /system/apex/com.android.adservices.capex [ 4.722044][ T128] apexd: Found pre-installed APEX /system/apex/com.android.apex.cts.shim.apex [ 4.731522][ T128] apexd: Found pre-installed APEX /system/apex/com.android.appsearch.apex [ 4.740606][ T128] apexd: Found pre-installed APEX /system/apex/com.android.art.capex [ 4.806139][ T161] loop0: detected capacity change from 0 to 96704 [ 4.813769][ T160] loop1: detected capacity change from 0 to 16240 [ 4.836196][ T127] ueventd: Coldboot took 0.424 seconds [ 4.871262][ T161] EXT4-fs (loop0): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 4.886846][ T161] loop2: detected capacity change from 0 to 74600 [ 4.891514][ T160] EXT4-fs (loop1): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 4.905455][ T160] loop3: detected capacity change from 0 to 1728 [ 4.932344][ T161] EXT4-fs (loop2): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 5.003944][ T160] EXT4-fs (loop3): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 5.028026][ T128] printk: apexd: 40 output lines suppressed due to ratelimiting [ 5.035842][ T128] apexd (128) used greatest stack depth: 11184 bytes left [ 5.152257][ T170] random: boringssl_self_: uninitialized urandom read (40 bytes read) [ 5.160727][ T170] random: boringssl_self_: uninitialized urandom read (4 bytes read) [ 5.168775][ T170] random: boringssl_self_: uninitialized urandom read (4 bytes read) [ 5.193226][ T170] : getrandom indicates that the entropy pool has not been initialized. Rather than continue with poor entropy, this process will block until entropy is available. [ 6.928810][ C3] random: crng init done [ 6.932939][ C3] random: 62 urandom warning(s) missed due to ratelimiting [ 7.175648][ T173] prng_seeder: Hanging forever because setup failed: hwrng.read_exact in new [ 7.175648][ T173] [ 7.186670][ T173] Caused by: [ 7.189897][ T173] No such device (os error 19) [ 7.251149][ T176] module built by leo at Wed 11 Sep 2024 05:32:27 AM UTC [ 7.252450][ T176] Galcore version 6.4.3.p4.398061 [ 7.370061][ T176] [drm] Initialized vivante 1.0.0 20170808 for 40000000.mix_gpu_ml on minor 1 [ 7.382530][ T176] Hot alarm is canceled. GPU3D clock will return to 64/64 [ 7.395963][ T1] Registered swp emulation handler [ 7.437194][ T176] Registered IR keymap rc-cec [ 7.442843][ T176] rc rc0: dw_hdmi as /devices/platform/soc@0/30c00000.bus/32fd8000.hdmi/rc/rc0 [ 7.452644][ T176] input: dw_hdmi as /devices/platform/soc@0/30c00000.bus/32fd8000.hdmi/rc/rc0/input1 [ 7.516843][ T182] logd.auditd: start [ 7.521027][ T182] logd.klogd: 7344211000 [ 7.539246][ T194] watchdogd: watchdogd started (interval 10, margin 20)! [ 7.550072][ T182] logd: Loaded bug_map file: /vendor/etc/selinux/selinux_denial_metadata [ 7.560957][ T182] logd: Loaded bug_map file: /system/etc/selinux/bug_map evk_8mp:/ $ [ 7.583939][ T176] input: audio-hdmi HDMI Jack as /devices/platform/sound-hdmi/sound/card0/input2 [ 7.612654][ T176] rt5651 1-001a: Failed to reguest IRQ 0: -22 [ 7.645912][ T176] mxc_hantro_vc8000e 38320000.vpu_vc8000e: hantro_enc: get trusty_dev node, use Trusty mode. [ 7.656014][ T176] hantro_enc driver probe fail! nr=0xb8000000 ret=-1. Use normal mode. [ 7.664899][ T176] hantroenc: HW at base <0000000038320000> with ID <0x80006200> [ 7.672609][ T176] hx280enc: module inserted. Major <504> [ 7.682956][ T176] vpu driver probe fail! nr=0xb7000000 ret=-1. Use normal mode. [ 7.690808][ T176] hantrodec 0 : module inserted. Major = 503 [ 7.693295][ T1] zram0: detected capacity change from 0 to 1228800 [ 7.697799][ T176] vpu driver probe fail! nr=0xb7000000 ret=-1. Use normal mode. [ 7.711201][ T176] hantrodec 1 : module inserted. Major = 503 [ 7.726357][ T176] imx mu driver is registered. [ 7.737502][ T202] type=1400 audit(7.560:3): avc: denied { ioctl } for comm="mkswap" path="/dev/block/zram0" dev="tmpfs" ino=494 ioctlcmd=0x1272 scontext=u:r:toolbox:s0 tcontext=u:object_r:ram_device:s0 tclass=blk_file permissive=1 [ 7.741056][ T1] mkswap: Swapspace size: 614396k, UUID=cf0d13d8-ee8a-4c59-825f-49a8e30f8b27 [ 7.767659][ T1] Adding 614396k swap on /dev/block/zram0. Priority:-2 extents:1 across:614396k SS [ 7.769074][ T176] remoteproc remoteproc0: imx-dsp-rproc is available [ 7.830147][ T176] rtc-ds1307 2-0068: registered as rtc0 [ 7.836364][ T176] rtc-ds1307 2-0068: setting system clock to 2024-09-11T05:56:30 UTC (1726034190) [ 7.862247][ T176] snvs_rtc 30370000.snvs:snvs-rtc-lp: snvs rtc: trusty snvs driver failed to probe! nr=0xb5000000 ret=-1. Use normal mode. [ 7.877768][ T176] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc1 [ 7.890605][ T71] imx6q-pcie 33800000.pcie: supply epdev_on not found, using dummy regulator [ 7.903655][ T71] imx6q-pcie 33800000.pcie: error -ENOENT: pcie_phy clock source missing or invalid [ 7.913042][ T71] imx6q-pcie: probe of 33800000.pcie failed with error -2 [ 7.927443][ T176] pps pps0: new PPS source ptp0 [ 7.946878][ T176] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00 [ 7.954543][ T176] fec 30be0000.ethernet: Using random MAC address: 9a:2a:df:9e:c3:41 [ 8.069874][ T176] fec 30be0000.ethernet eth0: registered PHC device 0 [ 8.102391][ T176] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found [ 8.109342][ T176] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51 [ 8.116906][ T176] imx-dwmac 30bf0000.ethernet: DWMAC4/5 [ 8.122481][ T176] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported [ 8.130390][ T176] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported [ 8.138331][ T176] imx-dwmac 30bf0000.ethernet: TX Checksum insertion supported [ 8.145790][ T176] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported [ 8.152851][ T176] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 8.161243][ T176] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8) [ 8.168814][ T176] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=8) [ 8.176297][ T176] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256) [ 8.184628][ T176] imx-dwmac 30bf0000.ethernet: Using 34 bits DMA width [ 8.196613][ T176] modprobe (176) used greatest stack depth: 11056 bytes left [ 8.369244][ T199] fsck.f2fs: Info: Fix the reported corruption. [ 8.375601][ T199] fsck.f2fs: Info: not exist /proc/version! [ 8.381467][ T199] fsck.f2fs: Info: Segments per section = 1 [ 8.387368][ T199] fsck.f2fs: Info: Sections per zone = 1 [ 8.392953][ T199] fsck.f2fs: Info: sector size = 4096 [ 8.398256][ T199] fsck.f2fs: Info: total sectors = 677888 (2648 MB) [ 8.404804][ T199] fsck.f2fs: Info: MKFS version [ 8.409607][ T199] fsck.f2fs: "5.15.74-ge32688ce04b2" [ 8.415009][ T199] fsck.f2fs: Info: FSCK version [ 8.419846][ T199] fsck.f2fs: from "5.15.74-ge32688ce04b2" [ 8.428207][ T199] F2FS-fs (dm-37): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0 [ 8.453629][ T199] F2FS-fs (dm-37): Mounted with checkpoint version = 10181d62 [ 8.563662][ T1] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce" [ 8.665473][ T199] vold: keystore2 Keystore earlyBootEnded returned service specific error: -68 [ 8.739324][ T198] logd: logd reinit [ 8.746169][ T198] logd: FrameworkListener: read() failed (Connection reset by peer) [ 8.746613][ T253] apexd: Scanning /system/apex for pre-installed ApexFiles [ 8.761696][ T253] apexd: Found pre-installed APEX /system/apex/com.android.adbd.capex [ 8.770688][ T253] apexd: Found pre-installed APEX /system/apex/com.android.adservices.capex [ 8.779847][ T253] apexd: Found pre-installed APEX /system/apex/com.android.apex.cts.shim.apex [ 8.789442][ T253] apexd: Found pre-installed APEX /system/apex/com.android.appsearch.apex [ 8.798469][ T253] apexd: Found pre-installed APEX /system/apex/com.android.art.capex [ 8.807081][ T253] apexd: Found pre-installed APEX /system/apex/com.android.btservices.apex [ 8.816232][ T253] apexd: Found pre-installed APEX /system/apex/com.android.cellbroadcast.capex [ 8.825695][ T253] apexd: Found pre-installed APEX /system/apex/com.android.conscrypt.capex [ 8.834769][ T253] apexd: Found pre-installed APEX /system/apex/com.android.extservices.capex [ 8.988917][ T255] loop4: detected capacity change from 0 to 41792 [ 8.996207][ T256] loop5: detected capacity change from 0 to 6952 [ 9.031832][ T255] EXT4-fs (loop4): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.044712][ T255] loop6: detected capacity change from 0 to 536 [ 9.057810][ T256] EXT4-fs (loop5): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.069946][ T256] loop7: detected capacity change from 0 to 1728 [ 9.099271][ T255] EXT4-fs (loop6): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.114684][ T255] loop8: detected capacity change from 0 to 536 [ 9.128167][ T256] EXT4-fs (loop7): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.139514][ T256] loop9: detected capacity change from 0 to 96704 [ 9.168734][ T255] EXT4-fs (loop8): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.179915][ T255] loop10: detected capacity change from 0 to 3920 [ 9.197169][ T256] EXT4-fs (loop9): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.208242][ T256] loop11: detected capacity change from 0 to 16240 [ 9.223219][ T255] EXT4-fs (loop10): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.235309][ T255] loop12: detected capacity change from 0 to 536 [ 9.278075][ T256] EXT4-fs (loop11): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.289817][ T256] loop13: detected capacity change from 0 to 74600 [ 9.306267][ T255] EXT4-fs (loop12): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.316956][ T255] loop14: detected capacity change from 0 to 1536 [ 9.347666][ T256] EXT4-fs (loop13): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.359405][ T256] loop15: detected capacity change from 0 to 19376 [ 9.379790][ T255] EXT4-fs (loop14): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.392187][ T255] loop16: detected capacity change from 0 to 17256 [ 9.410403][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.444778][ T256] EXT4-fs (dm-36): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.457226][ T256] loop17: detected capacity change from 0 to 40512 [ 9.461263][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.498550][ T255] EXT4-fs (dm-34): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.511333][ T255] loop18: detected capacity change from 0 to 17128 [ 9.513746][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.552155][ T256] EXT4-fs (dm-33): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.564383][ T256] loop19: detected capacity change from 0 to 1584 [ 9.594502][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.629730][ T255] EXT4-fs (dm-32): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.630124][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.643355][ T255] loop20: detected capacity change from 0 to 98952 [ 9.672115][ T256] EXT4-fs (dm-31): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.685673][ T256] loop21: detected capacity change from 0 to 5912 [ 9.715237][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.751673][ T255] EXT4-fs (dm-27): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.763949][ T255] loop22: detected capacity change from 0 to 13232 [ 9.776554][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.809548][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.818104][ T256] EXT4-fs (dm-25): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.832007][ T256] loop23: detected capacity change from 0 to 29504 [ 9.843583][ T255] EXT4-fs (dm-26): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.856066][ T255] loop24: detected capacity change from 0 to 10512 [ 9.892199][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.905215][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 9.924753][ T256] EXT4-fs (dm-24): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.938009][ T256] loop25: detected capacity change from 0 to 11168 [ 9.939980][ T255] EXT4-fs (dm-23): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 9.957285][ T255] loop26: detected capacity change from 0 to 17888 [ 10.002501][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.016578][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.036347][ T256] EXT4-fs (dm-15): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.049377][ T256] loop27: detected capacity change from 0 to 25600 [ 10.053553][ T255] EXT4-fs (dm-19): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.068327][ T255] loop28: detected capacity change from 0 to 16208 [ 10.111456][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.141728][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.146864][ T256] EXT4-fs (dm-17): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.162054][ T256] loop29: detected capacity change from 0 to 536 [ 10.176664][ T255] EXT4-fs (dm-18): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.189222][ T255] loop30: detected capacity change from 0 to 7920 [ 10.226817][ T256] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.263060][ T256] EXT4-fs (dm-29): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.277679][ T255] device-mapper: verity: sha256 using implementation "sha256-ce" [ 10.314628][ T255] EXT4-fs (dm-12): mounted filesystem without journal. Opts: (null). Quota mode: none. [ 10.371793][ T124] init: Wait for property 'apexd.status=activated' took 1539ms [ 10.412298][ T1] init: Parsing file /apex/com.android.adbd/etc/init.rc... [ 10.420605][ T1] init: Parsing file /apex/com.android.art/etc/init.rc... [ 10.429271][ T1] init: Parsing file /apex/com.android.media.swcodec/etc/mediaswcodec.32rc... [ 10.439198][ T1] init: Parsing file /apex/com.android.media/etc/mediatranscoding.32rc... [ 10.449061][ T1] init: Parsing file /apex/com.android.os.statsd/etc/init.rc... [ 10.457693][ T1] init: Parsing file /apex/com.android.sdkext/etc/derive_classpath.rc... [ 10.466787][ T1] init: Parsing file /apex/com.android.sdkext/etc/derive_sdk.rc... [ 10.537141][ T1] init: linkerconfig generated /linkerconfig with mounted APEX modules info [ 10.545796][ T1] init: Command 'perform_apex_config' action=post-fs-data (/system/etc/init/hw/init.rc:967) took 166ms and succeeded [ 11.096466][ T202] type=1400 audit(1726034193.756:4): avc: denied { open } for comm="odrefresh" path="/dev/__properties__/u:object_r:aac_drc_prop:s0" dev="tmpfs" ino=79 scontext=u:r:odrefresh:s0 tcontext=u:object_r:aac_drc_prop:s0 tclass=file permissive=1 [ 11.108249][ T310] audit: audit_backlog=65 > audit_backlog_limit=64 [ 11.119621][ T202] type=1400 audit(1726034193.756:5): avc: denied { getattr } for comm="odrefresh" path="/dev/__properties__/u:object_r:aac_drc_prop:s0" dev="tmpfs" ino=79 scontext=u:r:odrefresh:s0 tcontext=u:object_r:aac_drc_prop:s0 tclass=file permissive=1 [ 11.125596][ T310] audit: audit_lost=1 audit_rate_limit=0 audit_backlog_limit=64 [ 11.125603][ T310] audit: backlog limit exceeded [ 11.148692][ T202] type=1400 audit(1726034193.756:6): avc: denied { map } for comm="odrefresh" path="/dev/__properties__/u:object_r:aac_drc_prop:s0" dev="tmpfs" ino=79 scontext=u:r:odrefresh:s0 tcontext=u:object_r:aac_drc_prop:s0 tclass=file permissive=1 [ 11.156334][ T310] audit: audit_backlog=65 > audit_backlog_limit=64 [ 11.189784][ T310] audit: audit_lost=2 audit_rate_limit=0 audit_backlog_limit=64 [ 11.197287][ T310] audit: backlog limit exceeded [ 11.302444][ T312] apexd: Snapshot DE subcommand detected [ 11.311310][ T312] apexd: Marking APEXd as ready [ 11.427964][ T314] clean_scratch_f (314) used greatest stack depth: 11040 bytes left [ 11.439224][ T316] LibBpfLoader: Section bpfloader_min_ver value is 2 [0x2] [ 11.446569][ T316] LibBpfLoader: Section bpfloader_max_ver value is 65536 [0x10000] [ 11.454480][ T316] LibBpfLoader: Section size_of_bpf_map_def value is 116 [0x74] [ 11.462128][ T316] LibBpfLoader: Section size_of_bpf_prog_def value is 92 [0x5c] [ 11.469665][ T316] LibBpfLoader: BpfLoader version 0x00013 processing ELF object /apex/com.android.tethering/etc/bpf/test.o with ver [0x00002,0x10000) [ 14.537467][ T316] printk: bpfloader: 1679 output lines suppressed due to ratelimiting [ 14.580182][ T319] update_verifier: Started with arg 1: nonencrypted [ 14.590954][ T319] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1 [ 14.598905][ T319] update_verifier: Leaving update_verifier. [ 14.719718][ T125] Mass Storage Function, version: 2009/09/11 [ 14.725665][ T125] LUN: removable file: (no medium) [ 14.736005][ T125] using random self ethernet address [ 14.741240][ T125] using random host ethernet address [ 14.747556][ T125] file system registered [ 15.203260][ T354] healthd: batteryCapacityLevelPath not found [ 15.226293][ T202] type=1400 audit(1726034197.888:521): avc: denied { map } for comm="android.hardwar" path="/dev/binderfs/vndbinder" dev="binder" ino=6 scontext=u:r:hal_gnss_default:s0 tcontext=u:object_r:vndbinder_device:s0 tclass=chr_file permissive=1 [ 15.237502][ T354] healthd: batteryChargeTimeToFullNowPath. not found [ 15.238449][ T125] export_store: invalid GPIO 496 [ 15.239548][ T125] export_store: invalid GPIO 497 [ 15.240415][ T125] export_store: invalid GPIO 498 [ 15.241347][ T125] export_store: invalid GPIO 499 [ 15.242183][ T125] export_store: invalid GPIO 500 [ 15.242985][ T125] export_store: invalid GPIO 501 [ 15.243734][ T125] export_store: invalid GPIO 502 [ 15.244476][ T125] export_store: invalid GPIO 503 [ 15.294544][ T354] healthd: batteryFullChargeDesignCapacityUahPath. not found [ 15.310692][ T354] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400000 fc=4000000 cc=32 chg=a [ 15.382325][ T1] init: processing action (enable_property_trigger) from (:0) [ 15.391668][ T202] type=1400 audit(1726034198.044:522): avc: denied { getattr } for comm="mcu.power.sh" path="/system/bin/tinymix" dev="dm-5" ino=6361883 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:system_file:s0 tclass=file permissive=1 [ 15.393355][ T1] init: processing action (apexd.status=ready && ro.product.cpu.abilist32=*) from (/system/etc/init/hw/init.rc:94) [ 15.428017][ T202] type=1400 audit(1726034198.044:523): avc: denied { execute } for comm="mcu.power.sh" name="tinymix" dev="dm-5" ino=6361883 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:system_file:s0 tclass=file permissive=1 [ 15.449167][ T202] type=1400 audit(1726034198.088:524): avc: denied { read open } for comm="mcu.power.sh" path="/system/bin/tinymix" dev="dm-5" ino=6361883 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:system_file:s0 tclass=file permissive=1 [ 15.450137][ T1] init: starting service 'boringssl_self_test_apex32'... [ 15.471216][ T202] type=1400 audit(1726034198.088:525): avc: denied { execute_no_trans } for comm="mcu.power.sh" path="/system/bin/tinymix" dev="dm-5" ino=6361883 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:system_file:s0 tclass=file permissive=1 [ 15.483458][ T1] init: SVC_EXEC service 'boringssl_self_test_apex32' pid 381 (uid 0 gid 0+0 context default) started; waiting... [ 15.502000][ T202] type=1400 audit(1726034198.164:526): avc: denied { map } for comm="tinymix" path="/system/bin/tinymix" dev="dm-5" ino=6361883 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:system_file:s0 tclass=file permissive=1 [ 15.512949][ T1] init: Command 'exec_start boringssl_self_test_apex32' action=apexd.status=ready && ro.product.cpu.abilist32=* (/system/etc/init/hw/init.rc:95) took 87ms and succeeded [ 15.550991][ T1] init: Service 'exec 15 (/system/bin/gsid run-startup-tasks)' (pid 376) exited with status 0 oneshot service took 0.215000 seconds in background [ 15.565853][ T1] init: Sending signal 9 to service 'exec 15 (/system/bin/gsid run-startup-tasks)' (pid 376) process group... [ 15.577758][ T1] libprocessgroup: Successfully killed process cgroup uid 0 pid 376 in 0ms [ 15.594187][ T202] type=1400 audit(1726034198.188:527): avc: denied { search } for comm="tinymix" name="snd" dev="tmpfs" ino=481 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:audio_device:s0 tclass=dir permissive=1 [ 15.630691][ T202] type=1400 audit(1726034198.188:528): avc: denied { dac_override } for comm="tinymix" capability=1 scontext=u:r:mcu-power-sh:s0 tcontext=u:r:mcu-power-sh:s0 tclass=capability permissive=1 [ 15.661429][ T202] type=1400 audit(1726034198.188:529): avc: denied { read write } for comm="tinymix" name="controlC1" dev="tmpfs" ino=557 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:audio_device:s0 tclass=chr_file permissive=1 [ 15.682574][ T202] type=1400 audit(1726034198.188:530): avc: denied { open } for comm="tinymix" path="/dev/snd/controlC1" dev="tmpfs" ino=557 scontext=u:r:mcu-power-sh:s0 tcontext=u:object_r:audio_device:s0 tclass=chr_file permissive=1 [ 15.733759][ T1] init: Service 'boringssl_self_test_apex32' (pid 381) exited with status 0 waiting took 0.253000 seconds [ 15.749827][ T1] init: Sending signal 9 to service 'boringssl_self_test_apex32' (pid 381) process group... [ 17.005704][ T490] read descriptors [ 17.025409][ T490] read strings [ 17.340405][ T69] android_work: sent uevent USB_STATE=CONNECTED [ 17.369853][ T69] android_work: sent uevent USB_STATE=CONFIGURED [ 21.644533][ T202] type=1400 audit(1726034204.304:586): avc: denied { search } for comm="RenderEngine" name=".opencl-cache" dev="dm-37" ino=303 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:opencl_cache_file:s0 tclass=dir permissive=1 [ 21.666608][ T202] type=1400 audit(1726034204.304:587): avc: denied { read } for comm="RenderEngine" name="viv_gc_img_builtin.lib" dev="dm-37" ino=358 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:opencl_cache_file:s0 tclass=file permissive=1 [ 21.689531][ T202] type=1400 audit(1726034204.304:588): avc: denied { open } for comm="RenderEngine" path="/data/vendor/.opencl-cache/viv_gc_img_builtin.lib" dev="dm-37" ino=358 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:opencl_cache_file:s0 tclass=file permissive=1 [ 21.714402][ T202] type=1400 audit(1726034204.308:589): avc: denied { lock } for comm="RenderEngine" path="/data/vendor/.opencl-cache/viv_gc_img_builtin.lib" dev="dm-37" ino=358 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:opencl_cache_file:s0 tclass=file permissive=1 [ 21.739330][ T202] type=1400 audit(1726034204.308:590): avc: denied { getattr } for comm="RenderEngine" path="/data/vendor/.opencl-cache/viv_gc_img_builtin.lib" dev="dm-37" ino=358 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:opencl_cache_file:s0 tclass=file permissive=1 [ 21.886693][ T202] type=1400 audit(1726034204.548:591): avc: denied { read } for comm="main" name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 21.908932][ T202] type=1400 audit(1726034204.548:592): avc: denied { open } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 21.933456][ T202] type=1400 audit(1726034204.548:593): avc: denied { getattr } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 21.958145][ T202] type=1400 audit(1726034204.548:594): avc: denied { map } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 24.603438][ T202] type=1400 audit(1726034207.264:595): avc: denied { read } for comm="binder:210_2" name="wakeup7" dev="sysfs" ino=38495 scontext=u:r:system_suspend:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=1 [ 25.233241][ T301] apexd: Can't open /system_ext/apex for reading : No such file or directory [ 25.242110][ T301] apexd: Can't open /product/apex for reading : No such file or directory [ 25.250798][ T301] apexd: Can't open /vendor/apex for reading : No such file or directory [ 26.009176][ T1] init: service 'idmap2d' requested start, but it is already running (flags: 4) [ 26.018221][ T1] init: Control message: Processed ctl.start for 'idmap2d' from pid: 575 (system_server) [ 26.171641][ T354] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400000 fc=4000000 cc=32 chg=a [ 26.588568][ T1] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/system/etc/init/hw/init.rc:1196) [ 26.601110][ T1] init: starting service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)'... [ 26.618439][ T1] init: SVC_EXEC service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)' pid 669 (uid 0 gid 0+0 context default) started; waiting... [ 26.859661][ T682] bc (682) used greatest stack depth: 10736 bytes left [ 26.900566][ T1] init: Service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)' (pid 669) exited with status 0 waiting took 0.288000 seconds [ 26.914751][ T1] init: Sending signal 9 to service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)' (pid 669) process group... [ 26.930271][ T1] libprocessgroup: Successfully killed process cgroup uid 0 pid 669 in 0ms evk_8mp:/ $ [ 27.545953][ T635] read descriptors [ 27.549703][ T635] read strings [ 27.553122][ T635] read descriptors [ 27.556734][ T635] read strings [ 27.575405][ T301] AidlLazyServiceRegistrar: Process has 1 (of 1 available) client(s) in use after notification apexservice has clients: 1 [ 27.588279][ T301] AidlLazyServiceRegistrar: Shutdown prevented by forcePersist override flag. [ 27.593152][ T202] type=1400 audit(1726034210.252:600): avc: denied { search } for comm="usb@1.3-service" name="usb" dev="sysfs" ino=29067 scontext=u:r:hal_usb_impl:s0 tcontext=u:object_r:sysfs_batteryinfo:s0 tclass=dir permissive=1 [ 27.597994][ T301] AidlLazyServiceRegistrar: Process has 0 (of 1 available) client(s) in use after notification apexservice has clients: 0 [ 27.634268][ T301] AidlLazyServiceRegistrar: Shutdown prevented by forcePersist override flag. [ 28.000874][ T321] imx-dwmac 30bf0000.ethernet eth1: PHY [stmmac-1:01] driver [RTL8211F Gigabit Ethernet] (irq=POLL) [ 28.013651][ T321] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0 [ 28.032667][ T321] imx-dwmac 30bf0000.ethernet eth1: No Safety Features support found [ 28.040691][ T321] imx-dwmac 30bf0000.ethernet eth1: IEEE 1588-2008 Advanced Timestamp supported [ 28.051729][ T321] imx-dwmac 30bf0000.ethernet eth1: registered PTP clock [ 28.064127][ T321] imx-dwmac 30bf0000.ethernet eth1: FPE workqueue start [ 28.071201][ T321] imx-dwmac 30bf0000.ethernet eth1: configuring for phy/rgmii-id link mode [ 28.105340][ T321] 8021q: adding VLAN 0 to HW filter on device eth1 re[ 28.308954][ T321] Generic PHY 30be0000.ethernet-1:01: attached PHY driver (mii_bus:phy_addr=30be0000.ethernet-1:01, irq=POLL) bo[ 28.792999][ T202] type=1400 audit(1726034211.452:601): avc: denied { read } for comm="main" name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 28.815896][ T202] type=1400 audit(1726034211.452:602): avc: denied { open } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 28.842279][ T202] type=1400 audit(1726034211.452:603): avc: denied { getattr } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 [ 28.868639][ T202] type=1400 audit(1726034211.452:604): avc: denied { map } for comm="main" path="/dev/__properties__/u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=321 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=1 ot [ 29.835152][ T124] init: Received sys.powerctl='reboot,shell' from pid: 832 (reboot) [ 29.843184][ T124] init: sys.powerctl: do_shutdown: 0 IsShuttingDown: 0 [ 29.982732][ T301] printk: binder:253_2: 109 output lines suppressed due to ratelimiting [ 30.094537][ T58] Unable to handle kernel paging request at virtual address ffffff80a0000000 [ 30.103304][ T58] Mem abort info: [ 30.106889][ T58] ESR = 0x96000045 [ 30.110733][ T58] EC = 0x25: DABT (current EL), IL = 32 bits [ 30.116859][ T58] SET = 0, FnV = 0 [ 30.120639][ T58] EA = 0, S1PTW = 0 [ 30.124638][ T58] FSC = 0x05: level 1 translation fault [ 30.130359][ T58] Data abort info: [ 30.134039][ T58] ISV = 0, ISS = 0x00000045 [ 30.138680][ T58] CM = 0, WnR = 1 [ 30.142455][ T58] swapper pgtable: 4k pages, 39-bit VAs, pgdp=0000000042a46000 [ 30.149942][ T58] [ffffff80a0000000] pgd=0000000000000000, p4d=0000000000000000, pud=0000000000000000 [ 30.159470][ T58] Internal error: Oops: 96000045 [#1] PREEMPT SMP [ 30.165759][ T58] Modules linked in: brcmfmac(E) dwmac_imx(E) dwmac_generic(E) stmmac_platform(E) stmmac(E) pcs_xpcs(E) realtek(E) fec(E) pci_imx6(E) rtc_snvs(E) rtc_ds1307(E) snd_sof_imx8m(E) imx_common(E) snd_sof_xtensa_dsp(E) snd_sof_of(E) snd_sof(E) imx_dsp(E) snd_soc_imx_rpmsg(E) snd_soc_imx_pcm512x_rpmsg(E) imx_audio_rpmsg(E) snd_soc_fsl_rpmsg(E) imx_pcm_rpmsg(E) i2c_rpmsg_imx(E) imx_dsp_rproc(E) imx_rproc(E) virtio_rpmsg_bus(E) rpmsg_ns(E) imx_mailbox(E) vsiv4l2(E) hantrodec_845s(E) hx280enc_vc8000e(E) snd_soc_fsl_asoc_card(E) snd_soc_imx_audmux(E) snd_soc_rt5651(E) snd_soc_imx_hdmi(E) snd_soc_imx_card(E) snd_soc_simple_card(E) snd_soc_simple_card_utils(E) snd_soc_bt_sco(E) snd_soc_hdmi_codec(E) dw_hdmi_gp_audio(E) dw_hdmi_cec(E) snd_soc_fsl_sai(E) snd_soc_fsl_easrc(E) snd_soc_fsl_asrc(E) snd_soc_fsl_aud2htx(E) snd_soc_fsl_micfil(E) imx_pcm_dma(E) imx8mm_thermal(E) galcore(E) brcmutil(E) pl2303(E) spi_nxp_fspi(E) spi_imx(E) spi_bitbang(E) spidev(E) st_lsm6dsx_i2c(E) [ 30.165910][ T58] st_lsm6dsx(E) kfifo_buf(E) simcom_wwan(E) option(E) usb_wwan(E) usbserial(E) gpio_pcf857x(E) leds_gpio(E) mac80211(E) cfg80211(E) vvcam_video(OE) vvcam_isp(OE) vvcam_dwe(OE) imx8_media_dev(CE) os08a20(OE) basler_camera_driver_vvcam(OE) trusty_virtio(E) trusty_ipc(E) trusty_log(E) trusty_irq(E) imx_sdma(E) imx8_mipi_csi2_sam(CE) imx8_capture(CE) imx8_isi_capture(CE) imx8_isi_mem2mem(CE) imx8_isi_hw(CE) ov5640(E) v4l2_fwnode(E) v4l2_async(E) imx_cpufreq_dt(E) cpufreq_dt(E) fsl_imx8_ddr_perf(E) device_cooling(E) nvmem_imx_ocotp(E) dummy_battery(E) gpio_switch(E) dwc3_imx8mp(E) panel_simple(E) drm_dp_aux_bus(E) panel_raydium_rm67191(E) sec_mipi_dsim_imx(E) imx_lcdifv3_crtc(E) imx_lcdifv3_core(E) imx_lcdif_crtc(E) imx8mp_ldb(E) dw_hdmi_imx(E) imx8mp_hdmi_pavi(E) imxdrm(E) cdns_mhdp_imx(E) dw_hdmi(E) sec_dsim(E) fsl_imx_ldb(E) cdns_mhdp_drmcore(E) imx_lcdif_core(E) synaptics_dsx_i2c(E) goodix(E) snvs_pwrkey(E) phy_fsl_imx8_pcie(E) phy_fsl_imx8mq_usb(E) [ 30.252445][ T58] phy_fsl_samsung_hdmi(E) phy_fsl_imx8mp_lvds(E) reset_imx7(E) dma_buf_imx(E) dsp_heap(E) secure_heap(E) cma_heap(E) system_heap(E) sdhci_esdhc_imx(E) pwm_bl(E) pwm_imx27(E) pca9450_regulator(E) i2c_dev(E) i2c_imx(E) imx2_wdt(E) imx(E) gpio_mxc(E) pinctrl_imx8mp(E) pinctrl_imx(E) irq_imx_irqsteer(E) trusty_core(E) busfreq_imx8mq(E) timer_imx_sysctr(E) imx8m_pm_domains(E) clk_blk_ctrl(E) clk_imx8mp(E) mxc_clk(E) mx8_mu(E) soc_imx8m(E) zram(E) zsmalloc(E) [ 30.379953][ T58] CPU: 3 PID: 58 Comm: dmabuf-deferred Tainted: G C OE 5.15.74-ge32688ce04b2 #4 [ 30.389872][ T58] Hardware name: NXP i.MX8MPlus EVK board (DT) [ 30.395882][ T58] pstate: 40400005 (nZcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 30.403544][ T58] pc : __memset+0x16c/0x188 [ 30.407915][ T58] lr : secure_heap_zero_buffer+0xb0/0x12c [secure_heap] [ 30.414715][ T58] sp : ffffffc00b5bbd10 [ 30.418725][ T58] x29: ffffffc00b5bbd30 x28: 0000000000000000 x27: ffffff800377d6c0 [ 30.426565][ T58] x26: ffffff800368da00 x25: 0000000000001800 x24: ffffffc00a8100a0 [ 30.434402][ T58] x23: 0000000000000800 x22: ffffff801b908578 x21: ffffffc0012e2234 [ 30.442244][ T58] x20: ffffff800368da10 x19: ffffff800368da00 x18: ffffffc00acad028 [ 30.450083][ T58] x17: 0000000000000000 x16: 000000000000033b x15: 00000000efe4b99a [ 30.457922][ T58] x14: 0000000000000010 x13: 0000000000007ff3 x12: 0000000000800000 [ 30.465759][ T58] x11: 0000000000000000 x10: 0000000000000001 x9 : 0000000000000000 [ 30.473598][ T58] x8 : ffffff80a0000000 x7 : 0000000000000000 x6 : 000000000000003f [ 30.481436][ T58] x5 : 0000000000000040 x4 : 0000000000000000 x3 : 0000000000000004 [ 30.489274][ T58] x2 : 0000000000000fc0 x1 : 0000000000000000 x0 : ffffff80a0000000 [ 30.497112][ T58] Call trace: [ 30.500257][ T58] __memset+0x16c/0x188 [ 30.504274][ T58] secure_heap_buf_free+0x2c/0xa0 [secure_heap] [ 30.510379][ T58] free_one_item+0xd0/0x10c [ 30.514743][ T58] deferred_free_thread+0x5c/0x10c [ 30.519725][ T58] kthread+0x170/0x1dc [ 30.523656][ T58] ret_from_fork+0x10/0x20 [ 30.527933][ T58] Code: 91010108 54ffff4a 8b040108 cb050042 (d50b7428) [ 30.534724][ T58] ---[ end trace a720f38a3ea3fddd ]--- [ 30.552554][ T58] Kernel panic - not syncing: Oops: Fatal exception [ 30.559006][ T58] SMP: stopping secondary CPUs [ 30.563939][ T58] Kernel Offset: disabled [ 30.568126][ T58] CPU features: 0x0,00004003,20000846 [ 30.573355][ T58] Memory Limit: none U-Boot SPL 2022.04-g534ef312df (Sep 11 2024 - 09:54:15 +0800) DDRINFO: start DRAM init DDRINFO: DRAM rate 4000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from MMC2 NOTICE: BL31: v2.6(release):43e7343944 NOTICE: BL31: Built : 03:00:34, May 24 2023 U-Boot 2022.04-g534ef312df (Sep 11 2024 - 09:54:15 +0800) CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz) CPU: Industrial temperature grade (-40C to 105C) at 47C Reset cause: POR Model: NXP i.MX8MPlus LPDDR4 EVK board DRAM: 2 GiB Core: 85 devices, 23 uclasses, devicetree: separate MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial BuildInfo: - ATF 43e7343 flash target is MMC:2 Net: Warning: ethernet@30bf0000 (eth1) using random MAC address - 66:7f:8b:44:4e:03 Could not get PHY for FEC0: addr 1 Could not get PHY for FEC0: addr 1 eth1: ethernet@30bf0000 [PRIME] Fastboot: Normal Normal Boot Hit any key to stop autoboot: 2