[2023-12-14 11:07:14] U-Boot SPL 2022.04-imx_v2022.04_5.15.71-2.2.0+gdd855a0ccf (Oct 09 2023 - 12:19:36 +0000) [2023-12-14 11:07:14] DDRINFO: start DRAM init [2023-12-14 11:07:14] DDRINFO: DRAM rate 4000MTS [2023-12-14 11:07:14] DDRINFO:ddrphy calibration done [2023-12-14 11:07:14] DDRINFO: ddrmix config done [2023-12-14 11:07:14] AURORA: setup init AURORA ... Done [2023-12-14 11:07:14] SEC0: RNG instantiated [2023-12-14 11:07:14] Normal Boot [2023-12-14 11:07:14] Trying to boot from BOOTROM [2023-12-14 11:07:14] Boot Stage: Primary boot [2023-12-14 11:07:14] image offset 0x8000, pagesize 0x200, ivt offset 0x0 [2023-12-14 11:07:14] NOTICE: BL31: v2.6(release):automotive-13.0.0_1.1.0-0-g3c1583ba0 [2023-12-14 11:07:14] NOTICE: BL31: Built : 11:00:38, Nov 21 2022 [2023-12-14 11:07:14] [2023-12-14 11:07:14] [2023-12-14 11:07:14] U-Boot 2022.04-imx_v2022.04_5.15.71-2.2.0+gdd855a0ccf (Oct 09 2023 - 12:19:36 +0000) [2023-12-14 11:07:14] [2023-12-14 11:07:14] CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz) [2023-12-14 11:07:14] CPU: Industrial temperature grade (-40C to 105C) at 29C [2023-12-14 11:07:15] Reset cause: POR [2023-12-14 11:07:15] Model: MNAS0080 [2023-12-14 11:07:15] DRAM: 2 GiB [2023-12-14 11:07:15] Core: 86 devices, 23 uclasses, devicetree: separate [2023-12-14 11:07:15] MMC: FSL_SDHC: 1, FSL_SDHC: 2 [2023-12-14 11:07:15] Loading Environment from MMC... *** Warning - bad CRC, using default environment [2023-12-14 11:07:15] [2023-12-14 11:07:15] In: serial [2023-12-14 11:07:15] Out: serial [2023-12-14 11:07:15] Err: serial [2023-12-14 11:07:15] SEC0: RNG instantiated [2023-12-14 11:07:15] [2023-12-14 11:07:15] BuildInfo: [2023-12-14 11:07:15] - ATF 3c1583b [2023-12-14 11:07:15] [2023-12-14 11:07:15] switch to partitions #0, OK [2023-12-14 11:07:15] mmc1 is current device [2023-12-14 11:07:15] flash target is MMC:1 [2023-12-14 11:07:15] Net: [2023-12-14 11:07:15] Warning: ethernet@30bf0000 (eth1) using random MAC address - ee:6d:80:6f:e2:cb [2023-12-14 11:07:15] eth1: ethernet@30bf0000 [PRIME] [2023-12-14 11:07:15] Fastboot: Normal [2023-12-14 11:07:15] Normal Boot [2023-12-14 11:07:15] Hit any key to stop autoboot: 0 [2023-12-14 11:07:17] switch to partitions #0, OK [2023-12-14 11:07:17] mmc1 is current device [2023-12-14 11:07:17] Scanning mmc 1:1... [2023-12-14 11:07:17] switch to partitions #0, OK [2023-12-14 11:07:17] mmc2(part 0) is current device [2023-12-14 11:07:17] Scanning mmc 2:1... [2023-12-14 11:07:17] Running BSP bootcmd ... [2023-12-14 11:07:17] switch to partitions #0, OK [2023-12-14 11:07:17] mmc1 is current device [2023-12-14 11:07:17] Failed to load 'boot.scr' [2023-12-14 11:07:17] Error reading cluster [2023-12-14 11:07:17] ** Unable to read file Image ** [2023-12-14 11:07:17] Failed to load 'Image' [2023-12-14 11:07:17] END BOOTING