U-Boot SPL 2022.04 (Jul 06 2023 - 17:26:33 +0530) Normal Boot Trying to boot from MMC1 Authentication key not yet programmed Booting from bootloader_a... UU boot args 0x*** 0x*** 0x*** 0x0 initializing trusty (Project: imx8qm_a72, Build: build@pantakill-5, Built: 10:05:29 Nov 8 2022) Core: 180 devices, 28 uclasses, devicetree: separate MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment [*]-Video Link 0it6263_i2c_reg_read, read err 3 faill to read from it6263 revision, ret 3 (1280 x 720) [0] dpu@56180000, video [1] lvds-channel@0, display [2] lvds-to-hdmi-bridge@4c, video_bridge In: serial Out: serial Err: serial BuildInfo: - SCFW 6638c032, SECO-FW c9de51c0, IMX-MKIMAGE 3bfcfccb, ATF 3c1583b - U-Boot 2022.04 flash target is MMC:0 Net: eth0: ethernet@5b040000 [PRIME], eth1: ethernet@5b050000 INFO Initializing Trusty device INFO selected trusty api version: 3 (requested 3) INFO Initializing Trusty IPC device INFO Initializing RPMB storage proxy service Authentication key not yet programmed rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7 Authentication key not yet programmed rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7 Authentication key not yet programmed rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7 failed to read rpmb write counter Authentication key not yet programmed rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7 ss: block_device_tipc_init: bad static rpmb size, 2048 ss: proxy_connect: block_device_tipc_init failed (-1) Authentication key not yet programmed INFO Initializing Trusty Hardware Crypto client Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized Verifying slot _a ... avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized fsl_validate_vbmeta_public_key_rpmb: Read public key error avb_slot_verify.c:899: ERROR: vbmeta_a: Public key used to sign data rejected. avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized fsl_read_rollback_index_rpmb: read rollback from Trusty error! Authentication key not yet programmed avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized fsl_read_rollback_index_rpmb: read rollback from Trusty error! Authentication key not yet programmed avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized fsl_read_rollback_index_rpmb: read rollback from Trusty error! Authentication key not yet programmed avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized verify FAIL, state: UNLOCK boot 'boot_a' still Kernel load addr 0x80280000 size 21851 KiB kernel @ 80280000 (43253760) ramdisk @ fc000000 (19755629) fdt @ 82d40400 (138648) avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized ERROR - failed to read public key for keymaster keymaster.c:318: ERROR Keymaster TIPC client not initialized! keymaster.c:684: ERROR Keymaster TIPC client not initialized! boota: set boot patch level failed. avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized Authentication key not yet programmed Moving Image from 0x80280000 to 0x80400000, end=82d40000 ## Flattened Device Tree blob at 82d40400 Booting using the fdt blob at 0x82d40400 ERROR: reserving fdt memory region failed (addr=900ff000 size=1000 flags=4) ERROR: reserving fdt memory region failed (addr=90400000 size=100000 flags=4) ERROR: reserving fdt memory region failed (addr=90100000 size=8000 flags=4) ERROR: reserving fdt memory region failed (addr=90108000 size=8000 flags=4) ERROR: reserving fdt memory region failed (addr=90110000 size=8000 flags=4) ERROR: reserving fdt memory region failed (addr=90118000 size=8000 flags=4) ERROR: reserving fdt memory region failed (addr=901ff000 size=1000 flags=4) ERROR: reserving fdt memory region failed (addr=91f00000 size=100000 flags=0) Using Device Tree in place at 0000000082d40400, end 0000000082d65197 Starting kernel ... [ 0.000000][ T0] Booting Linux on physical CPU 0x0000000100 [0x410fd082] [ 0.000000][ T0] Linux version 5.15.71-dirty (quest@TVMLT1796) (Android (8508608, based on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4c603 [ 0.000000][ T0] Machine model: Freescale i.MX8QM MEK [ 0.000000][ T0] Stack Depot is disabled [ 0.000000][ T0] earlycon: lpuart32 at MMIO32 0x000000005a060000 (options '') [ 0.000000][ T0] printk: bootconsole [lpuart32] enabled [ 0.000000][ T0] efi: UEFI not found. [ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB [ 0.000000][ T0] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool [ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB [ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool [ 0.000000][ T0] kvm [0]: Reserved 36 MiB at 0x97d000000 [ 0.000000][ T0] Zone ranges: [ 0.000000][ T0] DMA32 [mem 0x0000000080200000-0x00000000ffffffff] [ 0.000000][ T0] Normal [mem 0x0000000100000000-0x000000097fffffff] [ 0.000000][ T0] Movable zone start for each node [ 0.000000][ T0] Early memory node ranges [ 0.000000][ T0] node 0: [mem 0x0000000080200000-0x0000000083ffffff] [ 0.000000][ T0] node 0: [mem 0x0000000084000000-0x00000000863fffff] [ 0.000000][ T0] node 0: [mem 0x0000000086400000-0x00000000887fffff] [ 0.000000][ T0] node 0: [mem 0x000000008a800000-0x000000008fffffff] [ 0.000000][ T0] node 0: [mem 0x0000000090c00000-0x0000000091ffffff] [ 0.000000][ T0] node 0: [mem 0x0000000092000000-0x00000000920fffff] [ 0.000000][ T0] node 0: [mem 0x0000000092100000-0x00000000923fffff] [ 0.000000][ T0] node 0: [mem 0x0000000092400000-0x00000000951fffff] [ 0.000000][ T0] node 0: [mem 0x0000000095200000-0x00000000fdffffff] [ 0.000000][ T0] node 0: [mem 0x0000000880000000-0x000000088fffffff] [ 0.000000][ T0] node 0: [mem 0x0000000890000000-0x000000097fffffff] [ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff] [ 0.000000][ T0] On node 0, zone DMA32: 512 pages in unavailable ranges [ 0.000000][ T0] On node 0, zone DMA32: 8192 pages in unavailable ranges [ 0.000000][ T0] On node 0, zone DMA32: 3072 pages in unavailable ranges [ 0.000000][ T0] On node 0, zone Normal: 8192 pages in unavailable ranges [ 0.000000][ T0] cma: Reserved 928 MiB at 0x00000000c2000000 [ 0.000000][ T0] psci: probing for conduit method from DT. [ 0.000000][ T0] psci: PSCIv1.1 detected in firmware. [ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs [ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000][ T0] psci: SMC Calling Convention v1.2 [ 0.000000][ T0] Load bootconfig: 1018 bytes 64 nodes [ 0.000000][ T0] percpu: Embedded 29 pages/cpu s81752 r8192 d28840 u118784 [ 0.000000][ T0] Detected PIPT I-cache on CPU0 [ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0 [ 0.000000][ T0] CPU features: detected: GIC system register CPU interface [ 0.000000][ T0] CPU features: detected: Spectre-v2 [ 0.000000][ T0] CPU features: detected: Spectre-v3a [ 0.000000][ T0] CPU features: detected: Spectre-BHB [ 0.000000][ T0] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 1528328 [ 0.000000][ T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init firmware_clag [ 0.000000][ T0] cgroup: Disabling pressure control group feature [ 0.000000][ T0] Unknown kernel command line parameters "buildvariant=userdebug", will be passed to user space. [ 0.000000][ T0] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear) [ 0.000000][ T0] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off [ 0.000000][ T0] software IO TLB: mapped [mem 0x00000000be000000-0x00000000c2000000] (64MB) [ 0.000000][ T0] Memory: 4624248K/6211584K available (18496K kernel code, 2262K rwdata, 19200K rodata, 1472K init, 613K bss, 637064K reserved, 950272K cma-reserved) [ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1 [ 0.000000][ T0] trace event string verifier disabled [ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation. [ 0.000000][ T0] rcu: RCU event tracing is enabled. [ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled. [ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=6. [ 0.000000][ T0] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000][ T0] Trampoline variant of Tasks RCU enabled. [ 0.000000][ T0] Tracing variant of Tasks RCU enabled. [ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6 [ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000][ T0] GICv3: 512 SPIs implemented [ 0.000000][ T0] GICv3: 0 Extended SPIs implemented [ 0.000000][ T0] GICv3: Distributor has no Range Selector support [ 0.000000][ T0] Root IRQ handler: gic_handle_irq.0063cfc43c850c778600e9fd9282e821.cfi_jt [ 0.000000][ T0] GICv3: 16 PPIs implemented [ 0.000000][ T0] GICv3: CPU0: found redistributor 100 region 0:0x0000000051b80000 [ 0.000000][ T0] ITS: No ITS available, not enabling LPIs [ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none). [ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____) [ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys). [ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns [ 0.000000][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns [ 0.009346][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000) [ 0.019965][ T0] pid_max: default: 32768 minimum: 301 [ 0.025434][ T0] LSM: Security Framework initializing [ 0.030612][ T0] SELinux: Initializing. [ 0.034961][ T0] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.043027][ T0] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.053436][ T1] rcu: Hierarchical SRCU implementation. [ 0.059259][ T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build [ 0.067773][ T1] EFI services will not be available. [ 0.073121][ T1] smp: Bringing up secondary CPUs ... [ 0.079248][ T0] Detected PIPT I-cache on CPU1 [ 0.079286][ T0] GICv3: CPU1: found redistributor 101 region 0:0x0000000051ba0000 [ 0.079321][ T0] CPU1: Booted secondary processor 0x0000000101 [0x410fd082] [ 0.081646][ T0] CPU features: detected: ARM erratum 845719 [ 0.081665][ T0] Detected VIPT I-cache on CPU2 [ 0.081697][ T0] GICv3: CPU2: found redistributor 0 region 0:0x0000000051b00000 [ 0.081750][ T0] CPU2: Booted secondary processor 0x0000000000 [0x410fd034] [ 0.083101][ T0] Detected VIPT I-cache on CPU3 [ 0.083120][ T0] GICv3: CPU3: found redistributor 1 region 0:0x0000000051b20000 [ 0.083145][ T0] CPU3: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.084398][ T0] Detected VIPT I-cache on CPU4 [ 0.084418][ T0] GICv3: CPU4: found redistributor 2 region 0:0x0000000051b40000 [ 0.084443][ T0] CPU4: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.085681][ T0] Detected VIPT I-cache on CPU5 [ 0.085701][ T0] GICv3: CPU5: found redistributor 3 region 0:0x0000000051b60000 [ 0.085725][ T0] CPU5: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.085838][ T1] smp: Brought up 1 node, 6 CPUs [ 0.193608][ T1] SMP: Total of 6 processors activated. [ 0.198985][ T1] CPU features: detected: 32-bit EL0 Support [ 0.204813][ T1] CPU features: detected: 32-bit EL1 Support [ 0.210624][ T1] CPU features: detected: CRC32 instructions [ 0.216455][ T1] CPU features: detected: Protected KVM [ 0.222015][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching [ 0.252962][ T1] CPU: All CPU(s) started at EL2 [ 0.257473][ T19] alternatives: patching kernel code [ 0.279438][ T1] Registered cp15_barrier emulation handler [ 0.284865][ T1] Registered setend emulation handler [ 0.290071][ T1] KASLR disabled due to lack of seed [ 0.295393][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.305667][ T1] futex hash table entries: 2048 (order: 5, 131072 bytes, linear) [ 0.327068][ T1] pinctrl core: initialized pinctrl subsystem [ 0.333595][ T1] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.342462][ T1] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations [ 0.350776][ T1] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.359226][ T1] audit: initializing netlink subsys (disabled) [ 0.365397][ T58] audit: type=2000 audit(0.268:1): state=initialized audit_enabled=0 res=1 [ 0.365744][ T1] thermal_sys: Registered thermal governor 'step_wise' [ 0.373658][ T1] thermal_sys: Registered thermal governor 'user_space' [ 0.380341][ T1] thermal_sys: Registered thermal governor 'power_allocator' [ 0.387706][ T1] cpuidle: using governor menu [ 0.399360][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.406799][ T1] ASID allocator initialised with 65536 entries [ 0.412851][ T1] Serial: AMBA PL011 UART driver [ 0.417571][ T1] imx mu driver is registered. [ 0.422139][ T1] imx rpmsg driver is registered. [ 0.428267][ T1] printk: console [ramoops-1] enabled [ 0.433236][ T1] pstore: Registered ramoops as persistent store backend [ 0.440018][ T1] ramoops: using 0x100000@0x91f00000, ecc: 0 [ 0.473560][ T1] platform bus@56240000:ldb@562410e0: Fixing up cyclic dependency with 56180000.dpu [ 0.494098][ T63] cryptomgr_test (63) used greatest stack depth: 14064 bytes left [ 0.507389][ C1] SError Interrupt on CPU1, code 0xbf000002 -- SError [ 0.507398][ C1] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.15.71-dirty #1 [ 0.507403][ C1] Hardware name: Freescale i.MX8QM MEK (DT) [ 0.507406][ C1] pstate: 20400005 (nzCv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 0.507411][ C1] pc : log_post_write_mmio+0x20/0xfc [ 0.507424][ C1] lr : writel+0x5c/0x74 [ 0.507432][ C1] sp : ffffffc00a98b940 [ 0.507434][ C1] x29: ffffffc00a98b960 x28: 0000000000000000 x27: 0000000000000000 [ 0.507442][ C1] x26: 0000000000000000 x25: 0000000000000000 x24: 0000000000000000 [ 0.507448][ C1] x23: ffffffc00a917b50 x22: ffffff88ff4812a0 x21: 00000000ffffffff [ 0.507453][ C1] x20: 00000000ffffffff x19: ffffffc00b130018 x18: ffffffc00a9550a8 [ 0.507459][ C1] x17: 00000000fc9cb141 x16: 00000000000000b4 x15: ffffffc00b141000 [ 0.507464][ C1] x14: ffffffc009d0a7e0 x13: 00000000000000d0 x12: 000000003d090000 [ 0.507470][ C1] x11: 0000000000000000 x10: ffffff88102d5a00 x9 : ffffffc00b130000 [ 0.507475][ C1] x8 : 0000000000000018 x7 : 7f7f7f7f7f7f7f7f x6 : feff6e686f662c34 [ 0.507480][ C1] x5 : 8080000000000000 x4 : 0000000000000030 x3 : ffffffc008021024 [ 0.507485][ C1] x2 : ffffffc00b130018 x1 : 0000000000000020 x0 : 00000000ffffffff [ 0.507492][ C1] Kernel panic - not syncing: Asynchronous SError Interrupt [ 0.507495][ C1] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.15.71-dirty #1 [ 0.507498][ C1] Hardware name: Freescale i.MX8QM MEK (DT) [ 0.507501][ C1] Call trace: [ 0.507502][ C1] dump_backtrace.cfi_jt+0x0/0x4 [ 0.507511][ C1] show_stack+0x1c/0x2c [ 0.507517][ C1] dump_stack_lvl+0x64/0x94 [ 0.507521][ C1] panic+0x164/0x414 [ 0.507526][ C1] nmi_panic+0x98/0xbc [ 0.507530][ C1] arm64_serror_panic+0x70/0x98 [ 0.507533][ C1] do_serror+0x104/0x148 [ 0.507537][ C1] el1h_64_error_handler+0x38/0x50 [ 0.507545][ C1] el1h_64_error+0x7c/0x80 [ 0.507548][ C1] log_post_write_mmio+0x20/0xfc [ 0.507552][ C1] writel+0x5c/0x74 [ 0.507556][ C1] mxc_gpio_probe+0x264/0x60c [ 0.507563][ C1] platform_probe+0xc8/0x114 [ 0.507570][ C1] really_probe+0x14c/0x4cc [ 0.507574][ C1] __driver_probe_device+0xbc/0xe8 [ 0.507578][ C1] driver_probe_device+0x4c/0x1a0 [ 0.507582][ C1] __driver_attach+0x114/0x1fc [ 0.507586][ C1] bus_for_each_dev+0xac/0x124 [ 0.507589][ C1] driver_attach+0x28/0x38 [ 0.507592][ C1] bus_add_driver+0x114/0x204 [ 0.507596][ C1] driver_register+0x7c/0x11c [ 0.507599][ C1] __platform_driver_register+0x28/0x38 [ 0.507604][ C1] gpio_mxc_init+0x2c/0x3c [ 0.507612][ C1] __initstub__kmod_gpio_mxc__348_842_gpio_mxc_init4.cfi+0x14/0x24 [ 0.507618][ C1] do_one_initcall+0xe0/0x344 [ 0.507623][ C1] do_initcall_level+0xc4/0x188 [ 0.507629][ C1] do_initcalls+0x58/0x9c [ 0.507634][ C1] do_basic_setup+0x20/0x30 [ 0.507638][ C1] kernel_init_freeable+0xe8/0x148 [ 0.507643][ C1] kernel_init+0x24/0x1ac [ 0.507647][ C1] ret_from_fork+0x10/0x20 [ 0.507651][ C1] SMP: stopping secondary CPUs