////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// uuu log U-Boot SPL 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000) power_bd71837_init DDRINFO: start DRAM init DDRINFO: DRAM rate 3000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from USB SDP SDP: initialize... SDP: handle requests... Downloading file of size 1793152 to 0x40400000... done Jumping to header at 0x40400000 Header Tag is not an IMX image Found header at 0x404285a0 NOTICE: BL31: v2.4(release):lf-5.15.5-1.0.0-0-g05f788b9b NOTICE: BL31: Built : 05:49:10, Mar 2 2022 U-Boot 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000) CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz) CPU: Commercial temperature grade (0C to 95C) at 30C Reset cause: POR Model: NXP i.MX8MM EVK board DRAM: 2 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52] Power supply on USB2 TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50] MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... MMC: no card present *** Warning - No block device, using default environment Fail to setup video link In: serial Out: serial Err: serial SEC0: RNG instantiated BuildInfo: - ATF 05f788b MMC: no card present Detect USB boot. Will enter fastboot mode! Net: eth0: ethernet@30be0000 Fastboot: Normal Boot from USB for mfgtools *** Warning - Use default environment for mfgtools , using default environment Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi; Hit any key to stop autoboot: 0 ## Checking Image at 43800000 ... Unknown image format! Run fastboot ... Detect USB boot. Will enter fastboot mode! flash target is MMC:1 MMC: no card present MMC card init failed! MMC: no card present ** Block device MMC 1 not supported Detect USB boot. Will enter fastboot mode! flash target is MMC:2 switch to partitions #0, OK mmc2(part 0) is current device Detect USB boot. Will enter fastboot mode! Starting download of 16776232 bytes .......................................................................... ..................................................... downloading of 16776232 bytes finished writing to partition 'all' sparse flash target is mmc:2 writing to partition 'all' for sparse, buffer size 16776232 Flashing sparse image at offset 0 Flashing Sparse Image ........ wrote 16776192 bytes to 'all' Starting download of 16776244 bytes /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Normal boot log U-Boot SPL 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000) power_bd71837_init DDRINFO: start DRAM init DDRINFO: DRAM rate 3000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from MMC2 NOTICE: BL31: v2.4(release):lf-5.15.5-1.0.0-0-g05f788b9b NOTICE: BL31: Built : 05:49:10, Mar 2 2022 U-Boot 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000) CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz) CPU: Commercial temperature grade (0C to 95C) at 31C Reset cause: POR Model: NXP i.MX8MM EVK board DRAM: 2 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52] Power supply on USB2 TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50] MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... *** Warning - bad CRC, using default environment Fail to setup video link In: serial Out: serial Err: serial SEC0: RNG instantiated BuildInfo: - ATF 05f788b switch to partitions #0, OK mmc2(part 0) is current device flash target is MMC:2 Net: eth0: ethernet@30be0000 Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 starting USB... Bus usb@32e40000: Port not available. USB is stopped. Please issue 'usb start' first. MMC: no card present switch to partitions #0, OK mmc2(part 0) is current device Scanning mmc 2:1... 43714 bytes read in 10 ms (4.2 MiB/s) MMC: no card present Scanning disk mmc@30b50000.blk... Disk mmc@30b50000.blk not ready Scanning disk mmc@30b60000.blk... Found 3 disks No EFI system partition BootOrder not defined EFI boot manager: Cannot load any image Running BSP bootcmd ... switch to partitions #0, OK mmc2(part 0) is current device Failed to load 'boot.scr' 33055232 bytes read in 100 ms (315.2 MiB/s) Booting from mmc ... 43714 bytes read in 13 ms (3.2 MiB/s) Moving Image from 0x40480000 to 0x40600000, end=42620000 ## Flattened Device Tree blob at 43000000 Booting using the fdt blob at 0x43000000 Using Device Tree in place at 0000000043000000, end 000000004300dac1 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.15.5-lts-next+ge347576a1d23 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #1 SMP PREEMPT Mon Mar 7 20:03:59 UTC 2022 [ 0.000000] Machine model: FSL i.MX8MM EVK board [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 640 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] NUMA: No NUMA configuration found [ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] NUMA: NODE_DATA [mem 0x95bd8800-0x95bdafff] [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 20 pages/cpu s41048 r8192 d32680 u81920 [ 0.000000] Detected VIPT I-cache on CPU0