U-Boot SPL 2021.04-00445-g5ef62652ae (Oct 13 2022 - 10:09:52 +0000) Can't find PMIC:PFUZE100 DDRINFO: start DRAM init DDRINFO: DRAM rate 3200MTS=Select Entry DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from MMC2 U-Boot 2021.04-00445-g5ef62652ae (Oct 13 2022 - 10:09:52 +0000) CPU: i.MX8MQ rev2.1 1300 MHz (running at 800 MHz) CPU: Industrial temperature grade (-40C to 105C) at 56C Reset cause: POR Model: NXP i.MX8MQ EVK DRAM: 3 GiB setup_typec: tcpc init failed, err=-62 MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment [*]-Video Link 0imx8m_hdmi_probe cdn_api_checkalive: keep-alive counter did not increment for 10us... HDMI enable failed, ret -1! (1280 x 720) [0] display-controller@32e00000, video [1] hdmi@32c00000, display In: serial Out: serial Err: serial SEC0: RNG instantiated BuildInfo: - ATF 24ddf8f switch to partitions #0, OK mmc1 is current device flash target is MMC:1 Net: Could not get PHY for FEC0: addr 0 Could not get PHY for FEC0: addr 0 No ethernet found. Fastboot: Normal Normal Boot starting USB... Bus usb@38100000: Failed to initialize board for imx8m USB probe failed, error -5 Bus usb@38200000: Register 2000140 NbrPorts 2 Starting the controller USB XHCI 1.10 scanning bus usb@38200000 for devices... 1 USB Device(s) found scanning usb for storage devices... 0 Storage Device(s) found switch to partitions #0, OK mmc1 is current device MMC read: dev # 1, block # 3946, count 4096 ... 4096 blocks read: OK ## Loading kernel from FIT Image at 40480000 ... Using 'conf-1' configuration Trying 'uefi' kernel subimage Description: UEFI Type: Kernel Image Compression: uncompressed Data Start: 0x404800a4 Data Size: 2064384 Bytes = 2 MiB Architecture: AArch64 OS: Linux Load Address: 0x50004000 Entry Point: 0x50004000 Hash algo: sha256 Hash value: 512ecc4f0d6276f6aff0624d7887cdba51d305ac7d82b48ba4d5bfd2185e06e1 Verifying Hash Integrity ... sha256+ OK Loading Kernel Image Starting kernel ... UEFI Debug Serial Port Init UEFI firmware (version 2020-06-07 built at 10:13:33 on Oct 13 2022)