/* * Copyright 2020 NXP * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * as published by the Free Software Foundation; either version 2 * of the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. */ #include "imx8qm-mek-car2.dts" / { lvds1_panel { compatible = "jdi,tx26d202vm0bwa"; backlight = <&lvds_backlight1>; port { panel_lvds1_in: endpoint { remote-endpoint = <&lvds1_out>; }; }; }; }; &ldb1_phy { status = "disabled"; }; &ldb1 { status = "disabled"; }; &i2c1_lvds0 { lvds-to-hdmi-bridge@4c { status = "disabled"; }; }; /delete-node/ &it6263_1_in; &ldb2 { status = "okay"; fsl,dual-channel; lvds-channel@0 { fsl,data-mapping = "spwg"; fsl,data-width = <24>; status = "okay"; port@1 { reg = <1>; lvds1_out: endpoint { remote-endpoint = <&panel_lvds1_in>; }; }; }; };