uuu.exe -v -b emmc_all signed_flash.bin imx-image-core-imx8mq-evk-20220523101745.rootfs.wic uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.193-0-ge56424c Build in config: Pctl Chip Vid Pid BcdVersion ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 Run built-in script: uuu_version 1.4.149 # @_flash.bin | bootloader, which can extract from wic image # @_image [_flash.bin] | wic image burn to emmc. # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f signed_flash.bin -scanlimited 0x800000 # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -scanterm -f signed_flash.bin -scanlimited 0x800000 # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f signed_flash.bin -offset 0x57c00 SDPU: jump -scanlimited 0x800000 # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f signed_flash.bin -skipspl -scanterm -scanlimited 0x800000 SDPV: jump -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all imx-image-core-imx8mq-evk-20220523101745.rootfs.wic FB: flash -scanterm -scanlimited 0x800000 bootloader signed_flash.bin FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done Wait for Known USB Device Appear... New USB Device Attached at 1:3 1:3>Start Cmd:SDP: boot -f signed_flash.bin -scanlimited 0x800000 100%1:3>Okay (0.622s) New USB Device Attached at 1:3 1:3>Start Cmd:SDPV: delay 1000 1:3>Okay (1.002s) 1:3>Start Cmd:SDPV: write -f signed_flash.bin -skipspl -scanterm -scanlimited 0x800000 100%1:3>Okay (2.459s) 1:3>Start Cmd:SDPV: jump -scanlimited 0x800000 100%1:3>Okay (0.942s) New USB Device Attached at 1:3 1:3>Start Cmd:SDP: boot -f signed_flash.bin -scanlimited 0x800000 100%1:3>Okay (0.643s) New USB Device Attached at 1:3 1:3>Start Cmd:SDPV: delay 1000 1:3>Okay (1.002s) 1:3>Start Cmd:SDPV: write -f signed_flash.bin -skipspl -scanterm -scanlimited 0x800000 100%1:3>Okay (2.482s) 1:3>Start Cmd:SDPV: jump -scanlimited 0x800000 100%1:3>Okay (0.934s)