: serial switch to partitions #0, OK mmc0 is current device flash target is MMC:0 Net: No ethernet found. Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device 8655408 bytes read in 432 ms (19.1 MiB/s) Booting from mmc ... 50336 bytes read in 19 ms (2.5 MiB/s) Kernel image @ 0x12000000 [ 0x000000 - 0x841230 ] ## Flattened Device Tree blob at 18000000 Booting using the fdt blob at 0x18000000 Using Device Tree in place at 18000000, end 1800f49f switch to ldo_bypass mode! Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.4.47-2.2.0+g5ec03d06f54e (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Nov 30 13:43:33 UTC 2021 [ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TSV i.MX6 Quad Plus Starlite X Board [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] percpu: Embedded 15 pages/cpu s32076 r8192 d21172 u61440 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259840 [ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 691364K/1048576K available (11264K kernel code, 587K rwdata, 4216K rodata, 1024K init, 441K bss, 29532K reserved, 327680K cma-reserved, 0K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] L2C-310 erratum 769419 enabled [ 0.000000] L2C-310 enabling early BRESP for Cortex-A9 [ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9 [ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines [ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled [ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB [ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001 [ 0.000000] random: get_random_bytes called from start_kernel+0x2c8/0x488 with crng_init=0 [ 0.000000] Switching to timer-based delay loop, resolution 333ns [ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns [ 0.000031] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns [ 0.001420] Console: colour dummy device 80x30 [ 0.001450] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000) [ 0.001465] pid_max: default: 32768 minimum: 301 [ 0.001642] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.001663] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.002415] CPU: Testing write buffer coherency: ok [ 0.002446] CPU0: Spectre v2: using BPIALL workaround [ 0.002735] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.059653] Setting up static identity map for 0x10100000 - 0x10100060 [ 0.079598] rcu: Hierarchical SRCU implementation. [ 0.119598] smp: Bringing up secondary CPUs ... [ 0.199865] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.199872] CPU1: Spectre v2: using BPIALL workaround [ 0.279858] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002 [ 0.279866] CPU2: Spectre v2: using BPIALL workaround [ 0.359857] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003 [ 0.359866] CPU3: Spectre v2: using BPIALL workaround [ 0.359975] smp: Brought up 1 node, 4 CPUs [ 0.359986] SMP: Total of 4 processors activated (24.00 BogoMIPS). [ 0.359994] CPU: All CPU(s) started in SVC mode. [ 0.360347] devtmpfs: initialized [ 0.369452] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 [ 0.369889] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.369911] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.386734] pinctrl core: initialized pinctrl subsystem [ 0.387762] NET: Registered protocol family 16 [ 0.395574] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.396535] cpuidle: using governor menu [ 0.396720] CPU identified as i.MX6QP, silicon rev 1.0 [ 0.404233] vdd1p1: supplied by regulator-dummy [ 0.404767] vdd3p0: supplied by regulator-dummy [ 0.405252] vdd2p5: supplied by regulator-dummy [ 0.405752] vddarm: bypassed regulator has no supply! [ 0.405762] vddarm: failed to get the current voltage(-517) [ 0.405779] anatop_regulator 20c8000.anatop:regulator-vddcore: failed to register vddarm [ 0.406486] vddsoc: bypassed regulator has no supply! [ 0.406496] vddsoc: failed to get the current voltage(-517) [ 0.406510] anatop_regulator 20c8000.anatop:regulator-vddsoc: failed to register vddsoc [ 0.406881] mxs_phy 20c9000.usbphy: 20c9000.usbphy supply phy-3p0 not found, using dummy regulator [ 0.407331] mxs_phy 20ca000.usbphy: 20ca000.usbphy supply phy-3p0 not found, using dummy regulator [ 0.418899] No ATAGs? [ 0.419037] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. [ 0.419052] hw-breakpoint: maximum watchpoint size is 4 bytes. [ 0.420630] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver [ 0.422909] imx mu driver is registered. [ 0.423342] imx rpmsg driver is registered. [ 0.452025] vgaarb: loaded [ 0.452767] SCSI subsystem initialized [ 0.453217] usbcore: registered new interface driver usbfs [ 0.453270] usbcore: registered new interface driver hub [ 0.453354] usbcore: registered new device driver usb [ 0.453491] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator [ 0.453707] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator [ 0.454986] i2c i2c-1: IMX I2C adapter registered [ 0.455453] gpio-3 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file [ 0.455861] i2c i2c-2: IMX I2C adapter registered [ 0.456240] videodev: Linux video capture interface: v2.00 [ 0.456301] pps_core: LinuxPPS API ver. 1 registered [ 0.456310] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.456330] PTP clock support registered [ 0.479719] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) [ 0.509658] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) [ 0.510726] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed [ 0.511070] imx-prg 21cc000.prg: driver probed [ 0.511200] imx-prg 21cd000.prg: driver probed [ 0.511575] imx-pre 21c8000.pre: driver probed [ 0.511773] imx-pre 21c9000.pre: driver probed [ 0.511979] imx-pre 21ca000.pre: driver probed [ 0.512184] imx-pre 21cb000.pre: driver probed [ 0.512459] MIPI CSI2 driver module loaded [ 0.512511] Advanced Linux Sound Architecture Driver Initialized. [ 0.513483] Bluetooth: Core ver 2.22 [ 0.513528] NET: Registered protocol family 31 [ 0.513537] Bluetooth: HCI device and connection manager initialized [ 0.513552] Bluetooth: HCI socket layer initialized [ 0.513564] Bluetooth: L2CAP socket layer initialized [ 0.513588] Bluetooth: SCO socket layer initialized [ 0.514036] clocksource: Switched to clocksource mxc_timer1 [ 0.514218] VFS: Disk quotas dquot_6.6.0 [ 0.514307] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.522741] thermal_sys: Registered thermal governor 'step_wise' [ 0.523085] NET: Registered protocol family 2 [ 0.523614] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) [ 0.523651] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) [ 0.523733] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.523870] TCP: Hash tables configured (established 8192 bind 8192) [ 0.524072] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.524111] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.524312] NET: Registered protocol family 1 [ 0.524892] RPC: Registered named UNIX socket transport module. [ 0.524902] RPC: Registered udp transport module. [ 0.524911] RPC: Registered tcp transport module. [ 0.524918] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.524933] PCI: CLS 0 bytes, default 64 [ 0.525422] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.525638] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available [ 0.527639] Bus freq driver module loaded [ 0.528743] Initialise system trusted keyrings [ 0.528946] workingset: timestamp_bits=14 max_order=18 bucket_order=4 [ 0.535074] NFS: Registering the id_resolver key type [ 0.535098] Key type id_resolver registered [ 0.535106] Key type id_legacy registered [ 0.535146] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 0.535581] fuse: init (API version 7.31) [ 0.570778] Key type asymmetric registered [ 0.570791] Asymmetric key parser 'x509' registered [ 0.570813] io scheduler mq-deadline registered [ 0.570821] io scheduler kyber registered [ 0.574125] imx6q-pcie 1ffc000.pcie: 1ffc000.pcie supply epdev_on not found, using dummy regulator [ 0.575632] imx6q-pcie 1ffc000.pcie: host bridge /soc/pcie@1ffc000 ranges: [ 0.575677] imx6q-pcie 1ffc000.pcie: IO 0x01f80000..0x01f8ffff -> 0x00000000 [ 0.575702] imx6q-pcie 1ffc000.pcie: MEM 0x01000000..0x01efffff -> 0x01000000 [ 0.578270] mxc_sdc_fb fb@0: registered mxc display driver ldb [ 0.591680] init channel = 9 [ 0.614143] imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) [ 0.685713] Console: switching to colour frame buffer device 160x48 [ 0.709600] ldb ldb: LVDS channel1 is not online [ 0.709614] mxc_sdc_fb fb@1: NO mxc display driver found! [ 0.709683] mxc_sdc_fb fb@2: err interface_pix_fmt! [ 0.709694] mxc_sdc_fb fb@2: get mxcfb of property fail [ 0.709711] mxc_sdc_fb: probe of fb@2 failed with error -2 [ 0.709764] mxc_sdc_fb fb@3: err interface_pix_fmt! [ 0.709775] mxc_sdc_fb fb@3: get mxcfb of property fail [ 0.709789] mxc_sdc_fb: probe of fb@3 failed with error -2 [ 0.713838] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2 [ 0.713853] imx-sdma 20ec000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin [ 0.715539] mxs-dma 110000.dma-apbh: initialized [ 0.719465] pfuze100-regulator 2-0008: Full layer: 2, Metal layer: 1 [ 0.720170] pfuze100-regulator 2-0008: FAB: 0, FIN: 0 [ 0.720184] pfuze100-regulator 2-0008: pfuze100 found. [ 0.738946] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 25, base_baud = 5000000) is a IMX [ 1.578074] imx6q-pcie 1ffc000.pcie: Phy link never came up [ 1.585512] imx6q-pcie 1ffc000.pcie: failed to initialize host [ 1.592774] printk: console [ttymxc0] enabled [ 1.598606] imx6q-pcie 1ffc000.pcie: unable to add pcie port. [ 1.603839] imx sema4 driver is registered. [ 1.745227] brd: module loaded [ 1.758094] loop: module loaded [ 1.762661] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024 [ 1.770636] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480 [ 1.778700] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000 [ 1.786913] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000 [ 1.794694] ahci-imx 2200000.sata: 2200000.sata supply ahci not found, using dummy regulator [ 1.803218] ahci-imx 2200000.sata: 2200000.sata supply phy not found, using dummy regulator [ 1.811672] ahci-imx 2200000.sata: 2200000.sata supply target not found, using dummy regulator [ 1.823273] ahci-imx 2200000.sata: failed to reset phy: -110 [ 1.829143] ahci-imx: probe of 2200000.sata failed with error -110 [ 1.835459] imx ahci driver is registered. [ 1.843218] spi_master spi0: cannot find modalias for /soc/aips-bus@2000000/spba-bus@2000000/spi@2008000/mpu9250@0 [ 1.853640] spi_master spi0: Failed to create SPI device for /soc/aips-bus@2000000/spba-bus@2000000/spi@2008000/mpu9250@0 [ 1.864916] S25FL spi probed: device ecspi0.1 [ 1.869540] spi_imx 2008000.spi: probed [ 1.874272] spi_imx 200c000.spi: probed [ 1.879072] libphy: Fixed MDIO Bus: probed [ 1.883658] CAN device driver interface [ 1.892173] pps pps0: new PPS source ptp0 [ 1.897161] fec 2188000.ethernet: Invalid MAC address: 00:00:00:00:00:00 [ 1.903877] fec 2188000.ethernet: Using random MAC address: 22:3e:f2:98:ec:81 [ 1.914864] random: fast init done [ 1.918384] libphy: fec_enet_mii_bus: probed [ 1.923217] fec 2188000.ethernet eth0: registered PHC device 0 [ 1.929455] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k [ 1.935334] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 1.941844] usbcore: registered new interface driver r8152 [ 1.947413] usbcore: registered new interface driver lan78xx [ 1.953116] usbcore: registered new interface driver asix [ 1.958600] usbcore: registered new interface driver ax88179_178a [ 1.964757] usbcore: registered new interface driver cdc_ether [ 1.970639] usbcore: registered new interface driver smsc95xx [ 1.976476] usbcore: registered new interface driver net1080 [ 1.982176] usbcore: registered new interface driver cdc_subset [ 1.988156] usbcore: registered new interface driver zaurus [ 1.993769] usbcore: registered new interface driver MOSCHIP usb-ethernet driver [ 2.001236] usbcore: registered new interface driver cdc_ncm [ 2.006943] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 2.013476] ehci-pci: EHCI PCI platform driver [ 2.017986] ehci-mxc: Freescale On-Chip EHCI Host driver [ 2.023674] usbcore: registered new interface driver usb-storage [ 2.035863] snvs_rtc 20cc000.snvs:snvs-rtc-lp: registered as rtc0 [ 2.042186] rv1805 i2c probed [ 2.045696] RV1805 I2C DRIVER READ ADDRESS ERROR [ 2.050317] RV1805 identification error. [ 2.054588] RV1805 I2C DRIVER READ ADDRESS ERROR [ 2.059209] RV1805 identification error. [ 2.063225] i2c /dev entries driver [ 2.068159] In MVC:camera_init [ 2.071407] In MVC: init_camera_struct [ 2.075206] [ 2.075206] ------------------------------ipu_csi_set_window_size W=640 H=480 [ 2.083999] [ 2.083999] ------------------------------ipu_csi_set_window_pos CSI_OUT_FRM_CTRL=0x0 top=0 left=0 [ 2.094888] cam->enc_callback = camera_callback [ 2.099582] Video device registered: Mxc Camera #0 [ 2.106112] GS2971A spi probed: device ecspi1.0 [ 2.110707] In MVC: mxc_v4l2_master_attach [ 2.114834] slave.name = gs2971a [ 2.118325] master.name = mxc_v4l2_cap0 [ 2.122423] --------------ioctl_dev_exit-------------------------------------------- [ 2.130190] --------------ioctl_s_power-------------------------------------------- [ 2.137864] --------------ioctl_g_fmt_cap-------------------------------------------------- [ 2.146232] ioctl_g_fmt_cap W=1280 H=720 [ 2.150247] End of mxc_v4l2_master_attach: v2f pix widthxheight 288 x 352 [ 2.157050] End of mxc_v4l2_master_attach: crop_bounds widthxheight 1280 x 720 [ 2.164290] End of mxc_v4l2_master_attach: crop_defrect widthxheight 1280 x 720 [ 2.171601] End of mxc_v4l2_master_attach: crop_current widthxheight 1280 x 720 [ 2.178924] GS2971A V4L2 driver registered [ 7.204126] ---------------------FPGA STARTED [ 7.209096] mxc_v4l2_output v4l2_out: V4L2 device registered as video16 [ 7.215882] mxc_v4l2_output v4l2_out: V4L2 device registered as video17 [ 7.225085] imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0) [ 7.231575] Bluetooth: HCI UART driver ver 2.3 [ 7.236052] Bluetooth: HCI UART protocol H4 registered [ 7.241196] Bluetooth: HCI UART protocol BCSP registered [ 7.246555] Bluetooth: HCI UART protocol LL registered [ 7.251720] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 7.258036] Bluetooth: HCI UART protocol Marvell registered [ 7.263664] usbcore: registered new interface driver btusb [ 7.270146] sdhci: Secure Digital Host Controller Interface driver [ 7.276351] sdhci: Copyright(c) Pierre Ossman [ 7.280711] sdhci-pltfm: SDHCI platform and OF driver helper [ 7.318916] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA [ 7.326760] sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO [ 7.363691] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA [ 7.380877] mmc0: host does not support reading read-only switch, assuming write-enable [ 7.392448] mmc0: new high speed SDHC card at address aaaa [ 7.401569] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA [ 7.409328] mmcblk0: mmc0:aaaa SL08G 7.40 GiB [ 7.410659] leds-gpio: probe of leds failed with error -16 [ 7.420993] mmcblk0: p1 p2 p3 [ 7.421205] caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4) [ 7.430682] caam 2100000.caam: job rings = 2, qi = 0 [ 7.450395] caam algorithms registered in /proc/crypto [ 7.459344] caam_jr 2101000.jr0: registering rng-caam [ 7.464659] Device caam-keygen registered [ 7.474694] caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state [ 7.483366] usbcore: registered new interface driver usbhid [ 7.488972] usbhid: USB HID core driver [ 7.501277] fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW [ 7.513512] NET: Registered protocol family 26 [ 7.518651] NET: Registered protocol family 10 [ 7.524131] Segment Routing with IPv6 [ 7.527877] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 7.534423] NET: Registered protocol family 17 [ 7.538882] can: controller area network core (rev 20170425 abi 9) [ 7.545165] NET: Registered protocol family 29 [ 7.549617] can: raw protocol (rev 20170425) [ 7.553891] can: broadcast manager protocol (rev 20170425 t) [ 7.559577] can: netlink gateway (rev 20190810) max_hops=1 [ 7.565305] Bluetooth: RFCOMM TTY layer initialized [ 7.570198] Bluetooth: RFCOMM socket layer initialized [ 7.575424] Bluetooth: RFCOMM ver 1.11 [ 7.579189] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 7.584527] Bluetooth: BNEP filters: protocol multicast [ 7.589766] Bluetooth: BNEP socket layer initialized [ 7.594754] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 7.600685] Bluetooth: HIDP socket layer initialized [ 7.605709] lib80211: common routines for IEEE802.11 drivers [ 7.611418] Key type dns_resolver registered [ 7.616520] vddpu: supplied by SW1C [ 7.620280] Registering SWP/SWPB emulation handler [ 7.625301] Loading compiled-in X.509 certificates [ 7.657854] vddarm: supplied by SW2 [ 7.661795] vddsoc: supplied by SW1C [ 7.668438] Galcore version 6.4.3.p0.286725 [ 8.282920] mxc_vpu 2040000.vpu_fsl: VPU initialized [ 8.290366] imx_thermal tempmon: Extended Commercial CPU temperature grade - max:105C critical:100C passive:95C [ 8.302121] input: gpio-keys as /devices/soc0/gpio-keys/input/input0 [ 8.308905] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:06 UTC (6) [ 8.318836] ALSA device list: [ 8.321815] No soundcards found. [ 8.693641] EXT4-fs (mmcblk0p2): recovery complete [ 8.700140] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 8.708536] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 8.716409] devtmpfs: mounted [ 8.721155] Freeing unused kernel memory: 1024K [ 8.726105] Run /sbin/init as init process [ 9.000607] systemd[1]: System time before build time, advancing clock. [ 9.035202] systemd[1]: systemd 243.2+ running in system mode. (-PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 9.057520] systemd[1]: Detected architecture arm. Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)! [ 9.105755] systemd[1]: Set hostname to . [ 9.453433] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus/system_bus_socket â /run/dbus/system_bus_socket; please update the unit file accordingly. [ 9.646530] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/rpcbind.sock â /run/rpcbind.sock; please update the unit file accordingly. [ 9.680517] random: systemd: uninitialized urandom read (16 bytes read) [ 9.687362] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 9.699749] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 9.710619] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 9.744249] random: systemd: uninitialized urandom read (16 bytes read) [ 9.752185] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 9.784969] random: systemd: uninitialized urandom read (16 bytes read) [ 9.793928] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ OK ] Started Dispatch Password â¦ts to Console Directory Watch. [ OK ] Started Forward Password Râ¦uests to Wall Directory Watch. [ OK ] Reached target Paths. [ OK ] Reached target Remote File Systems. [ OK ] Reached target Slices. [ OK ] Reached target Swap. [ OK ] Listening on Syslog Socket. [ OK ] Listening on initctl Compatibility Named Pipe. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on udev Control Socket. [ OK ] Listening on udev Kernel Socket. Mounting POSIX Message Queue File System... Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)... Starting Create list of stâ¦odes for the current kernel... Starting Journal Service... Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Remount Root and Kernel File Systems... Starting Apply Kernel Variables... [ 10.597259] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) Starting udev Coldplug all Devices... [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Create list of sta⦠nodes for the current kernel. [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Apply Kernel Variables. Starting Flush Journal to Persistent Storage... [ 10.994915] systemd-journald[192]: Received client request to flush runtime journal. Starting Create Static Device Nodes in /dev... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Started udev Coldplug all Devices. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. Starting Network Service... [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Found device /dev/ttymxc0. [ OK ] Started Network Service. Starting Network Name Resolution... [ 11.748645] imx_vdoa: exports duplicate symbol vdoa_context_configure (owned by kernel) [ 11.750712] Micrel KSZ9021 Gigabit PHY 2188000.ethernet-1:00: attached PHY driver [Micrel KSZ9021 Gigabit PHY] (mii_bus:phy_addr=2188000.ethernet-1:00, irq=POLL) [ 11.783373] [ 11.783373] In MVC: mxc_v4l_open [ 11.797919] device name is Mxc Camera [ 11.804519] --------------ioctl_g_ifparm--------------------------------------------------- [ 11.826326] V4L2_IF_TYPE_BT656 [ 11.830103] --------------ioctl_g_fmt_cap-------------------------------------------------- [ 11.856558] ioctl_g_fmt_cap W=1280 H=720 [ 11.866014] End of mxc_v4l_open: v2f pix widthxheight 288 x 352 [ OK ] Started Update UTMP about System Boot/Shutdown. [ 11.910594] End of mxc_v4l_open: crop_bounds widthxheight 1280 x 720 [ 11.924185] End of mxc_v4l_open: crop_defrect widthxheight 1280 x 720 [ 11.932891] End of mxc_v4l_open: crop_current widthxheight 1280 x 720 [ 11.963614] On Open: Input to ipu size is 1280 x 720 [ 11.968682] [ 11.968682] ------------------------------ipu_csi_set_window_size W=1280 H=720 [ 11.977662] [ 11.977662] ------------------------------ipu_csi_set_window_pos CSI_OUT_FRM_CTRL=0x0 top=0 left=0 [ 11.989347] [ 11.989347] ------------------------------ipu_csi_init_interface W=1280 H=720 fmt=0x56595559 cfg=param = 0x81180001 ipu=1448695129 csi= 0 [ 12.003752] [ 12.003752] ------------------------------ipu_csi_init_interface GATED/NONGATED [ 12.003765] --------------ioctl_s_power-------------------------------------------- [ 12.003769] --------------ioctl_init-------------------------------------------- [ 12.003775] --------------ioctl_dev_init--------------------------------------------P_gs2971a_data->sensor.mclk= 148500000 [ 12.003798] In MVC:mxc_v4l_ioctl [ 12.003804] In MVC: mxc_v4l_do_ioctl 80685600 [ 12.003807] case VIDIOC_QUERYCAP [ 12.004221] In MVC:mxc_v4l_close [ 12.004227] --------------ioctl_s_power-------------------------------------------- [ 12.004236] mxc_v4l_close: release resource [ 12.004239] -----------------------CSI_IC_MEM [ 12.004242] MVC: In mxc_free_frame_buf [ 12.004246] In MVC:mxc_free_frames [ OK ] Started Network Time Synchronization. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ OK ] Started Daily apt download activities. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Kernel Logging Service. [ OK ] Started System Logging Service. [ OK ] Started D-Bus System Message Bus. [ OK ] Started Getty on tty1. [ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S). [ OK ] Started Init-target on . Starting Telephony service... [ OK ] Started User Space Regulatory Firmware Loading. [ OK ] Started User Space SDMA Firmware Loading. [ OK ] Started Serial Getty on ttymxc0. [ OK ] Reached target Login Prompts. [ 13.003903] init channel = 9 [ 13.081264] imx-sdma 20ec000.sdma: loaded firmware 3.5 Starting Login Service... [ OK ] Started Vsftpd ftp daemon. [ OK ] Started Xinetd A Powerful Replacement For Inetd. cat: can't open '/home/splash/image_boot_tagged.raw': No such file or directory [ OK ] Started Telephony service. [ OK ] Started Avahi mDNS/DNS-SD Stack. New password: Bad password: too short. Warning: weak password (enter it again to use it anyway). New password: Re-enter new password: [ OK ] Started Login Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ 13.324704] Console: switching to colour dummy device 80x30 ifconfig: SIOCSIFADDR: No such device [ 14.544065] random: crng init done [ 14.547480] random: 7 urandom warning(s) missed due to ratelimiting [ OK ] Started Load/Save Random Seed. NXP i.MX Release Distro 5.4-zeus imx6qpstarlitex ttymxc0 imx6qpstarlitex login: root (automatic login) [ 14.970628] init channel = 10 11 BUILD 18-0447 No config file found - Default values used +==========================[ 18.271281] [ 18.271281] In MVC: mxc_v4l_open =================================[ 18.278319] device name is Mxc Camera =======================+ | STAR[ 18.285103] --------------ioctl_g_ifparm--------------------------------------------------- LITE - APPLI VERSION = V03.77 [ 18.296280] V4L2_IF_TYPE_BT656 | | STARL[ 18.302200] --------------ioctl_g_fmt_cap-------------------------------------------------- ITE - QT Draw_PDF VERSION = V02.0[ 18.313425] ioctl_g_fmt_cap W=1280 H=720 0 | | STARLI[ 18.320277] End of mxc_v4l_open: v2f pix widthxheight 288 x 352 TE - QT SettingTime VERSION = V01[ 18.329096] End of mxc_v4l_open: crop_bounds widthxheight 1280 x 720 .07 | | STARLIT[ 18.338273] End of mxc_v4l_open: crop_defrect widthxheight 1280 x 720 E - QT ImageSetting VERSION = V02[ 18.347581] End of mxc_v4l_open: crop_current widthxheight 1280 x 720 .00 | | STARLITE[ 18.356869] On Open: Input to ipu size is 1280 x 720 - QT LinkSetting VERSION = V01.0[ 18.364713] [ 18.364713] ------------------------------ipu_csi_set_window_size W=1280 H=720 2 | | STARLITE [ 18.376431] [ 18.376431] ------------------------------ipu_csi_set_window_pos CSI_OUT_FRM_CTRL=0x0 top=0 left=0 - QT ConfSetting VERSION = V01.00[ 18.390170] [ 18.390170] ------------------------------ipu_csi_init_interface W=1280 H=720 fmt=0x56595559 cfg=param = 0x1 ipu=1448695129 csi= 0 | +============[ 18.406782] [ 18.406782] ------------------------------ipu_csi_init_interface GATED/NONGATED =================================[ 18.418484] --------------ioctl_s_power-------------------------------------------- =================================[ 18.429008] --------------ioctl_init-------------------------------------------- ====+ | Mode monitor on [ 18.439247] --------------ioctl_dev_init--------------------------------------------P_gs2971a_data->sensor.mclk= 148500000 : 0 | Mode monitor of[ 18.453183] In MVC:mxc_v4l_ioctl f : 1 | | Mod[ 18.459242] In MVC: mxc_v4l_do_ioctl c0045627 e recorder on : 2[ 18.466471] case VIDIOC_S_INPUT | Mode recorder off [ 18.472698] In MVC:mxc_streamoff : 3 | Mode player on [ 18.478808] csi_enc_select : 4 | Mode player [ 18.484392] case VIDIOC_S_INPUT CSI MEM off : 5 | Mode prerecord on : 6 | Mode prerecord off : 7 | | | Steady picture on : 10 | Steady picture off : 11 | | | Test sata on : 12 | Test sata off : 13 | Measurements : 14 | Mode monitor on without acq : 15 | Mode record without display : 16 | Mode display all flags : 17 | Toggle logo : 22 | Display time and temp : 23 | Display mire : 24 | Test ethernet link : 25 | Display memory status : 26 | Snap For LRA : 54 | Test Gamma FB : 59 | Test RTC : 66 | Test Connect to Camera : 69 | | | Exit from Application : 20 +==================================================================================+ Enter the choice: MONITOR MODE ON INIT IPU OUT [ 18.588939] init channel = 9 [ 18.588974] init channel = 10 INIT VPU [INFO] Product Info: i.MX6Q/D/S [ 18.693596] In MVC:mxc_v4l_ioctl [ 18.698875] In MVC: mxc_v4l_do_ioctl 80085617 [ 18.703254] case VIDIOC_G_STD [ 18.706638] --------------ioctl_g_fmt_cap-------------------------------------------------- [ 18.715053] --------------gs_get_std------------------------------------------------------- VIDEO MODE: 720P60 [ 18.723412] REG_RASTER_STRUC=0x0 [ 18.723414] REG_VD_STD=0x0 [ 18.723421] std=8 interlace=0 m=0 psf=0 3G=0 [ 18.832552] init channel = 10 [ 18.911083] init channel = 9 [ 18.911132] init channel = 10 [ 18.942330] In MVC:mxc_v4l_ioctl [ 18.945718] In MVC: mxc_v4l_do_ioctl c0cc5616 [ 18.950105] case VIDIOC_S_PARM [ 18.953445] In mxc_v4l2_s_param [ 18.956638] --------------ioctl_g_parm----------------------------------------------------- [ 18.965047] Current capabilities are 1001 [ 18.969327] Current capturemode is 0 change to 0 [ 18.974317] Current framerate is 60 change to 0 [ 18.979199] --------------ioctl_s_parm----------------------------------------------------- [ 18.987629] ioctl_s_parm: id_tab=3 W=1649 H=749 [ 18.992348] ioctl_s_parm id_v4l2=8 decim_factor=0 [ 18.997290] --------------ioctl_g_ifparm--------------------------------------------------- [ 19.005706] V4L2_IF_TYPE_BT656 [ 19.008773] --------------ioctl_g_fmt_cap-------------------------------------------------- [ 19.017178] ioctl_g_fmt_cap W=1649 H=749 [ 19.021196] g_fmt_cap returns widthxheight of input as 1649 x 749 [ 19.027626] [ 19.027626] ------------------------------ipu_csi_set_window_size W=1280 H=720 [ 19.036546] [ 19.036546] ------------------------------ipu_csi_set_window_pos CSI_OUT_FRM_CTRL=0x0 top=0 left=0 [ 19.047541] [ 19.047541] ------------------------------ipu_csi_init_interface W=1649 H=749 fmt=0x56595559 cfg=param = 0x81 ipu=1448695129 csi= 0 [ 19.061396] [ 19.061396] ------------------------------ipu_csi_init_interface GATED/NONGATED [ 19.070328] In MVC:mxc_v4l_ioctl [ 19.073566] In MVC: mxc_v4l_do_ioctl 4014563c [ 19.077990] case VIDIOC_S_CROP [ 19.081310] Cropping Input to ipu size 1280 x 720 [ 19.086335] [ 19.086335] ------------------------------ipu_csi_set_window_size W=1280 H=720 [ 19.095252] [ 19.095252] ------------------------------ipu_csi_set_window_pos CSI_OUT_FRM_CTRL=0x0 top=0 left=0 VIDIOC_G_CROP W=1280 H=720 left=0 top=0 UNINIT IPU INIT IPU IN [ 19.138322] In MVC:mxc_v4l_ioctl [ 19.141562] In MVC: mxc_v4l_do_ioctl 40045613 [ 19.145979] case VIDIOC_STREAMOFF [ 19.149559] In MVC:mxc_streamoff [ 19.152817] In MVC:mxc_v4l_ioctl [ 19.156123] In MVC: mxc_v4l_do_ioctl c0cc5605 [ 19.160494] case VIDIOC_S_FMT [ 19.163724] In MVC: mxc_v4l2_s_fmt [ 19.167191] type=V4L2_BUF_TYPE_VIDEO_CAPTURE [ 19.171735] End of mxc_v4l2_s_fmt: v2f pix widthxheight 1280 x 720 [ 19.177993] End of mxc_v4l2_s_fmt: crop_bounds widthxheight 1649 x 749 [ 19.184625] End of mxc_v4l2_s_fmt: crop_defrect widthxheight 1280 x 720 [ 19.191244] End of mxc_v4l2_s_fmt: crop_current widthxheight 1280 x 720 [ 19.197896] In MVC:mxc_v4l_ioctl [ 19.201144] In MVC: mxc_v4l_do_ioctl c0145608 [ 19.205551] case VIDIOC_REQBUFS [ 19.208965] In MVC:mxc_streamoff [ 19.212197] MVC: In mxc_free_frame_buf [ 19.215979] In MVC:mxc_allocate_frame_buf - size=1843200 [ 19.253553] In MVC:mxc_v4l_ioctl [ 19.256828] In MVC: mxc_v4l_do_ioctl c0445609 [ 19.261194] case VIDIOC_QUERYBUF [ 19.264768] In MVC:mxc_v4l2_buffer_status [ 19.268802] In MVC:mxc_mmap [ 19.271631] pgoff=0x45e00, start=0x673bc000, end=0x6757e000 [ 19.279485] In MVC:mxc_v4l_ioctl [ 19.282724] In MVC: mxc_v4l_do_ioctl c0445609 [ 19.287143] case VIDIOC_QUERYBUF [ 19.290642] In MVC:mxc_v4l2_buffer_status [ 19.294706] In MVC:mxc_mmap [ 19.297513] pgoff=0x46000, start=0x671fa000, end=0x673bc000 [ 19.305002] In MVC:mxc_v4l_ioctl [ 19.308238] In MVC: mxc_v4l_do_ioctl c0445609 [ 19.312596] case VIDIOC_QUERYBUF [ 19.316140] In MVC:mxc_v4l2_buffer_status [ 19.320179] In MVC:mxc_mmap [ 19.322978] pgoff=0x46200, start=0x67038000, end=0x671fa000 [ 19.330196] In MVC:mxc_v4l_ioctl [ 19.333433] In MVC: mxc_v4l_do_ioctl c044560f [ 19.337854] case VIDIOC_QBUF [ 19.341006] case VIDIOC_QBUF: end [ 19.344623] In MVC:mxc_v4l_ioctl [ 19.347862] In MVC: mxc_v4l_do_ioctl c044560f [ 19.352221] case VIDIOC_QBUF [ 19.355416] case VIDIOC_QBUF: end [ 19.359003] In MVC:mxc_v4l_ioctl [ 19.362234] In MVC: mxc_v4l_do_ioctl c044560f [ 19.366623] case VIDIOC_QBUF [ 19.369777] case VIDIOC_QBUF: end [ 19.373358] In MVC:mxc_v4l_ioctl [ 19.376655] In MVC: mxc_v4l_do_ioctl 40045612 [ 19.381019] case VIDIOC_STREAMON [ 19.384545] In MVC:mxc_streamon [ 19.387692] IPU:In csi_enc_enabling_tasks [ 19.402017] In csi_enc_setup [ 19.404934] [ 19.404934] ------------------------------ipu_csi_get_sensor_protocol ipu =-2127601744 [ 19.414395] init channel = 15 [ 19.417390] [ 19.417390] ------------------------------ipu_smfc_init channel channel=268435392 csi=0 SMFC_MAP=0x0 [ 19.428385] [ 19.428385] ------------------------------ipu_smfc_init channel channel=268435392 csi=0 SMFC_MAP=0x0 [ 19.439388] [ 19.439388] ------------------------------ipu_csi_init channel=268435392 csi=0 [ 19.448202] [ 19.448202] ------------------------------ipu_csi_init DEST_IDMAC [ 19.455825] [ 19.455825] ------------------------------ipu_csi_init channel CSI_SENS_CONF=0x4008900 [ 19.465343] In csi_enc_setup: pix.width=1280 pix.height=720 u_offset= 0 v_offset=0 bpl=2560 [ 19.474100] [ 19.474100] ------------------------------ipu_smfc_set_burst_size channel=268435392 bs=7 [ 19.483845] [ 19.483845] ************************TEST REGISTRES********************************* [ 19.493001] CSI_SENS_CONF = 0x4008900 [ 19.497067] CSI_SENS_FRM_SIZE = 0x2ec0670 [ 19.501082] CSI_ACT_FRM_SIZE = 0x2cf04ff [ 19.505125] CSI_OUT_FRM_CTRL = 0x0 [ 19.508619] CSI_SKIP = 0x0 [ 19.512109] SMFC_MAP = 0x0 [ 19.515672] SMFC_BS = 0x7 [ 19.519170] IC_PRP_ENC_RSC = 0x0 [ 19.522661] IC_PRP_VF_RSC = 0x0 [ 19.526177] IC_PP_RSC = 0x0 [ 19.529670] IPU_CONF = 0x0 [ 19.533159] IPU_CCIR_1 = 0x0 [ 19.536716] IPU_CCIR_2 = 0x0 [ 19.540211] IPU_CCIR_3 = 0x0 [ 19.543704] IPU_CONF = 0x00000000 [ 19.547139] IDMAC_CONF = 0x0276002F [ 19.550720] IDMAC_CHA_EN1 = 0x00000000 [ 19.554603] IDMAC_CHA_EN2 = 0x00000000 [ 19.558445] IDMAC_CHA_PRI1 = 0x18800003 [ 19.562369] IDMAC_CHA_PRI2 = 0x00000000 [ 19.566314] IDMAC_BAND_EN1 = 0x00000000 [ 19.570244] IDMAC_BAND_EN2 = 0x00000000 [ 19.574211] IPU_CHA_DB_MODE_SEL0 = 0x00000000 [ 19.578661] IPU_CHA_DB_MODE_SEL1 = 0x00000000 [ 19.583106] IPU_CHA_TRB_MODE_SEL0 = 0x00000000 [ 19.587669] IPU_CHA_TRB_MODE_SEL1 = 0x00000000 [ 19.592207] DMFC_WR_CHAN = 0x00000090 [ 19.596003] DMFC_WR_CHAN_DEF = 0x202020F6 [ 19.600104] DMFC_DP_CHAN = 0x00009694 [ 19.603854] DMFC_DP_CHAN_DEF = 0x2020F6F6 [ 19.607982] DMFC_IC_CTRL = 0x00000002 [ 19.611737] IPU_FS_PROC_FLOW1 = 0x00000000 [ 19.615971] IPU_FS_PROC_FLOW2 = 0x00000000 [ 19.620158] IPU_FS_PROC_FLOW3 = 0x00000000 [ 19.624370] IPU_FS_DISP_FLOW1 = 0x00000000 [ 19.628560] IPU_VDIC_VDI_FSIZE = 0x00000000 [ 19.632831] IPU_VDIC_VDI_C = 0x00000000 [ 19.636849] IPU_IC_CONF = 0x00000000 [ 19.640535] csi_enc_enable_csi [ 19.643605] In MVC:mxc_v4l_ioctl [ 19.646867] In MVC: mxc_v4l_do_ioctl c0445611 [ 19.651228] case VIDIOC_DQBUF [ 19.654511] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 20.404095] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream/source/stream.c at line 257: 'FD CAPTURE V4L2: VIDIOC_DQBUF FAILE[ 20.418655] init channel = 5 D' [ 20.421773] init channel = 2 [ 20.451538] init channel = 5 [ 20.464679] init channel = 5 [ 20.477774] In MVC:mxc_v4l_ioctl [ 20.481015] In MVC: mxc_v4l_do_ioctl c0445611 [ 20.485460] case VIDIOC_DQBUF [ 20.488725] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 21.204111] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 21.210797] init channel = 5 /source/stream.c at line 257: 'FD[ 21.216559] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 21.248666] init channel = 5 [ 21.261804] init channel = 5 [ 21.274939] In MVC:mxc_v4l_ioctl [ 21.278188] In MVC: mxc_v4l_do_ioctl c0445611 [ 21.282552] case VIDIOC_DQBUF [ 21.285833] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 22.004102] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 22.010780] init channel = 5 /source/stream.c at line 257: 'FD[ 22.016588] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 22.046213] init channel = 5 [ 22.059340] init channel = 5 [ 22.072518] In MVC:mxc_v4l_ioctl [ 22.075811] In MVC: mxc_v4l_do_ioctl c0445611 [ 22.080174] case VIDIOC_DQBUF [ 22.083408] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 22.804102] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 22.810771] init channel = 5 /source/stream.c at line 257: 'FD[ 22.816529] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 22.846839] init channel = 5 [ 22.859986] init channel = 5 [ 22.873083] In MVC:mxc_v4l_ioctl [ 22.876352] In MVC: mxc_v4l_do_ioctl c0445611 [ 22.880716] case VIDIOC_DQBUF [ 22.880721] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 23.604101] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 23.610793] init channel = 5 /source/stream.c at line 257: 'FD[ 23.616570] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 23.648668] init channel = 5 [ 23.661741] init channel = 5 [ 23.674830] In MVC:mxc_v4l_ioctl [ 23.678070] In MVC: mxc_v4l_do_ioctl c0445611 [ 23.682478] case VIDIOC_DQBUF [ 23.685791] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 24.404110] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 24.410799] init channel = 5 /source/stream.c at line 257: 'FD[ 24.416533] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 24.448663] init channel = 5 [ 24.461733] init channel = 5 [ 24.474822] In MVC:mxc_v4l_ioctl [ 24.478079] In MVC: mxc_v4l_do_ioctl c0445611 [ 24.482442] case VIDIOC_DQBUF [ 24.482446] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 25.204107] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 25.210751] init channel = 5 /source/stream.c at line 257: 'FD[ 25.216603] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 25.243067] In MVC:mxc_v4l_ioctl [ 25.246388] In MVC: mxc_v4l_do_ioctl c0445611 [ 25.250764] case VIDIOC_DQBUF [ 25.254010] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 26.004115] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 26.010761] init channel = 5 /source/stream.c at line 257: 'FD[ 26.016540] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 26.043069] In MVC:mxc_v4l_ioctl [ 26.046338] In MVC: mxc_v4l_do_ioctl c0445611 [ 26.050701] case VIDIOC_DQBUF [ 26.050705] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 26.804113] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 26.810759] init channel = 5 /source/stream.c at line 257: 'FD[ 26.816588] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 26.843082] In MVC:mxc_v4l_ioctl [ 26.846415] In MVC: mxc_v4l_do_ioctl c0445611 [ 26.850796] case VIDIOC_DQBUF [ 26.850804] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 27.604117] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 27.610766] init channel = 5 /source/stream.c at line 257: 'FD[ 27.616553] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 27.643058] In MVC:mxc_v4l_ioctl [ 27.646372] In MVC: mxc_v4l_do_ioctl c0445611 [ 27.650745] case VIDIOC_DQBUF [ 27.653991] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 28.404114] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 28.410776] init channel = 5 /source/stream.c at line 257: 'FD[ 28.416595] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 28.443071] In MVC:mxc_v4l_ioctl [ 28.446403] In MVC: mxc_v4l_do_ioctl 80085617 [ 28.450784] case VIDIOC_G_STD [ 28.450795] --------------ioctl_g_fmt_cap-------------------------------------------------- [ 28.450802] --------------gs_get_std------------------------------------------------------- [ 28.450810] REG_RASTER_STRUC=0x0 [ 28.450815] REG_VD_STD=0x0 [ 28.450832] std=8 interlace=0 m=0 psf=0 3G=0 [ 28.450855] In MVC:mxc_v4l_ioctl [ 28.484742] In MVC: mxc_v4l_do_ioctl c0445611 [ 28.489100] case VIDIOC_DQBUF [ 28.492328] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 29.204105] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 29.210754] init channel = 5 /source/stream.c at line 257: 'FD[ 29.216531] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 29.243074] In MVC:mxc_v4l_ioctl [ 29.246348] In MVC: mxc_v4l_do_ioctl c0445611 [ 29.250712] case VIDIOC_DQBUF [ 29.250717] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 30.004121] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 30.010781] init channel = 5 /source/stream.c at line 257: 'FD[ 30.016566] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 30.043200] In MVC:mxc_v4l_ioctl [ 30.046542] In MVC: mxc_v4l_do_ioctl c0445611 [ 30.050921] case VIDIOC_DQBUF [ 30.050930] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 30.804089] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 30.810795] init channel = 5 /source/stream.c at line 257: 'FD[ 30.816554] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 30.843001] In MVC:mxc_v4l_ioctl [ 30.846281] In MVC: mxc_v4l_do_ioctl c0445611 [ 30.850646] case VIDIOC_DQBUF [ 30.850650] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 31.604099] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 31.610740] init channel = 5 /source/stream.c at line 257: 'FD[ 31.616582] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 31.642991] In MVC:mxc_v4l_ioctl [ 31.646319] In MVC: mxc_v4l_do_ioctl c0445611 [ 31.650693] case VIDIOC_DQBUF [ 31.653939] In MVC:mxc_v4l_dqueue - wait_event_interruptible_timeout= 0 [ 32.404107] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 WARNING in file stream[ 32.410765] init channel = 5 /source/stream.c at line 257: 'FD[ 32.416554] init channel = 2 CAPTURE V4L2: VIDIOC_DQBUF FAILED' [ 32.443085] In MVC:mxc_v4l_ioctl [ 32.446355] In MVC: mxc_v4l_do_ioctl c0445611