root@imx8mpevk:~# gst-launch-1.0 filesrc location=./video.mp4 ! decodebin ! queu e ! waylandsink [ 33.252630] usb 1-1.2: reset high-speed USB device number 4 using xhci-hcd Setting pipeline to PAUSED ... Pipeline is PREROLLING ... ====== AIUR: 4.6.0 build on Jan 29 2021 08:22:32. ====== Core: MPEG4PARSER_06.17.17 build on Nov 12 2020 05:13:57 file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2 ------------------------ Track 00 [video_0] Enabled Duration: 0:00:30.000000000 Language: und Mime: video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format= (string)avc, width=(int)1920, height=(int)1080, framerate=(fraction)60/1, codec_ data=(buffer)0164002affe1001b6764002aacd940780227e5c044000003000400000301e03c60c 65801000668ebe3cb22c0 ------------------------ ====== VPUDEC: 4.6.0 build on Jan 29 2021 08:22:32. ====== wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Feb 18 2021 02:40:50) vpulib: 1.1.1 firmware: 1.1.1.65535 ------------------------ Track 01 [audio_0] Enabled Duration: 0:00:30.021333000 Language: und Mime: audio/mpeg, mpegversion=(int)4, channels=(int)6, rate=(int)48000, bitrat e=(int)192434, stream-format=(string)raw, codec_data=(buffer)11b0 ------------------------ ====== BEEP: 4.6.0 build on Jan[ 33.757119] can1-stby: disabling 29 2021 08:22:32. ====== Core:[ 33.761668] can2-stby: disabling AAC decoder Wrapper build on Jul 28 2020 10:45:34 file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm_elinux.so.3 CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_ARMV8 build on Sep 20 2017 15:02:50. Pipeline is PREROLLED ... Setting pipeline to PLAYING ... New clock: GstSystemClock ^Chandling interrupt. (6.6 %) Interrupt: Stopping pipeline ... Execution ended after 0:00:02.091443250 Setting pipeline to NULL ... [ 36.093073] ------------[ cut here ]------------ [ 36.097712] [CRTC:39:crtc-2] vblank wait timed out [ 36.102700] WARNING: CPU: 3 PID: 131 at drivers/gpu/drm/drm_atomic_helper.c:1 512 drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x290 [ 36.114785] Modules linked in: snd_usb_audio uvcvideo snd_hwdep snd_usbmidi_l ib fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes crct10dif_ce imx8_media_dev(C) flexcan can_dev caam secv io error [ 36.136561] CPU: 3 PID: 131 Comm: kworker/u8:2 Tainted: G C O 5. 10.9-1.0.0+g32513c25d8c7 #1 [ 36.146038] Hardware name: NXP i.MX8MPlus EVK board (DT) [ 36.151352] Workqueue: events_unbound commit_work [ 36.156058] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--) [ 36.162063] pc : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x290 [ 36.168590] lr : drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x290 [ 36.175114] sp : ffff8000126cbc80 [ 36.178426] x29: ffff8000126cbc80 x28: 0000000000000000 [ 36.183740] x27: 00000000000004ab x26: 0000000000000070 [ 36.189054] x25: ffff0000c1795800 x24: 0000000000000001 [ 36.194367] x23: 0000000000000038 x22: 0000000000000004 [ 36.199681] x21: ffff0000c6478d80 x20: ffff0000c1795088 [ 36.204994] x19: 0000000000000002 x18: 0000000000000030 [ 36.210310] x17: 0000000000000000 x16: 0000000000000000 [ 36.215623] x15: ffff0000c0aacbb8 x14: ffffffffffffffff [ 36.220937] x13: ffff800011aa1678 x12: 00000000000006ae [ 36.226250] x11: 000000000000023a x10: ffff800011af9678 [ 36.231564] x9 : 00000000fffff000 x8 : ffff800011aa1678 [ 36.236877] x7 : ffff800011af9678 x6 : 0000000000000000 [ 36.242190] x5 : 0000000000000000 x4 : ffff00017f3b3900 [ 36.247504] x3 : ffff00017f3ba830 x2 : ffff00017f3b3900 [ 36.252817] x1 : afa38aff86feac00 x0 : 0000000000000000 [ 36.258130] Call trace: [ 36.260578] drm_atomic_helper_wait_for_vblanks.part.0+0x278/0x290 [ 36.266757] drm_atomic_helper_wait_for_vblanks+0x1c/0x30 [ 36.272156] lcdifv3_drm_atomic_commit_tail+0x54/0x70 [ 36.277206] commit_tail+0xa4/0x184 [ 36.280694] commit_work+0x14/0x20 [ 36.284097] process_one_work+0x1cc/0x350 [ 36.288106] worker_thread+0x13c/0x470 [ 36.291855] kthread+0x154/0x160 [ 36.295083] ret_from_fork+0x10/0x30 [ 36.298657] ---[ end trace 48d33a8e21a2930c ]--- [ 36.409079] cpu cpu0: _set_opp_voltage: failed to set voltage (950000 950000 950000 mV): -110 [ 36.417622] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 36.857077] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 36.865877] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 37.309075] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 37.317875] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 37.745077] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 37.753876] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 38.193080] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 38.201879] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 38.645075] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 38.653874] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 39.089078] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 39.097877] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 39.521079] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 39.529881] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 39.953078] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 39.961878] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 40.401075] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 40.409875] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 40.853075] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 40.861874] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 41.293085] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 41.301895] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 41.741078] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 41.749878] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 42.173163] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 42.181972] cpufreq: __target_index: Failed to change cpu frequency: -110 [ 42.605080] cpu cpu0: _set_opp_voltage: failed to set voltage (1000000 100000 0 1000000 mV): -110 [ 42.613888] cpufreq: __target_index: Failed to change cpu frequency: -110