U-Boot SPL 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Jun 29 2021 - 01:48:31 +0000) power_bd71837_init DDRINFO: start DRAM init DDRINFO: DRAM rate 3000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done Normal Boot Trying to boot from MMC1 NOTICE: BL31: v2.2(release):rel_imx_5.4.47_2.2.0-0-gc949a888e NOTICE: BL31: Built : 02:22:03, Jun 29 2021 U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Jun 29 2021 - 01:48:31 +0000) CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz) CPU: Commercial temperature grade (0C to 95C) at 30C Reset cause: POR Model: NXP i.MX8MM EVK board DRAM: 2 GiB wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x52 retry=0 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x52 retry=1 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x52 retry=2 i2c_init_transfer: give up i2c_regs=0x30a30000 tcpc_init: Can't find device id=0x52 setup_typec: tcpc port2 init failed, err=-19 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x50 retry=0 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x50 retry=1 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x50 retry=2 i2c_init_transfer: give up i2c_regs=0x30a30000 tcpc_init: Can't find device id=0x50 setup_typec: tcpc port1 init failed, err=-19 MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... Run CMD11 1.8V switch *** Warning - bad CRC, using default environment [*]-Video Link 0wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=1 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=2 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 [0] lcdif@32e00000, video [1] mipi_dsi@32e10000, video_bridge [2] adv7535@3d, panel wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=1 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=2 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 In: serial Out: serial Err: serial BuildInfo: - ATF c949a88 - U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 Run CMD11 1.8V switch switch to partitions #0, OK mmc1 is current device flash target is MMC:1 Run CMD11 1.8V switch Net: Warning: ethernet@30be0000 using MAC address from ROM eth0: ethernet@30be0000 Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 Run CMD11 1.8V switch switch to partitions #0, OK mmc1 is current device Run CMD11 1.8V switch 27941376 bytes read in 628 ms (42.4 MiB/s) Booting from mmc ... 46570 bytes read in 10 ms (4.4 MiB/s) ## Flattened Device Tree blob at 43000000 Booting using the fdt blob at 0x43000000 Using Device Tree in place at 0000000043000000, end 000000004300e5e9 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=1 wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x3c retry=2 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.4.47-2.2.0+g5ec03d06f54e (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Jun 29 04:15:39 UTC 2021 [ 0.000000] Machine model: FSL i.MX8MM EVK board [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, size 640 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] NUMA: No NUMA configuration found [ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] NUMA: NODE_DATA [mem 0xbdbdb500-0xbdbdcfff] [ 0.000000] Zone ranges: [ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff] [ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bdffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.1 [ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Speculative Store Bypass Disable mitigation not required [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507008 [ 0.000000] Policy zone: DMA32 [ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1336084K/2060288K available (16508K kernel code, 1238K rwdata, 6528K rodata, 2944K init, 1015K bss, 68844K reserved, 655360K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 128 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000 [ 0.000000] ITS: No ITS available, not enabling LPIs [ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns [ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns [ 0.000383] Console: colour dummy device 80x25 [ 0.000443] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000) [ 0.000452] pid_max: default: 32768 minimum: 301 [ 0.000520] LSM: Security Framework initializing [ 0.000571] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.000582] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.024007] ASID allocator initialised with 32768 entries [ 0.032006] rcu: Hierarchical SRCU implementation. 0.040849] EFI services will not be available. U-Boot SPL 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Jun 29 2021 - 01:48:31 +0000) power_bd71837_init DDRINFO: start DRAM init DDRINFO: DRAM rate 3000MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done Normal Boot Trying to boot from MMC1 NOTICE: BL31: v2.2(release):rel_imx_5.4.47_2.2.0-0-gc949a888e NOTICE: BL31: Built : 02:22:03, Jun 29 2021 U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Jun 29 2021 - 01:48:31 +0000) CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz) CPU: Commercial temperature grade (0C to 95C) at 36C Reset cause: POR Model: NXP i.MX8MM EVK board DRAM: 2 GiB wait_for_sr_state: failed sr=81 cr=a0 state=2020 i2c_init_transfer: failed for chip 0x52 retry=0 i2c_idle_bus: failed to clear bus, sda=0 scl=0 i2c_init_transfer: give up i2c_regs=0x30a30000 tcpc_init: Can't find device id=0x52 setup_typec: tcpc port2 init failed, err=-19 wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020 i2c_init_transfer: failed for chip 0x50 retry=0 i2c_idle_bus: failed to clear bus, sda=0 scl=0 i2c_init_transfer: give up i2c_regs=0x30a30000 tcpc_init: Can't find device id=0x50 setup_typec: tcpc port1 init failed, err=-19 MMC: FSL_SDHC: 1, FSL_SDHC: 2 Loading Environment from MMC... Run CMD11 1.8V switch *** Warning - bad CRC, using default environment [*]-Video Link 0wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 i2c_idle_bus: failed to clear bus, sda=0 scl=0 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 [0] lcdif@32e00000, video [1] mipi_dsi@32e10000, video_bridge [2] adv7535@3d, panel wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 i2c_idle_bus: failed to clear bus, sda=0 scl=0 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 In: serial Out: serial Err: serial BuildInfo: - ATF c949a88 - U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 Run CMD11 1.8V switch switch to partitions #0, OK mmc1 is current device flash target is MMC:1 Run CMD11 1.8V switch Net: Warning: ethernet@30be0000 using MAC address from ROM eth0: ethernet@30be0000 Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 Run CMD11 1.8V switch switch to partitions #0, OK mmc1 is current device Run CMD11 1.8V switch 27941376 bytes read in 627 ms (42.5 MiB/s) Booting from mmc ... 46570 bytes read in 10 ms (4.4 MiB/s) ## Flattened Device Tree blob at 43000000 Booting using the fdt blob at 0x43000000 Using Device Tree in place at 0000000043000000, end 000000004300e5e9 wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020 i2c_init_transfer: failed for chip 0x3c retry=0 i2c_idle_bus: failed to clear bus, sda=0 scl=0 i2c_init_transfer: give up i2c_regs=0x30a30000 Can't find cec device id=0x3c fail to probe panel device adv7535@3d failed to get any video link display timings probe video device failed, ret -22 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.4.47-2.2.0+g5ec03d06f54e (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Jun 29 04:15:39 UTC 2021 [ 0.000000] Machine model: FSL i.MX8MM EVK board [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, size 640 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] NUMA: No NUMA configuration found [ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] NUMA: NODE_DATA [mem 0xbdbdb500-0xbdbdcfff] [ 0.000000] Zone ranges: [ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff] [ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bdffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.1 [ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Speculative Store Bypass Disable mitigation not required [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507008 [ 0.000000] Policy zone: DMA32 [ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1336084K/2060288K available (16508K kernel code, 1238K rwdata, 6528K rodata, 2944K init, 1015K bss, 68844K reserved, 655360K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 128 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000 [ 0.000000] ITS: No ITS available, not enabling LPIs [ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns [ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns [ 0.000386] Console: colour dummy device 80x25 [ 0.000451] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000) [ 0.000461] pid_max: default: 32768 minimum: 301 [ 0.000529] LSM: Security Framework initializing [ 0.000579] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.000591] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.024005] ASID allocator initialised with 32768 entries [ 0.032003] rcu: Hierarchical SRCU implementation. [ 0.040839] EFI services will not be available. [ 0.048033] smp: Bringing up secondary CPUs ... [ 0.080177] Detected VIPT I-cache on CPU1 [ 0.080201] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000 [ 0.080233] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.112205] Detected VIPT I-cache on CPU2 [ 0.112221] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000 [ 0.112237] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.144252] Detected VIPT I-cache on CPU3 [ 0.144267] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000 [ 0.144284] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.144336] smp: Brought up 1 node, 4 CPUs [ 0.144359] SMP: Total of 4 processors activated. [ 0.144367] CPU features: detected: 32-bit EL0 Support [ 0.144373] CPU features: detected: CRC32 instructions [ 0.151040] CPU: All CPU(s) started at EL2 [ 0.151060] alternatives: patching kernel code [ 0.152490] devtmpfs: initialized [ 0.159073] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.159090] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.175129] pinctrl core: initialized pinctrl subsystem [ 0.175823] DMI not present or invalid. [ 0.176066] NET: Registered protocol family 16 [ 0.190578] DMA: preallocated 256 KiB pool for atomic allocations [ 0.190608] audit: initializing netlink subsys (disabled) [ 0.190840] audit: type=2000 audit(0.188:1): state=initialized audit_enabled=0 res=1 [ 0.191632] cpuidle: using governor menu [ 0.192055] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.192865] Serial: AMBA PL011 UART driver [ 0.192924] imx mu driver is registered. [ 0.192945] imx rpmsg driver is registered. [ 0.198611] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver [ 0.221656] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.221667] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.221672] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.221677] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.222498] cryptd: max_cpu_qlen set to 1000 [ 0.225510] ACPI: Interpreter disabled. [ 0.226401] iommu: Default domain type: Translated [ 0.226537] vgaarb: loaded [ 0.226847] SCSI subsystem initialized [ 0.227157] usbcore: registered new interface driver usbfs [ 0.227191] usbcore: registered new interface driver hub [ 0.227239] usbcore: registered new device driver usb [ 0.228369] mc: Linux media interface: v0.10 [ 0.228393] videodev: Linux video capture interface: v2.00 [ 0.228483] pps_core: LinuxPPS API ver. 1 registered [ 0.228489] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.228501] PTP clock support registered [ 0.228638] EDAC MC: Ver: 3.0.0 [ 0.229401] No BMan portals available! [ 0.229627] QMan: Allocated lookup table at (____ptrval____), entry count 65537 [ 0.229882] No QMan portals available! [ 0.230266] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree [ 0.230669] FPGA manager framework [ 0.230742] Advanced Linux Sound Architecture Driver Initialized. [ 0.231112] Bluetooth: Core ver 2.22 [ 0.231135] NET: Registered protocol family 31 [ 0.231139] Bluetooth: HCI device and connection manager initialized [ 0.231147] Bluetooth: HCI socket layer initialized [ 0.231154] Bluetooth: L2CAP socket layer initialized [ 0.231165] Bluetooth: SCO socket layer initialized [ 0.231836] clocksource: Switched to clocksource arch_sys_counter [ 0.231989] VFS: Disk quotas dquot_6.6.0 [ 0.232033] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.232179] pnp: PnP ACPI: disabled [ 0.237662] thermal_sys: Registered thermal governor 'step_wise' [ 0.237665] thermal_sys: Registered thermal governor 'power_allocator' [ 0.237988] NET: Registered protocol family 2 [ 0.238296] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.238328] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.238436] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear) [ 0.238662] TCP: Hash tables configured (established 16384 bind 16384) [ 0.238739] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.238780] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.238907] NET: Registered protocol family 1 [ 0.239233] RPC: Registered named UNIX socket transport module. [ 0.239237] RPC: Registered udp transport module. [ 0.239241] RPC: Registered tcp transport module. [ 0.239246] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.239605] PCI: CLS 0 bytes, default 64 [ 0.240292] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.240647] kvm [1]: IPA Size Limit: 40bits [ 0.241230] kvm [1]: GICv3: no GICV resource entry [ 0.241235] kvm [1]: disabling GICv2 emulation [ 0.241251] kvm [1]: GIC system register CPU interface enabled [ 0.241309] kvm [1]: vgic interrupt IRQ1 [ 0.241400] kvm [1]: Hyp mode initialized successfully [ 0.244190] Initialise system trusted keyrings [ 0.244292] workingset: timestamp_bits=44 max_order=19 bucket_order=0 [ 0.249975] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.250589] NFS: Registering the id_resolver key type [ 0.250612] Key type id_resolver registered [ 0.250616] Key type id_legacy registered [ 0.250627] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.250645] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 0.250987] 9p: Installing v9fs 9p2000 file system support [ 0.263555] Key type asymmetric registered [ 0.263562] Asymmetric key parser 'x509' registered [ 0.263594] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.263600] io scheduler mq-deadline registered [ 0.263605] io scheduler kyber registered [ 0.268877] EINJ: ACPI disabled. [ 0.277592] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2 [ 0.277606] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin [ 0.285554] mxs-dma 33000000.dma-controller: initialized [ 0.286679] Bus freq driver module loaded [ 0.291864] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.294012] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 5000000) is a IMX [ 0.294476] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX [ 0.294836] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX [ 1.279054] printk: console [ttymxc1] enabled [ 1.289567] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.296204] [drm] No driver support for vblank timestamp query. [ 1.302194] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops) [ 1.320899] loop: module loaded [ 1.326186] imx ahci driver is registered. [ 1.333290] spi-nor spi3.0: n25q256ax1 (32768 Kbytes) [ 1.341682] libphy: Fixed MDIO Bus: probed [ 1.346571] tun: Universal TUN/TAP device driver, 1.6 [ 1.352388] thunder_xcv, ver 1.0 [ 1.355648] thunder_bgx, ver 1.0 [ 1.358915] nicpf, ver 1.0 [ 1.362457] pps pps0: new PPS source ptp0 [ 1.371616] libphy: fec_enet_mii_bus: probed [ 1.377050] fec 30be0000.ethernet eth0: registered PHC device 0 [ 1.383585] Freescale FM module, FMD API version 21.1.0 [ 1.389072] Freescale FM Ports module [ 1.392744] fsl_mac: fsl_mac: FSL FMan MAC API based driver [ 1.398477] fsl_dpa: FSL DPAA Ethernet driver [ 1.402973] fsl_advanced: FSL DPAA Advanced drivers: [ 1.407950] fsl_proxy: FSL DPAA Proxy initialization driver [ 1.413639] fsl_oh: FSL FMan Offline Parsing port driver [ 1.419823] hclge is initializing [ 1.423157] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version [ 1.430388] hns3: Copyright (c) 2017 Huawei Corporation. [ 1.435745] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI [ 1.442799] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 1.448583] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k [ 1.454422] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 1.460382] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k [ 1.467347] igb: Copyright (c) 2007-2014 Intel Corporation. [ 1.472957] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 1.480793] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 1.486880] sky2: driver version 1.30 [ 1.491478] VFIO - User Level meta-driver version: 0.3 [ 1.498461] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.505011] ehci-pci: EHCI PCI platform driver [ 1.509533] ehci-platform: EHCI generic platform driver [ 1.514948] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 1.521170] ohci-pci: OHCI PCI platform driver [ 1.525655] ohci-platform: OHCI generic platform driver [ 1.531556] usbcore: registered new interface driver uas [ 1.536919] usbcore: registered new interface driver usb-storage [ 1.542994] usbcore: registered new interface driver usbserial_generic [ 1.549551] usbserial: USB Serial support registered for generic [ 1.555587] usbcore: registered new interface driver ftdi_sio [ 1.561355] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.568696] usbcore: registered new interface driver usb_serial_simple [ 1.575246] usbserial: USB Serial support registered for carelink [ 1.581358] usbserial: USB Serial support registered for zio [ 1.587041] usbserial: USB Serial support registered for funsoft [ 1.593067] usbserial: USB Serial support registered for flashloader [ 1.599442] usbserial: USB Serial support registered for google [ 1.605388] usbserial: USB Serial support registered for libtransistor [ 1.611937] usbserial: USB Serial support registered for vivopay [ 1.617963] usbserial: USB Serial support registered for moto_modem [ 1.624251] usbserial: USB Serial support registered for motorola_tetra [ 1.630888] usbserial: USB Serial support registered for novatel_gps [ 1.637264] usbserial: USB Serial support registered for hp4x [ 1.643028] usbserial: USB Serial support registered for suunto [ 1.648968] usbserial: USB Serial support registered for siemens_mpi [ 1.655358] usbcore: registered new interface driver usb_ehset_test [ 1.663162] imx_usb 32e40000.usb: No over current polarity defined [ 1.670652] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/soc@0:bus@30000000/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0 [ 1.685817] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0 [ 1.692105] i2c /dev entries driver [ 1.696275] mx6s-csi 32e20000.csi1_bridge: initialising [ 1.702022] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phy not found, using dummy regulator [ 1.712219] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered [ 1.719194] CSI: Registered sensor subdevice: mxc_mipi-csi.0 [ 1.724875] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000 [ 1.738898] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0) [ 1.745493] Bluetooth: HCI UART driver ver 2.3 [ 1.749952] Bluetooth: HCI UART protocol H4 registered [ 1.755101] Bluetooth: HCI UART protocol BCSP registered [ 1.760442] Bluetooth: HCI UART protocol LL registered [ 1.765589] Bluetooth: HCI UART protocol ATH3K registered [ 1.771016] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 1.777380] Bluetooth: HCI UART protocol Broadcom registered [ 1.783062] Bluetooth: HCI UART protocol QCA registered [ 1.790263] sdhci: Secure Digital Host Controller Interface driver [ 1.796462] sdhci: Copyright(c) Pierre Ossman [ 1.801023] Synopsys Designware Multimedia Card Interface Driver [ 1.807625] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.814081] mmc0: CQHCI version 5.10 [ 1.818091] mmc1: CQHCI version 5.10 [ 1.822129] mmc2: CQHCI version 5.10 [ 1.857628] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA [ 1.867566] ledtrig-cpu: registered to indicate activity on CPUs [ 1.874807] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9) [ 1.881570] caam 30900000.crypto: job rings = 2, qi = 0 [ 1.913381] caam algorithms registered in /proc/crypto [ 1.922639] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto [ 1.932771] caam_jr 30901000.jr: registering rng-caam [ 1.938310] Device caam-keygen registered [ 1.944597] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state [ 1.953142] usbcore: registered new interface driver usbhid [ 1.958727] usbhid: USB HID core driver [ 1.964363] No fsl,qman node [ 1.967251] Freescale USDPAA process driver [ 1.971445] fsl-usdpaa: no region found [ 1.975289] Freescale USDPAA process IRQ driver [ 1.983320] optee: probing for conduit method from DT. [ 1.988503] optee: revision 3.10 (b3914e54) [ 1.989677] optee: dynamic shared memory is enabled [ 1.999086] optee: initialized driver [ 2.004046] galcore: clk_get vg clock failed, disable vg! [ 2.009759] Galcore version 6.4.3.p0.286725 [ 2.048750] mmc2: Command Queue Engine enabled [ 2.053279] mmc2: new HS400 Enhanced strobe MMC card at address 0001 [ 2.061067] mmcblk2: mmc2:0001 DG4016 14.7 GiB [ 2.065747] mmcblk2boot0: mmc2:0001 DG4016 partition 1 4.00 MiB [ 2.071806] mmcblk2boot1: mmc2:0001 DG4016 partition 2 4.00 MiB [ 2.078454] mmcblk2rpmb: mmc2:0001 DG4016 partition 3 4.00 MiB, chardev (237:0) [ 2.079626] hantrodec 0 : module inserted. Major = 236 [ 2.091515] hantrodec 1 : module inserted. Major = 236 [ 2.093490] Alternate GPT is invalid, using primary GPT. [ 2.097541] hx280enc: module inserted. Major <235> [ 2.102029] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 [ 2.110448] wm8524-codec audio-codec: Failed to get mute line: -517 [ 2.162055] fsl-micfil-dai 30080000.micfil: GET IRQ: 16 [ 2.167315] fsl-micfil-dai 30080000.micfil: GET IRQ: 17 [ 2.172559] fsl-micfil-dai 30080000.micfil: GET IRQ: 18 [ 2.177801] fsl-micfil-dai 30080000.micfil: GET IRQ: 19 [ 2.189326] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 30090000.spdif mapping ok [ 2.196962] imx-spdif sound-spdif: ASoC: no DMI vendor name! [ 2.205828] imx-ak4458 sound-ak4458: ASoC: failed to init link ak4458: -517 [ 2.212828] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517) [ 2.220208] debugfs: Directory '30080000.micfil' with parent 'imx-audio-micfil' already present! [ 2.229086] imx-micfil sound-micfil: snd-soc-dummy-dai <-> 30080000.micfil mapping ok [ 2.236928] imx-micfil sound-micfil: ASoC: no DMI vendor name! [ 2.243961] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 2.254671] NET: Registered protocol family 26 [ 2.259684] NET: Registered protocol family 10 [ 2.268786] Segment Routing with IPv6 [ 2.272502] NET: Registered protocol family 17 [ 2.277369] Bluetooth: RFCOMM TTY layer initialized [ 2.282264] Bluetooth: RFCOMM socket layer initialized [ 2.287434] Bluetooth: RFCOMM ver 1.11 [ 2.291195] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 2.296512] Bluetooth: BNEP filters: protocol multicast [ 2.301746] Bluetooth: BNEP socket layer initialized [ 2.306716] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 2.312645] Bluetooth: HIDP socket layer initialized [ 2.317648] 8021q: 802.1Q VLAN Support v1.8 [ 2.321851] lib80211: common routines for IEEE802.11 drivers [ 2.327616] 9pnet: Installing 9P2000 support [ 2.331923] tsn generic netlink module v1 init... [ 2.336690] Key type dns_resolver registered [ 2.341950] registered taskstats version 1 [ 2.346060] Loading compiled-in X.509 certificates [ 2.372547] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator [ 2.381328] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator [ 2.408229] ldo6: supplied by regulator-dummy [ 2.413384] i2c i2c-0: IMX I2C adapter registered [ 2.419269] adv7511 1-003d: 1-003d supply avdd not found, using dummy regulator [ 2.426664] adv7511 1-003d: 1-003d supply dvdd not found, using dummy regulator [ 2.434016] adv7511 1-003d: 1-003d supply pvdd not found, using dummy regulator [ 2.441364] adv7511 1-003d: 1-003d supply a2vdd not found, using dummy regulator [ 2.448799] adv7511 1-003d: 1-003d supply v3p3 not found, using dummy regulator [ 2.456150] adv7511 1-003d: 1-003d supply v1p2 not found, using dummy regulator [ 2.464432] adv7511: probe of 1-003d failed with error -11 [ 2.470470] tcpci: probe of 1-0050 failed with error -11 [ 2.475868] i2c i2c-1: IMX I2C adapter registered [ 2.484296] ak4458 2-0010: Failed to request supplies: -517 [ 2.490197] ak4458 2-0012: Failed to request supplies: -517 [ 2.496065] ak5558 2-0013: Failed to request supplies: -517 [ 2.501925] ak4458 2-0011: Failed to request supplies: -517 [ 2.507813] ov5640_mipi 2-003c: No sensor reset pin available [ 2.513598] ov5640_mipi 2-003c: 2-003c supply DOVDD not found, using dummy regulator [ 2.521403] ov5640_mipi 2-003c: 2-003c supply DVDD not found, using dummy regulator [ 2.529119] ov5640_mipi 2-003c: 2-003c supply AVDD not found, using dummy regulator [ 2.548135] ov5640_mipi 2-003c: Read reg error: reg=300a [ 2.553462] ov5640_mipi 2-003c: Camera is not found [ 2.558510] i2c i2c-2: IMX I2C adapter registered [ 2.564634] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator [ 2.564719] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 2.574055] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!. [ 2.580423] [drm] No driver support for vblank timestamp query. [ 2.591977] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops) [ 2.601268] ------------[ cut here ]------------ [ 2.605893] WARNING: CPU: 0 PID: 31 at drivers/reset/core.c:556 __reset_control_get_internal+0x64/0x110 [ 2.612209] imx6q-pcie 33800000.pcie: PCIe PLL locked after 20 us. [ 2.615284] Modules linked in: [ 2.621503] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges: [ 2.624516] CPU: 0 PID: 31 Comm: kworker/0:1 Not tainted 5.4.47-2.2.0+g5ec03d06f54e #1 [ 2.624520] Hardware name: FSL i.MX8MM EVK board (DT) [ 2.631767] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000000 [ 2.639655] Workqueue: events deferred_probe_work_func [ 2.644726] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000000 [ 2.652096] pstate: 20000005 (nzCv daif -PAN -UAO) [ 2.652102] pc : __reset_control_get_internal+0x64/0x110 [ 2.674719] lr : __of_reset_control_get+0x158/0x1b0 [ 2.679595] sp : ffff800011de3830 [ 2.682907] x29: ffff800011de3830 x28: 0000000000000000 [ 2.688220] x27: ffff000077644b38 x26: 0000000000000001 [ 2.693533] x25: 0000000000000000 x24: 0000000000000001 [ 2.698845] x23: 0000000000000000 x22: ffff0000768d9780 [ 2.704157] x21: 0000000000000005 x20: ffff0000768d97a0 [ 2.709470] x19: ffff00007693d800 x18: 0000000000000010 [ 2.714782] x17: 0000000000000000 x16: 0000000000000000 [ 2.720093] x15: ffff000076318470 x14: 72632d666964636c [ 2.725405] x13: 2d786d6920646e75 x12: 0000000000000000 [ 2.730718] x11: 0000000000000020 x10: 0101010101010101 [ 2.736030] x9 : fffffffffffffffd x8 : 7f7f7f7f7f7f7f7f [ 2.741343] x7 : 766f21ff726b6b64 x6 : 0000000080237077 [ 2.746655] x5 : fffffdfffe609724 x4 : 0000000000000000 [ 2.751967] x3 : 0000000000000001 x2 : 0000000000000005 [ 2.757279] x1 : 0000000000000005 x0 : 0000000000000000 [ 2.762593] Call trace: [ 2.765042] __reset_control_get_internal+0x64/0x110 [ 2.770008] __of_reset_control_get+0x158/0x1b0 [ 2.774539] of_reset_control_array_get+0xac/0x1a0 [ 2.779334] imx_sec_dsim_bind+0x208/0x348 [ 2.783433] component_bind_all+0xfc/0x258 [ 2.787532] imx_drm_bind+0xb8/0x150 [ 2.791106] try_to_bring_up_master+0x164/0x1c8 [ 2.795636] __component_add+0xa0/0x168 [ 2.799475] component_add+0x10/0x18 [ 2.803051] imx_sec_dsim_probe+0x4c/0x70 [ 2.807062] platform_drv_probe+0x50/0xa0 [ 2.811072] really_probe+0xd4/0x318 [ 2.814648] driver_probe_device+0x54/0xe8 [ 2.818746] __device_attach_driver+0x80/0xb8 [ 2.823105] bus_for_each_drv+0x74/0xc0 [ 2.826939] __device_attach+0xdc/0x138 [ 2.830776] device_initial_probe+0x10/0x18 [ 2.834959] bus_probe_device+0x90/0x98 [ 2.838796] deferred_probe_work_func+0x64/0x98 [ 2.843331] process_one_work+0x198/0x320 [ 2.847342] worker_thread+0x1f0/0x420 [ 2.851092] kthread+0xf0/0x120 [ 2.854235] ret_from_fork+0x10/0x18 [ 2.857810] ---[ end trace bbece0f244d7c6b1 ]--- [ 2.862499] ------------[ cut here ]------------ [ 2.867121] WARNING: CPU: 0 PID: 31 at drivers/reset/core.c:556 __reset_control_get_internal+0x64/0x110 [ 2.876511] Modules linked in: [ 2.879568] CPU: 0 PID: 31 Comm: kworker/0:1 Tainted: G W 5.4.47-2.2.0+g5ec03d06f54e #1 [ 2.888872] Hardware name: FSL i.MX8MM EVK board (DT) [ 2.893925] Workqueue: events deferred_probe_work_func [ 2.899065] pstate: 20000005 (nzCv daif -PAN -UAO) [ 2.903856] pc : __reset_control_get_internal+0x64/0x110 [ 2.909169] lr : __of_reset_control_get+0x158/0x1b0 [ 2.914046] sp : ffff800011de3830 [ 2.917359] x29: ffff800011de3830 x28: 0000000000000000 [ 2.922672] x27: ffff000077644b38 x26: 0000000000000001 [ 2.927984] x25: 0000000000000000 x24: 0000000000000001 [ 2.933296] x23: 0000000000000000 x22: ffff0000768d9d80 [ 2.938608] x21: 0000000000000009 x20: ffff0000768d9da0 [ 2.943921] x19: ffff00007693d900 x18: 0000000000000010 [ 2.949233] x17: 0000000000000000 x16: 0000000000000000 [ 2.954544] x15: ffff000076318470 x14: 72632d666964636c [ 2.959856] x13: 2d786d6920646e75 x12: 0000000000000000 [ 2.965168] x11: 0000000000000020 x10: 0101010101010101 [ 2.970481] x9 : fffffffffffffffd x8 : 7f7f7f7f7f7f7f7f [ 2.972125] random: fast init done [ 2.975795] x7 : 766f21ff726b6b64 x6 : 0000000080237077 [ 2.984498] x5 : fffffdfffe60976c x4 : 0000000000000000 [ 2.989810] x3 : 0000000000000001 x2 : 0000000000000009 [ 2.995123] x1 : 0000000000000009 x0 : 0000000000000000 [ 3.000435] Call trace: [ 3.002881] __reset_control_get_internal+0x64/0x110 [ 3.007847] __of_reset_control_get+0x158/0x1b0 [ 3.012379] of_reset_control_array_get+0xac/0x1a0 [ 3.017172] imx_sec_dsim_bind+0x208/0x348 [ 3.021270] component_bind_all+0xfc/0x258 [ 3.025369] imx_drm_bind+0xb8/0x150 [ 3.028943] try_to_bring_up_master+0x164/0x1c8 [ 3.033473] __component_add+0xa0/0x168 [ 3.037307] component_add+0x10/0x18 [ 3.040884] imx_sec_dsim_probe+0x4c/0x70 [ 3.044893] platform_drv_probe+0x50/0xa0 [ 3.048901] really_probe+0xd4/0x318 [ 3.052479] driver_probe_device+0x54/0xe8 [ 3.056574] __device_attach_driver+0x80/0xb8 [ 3.060934] bus_for_each_drv+0x74/0xc0 [ 3.064768] __device_attach+0xdc/0x138 [ 3.068604] device_initial_probe+0x10/0x18 [ 3.072788] bus_probe_device+0x90/0x98 [ 3.076622] deferred_probe_work_func+0x64/0x98 [ 3.081156] process_one_work+0x198/0x320 [ 3.085164] worker_thread+0x1f0/0x420 [ 3.088913] kthread+0xf0/0x120 [ 3.092053] ret_from_fork+0x10/0x18 [ 3.095626] ---[ end trace bbece0f244d7c6b2 ]--- [ 3.100321] ------------[ cut here ]------------ [ 3.104943] WARNING: CPU: 0 PID: 31 at drivers/reset/core.c:556 __reset_control_get_internal+0x64/0x110 [ 3.114333] Modules linked in: [ 3.117390] CPU: 0 PID: 31 Comm: kworker/0:1 Tainted: G W 5.4.47-2.2.0+g5ec03d06f54e #1 [ 3.126693] Hardware name: FSL i.MX8MM EVK board (DT) [ 3.131748] Workqueue: events deferred_probe_work_func [ 3.136885] pstate: 20000005 (nzCv daif -PAN -UAO) [ 3.141676] pc : __reset_control_get_internal+0x64/0x110 [ 3.146986] lr : __of_reset_control_get+0x158/0x1b0 [ 3.151862] sp : ffff800011de3830 [ 3.155176] x29: ffff800011de3830 x28: 0000000000000000 [ 3.160488] x27: ffff000077644b38 x26: 0000000000000001 [ 3.165801] x25: 0000000000000000 x24: 0000000000000001 [ 3.171113] x23: 0000000000000000 x22: ffff0000768db380 [ 3.176425] x21: 0000000000000001 x20: ffff0000768db3a0 [ 3.181738] x19: ffff00007693da80 x18: 0000000000000010 [ 3.187050] x17: 0000000000000000 x16: 0000000000000000 [ 3.192362] x15: ffff000076318470 x14: 72632d666964636c [ 3.197675] x13: 2d786d6920646e75 x12: 0000000000000000 [ 3.202987] x11: 0000000000000020 x10: 0101010101010101 [ 3.208299] x9 : fffffffffffffffd x8 : 7f7f7f7f7f7f7f7f [ 3.213612] x7 : 766f21ff726b6b64 x6 : 0000000080237077 [ 3.218924] x5 : fffffdfffe6097bc x4 : 0000000000000000 [ 3.224236] x3 : 0000000000000001 x2 : 0000000000000001 [ 3.229548] x1 : 0000000000000001 x0 : 0000000000000000 [ 3.234860] Call trace: [ 3.237307] __reset_control_get_internal+0x64/0x110 [ 3.242273] __of_reset_control_get+0x158/0x1b0 [ 3.246802] of_reset_control_array_get+0xac/0x1a0 [ 3.251595] imx_sec_dsim_bind+0x208/0x348 [ 3.255692] component_bind_all+0xfc/0x258 [ 3.259790] imx_drm_bind+0xb8/0x150 [ 3.263365] try_to_bring_up_master+0x164/0x1c8 [ 3.267894] __component_add+0xa0/0x168 [ 3.271728] component_add+0x10/0x18 [ 3.275305] imx_sec_dsim_probe+0x4c/0x70 [ 3.279315] platform_drv_probe+0x50/0xa0 [ 3.283324] really_probe+0xd4/0x318 [ 3.286903] driver_probe_device+0x54/0xe8 [ 3.290998] __device_attach_driver+0x80/0xb8 [ 3.295354] bus_for_each_drv+0x74/0xc0 [ 3.299188] __device_attach+0xdc/0x138 [ 3.303025] device_initial_probe+0x10/0x18 [ 3.307208] bus_probe_device+0x90/0x98 [ 3.311043] deferred_probe_work_func+0x64/0x98 [ 3.315576] process_one_work+0x198/0x320 [ 3.319584] worker_thread+0x1f0/0x420 [ 3.323333] kthread+0xf0/0x120 [ 3.326473] ret_from_fork+0x10/0x18 [ 3.330045] ---[ end trace bbece0f244d7c6b3 ]--- [ 3.334695] imx_sec_dsim_drv 32e10000.mipi_dsi: no invalid reset control exists [ 3.342023] imx-drm soc@0:bus@32c00000:display-subsystem: failed to bind 32e10000.mipi_dsi (ops imx_sec_dsim_ops): -22 [ 3.352836] imx-drm soc@0:bus@32c00000:display-subsystem: master bind failed: -22 [ 3.360356] imx_sec_dsim_drv: probe of 32e10000.mipi_dsi failed with error -22 [ 3.368768] imx_usb 32e40000.usb: No over current polarity defined [ 3.375020] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator [ 3.387692] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1 [ 3.400134] mmc0: CQHCI version 5.10 [ 3.436232] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA [ 3.444457] mmc1: CQHCI version 5.10 [ 3.448102] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 3.487631] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 3.497291] debugfs: Directory '30020000.sai' with parent 'bt-sco-audio' already present! [ 3.505611] asoc-simple-card sound-bt-sco: bt-sco-pcm <-> 30020000.sai mapping ok [ 3.513130] asoc-simple-card sound-bt-sco: ASoC: no DMI vendor name! [ 3.519540] debugfs: File 'Playback' in directory 'dapm' already present! [ 3.526358] debugfs: File 'Capture' in directory 'dapm' already present! [ 3.534454] mmc0: queuing unknown CIS tuple 0x01 (3 bytes) [ 3.541438] debugfs: Directory '30030000.sai' with parent 'wm8524-audio' already present! [ 3.550124] asoc-simple-card sound-wm8524: wm8524-hifi <-> 30030000.sai mapping ok [ 3.557729] asoc-simple-card sound-wm8524: ASoC: no DMI vendor name! [ 3.572009] mmc0: queuing unknown CIS tuple 0x1a (5 bytes) [ 3.580233] imx-ak4458 sound-ak4458: ASoC: failed to init link ak4458: -517 [ 3.587218] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517) [ 3.594286] mmc0: queuing unknown CIS tuple 0x1b (8 bytes) [ 3.600655] mmc0: queuing unknown CIS tuple 0x14 (0 bytes) [ 3.656507] imx6q-pcie 33800000.pcie: Phy link never came up [ 3.937302] imx6q-pcie 33800000.pcie: failed to initialize host [ 3.943248] imx6q-pcie 33800000.pcie: unable to add pcie port. [ 3.948618] ak4458 2-0010: ASoC: failed to probe component -6 [ 3.954887] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6 [ 3.963725] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6) [ 3.971921] mmc0: queuing unknown CIS tuple 0x80 (1 bytes) [ 3.977509] mmc0: queuing unknown CIS tuple 0x81 (1 bytes) [ 3.983039] mmc1: host does not support reading read-only switch, assuming write-enable [ 3.991108] mmc0: queuing unknown CIS tuple 0x82 (1 bytes) [ 3.996637] mmc0: new ultra high speed SDR104 SDIO card at address 0001 [ 4.004916] input: bd718xx-pwrkey as /devices/platform/soc@0/soc@0:bus@30800000/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input1 [ 4.017886] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:02 UTC (2) [ 4.027304] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 4.039456] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 4.046056] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 4.054287] ALSA device list: [ 4.054687] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db [ 4.057657] #0: imx-spdif [ 4.068201] #1: imx-audio-micfil [ 4.071611] #2: bt-sco-audio [ 4.074843] #3: wm8524-audio [ 4.078120] Waiting for root device /dev/mmcblk1p2... [ 4.116251] mmc1: new ultra high speed DDR50 SDHC card at address e624 [ 4.123352] mmcblk1: mmc1:e624 SB16G 14.8 GiB [ 4.132678] mmcblk1: p1 p2 [ 4.207049] EXT4-fs (mmcblk1p2): recovery complete [ 4.212999] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 4.221220] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 4.231730] devtmpfs: mounted [ 4.235527] Freeing unused kernel memory: 2944K [ 4.240135] Run /sbin/init as init process [ 4.453372] systemd[1]: System time before build time, advancing clock. [ 4.481694] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 4.504015] systemd[1]: Detected architecture arm64. Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)! [ 4.554978] systemd[1]: Set hostname to . [ 4.762462] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus/system_bus_socket → /run/dbus/system_bus_socket; please update the unit file accordingly. [ 4.791987] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslogd.pid → /run/syslogd.pid; please update the unit file accordingly. [ 4.823812] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/rpcbind.sock → /run/rpcbind.sock; please update the unit file accordingly. [ 4.849846] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/klogd.pid → /run/klogd.pid; please update the unit file accordingly. [ 4.953501] random: systemd: uninitialized urandom read (16 bytes read) [ 4.960317] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 4.972704] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 4.982960] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 5.004026] random: systemd: uninitialized urandom read (16 bytes read) [ OK ] Created slice system-serial\x2dgetty.slice. [ 5.027965] random: systemd: uninitialized urandom read (16 bytes read) [ OK ] Created slice User and Session Slice. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ OK ] Reached target Host and Network Name Lookups. [ OK ] Reached target Paths. [ OK ] Reached target Remote File Systems. [ OK ] Reached target Slices. [ OK ] Reached target Swap. [ OK ] Listening on Syslog Socket. [ OK ] Listening on initctl Compatibility Named Pipe. [ OK ] Listening on Journal Audit Socket. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on udev Control Socket. [ OK ] Listening on udev Kernel Socket. Mounting Huge Pages File System... Mounting POSIX Message Queue File System... Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)... Starting Create list of st…odes for the current kernel... Starting Journal Service... Mounting Kernel Configuration File System... Starting Remount Root and Kernel File Systems... [ 5.434091] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) Starting Apply Kernel Variables... Starting udev Coldplug all Devices... Starting Setup Virtual Console... [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Create list of sta… nodes for the current kernel. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Apply Kernel Variables. [ OK ] Started Setup Virtual Console. Starting Flush Journal to Persistent Storage... [ 5.683603] systemd-journald[256]: Received client request to flush runtime journal. Starting Create Static Device Nodes in /dev... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Started udev Coldplug all Devices. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Create Volatile Files and Directories. Starting Start Psplash Boot Screen... Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Start Psplash Boot Screen. [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ 6.137257] Registered IR keymap rc-empty [ 6.141414] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0 [ 6.148988] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input2 [ OK ] Reached target System Time Synchronized. [ OK ] Started Daily apt download activities. [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on dropbear.socket. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. Starting Console System Startup Logging... [ 6.419933] qca9377: loading out-of-tree module taints kernel. [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. [ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S). Starting Packet Filtering Framework... Starting Network Time Service (one-shot ntpdate mode)... Starting Telephony service... [ OK ] Started Updates psplash to basic. [ OK ] Started User Space Regulatory Firmware Loading. Starting RPC Bind Service... [ OK ] Started User Space SDMA Firmware Loading. Starting System Logging Service... Starting Login Service... [ 6.667523] qca9377: loading driver v4.5.24.4 [ 6.674053] imx-sdma 30bd0000.dma-controller: loaded firmware 4.5 [ 6.675402] hifDeviceInserted: Dumping clocks (50000000,400000000) [ OK ] Started TEE Supplicant. [ 6.696570] AR6000: Set async interrupt delay clock as 2. [ OK ] Started Console System Startup Logging. [ OK ] Started Packet Filtering Framework. [ OK ] Started Network Time Service (one-shot ntpdate mode). [ OK ] Started RPC Bind Service. [ OK ] Started System Logging Service. [ OK ] Started Telephony service. [ 6.852094] AR6000: configuration opcode 3 is not used for Linux SDIO stack [ 6.862515] NUM_DEV=1 FWMODE=0x2 FWSUBMODE=0x0 FWBR_BUF 0 [ OK ] Started Login Service. [ OK ] Reached target Network (Pre). Starting Save/Restore Sound Card State... Starting Connection service... Starting Kernel Logging Service... Starting Network Service... [ OK ] Started Save/Restore Sound Card State. [ OK ] Reached target Sound Card. [ OK [ 7.212910] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL) ] Started Network Service. [ OK ] Started Connection service. [ OK ] Reached target Network. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Update psplash to network. Starting Terminate Psplash Boot Screen... Starting /etc/rc.local Compatibility... Starting Permit User Sessions... [FAILED] Failed to start Terminate Psplash Boot Screen. See 'systemctl status psplash-quit.service' for details. [ OK ] Started Kernel Logging Service. [ OK ] Started /etc/rc.local Compatibility. [ OK ] Started Permit User Sessions. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttymxc1. [ OK ] Reached target Login Prompts. [ OK ] Reached target Multi-User System. Starting Hostname Service... Starting Update UTMP about System Runlevel Changes... Starting WPA supplicant... [ 7.686982] random: crng init done [ 7.690392] random: 7 urandom warning(s) missed due to ratelimiting [ OK ] Started Load/Save Ra[ 7.710610] HIF Interrupt processing is SYNC ONLY ndom Seed. [ 7.718367] AR6000: configuration opcode 7 is only used for RTOS systems, not Linux systems [ 7.728084] AR6000: configuration opcode 5 is not used for Linux SDIO stack [ 7.736407] +HWT [ 7.743522] -HWT [ 7.745647] MAILBOX SWAP Service is enabled! [ 7.750096] Reduced Tx Complete service is enabled! [ OK ] [ 7.756452] HTCConnectService, host indicate support b2b bundle Started Hostname Service[ 7.764124] HTCConnectService, firmware decide to disabled b2b bundle . [ 7.772154] HTC Service:0x0300 ep:1 TX flow control disabled [ 7.779383] HTCConnectService, host indicate support b2b bundle [ 7.785575] HTCConnectService, firmware decide to disabled b2b bundle [ 7.807656] target uses HTT version 3.53; host uses 3.28 [ 7.813227] Host SW:4.5.24.4, FW:0.0.0.23, HW:QCA93x7_REV1_1 [ 7.819396] ol_pktlog_init: pktlogmod_init successfull [ 7.824951] ath_hif_sdio: HIF (Atheros/multi-bss) [ 7.830457] qca9377: driver loaded in 1164000 [ OK ] Started WPA supplicant. [ OK ] Started Update UTMP about System Runlevel Changes. [ OK ] Created slice system-systemd\x2dfsck.slice. Starting File System Check on /dev/mmcblk1p1... Starting File System Check on /dev/mmcblk2p10... Starting File System Check on /dev/mmcblk2p11... Starting File System Check on /dev/mmcblk2p12... Starting File System Check on /dev/mmcblk2p5... Starting File System Check on /dev/mmcblk2p6... [ OK ] Started File System Check on /dev/mmcblk1p1. Mounting /run/media/mmcblk1p1... [ OK ] Started File System Check on /dev/mmcblk2p12. Mounting /run/media/mmcblk2p12... [ 8.220633] EXT4-fs (mmcblk2p12): The kernel was not built with CONFIG_QUOTA and CONFIG_QFMT_V2 [FAILED] Failed to mount /run/media/mmcblk2p12. See 'systemctl status run-media-mmcblk2p12.mount' for details. [ OK ] Mounted /run/media/mmcblk1p1. [ OK ] Started File System Check on /dev/mmcblk2p11. Mounting /run/media/mmcblk2p11... [ OK ] Started File System Check on /dev/mmcblk2p10. Mounting /run/media/mmcblk2p10... [ 8.536919] EXT4-fs (mmcblk2p11): mounted filesystem without journal. Opts: (null) [ 8.544760] ext4 filesystem being mounted at /run/media/mmcblk2p11 supports timestamps until 2038 (0x7fffffff) [ OK ] Mounted /run/media/mmcblk2p11. [ 8.572713] EXT4-fs (mmcblk2p10): mounted filesystem without journal. Opts: (null) [ 8.580530] ext4 filesystem being mounted at /run/media/mmcblk2p10 supports timestamps until 2038 (0x7fffffff) [ OK ] Mounted /run/media/mmcblk2p10. [ OK ] Started File System Check on /dev/mmcblk2p6. [ OK ] Started File System Check on /dev/mmcblk2p5. Mounting /run/media/mmcblk2p5... Mounting /run/media/mm[ 8.802048] EXT4-fs (mmcblk2p5): mounted filesystem without journal. Opts: (null) cblk2p6... [ 8.819461] EXT4-fs (mmcblk2p6): mounted filesystem without journal. Opts: (null) [ OK ] Mounted /run/media/mmcblk2p5. [ OK ] Mounted /run/media/mmcblk2p6. NXP i.MX Release Distro 5.4-zeus imx8mmevk ttymxc1 imx8mmevk login: