U-Boot 2014.04-00010-g10c4776543-dirty (Apr 12 2021 - 17:59:48) CPU: Freescale i.MX6D rev1.5 at 792 MHz CPU: Temperature 26 C, calibration data: 0x56d4ef69 Reset cause: POR Board: MX6-NANO I2C: ready DRAM: 256 MiB MMC: FSL_SDHC: 0, FSL_SDHC: 1 No panel detected: default to Hannstar-XGA Display: Hannstar-XGA (1024x768) In: serial Out: serial Err: serial Found PFUZE100 deviceid=10,revid=21 mmc0 is current device Net: FEC [PRIME] Warning: failed to set MAC address Normal Boot Hit any key to stop autoboot: 0 mmc0 is current device reading uImage 6081752 bytes read in 283 ms (20.5 MiB/s) reading imx6qd-nano.dtb 40935 bytes read in 19 ms (2.1 MiB/s) ## Booting kernel from Legacy Image at 12000000 ... Image Name: Linux-3.14.28+gfd07114f13f2 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 6081688 Bytes = 5.8 MiB Load Address: 10008000 Entry Point: 10008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 18000000 Booting using the fdt blob at 0x18000000 Loading Kernel Image ... OK Using Device Tree in place at 18000000, end 1800cfe6 switch to ldo_bypass mode! Starting kernel ... Booting Linux on physical CPU 0x0 Linux version 3.14.28+gfd07114f13f2 (shivashankar@SVR0025U) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Mon Apr 5 16:54:36 IST 2021 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 Quad NANO Board cma: CMA: failed to reserve 320 MiB Memory policy: Data cache writealloc On node 0 totalpages: 65536 free_area_init_node: node 0, pgdat 80e13f80, node_mem_map 8fdf7000 DMA zone: 512 pages used for memmap DMA zone: 0 pages reserved DMA zone: 65536 pages, LIFO batch:15 PERCPU: Embedded 8 pages/cpu @8fdd6000 s9088 r8192 d15488 u32768 pcpu-alloc: s9088 r8192 d15488 u32768 alloc=8*4096 pcpu-alloc: [0] 0 [0] 1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 Kernel command line: console=ttymxc0,115200 loglevel=8 video=mxcfb1:dev=hdmi,1920x1024M@60,bpp=24 fbmem=24M video=mxcfb0:off videot PID hash table entries: 1024 (order: 0, 4096 bytes) Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Memory: 244856K/262144K available (7353K kernel code, 404K rwdata, 6284K rodata, 340K init, 430K bss, 17288K reserved, 0K highmem) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) vmalloc : 0x90800000 - 0xff000000 (1768 MB) lowmem : 0x80000000 - 0x90000000 ( 256 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .text : 0x80008000 - 0x80d59660 (13638 kB) .init : 0x80d5a000 - 0x80daf380 ( 341 kB) .data : 0x80db0000 - 0x80e153a0 ( 405 kB) .bss : 0x80e153ac - 0x80e80bdc ( 431 kB) SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 Preemptible hierarchical RCU implementation. RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2. RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 NR_IRQS:16 nr_irqs:16 16 L310 cache controller enabled l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB Switching to timer-based delay loop sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns Console: colour dummy device 80x30 Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 Setting up static identity map for 0x106fe6b8 - 0x106fe710 CPU1: Booted secondary processor CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 Brought up 2 CPUs SMP: Total of 2 processors activated. CPU: All CPU(s) started in SVC mode. devtmpfs: initialized VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 pinctrl core: initialized pinctrl subsystem regulator-dummy: no parameters NET: Registered protocol family 16 DMA: failed to allocate 256 KiB pool for atomic coherent allocation cpuidle: using governor ladder cpuidle: using governor menu CPU identified as i.MX6Q, silicon rev 1.5 Use WDOG1 as reset source syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered vdd1p1: 800 <--> 1375 mV at 1100 mV vdd3p0: 2800 <--> 3150 mV at 3000 mV vdd2p5: 2000 <--> 2750 mV at 2400 mV vddarm: 725 <--> 1450 mV vddpu: 725 <--> 1450 mV vddsoc: 725 <--> 1450 mV syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. hw-breakpoint: maximum watchpoint size is 4 bytes. imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver bio: create slab at 0 mxs-dma 110000.dma-apbh: initialized wlreg_on: 5000 mV usb_otg_vbus: 5000 mV usb_h1_vbus: 5000 mV wm8962-supply: no parameters sensor-supply: 3300 mV sgtl-3p15v: 3150 mV sgtl-3p3v: 3300 mV vgaarb: loaded i2c-core: driver [max17135] using legacy suspend method i2c-core: driver [max17135] using legacy resume method SCSI subsystem initialized libata version 3.00 loaded. usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb usbphy_nop1.12 supply vcc not found, using dummy regulator usbphy_nop2.13 supply vcc not found, using dummy regulator i2c i2c-0: IMX I2C adapter registered i2c i2c-1: IMX I2C adapter registered i2c i2c-2: IMX I2C adapter registered Linux video capture interface: v2.00 pps_core: LinuxPPS API ver. 1 registered pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti PTP clock support registered imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a MIPI CSI2 driver module loaded Advanced Linux Sound Architecture Driver Initialized. Bluetooth: Core ver 2.18 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized Bluetooth: L2CAP socket layer initialized Bluetooth: SCO socket layer initialized cfg80211: Calling CRDA to update world regulatory domain Switched to clocksource mxc_timer1 NET: Registered protocol family 2 TCP established hash table entries: 2048 (order: 1, 8192 bytes) TCP bind hash table entries: 2048 (order: 2, 16384 bytes) TCP: Hash tables configured (established 2048 bind 2048) TCP: reno registered UDP hash table entries: 256 (order: 1, 8192 bytes) UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. PCI: CLS 0 bytes, default 64 hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available imx6_busfreq busfreq.16: DDR medium rate not supported. Bus freq driver module loaded futex hash table entries: 512 (order: 3, 32768 bytes) VFS: Disk quotas dquot_6.5.2 Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) NFS: Registering the id_resolver key type Key type id_resolver registered Key type id_legacy registered jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. fuse init (API version 7.22) msgmni has been set to 478 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) imx-weim 21b8000.weim: Driver registered. imx6q-pcie 1ffc000.pcie: phy link never came up imx6q-pcie 1ffc000.pcie: Failed to bring link up! imx6q-pcie 1ffc000.pcie: failed to initialize host imx6q-pcie: probe of 1ffc000.pcie failed with error -22 backlight.26 supply power not found, using dummy regulator MIPI DSI driver module loaded mxc_sdc_fb fb.24: Can't get fb option for mxcfb0! mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1 fbcvt: Aspect ratio not CVT standard fbcvt: 1920x1024@60: CVT Name - Not a CVT standard - 1.966 Mega Pixel Image mxc_sdc_fb fb.25: registered mxc display driver hdmi mxc_sdc_fb fb.25: Unable to allocate framebuffer memory detected fb_set_par error, error code: -12 mxc_sdc_fb fb.25: Error fb_set_var ret:-12 mxc_sdc_fb: probe of fb.25 failed with error -12 imx-sdma 20ec000.sdma: no iram assigned, using external mem imx-sdma 20ec000.sdma: initialisation failed with -12 imx-sdma: probe of 20ec000.sdma failed with error -12 pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1 pfuze100-regulator 1-0008: FAB: 0, FIN: 0 pfuze100-regulator 1-0008: pfuze100 found. SW1AB: 300 <--> 1875 mV at 1150 mV SW1C: 300 <--> 1875 mV at 1175 mV SW2: 800 <--> 3300 mV at 3150 mV SW3A: 400 <--> 1975 mV at 1200 mV SW3B: 400 <--> 1975 mV at 1200 mV SW4: 800 <--> 1975 mV at 1800 mV SWBST: 5000 <--> 5150 mV at 5000 mV VSNVS: 1000 <--> 3000 mV at 3000 mV VREFDDR: 750 mV VGEN1: 800 <--> 1550 mV at 1200 mV VGEN2: 800 <--> 1550 mV at 800 mV VGEN3: 1800 <--> 3300 mV at 2800 mV VGEN4: 1800 <--> 3300 mV at 1800 mV VGEN5: 1800 <--> 3300 mV at 3000 mV VGEN6: 1800 <--> 3300 mV at 1800 mV Serial: IMX driver 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX console [ttymxc0] enabled 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX serial: Freescale lpuart driver imx sema4 driver is registered. [drm] Initialized drm 1.1.0 20060810 [drm] Initialized vivante 1.0.0 20120216 on minor 0 brd: module loaded loop: module loaded physmap platform flash device: 02000000 at 08000000 physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000020 Chip ID 0x00227e Amd/Fujitsu Extended Query Table at 0x0040 Amd/Fujitsu Extended Query version 1.3. number of CFI chips: 1 of-flash: probe of 8000000.nor failed with error -16 spi_imx 2008000.ecspi: cannot get the TX DMA channel! spi_imx 2008000.ecspi: dma setup error,use pio instead spi_imx 2008000.ecspi: probed CAN device driver interface 2188000.ethernet supply phy not found, using dummy regulator pps pps0: new PPS source ptp0 fec: probe of 2188000.ethernet failed with error -12 ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver ehci-pci: EHCI PCI platform driver ehci-mxc: Freescale On-Chip EHCI Host driver usbcore: registered new interface driver usb-storage 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator ci_hdrc ci_hdrc.0: doesn't support gadget ci_hdrc ci_hdrc.1: doesn't support gadget ci_hdrc ci_hdrc.1: EHCI Host Controller ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.1: can't setup: -12 ci_hdrc ci_hdrc.1: USB bus 1 deregistered ci_hdrc ci_hdrc.1: can't start host role ci_hdrc: probe of ci_hdrc.1 failed with error -12 mousedev: PS/2 mouse device common for all mice input: st1232-touchscreen as /devices/soc0/soc.0/2100000.aips-bus/21a4000.i2c/i2c-1/1-0055/input/input0 i2c-core: driver [isl29023] using legacy suspend method i2c-core: driver [isl29023] using legacy resume method snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0 i2c /dev entries driver IR NEC protocol handler initialized IR RC5(x) protocol handler initialized IR RC6 protocol handler initialized IR JVC protocol handler initialized IR Sony protocol handler initialized IR RC5 (streamzap) protocol handler initialized IR SANYO protocol handler initialized IR MCE Keyboard/mouse protocol handler initialized i2c-core: driver [mag3110] using legacy suspend method i2c-core: driver [mag3110] using legacy resume method imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0) Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCI H4 protocol initialized Bluetooth: HCI BCSP protocol initialized Bluetooth: HCIATH3K protocol initialized usbcore: registered new interface driver bcm203x usbcore: registered new interface driver btusb Bluetooth: Generic Bluetooth SDIO driver ver 0.1 usbcore: registered new interface driver ath3k sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman sdhci-pltfm: SDHCI platform and OF driver helper sdhci-esdhc-imx 2190000.usdhc: assigned as wifi host mmc0: no vqmmc regulator found mmc0: no vmmc regulator found mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA mmc1: no vqmmc regulator found mmc1: no vmmc regulator found mmc0: queuing unknown CIS tuple 0x80 (7 bytes) mmc0: queuing unknown CIS tuple 0x80 (6 bytes) mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA mmc2: no vqmmc regulator found mmc2: no vmmc regulator found mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA mmc0: queuing unknown CIS tuple 0x91 (3 bytes) mmc0: new high speed SDIO card at address 0001 Galcore version 5.0.11.25762 Unable to handle kernel paging request at virtual address d7f9d009 pgd = 80004000 [d7f9d009] *pgd=00000000 Internal error: Oops: 5 [#1] PREEMPT SMP ARM Modules linked in: CPU: 1 PID: 1 Comm: swapper/0 Not tainted 3.14.28+gfd07114f13f2 #1 task: 8c0a0000 ti: 8c09e000 task.ti: 8c09e000 PC is at gckOS_FreeNonPagedMemory+0x40/0x108 LR is at gckOS_AcquireMutex+0x58/0x68 pc : [<804bfddc>] lr : [<804bf6bc>] psr: 60000113 sp : 8c09fcc8 ip : 8c39c700 fp : 02208000 r10: 8c3a4204 r9 : 8c3a4200 r8 : 00000000 r7 : 00000000 r6 : 8c0e0300 r5 : 00000000 r4 : d7f9d001 r3 : 00000000 r2 : 00000000 r1 : 8c39c100 r0 : 00000000 Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel Control: 10c53c7d Table: 1000404a DAC: 00000015 Process swapper/0 (pid: 1, stack limit = 0x8c09e238) Stack: (0x8c09fcc8 to 0x8c0a0000) fcc0: 8c3a4200 8c3a4204 02208000 804bf0f4 8c3a4400 8c0e0300 fce0: fffffffd 804d7260 8c0e0000 804c7b98 0000002a 8c0df600 8c3a4200 00000000 fd00: 8c09fdc4 02208000 00000029 0000002a 00000000 804bdad0 8c3a4204 00000000 fd20: 00000000 80dfdeac 00000000 80dfdd94 00000000 00000000 00000000 00000000 fd40: 00000001 00000001 00000800 806f65fc 80cbfe3c 80dfdd94 00000000 80e6f5ac fd60: 8c158600 00000030 00000000 00000000 ffffffff 804c5bc0 00134000 00004000 fd80: 0000002b 02204000 00004000 00000000 08000000 00000000 ffffffff ffffffff fda0: 00000000 00000000 00000030 00000000 ffffffff 00000000 8c09fdc4 8c09fdc0 fdc0: 00000000 00000001 00000001 00000001 00000000 80e6f5ac 00000001 00000029 fde0: 00130000 00004000 0000002a 00134000 00004000 0000002b 02204000 00004000 fe00: 08000000 00000000 00000000 00000000 ffffffff ffffffff ffffffff 00000000 fe20: 00000030 00000000 00000000 00000000 00000001 00000001 00000000 00000001 fe40: 8c39b480 80e6bdec 8c158610 80dfdda8 fffffdfb 00000000 00000114 80da01f4 fe60: 00000000 803534b8 80353474 80e6bdec 8c158610 00000000 80dfdda8 80351d44 fe80: 8c158610 80dfdda8 8c158644 80ddc1a0 80e153c0 80351f50 00000000 80dfdda8 fea0: 80351ec4 8035029c 8c08665c 8c14e3b4 80dfdda8 8c396c00 00000000 803514fc fec0: 80cbfb08 80dfdda8 80e6f5ac 80dfdda8 80e6f5ac 80da01ec 80e153c0 8035254c fee0: 00000000 80e6f5ac 80e6f5ac 80d8deb0 00000000 8c09e000 80d8dd98 8000889c ff00: 8c011900 80c49f28 8c10de00 80701e84 00000000 00000000 000053c0 8012a214 random: nonblocking pool is initialized ff20: 00000000 80dc3530 60000113 00000001 00000008 00000000 8fde868d 80046580 ff40: 80ca8c94 00000006 00000006 8fde8695 80dc3520 80dabe38 00000006 80da01ec ff60: 80e153c0 80e153c0 00000114 80da01f4 00000000 80d5ac54 00000006 00000006 ff80: 80d5a514 8004f290 00000000 806f3ac8 00000000 00000000 00000000 00000000 ffa0: 00000000 806f3ad0 00000000 8000e4f8 00000000 00000000 00000000 00000000 ffc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 ffe0: 00000000 00000000 00000000 00000000 00000013 00000000 10444109 30022440 [<804bfddc>] (gckOS_FreeNonPagedMemory) from [<804d7260>] (gckHARDWARE_Destroy+0x64/0x80) [<804d7260>] (gckHARDWARE_Destroy) from [<804c7b98>] (gckKERNEL_Construct+0x1c0/0x43c) [<804c7b98>] (gckKERNEL_Construct) from [<804bdad0>] (gckGALDEVICE_Construct+0x19c/0x99c) [<804bdad0>] (gckGALDEVICE_Construct) from [<804c5bc0>] (gpu_probe+0x244/0x394) [<804c5bc0>] (gpu_probe) from [<803534b8>] (platform_drv_probe+0x44/0xa4) [<803534b8>] (platform_drv_probe) from [<80351d44>] (driver_probe_device+0x110/0x24c) [<80351d44>] (driver_probe_device) from [<80351f50>] (__driver_attach+0x8c/0x90) [<80351f50>] (__driver_attach) from [<8035029c>] (bus_for_each_dev+0x6c/0xa0) [<8035029c>] (bus_for_each_dev) from [<803514fc>] (bus_add_driver+0x148/0x1f0) [<803514fc>] (bus_add_driver) from [<8035254c>] (driver_register+0x78/0xf8) [<8035254c>] (driver_register) from [<80d8deb0>] (gpu_init+0x118/0x138) [<80d8deb0>] (gpu_init) from [<8000889c>] (do_one_initcall+0xf8/0x154) [<8000889c>] (do_one_initcall) from [<80d5ac54>] (kernel_init_freeable+0x138/0x1d8) [<80d5ac54>] (kernel_init_freeable) from [<806f3ad0>] (kernel_init+0x8/0xe8) [<806f3ad0>] (kernel_init) from [<8000e4f8>] (ret_from_fork+0x14/0x3c) Code: e5901008 e3e02000 e1a06000 ebfffe21 (e5941008) ---[ end trace 83a46f85474867d2 ]--- Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b CPU0: stopping CPU: 0 PID: 103 Comm: kworker/u5:0 Tainted: G D 3.14.28+gfd07114f13f2 #1 Workqueue: hci0 hci_power_on +-----------------------------+ [<800155f0>] (unwind_backtrace) from [<800116d4>] | | [<800116d4>] (show_stack) from [<806f847c>] (dump_| Cannot open /dev/ttyUSB0! | [<806f847c>] (dump_stack) from [<80014590>] (handl| | [<80014590>] (handle_IPI) from [<80008598>] (gic_h+-----------------------------+ [<80008598>] (gic_handle_irq) from [<800121c0>] (__irq_svc+0x40/0x70) Exception stack(0x8c3a7d68 to 0x8c3a7db0) 7d60: 8c32139c 60000113 00000002 00002577 8c3212f0 8c398290 7d80: 000000ff 8c39828c ffff8c38 00000000 8c3a6008 8c33da00 00000000 8c3a7db0 7da0: 804fb970 806fde14 20000113 ffffffff [<800121c0>] (__irq_svc) from [<806fde14>] (_raw_spin_unlock_irqrestore+0x20/0x54) [<806fde14>] (_raw_spin_unlock_irqrestore) from [<804fb970>] (led_trigger_event+0x3c/0x58) [<804fb970>] (led_trigger_event) from [<804a3654>] (mmc_start_request+0xb0/0xe0) [<804a3654>] (mmc_start_request) from [<804a379c>] (__mmc_start_req+0x60/0x84) [<804a379c>] (__mmc_start_req) from [<804a3c38>] (mmc_wait_for_cmd+0x74/0xa0) [<804a3c38>] (mmc_wait_for_cmd) from [<804ae004>] (mmc_io_rw_direct_host+0xa0/0x144) [<804ae004>] (mmc_io_rw_direct_host) from [<804af3a8>] (sdio_enable_func+0xc0/0xf8) [<804af3a8>] (sdio_enable_func) from [<80498200>] (btsdio_open+0x40/0xbc) [<80498200>] (btsdio_open) from [<80650b0c>] (hci_dev_do_open+0x4c/0x68c) [<80650b0c>] (hci_dev_do_open) from [<80651518>] (hci_power_on+0x1c/0x128) [<80651518>] (hci_power_on) from [<80041ef0>] (process_one_work+0xf4/0x35c) [<80041ef0>] (process_one_work) from [<80042b40>] (worker_thread+0x130/0x3bc) [<80042b40>] (worker_thread) from [<80048260>] (kthread+0xcc/0xe4) [<80048260>] (kthread) from [<8000e4f8>] (ret_from_fork+0x14/0x3c)