[ 3.556804] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref] [ 3.563600] pci 0000:00:00.0: supports D1 [ 3.567627] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold [ 3.575902] pci 0000:01:00.0: [168c:003e] type 00 class 0x028000 [ 3.582009] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x001fffff 64bit] [ 3.589106] pci 0000:01:00.0: PME# supported from D0 D3hot D3cold [ 3.609019] pci 0000:00:00.0: BAR 14: assigned [mem 0x18000000-0x181fffff] [ 3.616022] pci 0000:00:00.0: BAR 0: assigned [mem 0x18200000-0x182fffff] [ 3.622830] pci 0000:00:00.0: BAR 6: assigned [mem 0x18300000-0x1830ffff pref] [ 3.630196] pci 0000:01:00.0: BAR 0: assigned [mem 0x18000000-0x181fffff 64bit] [ 3.637540] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 3.642788] pci 0000:00:00.0: bridge window [mem 0x18000000-0x181fffff] [ 3.649868] pcieport 0000:00:00.0: PME: Signaling with IRQ 237 [ 3.656410] pcieport 0000:00:00.0: AER: enabled with IRQ 237 [ 3.675019] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.683170] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.689516] devtmpfs: mounted [ 3.693289] Freeing unused kernel memory: 2880K [ 3.697888] Run /sbin/init as init process [ 3.750941] usb 1-1.1: new high-speed USB device number 3 using xhci-hcd [ 3.812465] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.834392] systemd[1]: Detected architecture arm64. [ 3.858009] usb-storage 1-1.1:1.0: USB Mass Storage device detected [ 3.866131] scsi host0: usb-storage 1-1.1:1.0 Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)! [ 3.887424] systemd[1]: Set hostname to . [ 3.954935] usb 1-1.2: new low-speed USB device number 4 using xhci-hcd [ 4.037281] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus/system_bus_socket → /run/dbus/system_bus_socket; please update the unit file accordingly. [ 4.063585] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslogd.pid → /run/syslogd.pid; please update the unit file accordingly. [ 4.089430] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/rpcbind.sock → /run/rpcbind.sock; please update the unit file accordingly. [ 4.112162] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/klogd.pid → /run/klogd.pid; please update the unit file accordingly. [ 4.146914] input: SZH usb keyboard as /devices/platform/soc@0/38200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.0/0003:C0F4:04E0.0001/input/input2 [ 4.217904] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 4.228245] hid-generic 0003:C0F4:04E0.0001: input: USB HID v1.10 Keyboard [SZH usb keyboard] on usb-xhci-hcd.1.auto-1.2/input0 [ 4.230305] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 4.244878] input: SZH usb keyboard Consumer Control as /devices/platform/soc@0/38200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:C0F4:04E0.0002/input/input3 [ 4.252085] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ OK ] Created slice User and Session Slice. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 4.327724] input: SZH usb keyboard System Control as /devices/platform/soc@0/38200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:C0F4:04E0.0002/input/input4 [ 4.343019] hid-generic 0003:C0F4:04E0.0002: input: USB HID v1.10 Device [SZH usb keyboard] on usb-xhci-hcd.1.auto-1.2/input1 [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ OK ] Reached target Host and Network Name Lookups. [ OK ] Reached target Paths. [ OK ] Reached target Remote File Systems. [ OK ] Reached target Slices. [ OK ] Reached targe[ 4.435495] usb 1-1.3: new low-speed USB device number 5 using xhci-hcd t Swap. [ OK ] Listening on Syslog Socket. [ OK ] Listening on initctl Compatibility Named Pipe. [ OK ] Listening on Journal Audit Socket. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on udev Control Socket. [ OK ] Listening on udev Kernel Socket. Mounting Huge Pages File System... [ 4.595234] input: PixArt Dell MS116 USB Optical Mouse as /devices/platform/soc@0/38200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.3/1-1.3:1.0/0003:413C:301A.0003/input/input5 [ 4.610881] hid-generic 0003:413C:301A.0003: input: USB HID v1.11 Mouse [PixArt Dell MS116 USB Optical Mouse] on usb-xhci-hcd.1.auto-1.3/input0 Mounting POSIX Message Queue File System... Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)... Starting Create list of st…odes for the current kernel... Starting Journal Service... [ 4.702943] usb 1-1.4: new high-speed USB device number 6 using xhci-hcd Mounting Kernel Configuration File System... Starting Remount Root and Kernel File Systems... [ 4.749858] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) Starting Apply Kernel Variables... Starting udev Coldplug all Devices... Starting Setup Virtual Console... [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ 4.899448] scsi 0:0:0:0: Direct-Access Mass Storage Device 1.00 PQ: 0 ANSI: 0 CCS [ OK ] Started Create list of sta… nodes for the current kernel. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Apply Kernel Variables. [ OK ] Started Setup Virtual Console. Starting Flush Journal to Persistent Storage... [ 5.006955] systemd-journald[260]: Received client request to flush runtime journal. Starting Create Static Device Nodes in /dev... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. [ OK ] Started udev Coldplug all Devices. [ 5.213233] sd 0:0:0:0: [sda] Attached SCSI removable disk [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Start Psplash Boot Screen... Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Start Psplash Boot Screen. [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ OK ] Started Daily apt do[ 5.454398] Registered IR keymap rc-empty wnload activities. [ 5.461843] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0 [ 5.470070] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input6 [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on dropbear.socket. [ 5.554964] uvcvideo: Found UVC 1.00 device (046d:0825) [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. [ OK ] Started Configuratio[ 5.674635] uvcvideo 1-1.4:1.0: Entity type for entity Extension 4 was not initialized! n for i.MX GPU (Former rc_gpu.S)[ 5.685426] uvcvideo 1-1.4:1.0: Entity type for entity Extension 6 was not initialized! [0m. [ 5.696281] uvcvideo 1-1.4:1.0: Entity type for entity Extension 7 was not initialized! [ 5.704816] uvcvideo 1-1.4:1.0: Entity type for entity Processing 2 was not initialized! [ 5.716436] uvcvideo 1-1.4:1.0: Entity type for entity Extension 3 was not initialized! Starting Packet Filterin[ 5.725866] uvcvideo 1-1.4:1.0: Entity type for entity Camera 1 was not initialized! g Framework... [ 5.735801] input: UVC Camera (046d:0825) as /devices/platform/soc@0/38200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.4/1-1.4:1.0/input/input7 [ 5.749819] usbcore: registered new interface driver uvcvideo [ 5.755647] USB Video Class driver (1.1.1) Starting Network Time Service (one-shot ntpdate mode)... Starting Telephony service... [ OK ] Started Updates psplash to basic. Starting RPC Bind Service... Starting System Logging Service... Starting Login Service... [ OK ] Started TEE Supplicant. [ OK ] Started Packet Filtering Framework. [ OK ] Started Network Time Service (one-shot ntpdate mode). [ OK ] Started RPC Bind Service. [ OK ] Started System Logging Service. [ OK ] Started Telephony service. [ OK ] Reached target Network (Pre). Starting Save/Restore Sound Card State... Starting Connection service... Starting Kernel Logging Service... Starting Network Service... [ OK ] Started Save/Restore Sound Card State. [ OK ] Started Login Service. [ OK ] Reached target Sound Card. [ OK ] Started Network Service. [ OK ] Started Connection service. [ 6.182254] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL) Starting Avahi mDNS/DNS-SD Stack... Starting Hostname Service... Starting WPA supplicant... [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started WPA supplicant. [ OK ] Reached target Network. [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Update psplash to network. Starting Terminate Psplash Boot Screen... Starting /etc/rc.local Compatibility... Starting Permit User Sessions... [ OK ] Started Target Communication Framework agent. [ OK ] Started Kernel Logging Service. [ OK ] Started Terminate Psplash Boot Screen. [ OK ] Started /etc/rc.local Compatibility. [ OK ] Started Permit User Sessions. [ OK ] Started Hostname Service. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttymxc0. [ OK ] Reached target Login Prompts. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ 7.234442] usb 1-1.4: set resolution quirk: cval->res = 384 [ 7.241541] usbcore: registered new interface driver snd-usb-audio [ 7.481592] imx-sdma 30bd0000.dma-controller: loaded firmware 4.5 [ 7.639830] audit: type=1006 audit(1617009682.831:2): pid=525 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 NXP i.MX Release Distro 5.4-zeus imx8mqevk ttymxc0 imx8mqevk login: [ 8.277426] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0