Unable to open serial port COM14: ᅬ솨쀄ᅭᄇᄏᄉ퓌ᄌᄊᄄ샤ᅫᅣᄐ￾ᄀᆪ u-boot=> u-boot=> reset resetting ... U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 (Nov 17 2020 - 17:53:08 +0800) power_pca9450_init DRAM PHY training for 2400MTS check ddr4_pmu_train_imem code check ddr4_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr4_pmu_train_dmem code pass Training PASS DRAM PHY training for 400MTS check ddr4_pmu_train_imem code check ddr4_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr4_pmu_train_dmem code pass Training PASS DRAM PHY training for 100MTS check ddr4_pmu_train_imem code check ddr4_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr4_pmu_train_dmem code pass Training PASS DRAM PHY training for 2400MTS check ddr4_pmu_train_imem code check ddr4_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr4_pmu_train_dmem code pass Training PASS Normal Boot Trying to boot from MMC1 U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 (Nov 17 2020 - 17:53:08 +0800) CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz) CPU: Commercial temperature grade (0C to 95C) at 50C Reset cause: POR Model: FSL i.MX8MM EVK board DRAM: 2 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52] Power supply on USB2 TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50] MMC: FSL_SDHC: 0 Loading Environment from MMC... MMC Device -1 not found *** Warning - No MMC card found, using default environment Failed (-5) No panel detected: default to MIPI2HDMI adv7535_init: Can't find device id=0x3d, on bus 1 Display: MIPI2HDMI (1920x1080) Video: 1920x1080x24 In: serial Out: serial Err: serial BuildInfo: - ATF - U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 switch to partitions #0, OK mmc0(part 0) is current device flash target is MMC:255 MMC Device 255 not found invalid mmc device 255 Net: No ethernet found. Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 MMC Device -1 not found no mmc device at slot ffffffff ** Bad device mmc 4294967295 ** ** Bad device mmc 4294967295 ** Booting from net ... No ethernet found. No ethernet found. WARN: Cannot load the DT u-boot=> u-boot=> u-boot=> mmcinfo Device: FSL_SDHC Manufacturer ID: 15 OEM: 100 Name: 8GTF4 Bus Speed: 52000000 Mode : MMC DDR52 (52MHz) Rd Block Len: 512 MMC version 5.1 High Capacity: Yes Capacity: 7.3 GiB Bus Width: 4-bit DDR Erase Group Size: 512 KiB HC WP Group Size: 8 MiB User Capacity: 7.3 GiB WRREL Boot Capacity: 4 MiB ENH RPMB Capacity: 512 KiB ENH u-boot=> u-boot=> u-boot=> printenv baudrate=115200 boot_fdt=try bootargs=console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 root=/dev/nfs ip=dhcp nfsroot=:,v3,tcp bootcmd=mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else booti ${loadaddr} - ${fdt_addr}; fi bootcmd_mfg=run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi; bootdelay=2 bootscript=echo Running bootscript from mmc ...; source console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 emmc_dev=0 ethprime=FEC fastboot_dev=mmc-1 fdt_addr=0x43000000 fdt_file=fsl-imx8mm-evk.dtb fdt_high=0xffffffffffffffff fdtcontroladdr=be908260 get_cmd=dhcp image=Image initrd_addr=0x43800000 initrd_high=0xffffffffffffffff jh_clk= jh_mmcboot=mw 0x303d0518 0xff; setenv fdt_file fsl-imx8mm-evk-root.dtb;setenv jh_clk clk_ignore_unused; if run loadimage; then run mmcboot; else run jh_netboot; fi; jh_netboot=mw 0x303d0518 0xff; setenv fdt_file fsl-imx8mm-evk-root.dtb; setenv jh_clk clk_ignore_unused; run netboot; kboot=booti loadaddr=0x40480000 loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script}; loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file} loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image} mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc clk_ignore_unused mmcargs=setenv bootargs ${jh_clk} console=${console} root=${mmcroot} mmcautodetect=yes mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then booti ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; else echo wait for boot; fi; mmcdev=4294967295 mmcpart=1 mmcroot=/dev/mmcblk0p2 rootwait rw netargs=setenv bootargs ${jh_clk} console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${loadaddr} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then booti ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; else booti; fi; script=boot.scr sd_dev=1 soc_type=imx8mm Environment size: 2506/4092 bytes u-boot=> run fastboot ## Error: "fastboot" not defined u-boot=> setenv mmcdev 0 u-boot=> saveenv Saving Environment to MMC... MMC Device -1 not found !No MMC card found Failed (1) u-boot=> u-boot=> mmcboot Unknown command 'mmcboot' - try 'help' u-boot=> run mmcboot Booting from mmc ... ** No partition table - mmc 0 ** WARN: Cannot load the DT u-boot=>