snir@snir-linux:~/ltib$ ./ltib -m scbuild -p winexe.spec Processing: winexe ==================== Build path taken because: directory build, build key set, no prebuilt rpm, rpmbuild --dbpath /home/snir/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/snir/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/snir/ltib/tmp' --define '_rpmdir /home/snir/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/snir/ltib/dist/lfs-5.1/winexe/winexe.spec Building target platforms: arm Building for target arm Executing(%build): /bin/sh -e /home/snir/ltib/tmp/rpm-tmp.88918 + umask 022 + cd /home/snir/ltib/rpm/BUILD + cd winexe-1.00 + cd source4 + ./autogen.sh ./autogen.sh: running script/mkversion.sh ./script/mkversion.sh: 'version.h' created for Samba("4.0.0alpha11-GIT-UNKNOWN") ./autogen.sh: running autoheader -I. -I../lib/replace ./autogen.sh: running autoconf -I. -I../lib/replace Now run ./configure (or ./configure.developer) and then make. + CONFIG_SITE=./winexe-1.00-default.site + ./configure --prefix=/usr --host=arm-linux --build=i686-pc-linux-gnu --target=arm-linux --with-sendfile-support --disable-cups --enable-fhs SAMBA VERSION: 4.0.0alpha11-GIT-UNKNOWN LIBREPLACE_LOCATION_CHECKS: START checking build system type... i686-pc-linux-gnu checking host system type... arm-unknown-linux-gnu checking target system type... arm-unknown-linux-gnu LIBREPLACE_LOCATION_CHECKS: END checking for perl... /usr/bin/perl checking for yapp... false LIBREPLACE_CC_CHECKS: START checking for arm-linux-gcc... gcc checking for C compiler default output... a.out checking whether the C compiler works... yes checking whether we are cross compiling... yes checking for suffix of executables... checking for suffix of object files... o checking whether we are using the GNU C compiler... yes checking whether gcc accepts -g... yes checking for gcc option to accept ANSI C... none needed checking for version of gcc... 4.4.4 checking how to run the C preprocessor... gcc -E checking for egrep... grep -E checking for AIX... no checking for ANSI C header files... yes checking for sys/types.h... yes checking for sys/stat.h... yes checking for stdlib.h... yes checking for string.h... yes checking for memory.h... yes checking for strings.h... yes checking for inttypes.h... yes checking for stdint.h... yes checking for unistd.h... yes checking minix/config.h usability... no checking minix/config.h presence... no checking for minix/config.h... no checking whether it is safe to define __EXTENSIONS__... yes checking whether byte ordering is bigendian... no checking for inline... inline checking for C99 designated initializers... yes checking for a BSD-compatible install... /usr/bin/install -c checking for library containing strerror... none required checking for special C compiler options needed for large files... no checking for _FILE_OFFSET_BITS value needed for large files... 64 checking for _LARGE_FILES value needed for large files... no checking standards.h usability... no checking standards.h presence... no checking for standards.h... no checking for long long... yes checking for int... yes checking size of int... 4 checking for char... yes checking size of char... 1 checking for short... yes checking size of short... 2 checking for long... yes checking size of long... 4 checking for long long... (cached) yes checking size of long long... 8 checking for uint_t... no checking for int8_t... yes checking for uint8_t... yes checking for int16_t... yes checking for uint16_t... yes checking for int32_t... yes checking for uint32_t... yes checking for int64_t... yes checking for uint64_t... yes checking for size_t... yes checking for ssize_t... yes checking for off_t... yes checking size of off_t... 8 checking for size_t... (cached) yes checking size of size_t... 4 checking for ssize_t... (cached) yes checking size of ssize_t... 4 checking for intptr_t... yes checking for uintptr_t... yes checking for ptrdiff_t... yes checking for immediate structures... yes LIBREPLACE_CC_CHECKS: END checking whether we are really using the Sun C compiler... no checking for C99 designated initializers... yes checking that the C compiler understands negative enum values... yes checking for test routines... configure: WARNING: cannot run when cross-compiling checking VISIBILITY_CFLAGS for gcc -fvisibility=hidden... -fvisibility=hidden checking whether the C compiler supports the visibility attribute... yes checking for gcov... /usr/bin/gcov checking for ld... /opt/freescale/ltib/usr/spoof/ld checking if the linker (/opt/freescale/ltib/usr/spoof/ld) is GNU ld... yes checking whether to try to build shared libraries on linux-gnu... true checking LD... gcc checking LDFLAGS... checking SYS_LDFLAGS... -Wl,--export-dynamic checking for ar... /opt/freescale/ltib/usr/spoof/ar checking STLD... /opt/freescale/ltib/usr/spoof/ar checking STLD_FLAGS... -rcs checking SHLD... gcc checking SHLD_FLAGS... -shared -Wl,-Bsymbolic checking MDLD... gcc checking MDLD_FLAGS... -shared -Wl,-Bsymbolic -Wl,--allow-shlib-undefined checking SHLIBEXT... so checking SONAMEFLAG... -Wl,-soname= checking PICFLAG... -fPIC checking whether building shared libraries actually works... yes checking whether building shared modules actually works... yes checking if we can link using the selected flags... configure: WARNING: cannot run when cross-compiling checking if binaries will use shared libraries... false checking for gmake... no checking for make... /usr/bin/make checking whether we have GNU make... yes found checking GNU make version... 3.81 checking for GNU make >= 3.81... yes checking CFLAGS for gcc -M -MT conftest.d -MF conftest.o... -M -MT conftest.d -MF conftest.o checking Whether to use automatic dependencies... no checking for xsltproc... /usr/bin/xsltproc checking for python2.6... /usr/bin/python2.6 checking for python2.6-config... /usr/bin/python2.6-config checking working python module support... no configure: error: Python not found. Please install Python 2.x and its development headers/libraries. error: Bad exit status from /home/snir/ltib/tmp/rpm-tmp.88918 (%build) RPM build errors: Bad exit status from /home/snir/ltib/tmp/rpm-tmp.88918 (%build) Build time for winexe: 18 seconds Failed building winexe f_scbuild() returned an error, exiting traceback: main:560 Exiting on error or interrupt