CPU: Freescale i.MX53 family 2.1V at 800 MHz mx53 pll1: 800MHz mx53 pll2: 400MHz mx53 pll3: 432MHz mx53 pll4: 455MHz ipg clock : 66666666Hz ipg per clock : 33333333Hz uart clock : 66666666Hz cspi clock : 108000000Hz ahb clock : 133333333Hz axi_a clock : 400000000Hz axi_b clock : 200000000Hz emi_slow clock: 133333333Hz ddr clock : 400000000Hz esdhc1 clock : 80000000Hz esdhc2 clock : 80000000Hz esdhc3 clock : 80000000Hz esdhc4 clock : 80000000Hz nfc clock : 26666666Hz Board: MX53-LOCO 1.0 Rev. A Boot Reason: [POR] Boot Device: SD I2C: ready DRAM: 1 GB MMC: FSL_ESDHC: 0,FSL_ESDHC: 1 In: serial Out: serial Err: serial da9052_i2c_is_connected - i2c write success.... Serial reinitilized! Net: got MAC address from IIM: 00:04:9f:01:df:e7 FEC0 [PRIME] Hit any key to stop autoboot: 0 MX53-LOCO U-Boot > printenv baudrate=115200 loadaddr=0x70800000 netdev=eth0 ethprime=FEC0 uboot=u-boot.bin kernel=uImage nfsroot=/opt/eldk/arm ethact=FEC0 bootdelay=5 lvds=video=mxcdi0fb:RGB666,XGA ldb vga=video=mxcdi1fb:GBR24,XGA di1_primary tve hdmi=video=mxcdi0fb:RGB24,1024x768@60 bootcmd=run bootcmd_mmc bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp lcd=video=mxcdi0fb:RGB24,SEIKO-WVGA bootargs=console=ttymxc0,115200 video=mxcdi0fb:RGB24,SEIKO-WVGA root=/dev/mmcblk0p1 rw rootwait bootcmd_mmc=run bootargs_base bootargs_mmc; mmc dev 0; mmc read ${loadaddr} 0x800 0x1800; bootm bootargs_mmc=set bootargs ${bootargs} root=/dev/mmcblk0p1 rw rootwait bootargs_base=set bootargs console=ttymxc0,115200 ${lcd} stdin=serial stdout=serial stderr=serial Environment size: 860/8188 bytes MX53-LOCO U-Boot > boot mmc0 is current device MMC read: dev # 0, block # 2048, count 6144 ... 6144 blocks read: OK ## Booting kernel from Legacy Image at 70800000 ... Image Name: Linux-2.6.35.3-1129-g691c08a Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3008108 Bytes = 2.9 MB Load Address: 70008000 Entry Point: 70008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Linux version 2.6.35.3-1129-g691c08a (r80115@bluebell) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1 PREEMPT Sat Sep 24 21:21:12 CDT 2011 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: Freescale MX53 LOCO Board Memory policy: ECC disabled, Data cache writeback Built 1 zonelists in Zone order, mobility grouping on. Total pages: 250880 Kernel command line: console=ttymxc0,115200 video=mxcdi0fb:RGB24,SEIKO-WVGA root=/dev/mmcblk0p1 rw rootwait PID hash table entries: 4096 (order: 2, 16384 bytes) Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 480MB 512MB = 992MB total Memory: 998220k/998220k available, 17588k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xf9e00000 - 0xffe00000 ( 96 MB) vmalloc : 0xe0800000 - 0xf4000000 ( 312 MB) lowmem : 0x80000000 - 0xe0000000 (1536 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .init : 0x80008000 - 0x80033000 ( 172 kB) .text : 0x80033000 - 0x807fa000 (7964 kB) .data : 0x80818000 - 0x80870120 ( 353 kB) SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Hierarchical RCU implementation. RCU-based detection of stalled CPUs is disabled. Verbose stalled-CPUs detection is disabled. NR_IRQS:368 MXC GPIO hardware MXC IRQ initialized MXC_Early serial console at MMIO 0x53fbc000 (options '115200') bootconsole [ttymxc0] enabled Console: colour dummy device 80x30 Calibrating delay loop... 999.42 BogoMIPS (lpj=4997120) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok regulator: core version 0.5 NET: Registered protocol family 16 i.MX IRAM pool: 128 KB@0xe0840000 IRAM READY CPU is i.MX53 Revision 2.1 Using SDMA I.API MXC DMA API initialized IMX usb wakeup probe IMX usb wakeup probe bio: create slab at 0 SCSI subsystem initialized Freescale USB OTG Driver loaded, $Revision: 1.55 $ ****************************** NOTICE ***************************** You have seen this notice as you have enabled OTG driver for mx53 LOCO board For mx53 loco board, the OTG function is unavailable due to hardware limitation So, Only one usb function (device or host) can be available for certain image Please config your kernel to disable OTG and the usb function you don't want to use And remain the other usb function you would like to use Below OTG configs should be removed: CONFIG_MXC_OTG, CONFIG_USB_OTG Choose one of below configs for host or device function But DO NOT choose them together OTG host config CONFIG_USB_EHCI_ARC_OTG OTG device config CONFIG_USB_GADGET usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb da9052_i2c_is_connected - i2c read success.... regulator: DA9052_LDO1: 600 <--> 1800 mV at 1300 mV normal regulator: DA9052_LDO2: 600 <--> 1800 mV at 1300 mV normal regulator: DA9052_LDO3: 1725 <--> 3300 mV at 3300 mV normal regulator: DA9052_LDO4: 1725 <--> 3300 mV at 2775 mV normal regulator: DA9052_LDO5: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_LDO6: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_LDO7: 1200 <--> 3600 mV at 2750 mV normal regulator: DA9052_LDO8: 1200 <--> 3600 mV at 1800 mV normal regulator: DA9052_LDO9: 1250 <--> 3650 mV at 1500 mV normal regulator: DA9052_LDO10: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_BUCK_CORE: 500 <--> 2075 mV at 1250 mV normal regulator: DA9052_BUCK_PRO: 500 <--> 2075 mV at 1300 mV normal regulator: DA9052_BUCK_MEM: 925 <--> 2500 mV at 1500 mV normal regulator: DA9052_BUCK_PERI: 1800 <--> 3600 mV at 3600 mV normal DA9053 chip ID reg read=0xa3 BB version probed IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) Advanced Linux Sound Architecture Driver Version 1.0.23. Bluetooth: Core ver 2.15 NET: Registered protocol family 31 Bluetooth: HCI device and connection manager initialized Bluetooth: HCI socket layer initialized Switching to clocksource mxc_timer1 NET: Registered protocol family 2 IP route cache hash table entries: 32768 (order: 5, 131072 bytes) TCP established hash table entries: 131072 (order: 8, 1048576 bytes) TCP bind hash table entries: 65536 (order: 6, 262144 bytes) TCP: Hash tables configured (established 131072 bind 65536) TCP reno registered UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. LPMode driver module loaded Static Power Management for Freescale i.MX5 PM driver module loaded sdram autogating driver module loaded Bus freq driver module loaded DI1 is primary mxc_dvfs_core_probe DVFS driver module loaded i.MXC CPU frequency driver DVFS PER driver module loaded JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. msgmni has been set to 1949 alg: No test for stdrng (krng) cryptodev: driver loaded. io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) regulator: get() with no identifier By setting, SII driver will not be enabled By setting, LDB driver will not be enabled mxc_ipu mxc_ipu: Channel already disabled 9 mxc_ipu mxc_ipu: Channel already uninitialized 9 IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) Console: switching to colour frame buffer device 128x48 mxc_ipu mxc_ipu: Channel already disabled 7 mxc_ipu mxc_ipu: Channel already uninitialized 7 mxc_ipu mxc_ipu: Channel already disabled 10 mxc_ipu mxc_ipu: Channel already uninitialized 10 Serial: MXC Internal UART driver mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX console [ttymxc0] enabled, bootconsole disabled console [ttymxc0] enabled, bootconsole disabled mxcintuart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a Freescale i.MX mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 33) is a Freescale i.MX mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX mxcintuart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a Freescale i.MX loop: module loaded MXC MTD nand Driver 3.0 i.MX GPMI NFC vcan: Virtual CAN interface driver Freescale FlexCAN Driver FEC Ethernet Driver fec_enet_mii_bus: probed ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1 fsl-ehci fsl-ehci.0: irq 18, io base 0x53f80000 fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2 fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200 fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected usbcore: registered new interface driver cdc_acm cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. ARC USBOTG Device Controller driver (1 August 2005) mice: PS/2 mouse device common for all mice input: gpio-keys as /devices/platform/gpio-keys/input/input0 MXC keypad loaded egalax_ts 2-0004: egalax_ts: failed to read firmware version egalax_ts: probe of 2-0004 failed with error -5 p1003_fwv33 2-0041: couldn't read panel infomation. p1003_fwv33: probe of 2-0041 failed with error -5 DA9052 TSI Device Driver, v1.0 input: da9052-tsi as /devices/virtual/input/input1 TSI Drv Successfully Inserted da9052-tsi input: da9052-onkey as /devices/platform/imx-i2c.0/i2c-0/0-0048/da9052-onkey/input/input2 mxc_rtc mxc_rtc.0: rtc core: registered mxc_rtc as rtc0 i2c /dev entries driver IR NEC protocol handler initialized IR RC5(x) protocol handler initialized IR RC6 protocol handler initialized IR JVC protocol handler initialized IR Sony protocol handler initialized Linux video capture interface: v2.00 mxc_v4l2_output mxc_v4l2_output.0: Registered device video0 usbcore: registered new interface driver uvcvideo USB Video Class driver (v0.1.0) APM Battery Driver check mma8450 chip ID mma8450 0-001c: build time Sep 24 2011 21:16:52 input: mma8450 as /devices/virtual/input/input3 add mma8450 i2c driver MXC WatchDog Driver 2.0 MXC Watchdog # 0 Timer: initial timeout 60 sec Bluetooth: Virtual HCI driver ver 1.3 Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCIATH3K protocol initialized Bluetooth: Generic Bluetooth USB driver ver 0.6 usbcore: registered new interface driver btusb VPU initialized mxc_asrc registered gpu mmu enabled mxsdhci: MXC Secure Digital Host Controller Interface driver mxsdhci: MXC SDHCI Controller Driver. mmc0: SDHCI detect irq 0 irq 1 INTERNAL DMA mxsdhci: MXC SDHCI Controller Driver. mmc1: SDHCI detect irq 203 irq 3 INTERNAL DMA usbcore: registered new interface driver usbhid usbhid: USB HID core driver Cirrus Logic CS42888 ALSA SoC Codec Driver sgtl5000-i2c 1-000a: SGTL5000 revision 17 mxc_spdif mxc_spdif.0: MXC SPDIF Audio Transmitter No device for codec mxc spdif No device for DAI mxc spdif No device for DAI imx-ssi-1-0 No device for DAI imx-ssi-1-1 No device for DAI imx-ssi-2-0 No device for DAI imx-ssi-2-1 No device for DAI imx-spdif-dai usb 1-1: new low speed USB device using fsl-ehci and address 2 DMA Sound Buffer Allocated: Playback UseIram=1 ext_ram=0 buf->addr=f8016000 buf->area=e0856000 size=24576 DMA Sound Buffer Allocated: Capture UseIram=1 ext_ram=1 buf->addr=cf348000 buf->area=fa8ad000 size=24576 asoc: SGTL5000 <-> imx-ssi-2-0 mapping ok mmc0: new high speed SDHC card at address b368 mmcblk0: mmc0:b368 00000 7.51 GiB mmcblk0: p1 DMA Sound Buffer Allocated: Playback UseIram=1 ext_ram=1 buf->addr=cf438000 buf->area=fa8b3000 size=24576 asoc: mxc spdif <-> imx-spdif-dai mapping ok ALSA device list: #0: imx-3stack (SGTL5000) #1: imx-3stack-spdif (mxc spdif) TCP cubic registered NET: Registered protocol family 17 can: controller area network core (rev 20090105 abi 8) NET: Registered protocol family 29 can: raw protocol (rev 20090105) can: broadcast manager protocol (rev 20090105 t) Bluetooth: L2CAP ver 2.14 Bluetooth: L2CAP socket layer initialized Bluetooth: SCO (Voice Link) ver 0.6 Bluetooth: SCO socket layer initialized Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: HIDP (Human Interface Emulation) ver 1.2 VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2 usb 1-1: device v413c p3200 is not supported regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_PERI on regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_MEM on regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_PRO on regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_CORE on regulator_init_complete: incomplete constraints, leaving DA9052_LDO10 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO8 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO6 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO5 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO4 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO3 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO2 on regulator_init_complete: incomplete constraints, leaving DA9052_LDO1 on mxc_rtc mxc_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0) input: Dell Dell USB Mouse as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/input/input4 generic-usb 0003:413C:3200.0001: input: USB HID v1.10 Mouse [Dell Dell USB Mouse] on usb-fsl-ehci.0-1/input0 EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended usb 2-1: new high speed USB device using fsl-ehci and address 2 hub 2-1:1.0: USB hub found hub 2-1:1.0: 4 ports detected VFS: Mounted root (ext2 filesystem) on device 179:1. Freeing init memory: 172K starting pid 1191, tty '': '/etc/rc.d/rcS' Mounting /proc and /sys usb 2-1.2: new low speed USB device using fsl-ehci and address 3 Starting the hotplug events dispatcher udevd Synthesizing initial hotplug events input: DELL Dell QuietKey Keyboard as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.2/2-1.2:1.0/input/input5 generic-usb 0003:413C:2106.0002: input: USB HID v1.10 Keyboard [DELL Dell QuietKey Keyboard] on usb-fsl-ehci.1-1.2/input0 Setting the hostname to freescale Mounting filesystems mount: mounting usbfs on /proc/bus/usb failed: No such file or directory Starting the dropbear ssh server: D-Bus per-session daemon address is: unix:abstract=/tmp/dbus-Zn9qOfV0R8,guid=9f337f250a8db0eea07d604c0000000a gtk: creating gdk-pixbuf.loaders pango: creating module list starting pid 2285, tty '': '/sbin/getty -L ttymxc0 115200 vt100' _XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6 _XSERVTransOpen: transport open failed for inet6/freescale:0 _XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6 (EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base (EE) XKB: No components provided for device Virtual core keyboard unrecognised device identifier! (EE) config/hal: NewInputDeviceRequest failed (2) unrecognised device identifier! (EE) config/hal: NewInputDeviceRequest failed (2) unrecognised device identifier! (EE) config/hal: NewInputDeviceRequest failed (2) arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4 root filesystem built on Thu, 29 Sep 2011 15:54:39 +0800 Freescale Semiconductor, Inc. freescale login: matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut n=next matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut p=prev matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut c=close matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut d=desktop matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut m=!matchbox-remote -mbmenu matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut x=!xterm matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut r=!rxvt matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut e=!!gpe-calender matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut Tab=next matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut Tab=prev matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut space=taskmenu matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut escape=!matchbox-remote -mbmenu matchbox: keyboard does not appear to have a key. matchbox: ignoring key shortcut f4=close matchbox: Cant find a keycode for keysym 65480 matchbox: ignoring key shortcut f11=fullscreen Failed to get root pixmap id matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None ) matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( None ) user_overides is (nil) mb-desktop-dotdesktop: failed to open /usr/local/share/applications mb-desktop-dotdesktop: failed to open //.applications mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name mb-applet-menu-launcher: failed to open /usr/local/share/applications mb-applet-menu-launcher: failed to open //.applications mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name mb-applet-menu-launcher: failed to open /usr/local/share/applications mb-applet-menu-launcher: failed to open //.applications arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4 root filesystem built on Thu, 29 Sep 2011 15:54:39 +0800 Freescale Semiconductor, Inc. freescale login: root login[2285]: root login on 'ttymxc0' BusyBox v1.18.5 () built-in shell (ash) Enter 'help' for a list of built-in commands. root@freescale ~$ cd / root@freescale /$ ls -l drwxr-xr-x 2 root root 4096 Sep 29 2011 bin drwxr-xr-x 9 root root 13100 Jan 1 00:00 dev drwxr-xr-x 9 root root 4096 Jan 1 00:00 etc drwxr-xr-x 3 root root 4096 Sep 29 2011 home drwxr-xr-x 5 root root 4096 Sep 29 2011 lib drwx------ 2 root root 16384 Sep 29 2011 lost+found drwxr-xr-x 7 root root 4096 Sep 29 2011 mnt drwxr-xr-x 2 root root 4096 Sep 29 2011 opt dr-xr-xr-x 60 root root 0 Jan 1 00:00 proc drwxr-xr-x 2 root root 4096 Jan 1 00:02 root drwxr-xr-x 2 root root 4096 Sep 29 2011 sbin drwxr-xr-x 12 root root 0 Jan 1 00:00 sys drwxrwxrwt 4 root root 4096 Jan 1 00:00 tmp drwxr-xr-x 2 root root 4096 Sep 29 2011 unit_tests drwxr-xr-x 12 root root 4096 Sep 29 2011 usr drwxr-xr-x 11 root root 4096 Sep 29 2011 var