root@imx8mpevk:/unit_tests/mindray# ./test_enc_arm_elinux_2023_05_26 -o coastguard_cif_352x288_300f_I420.h264 -f 2 -n 300 -color 0 -i coastguard_cif_352x288_300f_I420.yuv -w 352 -h 288 input YUV file : coastguard_cif_352x288_300f_I420.yuv max frame number : 300 vpu lib version : major.minor.rel=1.1.1 vpu fw version : major.minor.rel_rcode=1.1.1_r0 vpu wrapper version : major.minor.rel=3.0.0: VPUWRAPPER_ARM64_LINUX Build on May 26 2023 09:30:07 using VPU_EncOpenSimp Interface Init OK: min buffer cnt: 0, alignment: 1 EncodeLoop: encode frame : input is not used CallBack_EncOneFrameOK: one frame is OK , length: 36 CallBack_EncOneFrameOK: one frame is OK , length: 27455 CallBack_EncOneFrameOK: one frame is OK , length: 5150 CallBack_EncOneFrameOK: one frame is OK , length: 7922 CallBack_EncOneFrameOK: one frame is OK , length: 7714 CallBack_EncOneFrameOK: one frame is OK , length: 8454 CallBack_EncOneFrameOK: one frame is OK , length: 7244 CallBack_EncOneFrameOK: one frame is OK , length: 8086 CallBack_EncOneFrameOK: one frame is OK , length: 7812 CallBack_EncOneFrameOK: one frame is OK , length: 7367 CallBack_EncOneFrameOK: one frame is OK , length: 7880 CallBack_EncOneFrameOK: one frame is OK , length: 7627 CallBack_EncOneFrameOK: one frame is OK , length: 7647 CallBack_EncOneFrameOK: one frame is OK , length: 8204 CallBack_EncOneFrameOK: one frame is OK , length: 7637 CallBack_EncOneFrameOK: one frame is OK , length: 7652 CallBack_EncOneFrameOK: one frame is OK , length: 27976 CallBack_EncOneFrameOK: one frame is OK , length: 4986 CallBack_EncOneFrameOK: one frame is OK , length: 8067 CallBack_EncOneFrameOK: one frame is OK , length: 7996 CallBack_EncOneFrameOK: one frame is OK , length: 8024 CallBack_EncOneFrameOK: one frame is OK , length: 7661 CallBack_EncOneFrameOK: one frame is OK , length: 7947 CallBack_EncOneFrameOK: one frame is OK , length: 8097 CallBack_EncOneFrameOK: one frame is OK , length: 7607 CallBack_EncOneFrameOK: one frame is OK , length: 8259 CallBack_EncOneFrameOK: one frame is OK , length: 7839 CallBack_EncOneFrameOK: one frame is OK , length: 8030 CallBack_EncOneFrameOK: one frame is OK , length: 8098 CallBack_EncOneFrameOK: one frame is OK , length: 7895 CallBack_EncOneFrameOK: one frame is OK , length: 8359 CallBack_EncOneFrameOK: one frame is OK , length: 28852 CallBack_EncOneFrameOK: one frame is OK , length: 5604 CallBack_EncOneFrameOK: one frame is OK , length: 8158 CallBack_EncOneFrameOK: one frame is OK , length: 7885 CallBack_EncOneFrameOK: one frame is OK , length: 8229 CallBack_EncOneFrameOK: one frame is OK , length: 8421 CallBack_EncOneFrameOK: one frame is OK , length: 8313 CallBack_EncOneFrameOK: one frame is OK , length: 8157 CallBack_EncOneFrameOK: one frame is OK , length: 8597 CallBack_EncOneFrameOK: one frame is OK , length: 8769 CallBack_EncOneFrameOK: one frame is OK , length: 9265 CallBack_EncOneFrameOK: one frame is OK , length: 9105 CallBack_EncOneFrameOK: one frame is OK , length: 8744 CallBack_EncOneFrameOK: one frame is OK , length: 8585 CallBack_EncOneFrameOK: one frame is OK , length: 8711 CallBack_EncOneFrameOK: one frame is OK , length: 28243 CallBack_EncOneFrameOK: one frame is OK , length: 6722 CallBack_EncOneFrameOK: one frame is OK , length: 9994 CallBack_EncOneFrameOK: one frame is OK , length: 7949 CallBack_EncOneFrameOK: one frame is OK , length: 8311 CallBack_EncOneFrameOK: one frame is OK , length: 8282 CallBack_EncOneFrameOK: one frame is OK , length: 8516 CallBack_EncOneFrameOK: one frame is OK , length: 9453 CallBack_EncOneFrameOK: one frame is OK , length: 9837 CallBack_EncOneFrameOK: one frame is OK , length: 9112 CallBack_EncOneFrameOK: one frame is OK , length: 8385 CallBack_EncOneFrameOK: one frame is OK , length: 9781 CallBack_EncOneFrameOK: one frame is OK , length: 9851 CallBack_EncOneFrameOK: one frame is OK , length: 10296 CallBack_EncOneFrameOK: one frame is OK , length: 10263 CallBack_EncOneFrameOK: one frame is OK , length: 29158 CallBack_EncOneFrameOK: one frame is OK , length: 7965 CallBack_EncOneFrameOK: one frame is OK , length: 11725 CallBack_EncOneFrameOK: one frame is OK , length: 11293 CallBack_EncOneFrameOK: one frame is OK , length: 11391 CallBack_EncOneFrameOK: one frame is OK , length: 10565 CallBack_EncOneFrameOK: one frame is OK , length: 8340 CallBack_EncOneFrameOK: one frame is OK , length: 8620 CallBack_EncOneFrameOK: one frame is OK , length: 9153 CallBack_EncOneFrameOK: one frame is OK , length: 8565 CallBack_EncOneFrameOK: one frame is OK , length: 6484 CallBack_EncOneFrameOK: one frame is OK , length: 4832 CallBack_EncOneFrameOK: one frame is OK , length: 5624 CallBack_EncOneFrameOK: one frame is OK , length: 11178 CallBack_EncOneFrameOK: one frame is OK , length: 11942 CallBack_EncOneFrameOK: one frame is OK , length: 29220 CallBack_EncOneFrameOK: one frame is OK , length: 5997 CallBack_EncOneFrameOK: one frame is OK , length: 7619 CallBack_EncOneFrameOK: one frame is OK , length: 9743 CallBack_EncOneFrameOK: one frame is OK , length: 8803 CallBack_EncOneFrameOK: one frame is OK , length: 6931 CallBack_EncOneFrameOK: one frame is OK , length: 9682 CallBack_EncOneFrameOK: one frame is OK , length: 6297 CallBack_EncOneFrameOK: one frame is OK , length: 7812 CallBack_EncOneFrameOK: one frame is OK , length: 7948 CallBack_EncOneFrameOK: one frame is OK , length: 6962 CallBack_EncOneFrameOK: one frame is OK , length: 8273 CallBack_EncOneFrameOK: one frame is OK , length: 8813 CallBack_EncOneFrameOK: one frame is OK , length: 8053 CallBack_EncOneFrameOK: one frame is OK , length: 8227 CallBack_EncOneFrameOK: one frame is OK , length: 29618 CallBack_EncOneFrameOK: one frame is OK , length: 8009 CallBack_EncOneFrameOK: one frame is OK , length: 7855 CallBack_EncOneFrameOK: one frame is OK , length: 8405 CallBack_EncOneFrameOK: one frame is OK , length: 7503 CallBack_EncOneFrameOK: one frame is OK , length: 8063 CallBack_EncOneFrameOK: one frame is OK , length: 8813 CallBack_EncOneFrameOK: one frame is OK , length: 7486 CallBack_EncOneFrameOK: one frame is OK , length: 7782 CallBack_EncOneFrameOK: one frame is OK , length: 7322 CallBack_EncOneFrameOK: one frame is OK , length: 6770 CallBack_EncOneFrameOK: one frame is OK , length: 7498 CallBack_EncOneFrameOK: one frame is OK , length: 8466 CallBack_EncOneFrameOK: one frame is OK , length: 7231 CallBack_EncOneFrameOK: one frame is OK , length: 6477 CallBack_EncOneFrameOK: one frame is OK , length: 28029 CallBack_EncOneFrameOK: one frame is OK , length: 5593 CallBack_EncOneFrameOK: one frame is OK , length: 8025 CallBack_EncOneFrameOK: one frame is OK , length: 7531 CallBack_EncOneFrameOK: one frame is OK , length: 6091 CallBack_EncOneFrameOK: one frame is OK , length: 6417 CallBack_EncOneFrameOK: one frame is OK , length: 6869 CallBack_EncOneFrameOK: one frame is OK , length: 7513 CallBack_EncOneFrameOK: one frame is OK , length: 7464 CallBack_EncOneFrameOK: one frame is OK , length: 7232 CallBack_EncOneFrameOK: one frame is OK , length: 6784 CallBack_EncOneFrameOK: one frame is OK , length: 7493 CallBack_EncOneFrameOK: one frame is OK , length: 8129 CallBack_EncOneFrameOK: one frame is OK , length: 8423 CallBack_EncOneFrameOK: one frame is OK , length: 8164 CallBack_EncOneFrameOK: one frame is OK , length: 27939 CallBack_EncOneFrameOK: one frame is OK , length: 5551 CallBack_EncOneFrameOK: one frame is OK , length: 6278 CallBack_EncOneFrameOK: one frame is OK , length: 7086 CallBack_EncOneFrameOK: one frame is OK , length: 7720 CallBack_EncOneFrameOK: one frame is OK , length: 6676 CallBack_EncOneFrameOK: one frame is OK , length: 6121 CallBack_EncOneFrameOK: one frame is OK , length: 6567 CallBack_EncOneFrameOK: one frame is OK , length: 6769 CallBack_EncOneFrameOK: one frame is OK , length: 6459 CallBack_EncOneFrameOK: one frame is OK , length: 7037 CallBack_EncOneFrameOK: one frame is OK , length: 6082 CallBack_EncOneFrameOK: one frame is OK , length: 6334 CallBack_EncOneFrameOK: one frame is OK , length: 7253 CallBack_EncOneFrameOK: one frame is OK , length: 7781 CallBack_EncOneFrameOK: one frame is OK , length: 27258 CallBack_EncOneFrameOK: one frame is OK , length: 6310 CallBack_EncOneFrameOK: one frame is OK , length: 7674 CallBack_EncOneFrameOK: one frame is OK , length: 6663 CallBack_EncOneFrameOK: one frame is OK , length: 6956 CallBack_EncOneFrameOK: one frame is OK , length: 6981 CallBack_EncOneFrameOK: one frame is OK , length: 6605 CallBack_EncOneFrameOK: one frame is OK , length: 5951 CallBack_EncOneFrameOK: one frame is OK , length: 5879 CallBack_EncOneFrameOK: one frame is OK , length: 6181 CallBack_EncOneFrameOK: one frame is OK , length: 6595 CallBack_EncOneFrameOK: one frame is OK , length: 6126 CallBack_EncOneFrameOK: one frame is OK , length: 6215 CallBack_EncOneFrameOK: one frame is OK , length: 6400 CallBack_EncOneFrameOK: one frame is OK , length: 6405 CallBack_EncOneFrameOK: one frame is OK , length: 26945 CallBack_EncOneFrameOK: one frame is OK , length: 4376 CallBack_EncOneFrameOK: one frame is OK , length: 5460 CallBack_EncOneFrameOK: one frame is OK , length: 5851 CallBack_EncOneFrameOK: one frame is OK , length: 5750 CallBack_EncOneFrameOK: one frame is OK , length: 6740 CallBack_EncOneFrameOK: one frame is OK , length: 6586 CallBack_EncOneFrameOK: one frame is OK , length: 6078 CallBack_EncOneFrameOK: one frame is OK , length: 5924 CallBack_EncOneFrameOK: one frame is OK , length: 5705 CallBack_EncOneFrameOK: one frame is OK , length: 6956 CallBack_EncOneFrameOK: one frame is OK , length: 6482 CallBack_EncOneFrameOK: one frame is OK , length: 5975 CallBack_EncOneFrameOK: one frame is OK , length: 5800 CallBack_EncOneFrameOK: one frame is OK , length: 6025 CallBack_EncOneFrameOK: one frame is OK , length: 27121 CallBack_EncOneFrameOK: one frame is OK , length: 5052 CallBack_EncOneFrameOK: one frame is OK , length: 7153 CallBack_EncOneFrameOK: one frame is OK , length: 6971 CallBack_EncOneFrameOK: one frame is OK , length: 6896 CallBack_EncOneFrameOK: one frame is OK , length: 6812 CallBack_EncOneFrameOK: one frame is OK , length: 7109 CallBack_EncOneFrameOK: one frame is OK , length: 7238 CallBack_EncOneFrameOK: one frame is OK , length: 7538 CallBack_EncOneFrameOK: one frame is OK , length: 6632 CallBack_EncOneFrameOK: one frame is OK , length: 7015 CallBack_EncOneFrameOK: one frame is OK , length: 6760 CallBack_EncOneFrameOK: one frame is OK , length: 6822 CallBack_EncOneFrameOK: one frame is OK , length: 6711 CallBack_EncOneFrameOK: one frame is OK , length: 5888 CallBack_EncOneFrameOK: one frame is OK , length: 26621 CallBack_EncOneFrameOK: one frame is OK , length: 4685 CallBack_EncOneFrameOK: one frame is OK , length: 6172 CallBack_EncOneFrameOK: one frame is OK , length: 5994 CallBack_EncOneFrameOK: one frame is OK , length: 6428 CallBack_EncOneFrameOK: one frame is OK , length: 6590 CallBack_EncOneFrameOK: one frame is OK , length: 6105 CallBack_EncOneFrameOK: one frame is OK , length: 6153 CallBack_EncOneFrameOK: one frame is OK , length: 7054 CallBack_EncOneFrameOK: one frame is OK , length: 6510 CallBack_EncOneFrameOK: one frame is OK , length: 5838 CallBack_EncOneFrameOK: one frame is OK , length: 6183 CallBack_EncOneFrameOK: one frame is OK , length: 6847 CallBack_EncOneFrameOK: one frame is OK , length: 5689 CallBack_EncOneFrameOK: one frame is OK , length: 6102 CallBack_EncOneFrameOK: one frame is OK , length: 26698 CallBack_EncOneFrameOK: one frame is OK , length: 3988 CallBack_EncOneFrameOK: one frame is OK , length: 5931 CallBack_EncOneFrameOK: one frame is OK , length: 6386 CallBack_EncOneFrameOK: one frame is OK , length: 6266 CallBack_EncOneFrameOK: one frame is OK , length: 6435 CallBack_EncOneFrameOK: one frame is OK , length: 6242 CallBack_EncOneFrameOK: one frame is OK , length: 5900 CallBack_EncOneFrameOK: one frame is OK , length: 5961 CallBack_EncOneFrameOK: one frame is OK , length: 5889 CallBack_EncOneFrameOK: one frame is OK , length: 6063 CallBack_EncOneFrameOK: one frame is OK , length: 5973 CallBack_EncOneFrameOK: one frame is OK , length: 5585 CallBack_EncOneFrameOK: one frame is OK , length: 6073 CallBack_EncOneFrameOK: one frame is OK , length: 5627 CallBack_EncOneFrameOK: one frame is OK , length: 27241 CallBack_EncOneFrameOK: one frame is OK , length: 4949 CallBack_EncOneFrameOK: one frame is OK , length: 5927 CallBack_EncOneFrameOK: one frame is OK , length: 6064 CallBack_EncOneFrameOK: one frame is OK , length: 6351 CallBack_EncOneFrameOK: one frame is OK , length: 6613 CallBack_EncOneFrameOK: one frame is OK , length: 6925 CallBack_EncOneFrameOK: one frame is OK , length: 6719 CallBack_EncOneFrameOK: one frame is OK , length: 5788 CallBack_EncOneFrameOK: one frame is OK , length: 6091 CallBack_EncOneFrameOK: one frame is OK , length: 6315 CallBack_EncOneFrameOK: one frame is OK , length: 6315 CallBack_EncOneFrameOK: one frame is OK , length: 5789 CallBack_EncOneFrameOK: one frame is OK , length: 5942 CallBack_EncOneFrameOK: one frame is OK , length: 6072 CallBack_EncOneFrameOK: one frame is OK , length: 27034 CallBack_EncOneFrameOK: one frame is OK , length: 4019 CallBack_EncOneFrameOK: one frame is OK , length: 5524 CallBack_EncOneFrameOK: one frame is OK , length: 5465 CallBack_EncOneFrameOK: one frame is OK , length: 6489 CallBack_EncOneFrameOK: one frame is OK , length: 6158 CallBack_EncOneFrameOK: one frame is OK , length: 5870 CallBack_EncOneFrameOK: one frame is OK , length: 5816 CallBack_EncOneFrameOK: one frame is OK , length: 6466 CallBack_EncOneFrameOK: one frame is OK , length: 6352 CallBack_EncOneFrameOK: one frame is OK , length: 6098 CallBack_EncOneFrameOK: one frame is OK , length: 5883 CallBack_EncOneFrameOK: one frame is OK , length: 5924 CallBack_EncOneFrameOK: one frame is OK , length: 6737 CallBack_EncOneFrameOK: one frame is OK , length: 6250 CallBack_EncOneFrameOK: one frame is OK , length: 27063 CallBack_EncOneFrameOK: one frame is OK , length: 3862 CallBack_EncOneFrameOK: one frame is OK , length: 5727 CallBack_EncOneFrameOK: one frame is OK , length: 5604 CallBack_EncOneFrameOK: one frame is OK , length: 5855 CallBack_EncOneFrameOK: one frame is OK , length: 6074 CallBack_EncOneFrameOK: one frame is OK , length: 5771 CallBack_EncOneFrameOK: one frame is OK , length: 6134 CallBack_EncOneFrameOK: one frame is OK , length: 5648 CallBack_EncOneFrameOK: one frame is OK , length: 5829 CallBack_EncOneFrameOK: one frame is OK , length: 5725 CallBack_EncOneFrameOK: one frame is OK , length: 6060 CallBack_EncOneFrameOK: one frame is OK , length: 6023 CallBack_EncOneFrameOK: one frame is OK , length: 5992 CallBack_EncOneFrameOK: one frame is OK , length: 5956 CallBack_EncOneFrameOK: one frame is OK , length: 26764 CallBack_EncOneFrameOK: one frame is OK , length: 4045 CallBack_EncOneFrameOK: one frame is OK , length: 5483 CallBack_EncOneFrameOK: one frame is OK , length: 5724 CallBack_EncOneFrameOK: one frame is OK , length: 5479 CallBack_EncOneFrameOK: one frame is OK , length: 5630 CallBack_EncOneFrameOK: one frame is OK , length: 5953 CallBack_EncOneFrameOK: one frame is OK , length: 5682 CallBack_EncOneFrameOK: one frame is OK , length: 5807 CallBack_EncOneFrameOK: one frame is OK , length: 6137 CallBack_EncOneFrameOK: one frame is OK , length: 6598 CallBack_EncOneFrameOK: one frame is OK , length: 5724 CallBack_EncOneFrameOK: one frame is OK , length: 6160 CallBack_EncOneFrameOK: one frame is OK , length: 6334 CallBack_EncOneFrameOK: one frame is OK , length: 5634 CallBack_EncOneFrameOK: one frame is OK , length: 26560 CallBack_EncOneFrameOK: one frame is OK , length: 4092 CallBack_EncOneFrameOK: one frame is OK , length: 5675 CallBack_EncOneFrameOK: one frame is OK , length: 5959 CallBack_EncOneFrameOK: one frame is OK , length: 6060 CallBack_EncOneFrameOK: one frame is OK , length: 5930 CallBack_EncOneFrameOK: one frame is OK , length: 5769 CallBack_EncOneFrameOK: one frame is OK , length: 5828 CallBack_EncOneFrameOK: one frame is OK , length: 5531 CallBack_EncOneFrameOK: one frame is OK , length: 5650 CallBack_EncOneFrameOK: one frame is OK , length: 5538 CallBack_EncOneFrameOK: one frame is OK , length: 5435 CallBack_EncOneFrameOK: one frame is OK , length: 5478 CallBack_EncOneFrameOK: one frame is OK , length: 6429 CallBack_EncOneFrameOK: one frame is OK , length: 5783 CallBack_EncOneFrameOK: one frame is OK , length: 26058 CallBack_EncOneFrameOK: one frame is OK , length: 3857 CallBack_EncOneFrameOK: one frame is OK , length: 5790 CallBack_EncOneFrameOK: one frame is OK , length: 6264 CallBack_EncOneFrameOK: one frame is OK , length: 5708 CallBack_EncOneFrameOK: one frame is OK , length: 5629 CallBack_EncOneFrameOK: one frame is OK , length: 6076 CallBack_EncOneFrameOK: one frame is OK , length: 5587 CallBack_EncOneFrameOK: one frame is OK , length: 6163 CallBack_EncOneFrameOK: one frame is OK , length: 5587 CallBack_EncOneFrameOK: one frame is OK , length: 6301 CallBack_EncOneFrameOK: one frame is OK , length: 5980 CallBack_EncOneFrameOK: one frame is OK , length: 5553 CallBack_EncOneFrameOK: one frame is OK , length: 5939 CallBack_EncOneFrameOK: one frame is OK , length: 5419 Frame Num: 300, [width x height] = [352 x 288], enc FPS: 1719, total FPS: 235 Encode OK root@imx8mpevk:/unit_tests/mindray# ls coastguard_cif_352x288_300f_I420.h264 coastguard_cif_352x288_300f_I420.yuv ewl.trc test_enc_arm_elinux_2023_05_26 root@imx8mpevk:/unit_tests/mindray# gplay-1.0 coastguard_cif_352x288_300f_I420.h264 FSL_GPLAY2_01.00_LINUX build on Apr 2 2021 06:44:41 ====== VPUDEC: 4.5.7 build on Apr 2 2021 06:44:36. ====== wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Apr 2 2021 06:35:44) vpulib: 1.1.1 firmware: 1.1.1.0 [Stop (No Repeated)][Vol=1.0][00:00:00/00:00:00]=========== fsl_player_play() ================== FSL_GPLAY2_01.00_LINUX build on Apr 2 2021 06:44:41 [h]display the operation Help [p]Play [s]Stop [e]Seek [a]Pause when playing, play when paused [v]Volume [m]Switch to mute or not [>]Play next file [<]Play previous file [r]Switch to repeated mode or not [u]Select the video track [d]Select the audio track [b]Select the subtitle track [f]Set full screen [z]resize the width and height [t]Rotate [c]Setting play rate [i]Display the metadata [x]eXit State changed: buffering State changed: playing [Playing (No Repeated)][Vol=1.0][00:00:01/00:00:08]^C Aborted by signal[2] Interrupt... FSL_PLAYER_UI_MSG_EXIT Exit display thread Total showed frames (69), playing for (0:00:02.202993000), fps (31.321). fsl_player_deinit root@imx8mpevk:/unit_tests/mindray#