Device "S32K116 (ALLOW SECURITY)" selected. Connecting to target via SWD InitTarget() start InitTarget() Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. For debugger connection the device needs to be unsecured. Note: Unsecuring will trigger a mass erase of the internal flash. Executing default behavior previously saved in the registry. Device will be unsecured now. Timeout while halting CPU. InitTarget() end Found SW-DP with ID 0x0BC11477 DPIDR: 0x0BC11477 Scanning AP map to find all available APs AP[2]: Stopped AP scan as end of AP map has been reached AP[0]: AHB-AP (IDR: 0x04770031) AP[1]: JTAG-AP (IDR: 0x001C0020) Iterating through AP map to find AHB-AP to use AP[0]: Skipped. Could not read CPUID register AP[1]: Skipped. Not an AHB-AP InitTarget() start InitTarget() Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. For debugger connection the device needs to be unsecured. Note: Unsecuring will trigger a mass erase of the internal flash. Executing default behavior previously saved in the registry. Device will be unsecured now. Timeout while halting CPU. InitTarget() end Found SW-DP with ID 0x0BC11477 DPIDR: 0x0BC11477 Scanning AP map to find all available APs AP[2]: Stopped AP scan as end of AP map has been reached AP[0]: AHB-AP (IDR: 0x04770031) AP[1]: JTAG-AP (IDR: 0x001C0020) Iterating through AP map to find AHB-AP to use AP[0]: Skipped. Could not read CPUID register AP[1]: Skipped. Not an AHB-AP ****** Error: Could not find core in Coresight setup InitTarget() start InitTarget() Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. For debugger connection the device needs to be unsecured. Note: Unsecuring will trigger a mass erase of the internal flash. Executing default behavior previously saved in the registry. Device will be unsecured now. Timeout while halting CPU. InitTarget() end Found SW-DP with ID 0x0BC11477 DPIDR: 0x0BC11477 Scanning AP map to find all available APs AP[2]: Stopped AP scan as end of AP map has been reached AP[0]: AHB-AP (IDR: 0x04770031) AP[1]: JTAG-AP (IDR: 0x001C0020) Iterating through AP map to find AHB-AP to use AP[0]: Skipped. Could not read CPUID register AP[1]: Skipped. Not an AHB-AP InitTarget() start InitTarget() Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. For debugger connection the device needs to be unsecured. Note: Unsecuring will trigger a mass erase of the internal flash. Executing default behavior previously saved in the registry. Device will be unsecured now. Timeout while halting CPU. InitTarget() end Found SW-DP with ID 0x0BC11477 DPIDR: 0x0BC11477 Scanning AP map to find all available APs AP[2]: Stopped AP scan as end of AP map has been reached AP[0]: AHB-AP (IDR: 0x04770031) AP[1]: JTAG-AP (IDR: 0x001C0020) Iterating through AP map to find AHB-AP to use AP[0]: Skipped. Could not read CPUID register AP[1]: Skipped. Not an AHB-AP ****** Error: Could not find core in Coresight setup Cannot connect to target.