/* * FreeRTOS Kernel V10.4.6 * Copyright (C) 2021 Amazon.com, Inc. or its affiliates. All Rights Reserved. * * SPDX-License-Identifier: MIT * * Permission is hereby granted, free of charge, to any person obtaining a copy of * this software and associated documentation files (the "Software"), to deal in * the Software without restriction, including without limitation the rights to * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of * the Software, and to permit persons to whom the Software is furnished to do so, * subject to the following conditions: * * The above copyright notice and this permission notice shall be included in all * copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. * * https://www.FreeRTOS.org * https://github.com/FreeRTOS * */ /*----------------------------------------------------------- * Implementation of functions defined in portable.h for the ARM CM7 port. *----------------------------------------------------------*/ /* Scheduler includes. */ #include "FreeRTOS.h" #include "task.h" #ifndef __VFP_FP__ #error This port can only be used when the project options are configured to enable hardware floating point support. #endif #ifndef configSYSTICK_CLOCK_HZ #define configSYSTICK_CLOCK_HZ configCPU_CLOCK_HZ /* Ensure the SysTick is clocked at the same frequency as the core. */ #define portNVIC_SYSTICK_CLK_BIT ( 1UL << 2UL ) #else /* The way the SysTick is clocked is not modified in case it is not the same * as the core. */ #define portNVIC_SYSTICK_CLK_BIT ( 0 ) #endif /* Constants required to manipulate the core. Registers first... */ #define portNVIC_SYSTICK_CTRL_REG ( *( ( volatile uint32_t * ) 0xe000e010 ) ) #define portNVIC_SYSTICK_LOAD_REG ( *( ( volatile uint32_t * ) 0xe000e014 ) ) #define portNVIC_SYSTICK_CURRENT_VALUE_REG ( *( ( volatile uint32_t * ) 0xe000e018 ) ) #define portNVIC_SHPR3_REG ( *( ( volatile uint32_t * ) 0xe000ed20 ) ) /* ...then bits in the registers. */ #define portNVIC_SYSTICK_INT_BIT ( 1UL << 1UL ) #define portNVIC_SYSTICK_ENABLE_BIT ( 1UL << 0UL ) #define portNVIC_SYSTICK_COUNT_FLAG_BIT ( 1UL << 16UL ) #define portNVIC_PENDSVCLEAR_BIT ( 1UL << 27UL ) #define portNVIC_PEND_SYSTICK_CLEAR_BIT ( 1UL << 25UL ) #define portNVIC_PENDSV_PRI ( ( ( uint32_t ) configKERNEL_INTERRUPT_PRIORITY ) << 16UL ) #define portNVIC_SYSTICK_PRI ( ( ( uint32_t ) configKERNEL_INTERRUPT_PRIORITY ) << 24UL ) /* Constants required to check the validity of an interrupt priority. */ #define portFIRST_USER_INTERRUPT_NUMBER ( 16 ) #define portNVIC_IP_REGISTERS_OFFSET_16 ( 0xE000E3F0 ) #define portAIRCR_REG ( *( ( volatile uint32_t * ) 0xE000ED0C ) ) #define portMAX_8_BIT_VALUE ( ( uint8_t ) 0xff ) #define portTOP_BIT_OF_BYTE ( ( uint8_t ) 0x80 ) #define portMAX_PRIGROUP_BITS ( ( uint8_t ) 7 ) #define portPRIORITY_GROUP_MASK ( 0x07UL << 8UL ) #define portPRIGROUP_SHIFT ( 8UL ) /* Masks off all bits but the VECTACTIVE bits in the ICSR register. */ #define portVECTACTIVE_MASK ( 0xFFUL ) /* Constants required to manipulate the VFP. */ #define portFPCCR ( ( volatile uint32_t * ) 0xe000ef34 ) /* Floating point context control register. */ #define portASPEN_AND_LSPEN_BITS ( 0x3UL << 30UL ) /* Constants required to set up the initial stack. */ #define portINITIAL_XPSR ( 0x01000000 ) #define portINITIAL_EXC_RETURN ( 0xfffffffd ) /* The systick is a 24-bit counter. */ #define portMAX_24_BIT_NUMBER ( 0xffffffUL ) /* For strict compliance with the Cortex-M spec the task start address should * have bit-0 clear, as it is loaded into the PC on exit from an ISR. */ #define portSTART_ADDRESS_MASK ( ( StackType_t ) 0xfffffffeUL ) /* A fiddle factor to estimate the number of SysTick counts that would have * occurred while the SysTick counter is stopped during tickless idle * calculations. */ #define portMISSED_COUNTS_FACTOR ( 45UL ) /* Let the user override the pre-loading of the initial LR with the address of * prvTaskExitError() in case it messes up unwinding of the stack in the * debugger. */ #ifdef configTASK_RETURN_ADDRESS #define portTASK_RETURN_ADDRESS configTASK_RETURN_ADDRESS #else #define portTASK_RETURN_ADDRESS prvTaskExitError #endif /* * Setup the timer to generate the tick interrupts. The implementation in this * file is weak to allow application writers to change the timer used to * generate the tick interrupt. */ void vPortSetupTimerInterrupt( void ); /* * Exception handlers. */ void xPortPendSVHandler( void ) __attribute__( ( naked ) ); void xPortSysTickHandler( void ); void vPortSVCHandler( void ) __attribute__( ( naked ) ); /* * Start first task is a separate function so it can be tested in isolation. */ static void prvPortStartFirstTask( void ) __attribute__( ( naked ) ); /* * Function to enable the VFP. */ static void vPortEnableVFP( void ) __attribute__( ( naked ) ); /* * Used to catch tasks that attempt to return from their implementing function. */ static void prvTaskExitError( void ); /*-----------------------------------------------------------*/ /* Each task maintains its own interrupt status in the critical nesting * variable. */ static UBaseType_t uxCriticalNesting = 0xaaaaaaaa; /* * The number of SysTick increments that make up one tick period. */ #if ( configUSE_TICKLESS_IDLE == 1 ) static uint32_t ulTimerCountsForOneTick = 0; #endif /* configUSE_TICKLESS_IDLE */ /* * The maximum number of tick periods that can be suppressed is limited by the * 24 bit resolution of the SysTick timer. */ #if ( configUSE_TICKLESS_IDLE == 1 ) static uint32_t xMaximumPossibleSuppressedTicks = 0; #endif /* configUSE_TICKLESS_IDLE */ /* * Compensate for the CPU cycles that pass while the SysTick is stopped (low * power functionality only. */ #if ( configUSE_TICKLESS_IDLE == 1 ) static uint32_t ulStoppedTimerCompensation = 0; #endif /* configUSE_TICKLESS_IDLE */ /* * Used by the portASSERT_IF_INTERRUPT_PRIORITY_INVALID() macro to ensure * FreeRTOS API functions are not called from interrupts that have been assigned * a priority above configMAX_SYSCALL_INTERRUPT_PRIORITY. */ #if ( configASSERT_DEFINED == 1 ) static uint8_t ucMaxSysCallPriority = 0; static uint32_t ulMaxPRIGROUPValue = 0; static const volatile uint8_t * const pcInterruptPriorityRegisters = ( const volatile uint8_t * const ) portNVIC_IP_REGISTERS_OFFSET_16; #endif /* configASSERT_DEFINED */ /*-----------------------------------------------------------*/ /* * See header file for description. */ StackType_t * pxPortInitialiseStack( StackType_t * pxTopOfStack, TaskFunction_t pxCode, void * pvParameters ) { /* Simulate the stack frame as it would be created by a context switch * interrupt. */ /* Offset added to account for the way the MCU uses the stack on entry/exit * of interrupts, and to ensure alignment. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_XPSR; /* xPSR */ pxTopOfStack--; *pxTopOfStack = ( ( StackType_t ) pxCode ) & portSTART_ADDRESS_MASK; /* PC */ pxTopOfStack--; *pxTopOfStack = ( StackType_t ) portTASK_RETURN_ADDRESS; /* LR */ /* Save code space by skipping register initialisation. */ pxTopOfStack -= 5; /* R12, R3, R2 and R1. */ *pxTopOfStack = ( StackType_t ) pvParameters; /* R0 */ /* A save method is being used that requires each task to maintain its * own exec return value. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_EXC_RETURN; pxTopOfStack -= 8; /* R11, R10, R9, R8, R7, R6, R5 and R4. */ return pxTopOfStack; } /*-----------------------------------------------------------*/ static void prvTaskExitError( void ) { volatile uint32_t ulDummy = 0; /* A function that implements a task must not exit or attempt to return to * its caller as there is nothing to return to. If a task wants to exit it * should instead call vTaskDelete( NULL ). * * Artificially force an assert() to be triggered if configASSERT() is * defined, then stop here so application writers can catch the error. */ configASSERT( uxCriticalNesting == ~0UL ); portDISABLE_INTERRUPTS(); while( ulDummy == 0 ) { /* This file calls prvTaskExitError() after the scheduler has been * started to remove a compiler warning about the function being defined * but never called. ulDummy is used purely to quieten other warnings * about code appearing after this function is called - making ulDummy * volatile makes the compiler think the function could return and * therefore not output an 'unreachable code' warning for code that appears * after it. */ } } /*-----------------------------------------------------------*/ void vPortSVCHandler( void ) { __asm volatile ( " ldr r3, pxCurrentTCBConst2 \n"/* Restore the context. */ " ldr r1, [r3] \n"/* Use pxCurrentTCBConst to get the pxCurrentTCB address. */ " ldr r0, [r1] \n"/* The first item in pxCurrentTCB is the task top of stack. */ " ldmia r0!, {r4-r11, r14} \n"/* Pop the registers that are not automatically saved on exception entry and the critical nesting count. */ " msr psp, r0 \n"/* Restore the task stack pointer. */ " isb \n" " mov r0, #0 \n" " msr basepri, r0 \n" " bx r14 \n" " \n" " .align 4 \n" "pxCurrentTCBConst2: .word pxCurrentTCB \n" ); } /*-----------------------------------------------------------*/ static void prvPortStartFirstTask( void ) { /* Start the first task. This also clears the bit that indicates the FPU is * in use in case the FPU was used before the scheduler was started - which * would otherwise result in the unnecessary leaving of space in the SVC stack * for lazy saving of FPU registers. */ __asm volatile ( " ldr r0, =0xE000ED08 \n"/* Use the NVIC offset register to locate the stack. */ " ldr r0, [r0] \n" " ldr r0, [r0] \n" " msr msp, r0 \n"/* Set the msp back to the start of the stack. */ " mov r0, #0 \n"/* Clear the bit that indicates the FPU is in use, see comment above. */ " msr control, r0 \n" " cpsie i \n"/* Globally enable interrupts. */ " cpsie f \n" " dsb \n" " isb \n" " svc 0 \n"/* System call to start first task. */ " nop \n" " .ltorg \n" ); } /*-----------------------------------------------------------*/ /* * See header file for description. */ BaseType_t xPortStartScheduler( void ) { /* configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to 0. * See https://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html */ configASSERT( configMAX_SYSCALL_INTERRUPT_PRIORITY ); #if ( configASSERT_DEFINED == 1 ) { volatile uint32_t ulOriginalPriority; volatile uint8_t * const pucFirstUserPriorityRegister = ( volatile uint8_t * const ) ( portNVIC_IP_REGISTERS_OFFSET_16 + portFIRST_USER_INTERRUPT_NUMBER ); volatile uint8_t ucMaxPriorityValue; /* Determine the maximum priority from which ISR safe FreeRTOS API * functions can be called. ISR safe functions are those that end in * "FromISR". FreeRTOS maintains separate thread and ISR API functions to * ensure interrupt entry is as fast and simple as possible. * * Save the interrupt priority value that is about to be clobbered. */ ulOriginalPriority = *pucFirstUserPriorityRegister; /* Determine the number of priority bits available. First write to all * possible bits. */ *pucFirstUserPriorityRegister = portMAX_8_BIT_VALUE; /* Read the value back to see how many bits stuck. */ ucMaxPriorityValue = *pucFirstUserPriorityRegister; /* Use the same mask on the maximum system call priority. */ ucMaxSysCallPriority = configMAX_SYSCALL_INTERRUPT_PRIORITY & ucMaxPriorityValue; /* Calculate the maximum acceptable priority group value for the number * of bits read back. */ ulMaxPRIGROUPValue = portMAX_PRIGROUP_BITS; while( ( ucMaxPriorityValue & portTOP_BIT_OF_BYTE ) == portTOP_BIT_OF_BYTE ) { ulMaxPRIGROUPValue--; ucMaxPriorityValue <<= ( uint8_t ) 0x01; } #ifdef __NVIC_PRIO_BITS { /* Check the CMSIS configuration that defines the number of * priority bits matches the number of priority bits actually queried * from the hardware. */ configASSERT( ( portMAX_PRIGROUP_BITS - ulMaxPRIGROUPValue ) == __NVIC_PRIO_BITS ); } #endif #ifdef configPRIO_BITS { /* Check the FreeRTOS configuration that defines the number of * priority bits matches the number of priority bits actually queried * from the hardware. */ configASSERT( ( portMAX_PRIGROUP_BITS - ulMaxPRIGROUPValue ) == configPRIO_BITS ); } #endif /* Shift the priority group value back to its position within the AIRCR * register. */ ulMaxPRIGROUPValue <<= portPRIGROUP_SHIFT; ulMaxPRIGROUPValue &= portPRIORITY_GROUP_MASK; /* Restore the clobbered interrupt priority register to its original * value. */ *pucFirstUserPriorityRegister = ulOriginalPriority; } #endif /* configASSERT_DEFINED */ /* Make PendSV and SysTick the lowest priority interrupts. */ portNVIC_SHPR3_REG |= portNVIC_PENDSV_PRI; portNVIC_SHPR3_REG |= portNVIC_SYSTICK_PRI; /* Start the timer that generates the tick ISR. Interrupts are disabled * here already. */ vPortSetupTimerInterrupt(); /* Initialise the critical nesting count ready for the first task. */ uxCriticalNesting = 0; /* Ensure the VFP is enabled - it should be anyway. */ vPortEnableVFP(); /* Lazy save always. */ *( portFPCCR ) |= portASPEN_AND_LSPEN_BITS; /* Start the first task. */ prvPortStartFirstTask(); /* Should never get here as the tasks will now be executing! Call the task * exit error function to prevent compiler warnings about a static function * not being called in the case that the application writer overrides this * functionality by defining configTASK_RETURN_ADDRESS. Call * vTaskSwitchContext() so link time optimisation does not remove the * symbol. */ vTaskSwitchContext(); prvTaskExitError(); /* Should not get here! */ return 0; } /*-----------------------------------------------------------*/ void vPortEndScheduler( void ) { /* Not implemented in ports where there is nothing to return to. * Artificially force an assert. */ configASSERT( uxCriticalNesting == 1000UL ); } /*-----------------------------------------------------------*/ void vPortEnterCritical( void ) { portDISABLE_INTERRUPTS(); uxCriticalNesting++; /* This is not the interrupt safe version of the enter critical function so * assert() if it is being called from an interrupt context. Only API * functions that end in "FromISR" can be used in an interrupt. Only assert if * the critical nesting count is 1 to protect against recursive calls if the * assert function also uses a critical section. */ if( uxCriticalNesting == 1 ) { configASSERT( ( portNVIC_INT_CTRL_REG & portVECTACTIVE_MASK ) == 0 ); } } /*-----------------------------------------------------------*/ void vPortExitCritical( void ) { configASSERT( uxCriticalNesting ); uxCriticalNesting--; if( uxCriticalNesting == 0 ) { portENABLE_INTERRUPTS(); } } /*-----------------------------------------------------------*/ void xPortPendSVHandler( void ) { /* This is a naked function. */ __asm volatile ( " mrs r0, psp \n" " isb \n" " \n" " ldr r3, pxCurrentTCBConst \n"/* Get the location of the current TCB. */ " ldr r2, [r3] \n" " \n" " tst r14, #0x10 \n"/* Is the task using the FPU context? If so, push high vfp registers. */ " it eq \n" " vstmdbeq r0!, {s16-s31} \n" " \n" " stmdb r0!, {r4-r11, r14} \n"/* Save the core registers. */ " str r0, [r2] \n"/* Save the new top of stack into the first member of the TCB. */ " \n" " stmdb sp!, {r0, r3} \n" " mov r0, %0 \n" " cpsid i \n"/* Errata workaround. */ " msr basepri, r0 \n" " dsb \n" " isb \n" " cpsie i \n"/* Errata workaround. */ " bl vTaskSwitchContext \n" " mov r0, #0 \n" " msr basepri, r0 \n" " ldmia sp!, {r0, r3} \n" " \n" " ldr r1, [r3] \n"/* The first item in pxCurrentTCB is the task top of stack. */ " ldr r0, [r1] \n" " \n" " ldmia r0!, {r4-r11, r14} \n"/* Pop the core registers. */ " \n" " tst r14, #0x10 \n"/* Is the task using the FPU context? If so, pop the high vfp registers too. */ " it eq \n" " vldmiaeq r0!, {s16-s31} \n" " \n" " msr psp, r0 \n" " isb \n" " \n" #ifdef WORKAROUND_PMU_CM001 /* XMC4000 specific errata workaround. */ #if WORKAROUND_PMU_CM001 == 1 " push { r14 } \n" " pop { pc } \n" #endif #endif " \n" " bx r14 \n" " \n" " .align 4 \n" "pxCurrentTCBConst: .word pxCurrentTCB \n" ::"i" ( configMAX_SYSCALL_INTERRUPT_PRIORITY ) ); } /*-----------------------------------------------------------*/ void xPortSysTickHandler( void ) { /* The SysTick runs at the lowest interrupt priority, so when this interrupt * executes all interrupts must be unmasked. There is therefore no need to * save and then restore the interrupt mask value as its value is already * known. */ portDISABLE_INTERRUPTS(); { /* Increment the RTOS tick. */ if( xTaskIncrementTick() != pdFALSE ) { /* A context switch is required. Context switching is performed in * the PendSV interrupt. Pend the PendSV interrupt. */ portNVIC_INT_CTRL_REG = portNVIC_PENDSVSET_BIT; } } portENABLE_INTERRUPTS(); } /*-----------------------------------------------------------*/ #if ( configUSE_TICKLESS_IDLE == 1 ) __attribute__( ( weak ) ) void vPortSuppressTicksAndSleep( TickType_t xExpectedIdleTime ) { uint32_t ulReloadValue, ulCompleteTickPeriods, ulCompletedSysTickDecrements; TickType_t xModifiableIdleTime; /* Make sure the SysTick reload value does not overflow the counter. */ if( xExpectedIdleTime > xMaximumPossibleSuppressedTicks ) { xExpectedIdleTime = xMaximumPossibleSuppressedTicks; } /* Stop the SysTick momentarily. The time the SysTick is stopped for * is accounted for as best it can be, but using the tickless mode will * inevitably result in some tiny drift of the time maintained by the * kernel with respect to calendar time. */ portNVIC_SYSTICK_CTRL_REG &= ~portNVIC_SYSTICK_ENABLE_BIT; /* Calculate the reload value required to wait xExpectedIdleTime * tick periods. -1 is used because this code will execute part way * through one of the tick periods. */ ulReloadValue = portNVIC_SYSTICK_CURRENT_VALUE_REG + ( ulTimerCountsForOneTick * ( xExpectedIdleTime - 1UL ) ); if( ulReloadValue > ulStoppedTimerCompensation ) { ulReloadValue -= ulStoppedTimerCompensation; } /* Enter a critical section but don't use the taskENTER_CRITICAL() * method as that will mask interrupts that should exit sleep mode. */ __asm volatile ( "cpsid i" ::: "memory" ); __asm volatile ( "dsb" ); __asm volatile ( "isb" ); /* If a context switch is pending or a task is waiting for the scheduler * to be unsuspended then abandon the low power entry. */ if( eTaskConfirmSleepModeStatus() == eAbortSleep ) { /* Restart from whatever is left in the count register to complete * this tick period. */ portNVIC_SYSTICK_LOAD_REG = portNVIC_SYSTICK_CURRENT_VALUE_REG; /* Restart SysTick. */ portNVIC_SYSTICK_CTRL_REG |= portNVIC_SYSTICK_ENABLE_BIT; /* Reset the reload register to the value required for normal tick * periods. */ portNVIC_SYSTICK_LOAD_REG = ulTimerCountsForOneTick - 1UL; /* Re-enable interrupts - see comments above the cpsid instruction() * above. */ __asm volatile ( "cpsie i" ::: "memory" ); } else { /* Set the new reload value. */ portNVIC_SYSTICK_LOAD_REG = ulReloadValue; /* Clear the SysTick count flag and set the count value back to * zero. */ portNVIC_SYSTICK_CURRENT_VALUE_REG = 0UL; /* Restart SysTick. */ portNVIC_SYSTICK_CTRL_REG |= portNVIC_SYSTICK_ENABLE_BIT; /* Sleep until something happens. configPRE_SLEEP_PROCESSING() can * set its parameter to 0 to indicate that its implementation contains * its own wait for interrupt or wait for event instruction, and so wfi * should not be executed again. However, the original expected idle * time variable must remain unmodified, so a copy is taken. */ xModifiableIdleTime = xExpectedIdleTime; configPRE_SLEEP_PROCESSING( xModifiableIdleTime ); if( xModifiableIdleTime > 0 ) { __asm volatile ( "dsb" ::: "memory" ); __asm volatile ( "wfi" ); __asm volatile ( "isb" ); } configPOST_SLEEP_PROCESSING( xExpectedIdleTime ); /* Re-enable interrupts to allow the interrupt that brought the MCU * out of sleep mode to execute immediately. see comments above * __disable_interrupt() call above. */ __asm volatile ( "cpsie i" ::: "memory" ); __asm volatile ( "dsb" ); __asm volatile ( "isb" ); /* Disable interrupts again because the clock is about to be stopped * and interrupts that execute while the clock is stopped will increase * any slippage between the time maintained by the RTOS and calendar * time. */ __asm volatile ( "cpsid i" ::: "memory" ); __asm volatile ( "dsb" ); __asm volatile ( "isb" ); /* Disable the SysTick clock without reading the * portNVIC_SYSTICK_CTRL_REG register to ensure the * portNVIC_SYSTICK_COUNT_FLAG_BIT is not cleared if it is set. Again, * the time the SysTick is stopped for is accounted for as best it can * be, but using the tickless mode will inevitably result in some tiny * drift of the time maintained by the kernel with respect to calendar * time*/ portNVIC_SYSTICK_CTRL_REG = ( portNVIC_SYSTICK_CLK_BIT | portNVIC_SYSTICK_INT_BIT ); /* Determine if the SysTick clock has already counted to zero and * been set back to the current reload value (the reload back being * correct for the entire expected idle time) or if the SysTick is yet * to count to zero (in which case an interrupt other than the SysTick * must have brought the system out of sleep mode). */ if( ( portNVIC_SYSTICK_CTRL_REG & portNVIC_SYSTICK_COUNT_FLAG_BIT ) != 0 ) { uint32_t ulCalculatedLoadValue; /* The tick interrupt is already pending, and the SysTick count * reloaded with ulReloadValue. Reset the * portNVIC_SYSTICK_LOAD_REG with whatever remains of this tick * period. */ ulCalculatedLoadValue = ( ulTimerCountsForOneTick - 1UL ) - ( ulReloadValue - portNVIC_SYSTICK_CURRENT_VALUE_REG ); /* Don't allow a tiny value, or values that have somehow * underflowed because the post sleep hook did something * that took too long. */ if( ( ulCalculatedLoadValue < ulStoppedTimerCompensation ) || ( ulCalculatedLoadValue > ulTimerCountsForOneTick ) ) { ulCalculatedLoadValue = ( ulTimerCountsForOneTick - 1UL ); } portNVIC_SYSTICK_LOAD_REG = ulCalculatedLoadValue; /* As the pending tick will be processed as soon as this * function exits, the tick value maintained by the tick is stepped * forward by one less than the time spent waiting. */ ulCompleteTickPeriods = xExpectedIdleTime - 1UL; } else { /* Something other than the tick interrupt ended the sleep. * Work out how long the sleep lasted rounded to complete tick * periods (not the ulReload value which accounted for part * ticks). */ ulCompletedSysTickDecrements = ( xExpectedIdleTime * ulTimerCountsForOneTick ) - portNVIC_SYSTICK_CURRENT_VALUE_REG; /* How many complete tick periods passed while the processor * was waiting? */ ulCompleteTickPeriods = ulCompletedSysTickDecrements / ulTimerCountsForOneTick; /* The reload value is set to whatever fraction of a single tick * period remains. */ portNVIC_SYSTICK_LOAD_REG = ( ( ulCompleteTickPeriods + 1UL ) * ulTimerCountsForOneTick ) - ulCompletedSysTickDecrements; } /* Restart SysTick so it runs from portNVIC_SYSTICK_LOAD_REG * again, then set portNVIC_SYSTICK_LOAD_REG back to its standard * value. */ portNVIC_SYSTICK_CURRENT_VALUE_REG = 0UL; portNVIC_SYSTICK_CTRL_REG |= portNVIC_SYSTICK_ENABLE_BIT; vTaskStepTick( ulCompleteTickPeriods ); portNVIC_SYSTICK_LOAD_REG = ulTimerCountsForOneTick - 1UL; /* Exit with interrupts enabled. */ __asm volatile ( "cpsie i" ::: "memory" ); } } #endif /* #if configUSE_TICKLESS_IDLE */ /*-----------------------------------------------------------*/ /* * Setup the systick timer to generate the tick interrupts at the required * frequency. */ __attribute__( ( weak ) ) void vPortSetupTimerInterrupt( void ) { /* Calculate the constants required to configure the tick interrupt. */ #if ( configUSE_TICKLESS_IDLE == 1 ) { ulTimerCountsForOneTick = ( configSYSTICK_CLOCK_HZ / configTICK_RATE_HZ ); xMaximumPossibleSuppressedTicks = portMAX_24_BIT_NUMBER / ulTimerCountsForOneTick; ulStoppedTimerCompensation = portMISSED_COUNTS_FACTOR / ( configCPU_CLOCK_HZ / configSYSTICK_CLOCK_HZ ); } #endif /* configUSE_TICKLESS_IDLE */ /* Stop and clear the SysTick. */ portNVIC_SYSTICK_CTRL_REG = 0UL; portNVIC_SYSTICK_CURRENT_VALUE_REG = 0UL; /* Configure SysTick to interrupt at the requested rate. */ portNVIC_SYSTICK_LOAD_REG = ( configSYSTICK_CLOCK_HZ / configTICK_RATE_HZ ) - 1UL; portNVIC_SYSTICK_CTRL_REG = ( portNVIC_SYSTICK_CLK_BIT | portNVIC_SYSTICK_INT_BIT | portNVIC_SYSTICK_ENABLE_BIT ); } /*-----------------------------------------------------------*/ /* This is a naked function. */ static void vPortEnableVFP( void ) { __asm volatile ( " ldr.w r0, =0xE000ED88 \n"/* The FPU enable bits are in the CPACR. */ " ldr r1, [r0] \n" " \n" " orr r1, r1, #( 0xf << 20 ) \n"/* Enable CP10 and CP11 coprocessors, then save back. */ " str r1, [r0] \n" " bx r14 \n" " .ltorg \n" ); } /*-----------------------------------------------------------*/ #if ( configASSERT_DEFINED == 1 ) void vPortValidateInterruptPriority( void ) { uint32_t ulCurrentInterrupt; uint8_t ucCurrentPriority; /* Obtain the number of the currently executing interrupt. */ __asm volatile ( "mrs %0, ipsr" : "=r" ( ulCurrentInterrupt )::"memory" ); /* Is the interrupt number a user defined interrupt? */ if( ulCurrentInterrupt >= portFIRST_USER_INTERRUPT_NUMBER ) { /* Look up the interrupt's priority. */ ucCurrentPriority = pcInterruptPriorityRegisters[ ulCurrentInterrupt ]; /* The following assertion will fail if a service routine (ISR) for * an interrupt that has been assigned a priority above * configMAX_SYSCALL_INTERRUPT_PRIORITY calls an ISR safe FreeRTOS API * function. ISR safe FreeRTOS API functions must *only* be called * from interrupts that have been assigned a priority at or below * configMAX_SYSCALL_INTERRUPT_PRIORITY. * * Numerically low interrupt priority numbers represent logically high * interrupt priorities, therefore the priority of the interrupt must * be set to a value equal to or numerically *higher* than * configMAX_SYSCALL_INTERRUPT_PRIORITY. * * Interrupts that use the FreeRTOS API must not be left at their * default priority of zero as that is the highest possible priority, * which is guaranteed to be above configMAX_SYSCALL_INTERRUPT_PRIORITY, * and therefore also guaranteed to be invalid. * * FreeRTOS maintains separate thread and ISR API functions to ensure * interrupt entry is as fast and simple as possible. * * The following links provide detailed information: * https://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html * https://www.FreeRTOS.org/FAQHelp.html */ configASSERT( ucCurrentPriority >= ucMaxSysCallPriority ); } /* Priority grouping: The interrupt controller (NVIC) allows the bits * that define each interrupt's priority to be split between bits that * define the interrupt's pre-emption priority bits and bits that define * the interrupt's sub-priority. For simplicity all bits must be defined * to be pre-emption priority bits. The following assertion will fail if * this is not the case (if some bits represent a sub-priority). * * If the application only uses CMSIS libraries for interrupt * configuration then the correct setting can be achieved on all Cortex-M * devices by calling NVIC_SetPriorityGrouping( 0 ); before starting the * scheduler. Note however that some vendor specific peripheral libraries * assume a non-zero priority group setting, in which cases using a value * of zero will result in unpredictable behaviour. */ configASSERT( ( portAIRCR_REG & portPRIORITY_GROUP_MASK ) <= ulMaxPRIGROUPValue ); } #endif /* configASSERT_DEFINED */