Connection from "127.0.0.1" via 127.0.0.1. Connection from port "62890" to 6224 Connection from "127.0.0.1" via 127.0.0.1. Connection from port "62902" to 7224 Telnet server running on 127.0.0.1:51794 Searching for Kernel Symbols... rsp_qC - qSymbol: 5F74785F7468726561645F63757272656E745F707472 _tx_thread_current_ptr not found. ThreadX analysis not enabled. rsp_qC - qSymbol: 707843757272656E74544342 Symbol pxCurrentTCB found. (0x20400414) rsp_qC - qSymbol: 707852656164795461736B734C69737473 Symbol pxReadyTasksLists found. (0x2040046C) rsp_qC - qSymbol: 7844656C617965645461736B4C69737431 Symbol xDelayedTaskList1 found. (0x20400598) rsp_qC - qSymbol: 7844656C617965645461736B4C69737432 Symbol xDelayedTaskList2 found. (0x204005AC) rsp_qC - qSymbol: 7850656E64696E6752656164794C697374 Symbol xPendingReadyList found. (0x2040043C) rsp_qC - qSymbol: 757843757272656E744E756D6265724F665461736B73 Symbol uxCurrentNumberOfTasks found. (0x20400464) rsp_qC - qSymbol: 757844656C657465645461736B7357616974696E67436C65616E5570 Symbol uxDeletedTasksWaitingCleanUp found. (0x20400468) rsp_qC - qSymbol: 7853757370656E6465645461736B4C697374 Symbol xSuspendedTaskList found. (0x2040041C) rsp_qC - qSymbol: 785363686564756C657252756E6E696E67 Symbol xSchedulerRunning found. (0x204005C0) USING FREERTOS CORTEX-M V7 (WITH FPU) DRIVERS Successfully initialized kernel symbols. FreeRTOS analysis enabled. Copyright 2021 P&E Microcomputer Systems,Inc. Command Line :C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.4.202109291837\win32\pegdbserver_console -device=NXP_S32K3xx_S32K314 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -usejta? PEmicro Interface detected - Flash Version 11.22 CMD>RE Initializing. Target has been RESET and is active. CMD>CM C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.4.202109291837\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\nxp_s32k314_1x32x1012k_hse_disabled.arp Initializing. Initialized. ;version 1.00, 09/03/2021, Copyright 2021 P&E Microcomputer Systems, www.pemicro.com [S32K3x4_hse_disabled] ;device nxp, s32k314, 1x32x1012k,desc=hse_disabled ;begin_cs device=$00400000, length=$003F4000, ram=$20400000 Loading programming algorithm ... WARNING - Selected .ARP file has been modified. CRC16 = $7E41 Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Command is inactive for this .ARP file. VC is not implemented, falling back to VM CMD>VM Verifying. Verified. Application verified in memory. No need to reprogram. CMD>RE Initializing. Target has been RESET and is active. Starting reset script (C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.4.202109291837\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K314.mac) ... REM Enable clocks for selected cores in MC_ME module (the sequence below enables all clocks). REM Initialize RAM and DMA: REM Initialize DMA TCD: REM Copy valid executable code to RAM for each core to be used. REM Enable required cores in MC_ME: Delaying for 20mS ... Done. Reset script (C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.4.202109291837\win32\gdi\P&E\supportFiles_ARM\NXP\S32K3xx\S32K314.mac) completed. BusFault: An imprecise (asynchronous) data access error has occurred. HardFault: A fault has been escalated to a hard fault. Number of threads 1 (Scheduler not yet running) Number of threads 1 (Scheduler not yet running) Number of threads 1 (Scheduler not yet running)