#include "tftp_client.h" #include "lwip/udp.h" #include "lwip/timeouts.h" #include "lwip/debug.h" #include "lwip/apps/tftp_opts.h" #include "lwip/pbuf.h" #define TFTP_MAX_PAYLOAD_SIZE 512 #define TFTP_HEADER_LENGTH 4 #define TFTP_RRQ 1 #define TFTP_WRQ 2 #define TFTP_DATA 3 #define TFTP_ACK 4 #define TFTP_ERROR 5 enum tftp_error { TFTP_ERROR_FILE_NOT_FOUND = 1, TFTP_ERROR_ACCESS_VIOLATION = 2, TFTP_ERROR_DISK_FULL = 3, TFTP_ERROR_ILLEGAL_OPERATION = 4, TFTP_ERROR_UNKNOWN_TRFR_ID = 5, TFTP_ERROR_FILE_EXISTS = 6, TFTP_ERROR_NO_SUCH_USER = 7 }; #include struct tftp_state { const struct tftp_context *ctx; void *handle; struct pbuf *last_data; struct udp_pcb *upcb; ip_addr_t addr; u16_t port; int timer; int last_pkt; uint16_t blknum; uint8_t retries; uint8_t mode_write; uint8_t tftp_mode; }; static struct tftp_state tftp_state; static void tftp_tmr(void *arg); static void close_handle(void) { tftp_state.port = 0; ip_addr_set_any(0, &tftp_state.addr); if (tftp_state.last_data != NULL) { pbuf_free(tftp_state.last_data); tftp_state.last_data = NULL; } sys_untimeout(tftp_tmr, NULL); if (tftp_state.handle) { tftp_state.ctx->close(tftp_state.handle); tftp_state.handle = NULL; LWIP_DEBUGF(TFTP_DEBUG | LWIP_DBG_STATE, ("tftp: closing\n")); } } static struct pbuf* init_packet(u16_t opcode, u16_t extra, size_t size) { struct pbuf* p = pbuf_alloc(PBUF_TRANSPORT, (u16_t)(TFTP_HEADER_LENGTH + size), PBUF_RAM); u16_t* payload; if (p != NULL) { payload = (u16_t*) p->payload; payload[0] = PP_HTONS(opcode); payload[1] = lwip_htons(extra); } return p; } static err_t send_request(const ip_addr_t *addr, u16_t port, u16_t opcode, const char* fname, const char* mode) { size_t fname_length = strlen(fname)+1; size_t mode_length = strlen(mode)+1; struct pbuf* p = init_packet(opcode, 0, fname_length + mode_length - 2); char* payload; err_t ret; if (p == NULL) { return ERR_MEM; } payload = (char*) p->payload; MEMCPY(payload+2, fname, fname_length); MEMCPY(payload+2+fname_length, mode, mode_length); ret = udp_sendto(tftp_state.upcb, p, addr, port); pbuf_free(p); return ret; } static err_t send_error(const ip_addr_t *addr, u16_t port, enum tftp_error code, const char *str) { int str_length = strlen(str); struct pbuf *p; u16_t *payload; err_t ret; p = init_packet(TFTP_ERROR, code, str_length + 1); if (p == NULL) { return ERR_MEM; } payload = (u16_t *) p->payload; MEMCPY(&payload[2], str, str_length + 1); ret = udp_sendto(tftp_state.upcb, p, addr, port); pbuf_free(p); return ret; } static err_t send_ack(const ip_addr_t *addr, u16_t port, u16_t blknum) { struct pbuf *p; err_t ret; p = init_packet(TFTP_ACK, blknum, 0); if (p == NULL) { return ERR_MEM; } ret = udp_sendto(tftp_state.upcb, p, addr, port); pbuf_free(p); return ret; } static err_t resend_data(const ip_addr_t *addr, u16_t port) { err_t ret; struct pbuf *p = pbuf_alloc(PBUF_TRANSPORT, tftp_state.last_data->len, PBUF_RAM); if (p == NULL) { return ERR_MEM; } ret = pbuf_copy(p, tftp_state.last_data); if (ret != ERR_OK) { pbuf_free(p); return ret; } ret = udp_sendto(tftp_state.upcb, p, addr, port); pbuf_free(p); return ret; } static void send_data(const ip_addr_t *addr, u16_t port) { u16_t *payload; int ret; if (tftp_state.last_data != NULL) { pbuf_free(tftp_state.last_data); } tftp_state.last_data = init_packet(TFTP_DATA, tftp_state.blknum, TFTP_MAX_PAYLOAD_SIZE); if (tftp_state.last_data == NULL) { return; } payload = (u16_t *) tftp_state.last_data->payload; ret = tftp_state.ctx->read(tftp_state.handle, &payload[2], TFTP_MAX_PAYLOAD_SIZE); if (ret < 0) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Error occured while reading the file."); close_handle(); return; } pbuf_realloc(tftp_state.last_data, (u16_t)(TFTP_HEADER_LENGTH + ret)); resend_data(addr, port); } static void recv(void *arg, struct udp_pcb *upcb, struct pbuf *p, const ip_addr_t *addr, u16_t port) { u16_t *sbuf = (u16_t *) p->payload; int opcode; LWIP_UNUSED_ARG(arg); LWIP_UNUSED_ARG(upcb); if (((tftp_state.port != 0) && (port != tftp_state.port)) || (!ip_addr_isany_val(tftp_state.addr) && !ip_addr_cmp(&tftp_state.addr, addr))) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Only one connection at a time is supported"); pbuf_free(p); return; } opcode = sbuf[0]; tftp_state.last_pkt = tftp_state.timer; tftp_state.retries = 0; switch (opcode) { case PP_HTONS(TFTP_RRQ): /* fall through */ case PP_HTONS(TFTP_WRQ): { const char tftp_null = 0; char filename[TFTP_MAX_FILENAME_LEN + 1]; char mode[TFTP_MAX_MODE_LEN + 1]; u16_t filename_end_offset; u16_t mode_end_offset; if (tftp_state.handle != NULL) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Only one connection at a time is supported"); break; } if ((tftp_state.tftp_mode & LWIP_TFTP_MODE_SERVER) == 0) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "TFTP server not enabled"); break; } sys_timeout(TFTP_TIMER_MSECS, tftp_tmr, NULL); /* find \0 in pbuf -> end of filename string */ filename_end_offset = pbuf_memfind(p, &tftp_null, sizeof(tftp_null), 2); if ((u16_t)(filename_end_offset - 1) > sizeof(filename)) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Filename too long/not NULL terminated"); break; } pbuf_copy_partial(p, filename, filename_end_offset - 1, 2); /* find \0 in pbuf -> end of mode string */ mode_end_offset = pbuf_memfind(p, &tftp_null, sizeof(tftp_null), filename_end_offset + 1); if ((u16_t)(mode_end_offset - filename_end_offset) > sizeof(mode)) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Mode too long/not NULL terminated"); break; } pbuf_copy_partial(p, mode, mode_end_offset - filename_end_offset, filename_end_offset + 1); tftp_state.handle = tftp_state.ctx->open(filename, mode, opcode == PP_HTONS(TFTP_WRQ)); tftp_state.blknum = 1; if (!tftp_state.handle) { send_error(addr, port, TFTP_ERROR_FILE_NOT_FOUND, "Unable to open requested file."); break; } LWIP_DEBUGF(TFTP_DEBUG | LWIP_DBG_STATE, ("tftp: %s request from ", (opcode == PP_HTONS(TFTP_WRQ)) ? "write" : "read")); ip_addr_debug_print(TFTP_DEBUG | LWIP_DBG_STATE, addr); LWIP_DEBUGF(TFTP_DEBUG | LWIP_DBG_STATE, (" for '%s' mode '%s'\n", filename, mode)); ip_addr_copy(tftp_state.addr, *addr); tftp_state.port = port; if (opcode == PP_HTONS(TFTP_WRQ)) { tftp_state.mode_write = 1; send_ack(addr, port, 0); } else { tftp_state.mode_write = 0; send_data(addr, port); } break; } case PP_HTONS(TFTP_DATA): { int ret; u16_t blknum; if (tftp_state.handle == NULL) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "No connection"); break; } if (tftp_state.mode_write != 1) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Not a write connection"); break; } blknum = lwip_ntohs(sbuf[1]); if (blknum == tftp_state.blknum) { //pbuf_remove_header(p, TFTP_HEADER_LENGTH); ret = tftp_state.ctx->write(tftp_state.handle, p); if (ret < 0) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "error writing file"); close_handle(); } else { send_ack(addr, port, blknum); } if (p->tot_len < TFTP_MAX_PAYLOAD_SIZE) { close_handle(); } else { tftp_state.blknum++; } } else if ((u16_t)(blknum + 1) == tftp_state.blknum) { /* retransmit of previous block, ack again (casting to u16_t to care for overflow) */ send_ack(addr, port, blknum); } else { send_error(addr, port, TFTP_ERROR_UNKNOWN_TRFR_ID, "Wrong block number"); } break; } case PP_HTONS(TFTP_ACK): { u16_t blknum; int lastpkt; if (tftp_state.handle == NULL) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "No connection"); break; } if (tftp_state.mode_write != 0) { send_error(addr, port, TFTP_ERROR_ACCESS_VIOLATION, "Not a read connection"); break; } blknum = lwip_ntohs(sbuf[1]); if (blknum != tftp_state.blknum) { send_error(addr, port, TFTP_ERROR_UNKNOWN_TRFR_ID, "Wrong block number"); break; } lastpkt = 0; if (tftp_state.last_data != NULL) { lastpkt = tftp_state.last_data->tot_len != (TFTP_MAX_PAYLOAD_SIZE + TFTP_HEADER_LENGTH); } if (!lastpkt) { tftp_state.blknum++; send_data(addr, port); } else { close_handle(); } break; } case PP_HTONS(TFTP_ERROR): if (tftp_state.handle != NULL) { //pbuf_remove_header(p, TFTP_HEADER_LENGTH); //tftp_state.ctx->error(tftp_state.handle, sbuf[1], (const char*)p->payload, p->len); close_handle(); } break; default: send_error(addr, port, TFTP_ERROR_ILLEGAL_OPERATION, "Unknown operation"); break; } pbuf_free(p); } static void tftp_tmr(void *arg) { LWIP_UNUSED_ARG(arg); tftp_state.timer++; if (tftp_state.handle == NULL) { return; } sys_timeout(TFTP_TIMER_MSECS, tftp_tmr, NULL); if ((tftp_state.timer - tftp_state.last_pkt) > (TFTP_TIMEOUT_MSECS / TFTP_TIMER_MSECS)) { if ((tftp_state.last_data != NULL) && (tftp_state.retries < TFTP_MAX_RETRIES)) { LWIP_DEBUGF(TFTP_DEBUG | LWIP_DBG_STATE, ("tftp: timeout, retrying\n")); resend_data(&tftp_state.addr, tftp_state.port); tftp_state.retries++; } else { LWIP_DEBUGF(TFTP_DEBUG | LWIP_DBG_STATE, ("tftp: timeout\n")); close_handle(); } } } /** * Initialize TFTP client/server. * @param mode TFTP mode (client/server) * @param ctx TFTP callback struct */ err_t tftp_init_common(uint8_t mode, const struct tftp_context *ctx) { err_t ret; /* LWIP_ASSERT_CORE_LOCKED(); is checked by udp_new() */ struct udp_pcb *pcb = udp_new_ip_type(IPADDR_TYPE_ANY); if (pcb == NULL) { return ERR_MEM; } ret = udp_bind(pcb, IP_ANY_TYPE, TFTP_PORT); if (ret != ERR_OK) { udp_remove(pcb); return ret; } tftp_state.handle = NULL; tftp_state.port = 0; tftp_state.ctx = ctx; tftp_state.timer = 0; tftp_state.last_data = NULL; tftp_state.upcb = pcb; tftp_state.tftp_mode = mode; udp_recv(pcb, recv, NULL); return ERR_OK; } /** @ingroup tftp * Initialize TFTP server. * @param ctx TFTP callback struct */ err_t tftp_init_server(const struct tftp_context *ctx) { return tftp_init_common(LWIP_TFTP_MODE_SERVER, ctx); } /** @ingroup tftp * Initialize TFTP client. * @param ctx TFTP callback struct */ err_t tftp_init_client(const struct tftp_context *ctx) { return tftp_init_common(LWIP_TFTP_MODE_CLIENT, ctx); } /** @ingroup tftp * Deinitialize ("turn off") TFTP client/server. */ void tftp_cleanup(void) { LWIP_ASSERT("Cleanup called on non-initialized TFTP", tftp_state.upcb != NULL); udp_remove(tftp_state.upcb); close_handle(); memset(&tftp_state, 0, sizeof(tftp_state)); } static const char * mode_to_string(enum tftp_transfer_mode mode) { if (mode == TFTP_MODE_OCTET) { return "octet"; } if (mode == TFTP_MODE_NETASCII) { return "netascii"; } if (mode == TFTP_MODE_BINARY) { return "binary"; } return NULL; } err_t tftp_get(void* handle, const ip_addr_t *addr, u16_t port, const char* fname, enum tftp_transfer_mode mode) { LWIP_ERROR("TFTP client is not enabled (tftp_init)", (tftp_state.tftp_mode & LWIP_TFTP_MODE_CLIENT) != 0, return ERR_VAL); LWIP_ERROR("tftp_get: invalid file name", fname != NULL, return ERR_VAL); LWIP_ERROR("tftp_get: invalid mode", mode <= TFTP_MODE_BINARY, return ERR_VAL); tftp_state.handle = handle; tftp_state.blknum = 1; tftp_state.mode_write = 1; /* We want to receive data */ return send_request(addr, port, TFTP_RRQ, fname, mode_to_string(mode)); } err_t tftp_put(void* handle, const ip_addr_t *addr, u16_t port, const char* fname, enum tftp_transfer_mode mode) { LWIP_ERROR("TFTP client is not enabled (tftp_init)", (tftp_state.tftp_mode & LWIP_TFTP_MODE_CLIENT) != 0, return ERR_VAL); LWIP_ERROR("tftp_put: invalid file name", fname != NULL, return ERR_VAL); LWIP_ERROR("tftp_put: invalid mode", mode <= TFTP_MODE_BINARY, return ERR_VAL); tftp_state.handle = handle; tftp_state.blknum = 1; tftp_state.mode_write = 0; /* We want to send data */ return send_request(addr, port, TFTP_WRQ, fname, mode_to_string(mode)); }