#include "tftp.h" #include #include #include "lwip/mem.h" #include "lwip/udp.h" #include "uartPrintf/printf.h" /* Define this to a server IP string */ #define LWIP_TFTP_EXAMPLE_CLIENT_REMOTEIP "192.168.225.20" /* Define this to a file to get via tftp client */ #define LWIP_TFTP_EXAMPLE_CLIENT_FILENAME "somfile.txt" /* Define a base directory for TFTP access * ATTENTION: This code does NOT check for sandboxing, * i.e. '..' in paths is not checked! */ #define LWIP_TFTP_EXAMPLE_BASE_DIR "" #define TFTP_PORT 69 static char full_filename[256]; static void * tftp_open_file(const char* fname, u8_t is_write) { snprintf(full_filename, sizeof(full_filename), "%s%s", LWIP_TFTP_EXAMPLE_BASE_DIR, fname); full_filename[sizeof(full_filename)-1] = 0; if (is_write) { return (void*)fopen(full_filename, "wb"); } else { return (void*)fopen(full_filename, "rb"); } } static void* tftp_open(const char* fname, const char* mode, u8_t is_write) { LWIP_UNUSED_ARG(mode); return tftp_open_file(fname, is_write); } static void tftp_close(void* handle) { fclose((FILE*)handle); } static int tftp_read(void* handle, void* buf, int bytes) { int ret = fread(buf, 1, bytes, (FILE*)handle); if (ret <= 0) { return -1; } return ret; } static int tftp_write(void* handle, struct pbuf* p) { while (p != NULL) { if (fwrite(p->payload, 1, p->len, (FILE*)handle) != (size_t)p->len) { return -1; } p = p->next; } return 0; } /* For TFTP client only */ static void tftp_error(void* handle, int err, const char* msg, int size) { char message[100]; LWIP_UNUSED_ARG(handle); memset(message, 0, sizeof(message)); MEMCPY(message, msg, LWIP_MIN(sizeof(message)-1, (size_t)size)); printf("TFTP error: %d (%s)", err, message); } static const struct tftp_context tftp = { tftp_open, tftp_close, tftp_read, tftp_write, tftp_error }; void tftp_example_init_client(void) { void *f; err_t err; ip_addr_t srv; int ret = ipaddr_aton(LWIP_TFTP_EXAMPLE_CLIENT_REMOTEIP, &srv); if(ret != 1) { printf("ipaddr_aton failed \r\n"); } err = tftp_init_client(&tftp); if(err != ERR_OK) { printf("tftp_init_client failed, error : %d \r\n", err); } f = tftp_open_file(LWIP_TFTP_EXAMPLE_CLIENT_FILENAME, 1); if(f == NULL) { printf("failed to open file \r\n"); } err = tftp_get(f, &srv, TFTP_PORT, LWIP_TFTP_EXAMPLE_CLIENT_FILENAME, TFTP_MODE_OCTET); if(err != ERR_OK) { printf("tftp_get failed \r\n"); } }