/* ** ################################################################### ** Processor: S32K144 with 64 KB SRAM ** Compiler: GNU C Compiler ** ** Abstract: ** Linker file for the GNU C Compiler ** ** Copyright (c) 2015-2016 Freescale Semiconductor, Inc. ** Copyright 2017 NXP ** All rights reserved. ** ** THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR ** IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES ** OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. ** IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT, ** INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES ** (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR ** SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) ** HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, ** STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING ** IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF ** THE POSSIBILITY OF SUCH DAMAGE. ** ** http: www.freescale.com ** mail: support@freescale.com ** ** ################################################################### */ /* Entry Point */ ENTRY(Reset_Handler) /* To use "new" operator with EWL in C++ project the following symbol shall be defined */ /*EXTERN(_ZN10__cxxabiv119__terminate_handlerE)*/ HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000400; STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400; /* If symbol __flash_vector_table__=1 is defined at link time * the interrupt vector will not be copied to RAM. * Warning: Using the interrupt vector from Flash will not allow * INT_SYS_InstallHandler because the section is Read Only. */ M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400; /* Specify the memory areas */ MEMORY { /* Flash */ m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400 m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010 m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0 /* SRAM_L */ m_data (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000 /* SRAM_U */ m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00007000 } /* Define output sections */ SECTIONS { /* The startup code goes first into internal flash */ .interrupts : { __VECTOR_TABLE = .; __interrupts_start__ = .; . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ __interrupts_end__ = .; . = ALIGN(4); } > m_interrupts .flash_config : { . = ALIGN(4); KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */ . = ALIGN(4); } > m_flash_config /* The program code and other data goes into internal flash */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); } > m_text .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } > m_text .ARM : { __exidx_start = .; *(.ARM.exidx*) __exidx_end = .; } > m_text .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > m_text .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > m_text .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > m_text .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > m_text .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > m_text __etext = .; /* Define a global symbol at end of code. */ __DATA_ROM = .; /* Symbol is used by startup for data initialization. */ .interrupts_ram : { . = ALIGN(4); __VECTOR_RAM__ = .; __RAM_START = .; __interrupts_ram_start__ = .; /* Create a global symbol at data start. */ *(.m_interrupts_ram) /* This is a user defined section. */ . += M_VECTOR_RAM_SIZE; . = ALIGN(4); __interrupts_ram_end__ = .; /* Define a global symbol at data end. */ } > m_data __VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ; __RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ; .data : AT(__DATA_ROM) { . = ALIGN(4); __DATA_RAM = .; __data_start__ = .; /* Create a global symbol at data start. */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ KEEP(*(.jcr*)) . = ALIGN(4); __data_end__ = .; /* Define a global symbol at data end. */ } > m_data __DATA_END = __DATA_ROM + (__data_end__ - __data_start__); __CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */ .code : AT(__CODE_ROM) { . = ALIGN(4); __CODE_RAM = .; __code_start__ = .; /* Create a global symbol at code start. */ __code_ram_start__ = .; *(.code_ram) /* Custom section for storing code in RAM */ . = ALIGN(4); __code_end__ = .; /* Define a global symbol at code end. */ __code_ram_end__ = .; } > m_data __CODE_END = __CODE_ROM + (__code_end__ - __code_start__); __CUSTOM_ROM = __CODE_END; /* Custom Section Block that can be used to place data at absolute address. */ /* Use __attribute__((section (".customSection"))) to place data here. */ .customSectionBlock ORIGIN(m_data_2) : AT(__CUSTOM_ROM) { __customSection_start__ = .; KEEP(*(.customSection)) /* Keep section even if not referenced. */ __customSection_end__ = .; } > m_data_2 __CUSTOM_END = __CUSTOM_ROM + (__customSection_end__ - __customSection_start__); /* Uninitialized data section. */ .bss : { /* This is used by the startup in order to initialize the .bss section. */ . = ALIGN(4); __BSS_START = .; __bss_start__ = .; *(.bss) *(.bss*) *(COMMON) . = ALIGN(4); __bss_end__ = .; __BSS_END = .; } > m_data_2 .heap : { . = ALIGN(8); __end__ = .; __heap_start__ = .; PROVIDE(end = .); PROVIDE(_end = .); PROVIDE(__end = .); __HeapBase = .; . += HEAP_SIZE; __HeapLimit = .; __heap_limit = .; __heap_end__ = .; } > m_data_2 /* Initializes stack on the end of block */ __StackTop = ORIGIN(m_data_2) + LENGTH(m_data_2); __StackLimit = __StackTop - STACK_SIZE; PROVIDE(__stack = __StackTop); __RAM_END = __StackTop; .stack __StackLimit : { . = ALIGN(8); __stack_start__ = .; . += STACK_SIZE; __stack_end__ = .; } > m_data_2 /* Labels required by EWL */ __START_BSS = __BSS_START; __END_BSS = __BSS_END; __SP_INIT = __StackTop; .ARM.attributes 0 : { *(.ARM.attributes) } ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap") }