[ 231.678144] OOM killer enabled. [ 231.681278] Restarting tasks ... done. [ 231.690630] random: crng reseeded on system resumption [ 231.695878] PM: suspend exit -> AFTER WAKEUP [ 232.933449] fec 42890000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off [ 232.941232] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 257.892818] rcu: INFO: rcu_preempt self-detected stall on CPU [ 257.898565] rcu: 0-....: (5252 ticks this GP) idle=ad4c/1/0x4000000000000004 softirq=43382/43384 fqs=2372 [ 257.908200] (t=5250 jiffies g=94749 q=4300 ncpus=2) [ 257.913151] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G C 6.1.55+g770c5fe2c1d1 #1 [ 257.921745] Hardware name: NXP i.MX93 11X11 EVK board (DT) [ 257.927215] pstate: 40400009 (nZcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 257.934164] pc : _stext+0xa4/0x298 [ 257.937562] lr : _stext+0x6c/0x298 [ 257.940951] sp : ffff800008003f60 [ 257.944252] x29: ffff800008003f60 x28: ffff800009dd3240 x27: 0000000000000280 [ 257.951376] x26: 0000000000000000 x25: 00000000ffffc237 x24: ffff800009b7c000 [ 257.958500] x23: 0000000060400009 x22: ffff800009b83000 x21: ffff800009b7c880 [ 257.965624] x20: ffff800009dc50c0 x19: ffff800009dd3240 x18: 0000000000000000 [ 257.972748] x17: ffff80007600b000 x16: ffff800008000000 x15: 00003d0900007d00 [ 257.979872] x14: 0000000000017700 x13: 0000000000000196 x12: 0000000000000000 [ 257.986997] x11: 0000000000000000 x10: 0000000000000003 x9 : 0000000000000000 [ 257.994120] x8 : 000000371e53a700 x7 : 7fffffffffffffff x6 : 0000000159ed1786 [ 258.001244] x5 : 00ffffffffffffff x4 : 0000000000000015 x3 : ffff800009dd3240 [ 258.008368] x2 : ffff80007600b000 x1 : 00000000000000e0 x0 : ffff800009b83480 [ 258.015493] Call trace: [ 258.017929] _stext+0xa4/0x298 [ 258.020970] ____do_softirq+0x10/0x20 [ 258.024627] call_on_irq_stack+0x24/0x4c [ 258.028536] do_softirq_own_stack+0x1c/0x30 [ 258.032704] __irq_exit_rcu+0xec/0xf4 [ 258.036362] irq_exit_rcu+0x10/0x20 [ 258.039846] el1_interrupt+0x38/0x6c [ 258.043417] el1h_64_irq_handler+0x18/0x2c [ 258.047498] el1h_64_irq+0x64/0x68 [ 258.050887] cpuidle_enter_state+0x130/0x2fc [ 258.055151] cpuidle_enter+0x38/0x50 [ 258.058713] do_idle+0x230/0x2c0 [ 258.061937] cpu_startup_entry+0x28/0x30 [ 258.065846] kernel_init+0x0/0x12c [ 258.069235] arch_post_acpi_subsys_init+0x0/0x18 [ 258.073845] start_kernel+0x670/0x6b4 [ 258.077494] __primary_switched+0xbc/0xc4