NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb-dirty NOTICE: BL2: Built : 14:06:46, Jan 24 2022 NOTICE: UDIMM NOTICE: DDR PMU Hardware version-0x1210 NOTICE: DDR PMU Firmware vision-0x1001 (vA-2019.04) NOTICE: DDR4 UDIMM with 1-rank 64-bit bus (x8) NOTICE: 4 GB DDR4, 64-bit, CL=11, ECC on NOTICE: BL2: Booting BL31 NOTICE: BL31: v2.4(release):LSDK-21.08-0-g340b20bcb-dirty NOTICE: BL31: Built : 14:06:46, Jan 24 2022 NOTICE: Welcome to lx2160ardb BL31 Phase U-Boot 2021.04-00008-g5d9538a6a0-dirty (Jan 24 2022 - 14:06:21 +0800) SoC: LX2160AE Rev2.0 (0x87361020) Clock Configuration: CPU0(A72):1900 MHz CPU1(A72):1900 MHz CPU2(A72):1900 MHz CPU3(A72):1900 MHz CPU4(A72):1900 MHz CPU5(A72):1900 MHz CPU6(A72):1900 MHz CPU7(A72):1900 MHz CPU8(A72):1900 MHz CPU9(A72):1900 MHz CPU10(A72):1900 MHz CPU11(A72):1900 MHz CPU12(A72):1900 MHz CPU13(A72):1900 MHz CPU14(A72):1900 MHz CPU15(A72):1900 MHz Bus: 600 MHz DDR: 1600 MT/s Reset Configuration Word (RCW): 00000000: 4c434330 204c004c 00000000 00000000 00000010: 00000000 0c010000 00000000 00000000 00000020: 01a001a0 00002580 00000000 00000606 00000030: 00000000 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027005 00000000 00000070: 09870010 00150000 Model: NXP Layerscape LX2160ARDB Board Board: LX2160AE Rev2.0-RDB, Board version: @, boot from SD FPGA: v2.2 SERDES1 Reference: Clock1 = 100MHz Clock2 = 156.25MHz SERDES2 Reference: Clock1 = 100MHz Clock2 = 100MHz SERDES3 Reference: Clock1 = 100MHz Clock2 = 100MHz board/freescale/common/vid.c: read_voltage_from_PXC(): vout: 798 VID: Core voltage after adjustment is at 798 mV DRAM: 3.9 GiB DDR 3.9 GiB (DDR4, 64-bit, CL=11, ECC on) Using SERDES1 Protocol: 7 (0x7) Using SERDES2 Protocol: 12 (0xc) Using SERDES3 Protocol: 2 (0x2) PCIe1: pcie@3400000 disabled PCIe2: pcie@3500000 disabled PCIe3: pcie@3600000 disabled PCIe4: pcie@3700000 Root Complex: no link PCIe5: pcie@3800000 Root Complex: no link PCIe6: pcie@3900000 disabled WDT: Started with servicing (30s timeout) MMC: FSL_SDHC: 0 Loading Environment from MMC... *** Warning - bad CRC, using default environment EEPROM: NXID v1 In: serial_pl01x Out: serial_pl01x Err: serial_pl01x SEC0: RNG instantiated Net: Warning: DPMAC3@xfi (eth0) using random MAC address - 32:f8:fd:89:3f:6f eth0: DPMAC3@xfi, eth1: DPMAC4@xfi, eth2: DPMAC5@usxgmii, eth3: DPMAC6@usxgmii, eth4: DPMAC7@sgmii, eth5: DPMAC8@sgmii, eth6: DPMAC9@sgmii, eth7: DPMAC10@sgmii, eth8: DPMAC11@sgmii, eth9: DPMAC12@sgmii, eth10: DPMAC17@sgmii, eth11: DPMAC18@sgmii MMC read: dev # 0, block # 20480, count 4608 ... 4608 blocks read: OK MMC read: dev # 0, block # 28672, count 2048 ... 2048 blocks read: OK crc32+ fsl-mc: Booting Management Complex ... SUCCESS fsl-mc: Management Complex booted (version: 10.28.1, boot status: 0x1) Hit any key to stop autoboot: 10 9 0 =>